aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorJonathan Austin2012-12-17 17:59:41 -0600
committerLinus Torvalds2012-12-17 19:15:13 -0600
commitda01ee3c8e7954fb7ed0ceb002d482c79f8b2ccd (patch)
tree2b0ec06f862aefde2a4a2d122afb9b73aaf29f2d /.gitignore
parentac5f121b8f2cad52b7671f9af872f8761b0ea1d4 (diff)
downloadam43-linux-kernel-da01ee3c8e7954fb7ed0ceb002d482c79f8b2ccd.tar.gz
am43-linux-kernel-da01ee3c8e7954fb7ed0ceb002d482c79f8b2ccd.tar.xz
am43-linux-kernel-da01ee3c8e7954fb7ed0ceb002d482c79f8b2ccd.zip
.gitignore: remove stale entry for generated version.h
Since userspace headers were moved to generated/uapi it possible to have a stale copy of linux/version.h at that file's old location. This causes confusion after building an older kernel version, then checking out and building a new one; the old (stale) version header will still get picked up until it is manually removed. This upsets the C library. Since the uapi changes, include/linux/version.h is no longer generated and should not be ignored, so this patch removes it from .gitignore. Signed-off-by: Jonathan Austin <jonathan.austin@arm.com> Reported-by: Kevin Petit <kevin.petit@arm.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Diffstat (limited to '.gitignore')
-rw-r--r--.gitignore1
1 files changed, 0 insertions, 1 deletions
diff --git a/.gitignore b/.gitignore
index 92bd0e45dfa..3b8b9b33be3 100644
--- a/.gitignore
+++ b/.gitignore
@@ -60,7 +60,6 @@ modules.builtin
60# Generated include files 60# Generated include files
61# 61#
62include/config 62include/config
63include/linux/version.h
64include/generated 63include/generated
65arch/*/include/generated 64arch/*/include/generated
66 65