aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorMatt Kraai2009-06-04 23:43:10 -0500
committerJiri Kosina2009-06-12 11:01:51 -0500
commitff2f5ff0cf224780c3bd035d3e6ff4a30fcacae7 (patch)
tree62771c9a821c0808d5df79ea7eb1bf185f4ae117 /.gitignore
parent3ac49a1c9928b4a242b3cb1d83bc1d5c9b8fcb50 (diff)
downloadam43-linux-kernel-ff2f5ff0cf224780c3bd035d3e6ff4a30fcacae7.tar.gz
am43-linux-kernel-ff2f5ff0cf224780c3bd035d3e6ff4a30fcacae7.tar.xz
am43-linux-kernel-ff2f5ff0cf224780c3bd035d3e6ff4a30fcacae7.zip
trivial: Remove the hyphen from git commands
Signed-off-by: Matt Kraai <kraai@ftbfs.org> Signed-off-by: Jiri Kosina <jkosina@suse.cz>
Diffstat (limited to '.gitignore')
-rw-r--r--.gitignore2
1 files changed, 1 insertions, 1 deletions
diff --git a/.gitignore b/.gitignore
index 51bd99d6a26..caa8395f635 100644
--- a/.gitignore
+++ b/.gitignore
@@ -3,7 +3,7 @@
3# subdirectories here. Add them in the ".gitignore" file 3# subdirectories here. Add them in the ".gitignore" file
4# in that subdirectory instead. 4# in that subdirectory instead.
5# 5#
6# NOTE! Please use 'git-ls-files -i --exclude-standard' 6# NOTE! Please use 'git ls-files -i --exclude-standard'
7# command after changing this file, to see if there are 7# command after changing this file, to see if there are
8# any tracked files which get ignored after the change. 8# any tracked files which get ignored after the change.
9# 9#