diff options
author | Bing Zhao | 2013-02-26 14:58:35 -0600 |
---|---|---|
committer | John W. Linville | 2013-02-27 13:12:52 -0600 |
commit | 466026989f112e0546ca39ab00a759af82dbe83a (patch) | |
tree | e395b60206201fdc46c50b47583ceab81a55fba6 | |
parent | 6ef9e2f6d12ce9e2120916804d2ddd46b954a70b (diff) | |
download | am43-linux-kernel-466026989f112e0546ca39ab00a759af82dbe83a.tar.gz am43-linux-kernel-466026989f112e0546ca39ab00a759af82dbe83a.tar.xz am43-linux-kernel-466026989f112e0546ca39ab00a759af82dbe83a.zip |
libertas: fix crash for SD8688
For SD8688, FUNC_INIT command is queued before fw_ready flag is
set. This causes the following crash as lbs_thread blocks any
command if fw_ready is not set.
[ 209.338953] [<c0502248>] (__schedule+0x610/0x764) from [<bf20ae24>] (__lbs_cmd+0xb8/0x130 [libertas])
[ 209.348340] [<bf20ae24>] (__lbs_cmd+0xb8/0x130 [libertas]) from [<bf222474>] (if_sdio_finish_power_on+0xec/0x1b0 [libertas_sdio])
[ 209.360136] [<bf222474>] (if_sdio_finish_power_on+0xec/0x1b0 [libertas_sdio]) from [<bf2226c4>] (if_sdio_power_on+0x18c/0x20c [libertas_sdio])
[ 209.373052] [<bf2226c4>] (if_sdio_power_on+0x18c/0x20c [libertas_sdio]) from [<bf222944>] (if_sdio_probe+0x200/0x31c [libertas_sdio])
[ 209.385316] [<bf222944>] (if_sdio_probe+0x200/0x31c [libertas_sdio]) from [<bf01d820>] (sdio_bus_probe+0x94/0xfc [mmc_core])
[ 209.396748] [<bf01d820>] (sdio_bus_probe+0x94/0xfc [mmc_core]) from [<c02e729c>] (driver_probe_device+0x12c/0x348)
[ 209.407214] [<c02e729c>] (driver_probe_device+0x12c/0x348) from [<c02e7530>] (__driver_attach+0x78/0x9c)
[ 209.416798] [<c02e7530>] (__driver_attach+0x78/0x9c) from [<c02e5658>] (bus_for_each_dev+0x50/0x88)
[ 209.425946] [<c02e5658>] (bus_for_each_dev+0x50/0x88) from [<c02e6810>] (bus_add_driver+0x108/0x268)
[ 209.435180] [<c02e6810>] (bus_add_driver+0x108/0x268) from [<c02e782c>] (driver_register+0xa4/0x134)
[ 209.444426] [<c02e782c>] (driver_register+0xa4/0x134) from [<bf22601c>] (if_sdio_init_module+0x1c/0x3c [libertas_sdio])
[ 209.455339] [<bf22601c>] (if_sdio_init_module+0x1c/0x3c [libertas_sdio]) from [<c00085b8>] (do_one_initcall+0x98/0x174)
[ 209.466236] [<c00085b8>] (do_one_initcall+0x98/0x174) from [<c0076504>] (load_module+0x1c5c/0x1f80)
[ 209.475390] [<c0076504>] (load_module+0x1c5c/0x1f80) from [<c007692c>] (sys_init_module+0x104/0x128)
[ 209.484632] [<c007692c>] (sys_init_module+0x104/0x128) from [<c0008c40>] (ret_fast_syscall+0x0/0x38)
Fix it by setting fw_ready flag prior to queuing FUNC_INIT command.
Cc: <stable@vger.kernel.org> # 3.5+
Reported-by: Lubomir Rintel <lkundrak@v3.sk>
Tested-by: Lubomir Rintel <lkundrak@v3.sk>
Signed-off-by: Bing Zhao <bzhao@marvell.com>
Signed-off-by: John W. Linville <linville@tuxdriver.com>
-rw-r--r-- | drivers/net/wireless/libertas/if_sdio.c | 6 |
1 files changed, 5 insertions, 1 deletions
diff --git a/drivers/net/wireless/libertas/if_sdio.c b/drivers/net/wireless/libertas/if_sdio.c index 739309e70d8..45578335e42 100644 --- a/drivers/net/wireless/libertas/if_sdio.c +++ b/drivers/net/wireless/libertas/if_sdio.c | |||
@@ -825,6 +825,11 @@ static void if_sdio_finish_power_on(struct if_sdio_card *card) | |||
825 | 825 | ||
826 | sdio_release_host(func); | 826 | sdio_release_host(func); |
827 | 827 | ||
828 | /* Set fw_ready before queuing any commands so that | ||
829 | * lbs_thread won't block from sending them to firmware. | ||
830 | */ | ||
831 | priv->fw_ready = 1; | ||
832 | |||
828 | /* | 833 | /* |
829 | * FUNC_INIT is required for SD8688 WLAN/BT multiple functions | 834 | * FUNC_INIT is required for SD8688 WLAN/BT multiple functions |
830 | */ | 835 | */ |
@@ -839,7 +844,6 @@ static void if_sdio_finish_power_on(struct if_sdio_card *card) | |||
839 | netdev_alert(priv->dev, "CMD_FUNC_INIT cmd failed\n"); | 844 | netdev_alert(priv->dev, "CMD_FUNC_INIT cmd failed\n"); |
840 | } | 845 | } |
841 | 846 | ||
842 | priv->fw_ready = 1; | ||
843 | wake_up(&card->pwron_waitq); | 847 | wake_up(&card->pwron_waitq); |
844 | 848 | ||
845 | if (!card->started) { | 849 | if (!card->started) { |