aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorPaul Gortmaker2011-03-14 18:32:21 -0500
committerJames Morris2011-03-21 17:35:12 -0500
commit5806896019ceaa0a1e808182afb4bba33c948ad6 (patch)
treed0fe25384a3c87048b5eec639a11e57c9629d854
parent4aab1e896a0a9d57420ff2867caa5a369123d8cb (diff)
downloadam43-linux-kernel-5806896019ceaa0a1e808182afb4bba33c948ad6.tar.gz
am43-linux-kernel-5806896019ceaa0a1e808182afb4bba33c948ad6.tar.xz
am43-linux-kernel-5806896019ceaa0a1e808182afb4bba33c948ad6.zip
security: select correct default LSM_MMAP_MIN_ADDR on ARM.
The default for this is universally set to 64k, but the help says: For most ia64, ppc64 and x86 users with lots of address space a value of 65536 is reasonable and should cause no problems. On arm and other archs it should not be higher than 32768. The text is right, in that we are seeing selinux-enabled ARM targets that fail to launch /sbin/init because selinux blocks a memory map. So select the right value if we know we are building ARM. Signed-off-by: Paul Gortmaker <paul.gortmaker@windriver.com> Signed-off-by: James Morris <jmorris@namei.org>
-rw-r--r--security/Kconfig1
1 files changed, 1 insertions, 0 deletions
diff --git a/security/Kconfig b/security/Kconfig
index 95accd442d5..e0f08b52e4a 100644
--- a/security/Kconfig
+++ b/security/Kconfig
@@ -167,6 +167,7 @@ config INTEL_TXT
167config LSM_MMAP_MIN_ADDR 167config LSM_MMAP_MIN_ADDR
168 int "Low address space for LSM to protect from user allocation" 168 int "Low address space for LSM to protect from user allocation"
169 depends on SECURITY && SECURITY_SELINUX 169 depends on SECURITY && SECURITY_SELINUX
170 default 32768 if ARM
170 default 65536 171 default 65536
171 help 172 help
172 This is the portion of low virtual memory which should be protected 173 This is the portion of low virtual memory which should be protected