diff options
author | Jeff Dike | 2006-12-13 02:34:12 -0600 |
---|---|---|
committer | Linus Torvalds | 2006-12-13 11:05:48 -0600 |
commit | 011e3a9ad4891ba1b27e281e085228189c56b137 (patch) | |
tree | 3e9ac42e237bc163e37a89bb3d090608a5e1320b /Makefile | |
parent | dd47ea755693228bf842c779e8afdfa47efb20a3 (diff) | |
download | am43-linux-kernel-011e3a9ad4891ba1b27e281e085228189c56b137.tar.gz am43-linux-kernel-011e3a9ad4891ba1b27e281e085228189c56b137.tar.xz am43-linux-kernel-011e3a9ad4891ba1b27e281e085228189c56b137.zip |
[PATCH] Fix crossbuilding checkstack
The previous checkstack fix for UML, which needs to use the host's tools,
was wrong in the crossbuilding case. It would use the build host's, rather
than the target's, toolchain.
This patch removes the old fix and adds an explicit special case for UML,
leaving everyone else alone.
Signed-off-by: Jeff Dike <jdike@addtoit.com>
Signed-off-by: Andrew Morton <akpm@osdl.org>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
Diffstat (limited to 'Makefile')
-rw-r--r-- | Makefile | 14 |
1 files changed, 10 insertions, 4 deletions
@@ -1390,12 +1390,18 @@ endif #ifeq ($(mixed-targets),1) | |||
1390 | 1390 | ||
1391 | PHONY += checkstack kernelrelease kernelversion | 1391 | PHONY += checkstack kernelrelease kernelversion |
1392 | 1392 | ||
1393 | # Use $(SUBARCH) here instead of $(ARCH) so that this works for UML. | 1393 | # UML needs a little special treatment here. It wants to use the host |
1394 | # In the UML case, $(SUBARCH) is the name of the underlying | 1394 | # toolchain, so needs $(SUBARCH) passed to checkstack.pl. Everyone |
1395 | # architecture, while for all other arches, it is the same as $(ARCH). | 1395 | # else wants $(ARCH), including people doing cross-builds, which means |
1396 | # that $(SUBARCH) doesn't work here. | ||
1397 | ifeq ($(ARCH), um) | ||
1398 | CHECKSTACK_ARCH := $(SUBARCH) | ||
1399 | else | ||
1400 | CHECKSTACK_ARCH := $(ARCH) | ||
1401 | endif | ||
1396 | checkstack: | 1402 | checkstack: |
1397 | $(OBJDUMP) -d vmlinux $$(find . -name '*.ko') | \ | 1403 | $(OBJDUMP) -d vmlinux $$(find . -name '*.ko') | \ |
1398 | $(PERL) $(src)/scripts/checkstack.pl $(SUBARCH) | 1404 | $(PERL) $(src)/scripts/checkstack.pl $(CHECKSTACK_ARCH) |
1399 | 1405 | ||
1400 | kernelrelease: | 1406 | kernelrelease: |
1401 | $(if $(wildcard include/config/kernel.release), $(Q)echo $(KERNELRELEASE), \ | 1407 | $(if $(wildcard include/config/kernel.release), $(Q)echo $(KERNELRELEASE), \ |