diff options
author | Linus Torvalds | 2012-10-12 20:05:52 -0500 |
---|---|---|
committer | Linus Torvalds | 2012-10-12 20:05:52 -0500 |
commit | 4e21fc138bfd7fe625ff5dc81541399aaf9d429b (patch) | |
tree | 43bedf14d2eee7711b8241dcfd6bd7b8737d9bd5 /arch/Kconfig | |
parent | 8418263e3547ed3816475e4c55a77004f0426ee6 (diff) | |
parent | 5522be6a4624a5f505555569e4d9cee946630686 (diff) | |
download | am43-linux-kernel-4e21fc138bfd7fe625ff5dc81541399aaf9d429b.tar.gz am43-linux-kernel-4e21fc138bfd7fe625ff5dc81541399aaf9d429b.tar.xz am43-linux-kernel-4e21fc138bfd7fe625ff5dc81541399aaf9d429b.zip |
Merge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/signal
Pull third pile of kernel_execve() patches from Al Viro:
"The last bits of infrastructure for kernel_thread() et.al., with
alpha/arm/x86 use of those. Plus sanitizing the asm glue and
do_notify_resume() on alpha, fixing the "disabled irq while running
task_work stuff" breakage there.
At that point the rest of kernel_thread/kernel_execve/sys_execve work
can be done independently for different architectures. The only
pending bits that do depend on having all architectures converted are
restrictred to fs/* and kernel/* - that'll obviously have to wait for
the next cycle.
I thought we'd have to wait for all of them done before we start
eliminating the longjump-style insanity in kernel_execve(), but it
turned out there's a very simple way to do that without flagday-style
changes."
* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/signal:
alpha: switch to saner kernel_execve() semantics
arm: switch to saner kernel_execve() semantics
x86, um: convert to saner kernel_execve() semantics
infrastructure for saner ret_from_kernel_thread semantics
make sure that kernel_thread() callbacks call do_exit() themselves
make sure that we always have a return path from kernel_execve()
ppc: eeh_event should just use kthread_run()
don't bother with kernel_thread/kernel_execve for launching linuxrc
alpha: get rid of switch_stack argument of do_work_pending()
alpha: don't bother passing switch_stack separately from regs
alpha: take SIGPENDING/NOTIFY_RESUME loop into signal.c
alpha: simplify TIF_NEED_RESCHED handling
Diffstat (limited to 'arch/Kconfig')
-rw-r--r-- | arch/Kconfig | 3 |
1 files changed, 3 insertions, 0 deletions
diff --git a/arch/Kconfig b/arch/Kconfig index 26a28419caf..a79a1ad8bb9 100644 --- a/arch/Kconfig +++ b/arch/Kconfig | |||
@@ -274,6 +274,9 @@ config ARCH_WANT_OLD_COMPAT_IPC | |||
274 | config GENERIC_KERNEL_THREAD | 274 | config GENERIC_KERNEL_THREAD |
275 | bool | 275 | bool |
276 | 276 | ||
277 | config GENERIC_KERNEL_EXECVE | ||
278 | bool | ||
279 | |||
277 | config HAVE_ARCH_SECCOMP_FILTER | 280 | config HAVE_ARCH_SECCOMP_FILTER |
278 | bool | 281 | bool |
279 | help | 282 | help |