diff options
author | Vineet Gupta | 2013-01-18 03:42:20 -0600 |
---|---|---|
committer | Vineet Gupta | 2013-02-15 11:45:56 -0600 |
commit | 450dd430bf45ab212a91acfb9bed2528d17f30cd (patch) | |
tree | deaf7d7aef0616834e804de041eea9de3e0a52c8 /arch/arc | |
parent | 999159a5381bff3bd6f688c5d20fbec9d8789e53 (diff) | |
download | am43-linux-kernel-450dd430bf45ab212a91acfb9bed2528d17f30cd.tar.gz am43-linux-kernel-450dd430bf45ab212a91acfb9bed2528d17f30cd.tar.xz am43-linux-kernel-450dd430bf45ab212a91acfb9bed2528d17f30cd.zip |
ARC: [DeviceTree] Convert some Kconfig items to runtime values
* mem size now runtime configured (prev CONFIG_ARC_PLAT_SDRAM_SIZE)
* core cpu clk runtime configured (prev CONFIG_ARC_PLAT_CLK)
Signed-off-by: Vineet Gupta <vgupta@synopsys.com>
Cc: Arnd Bergmann <arnd@arndb.de>
Cc: Grant Likely <grant.likely@secretlab.ca>
Diffstat (limited to 'arch/arc')
-rw-r--r-- | arch/arc/Kconfig | 12 | ||||
-rw-r--r-- | arch/arc/boot/dts/skeleton.dtsi | 6 | ||||
-rw-r--r-- | arch/arc/include/asm/clk.h | 2 | ||||
-rw-r--r-- | arch/arc/kernel/clk.c | 12 | ||||
-rw-r--r-- | arch/arc/kernel/devtree.c | 13 | ||||
-rw-r--r-- | arch/arc/mm/init.c | 9 |
6 files changed, 37 insertions, 17 deletions
diff --git a/arch/arc/Kconfig b/arch/arc/Kconfig index 76668579b54..7db978570fb 100644 --- a/arch/arc/Kconfig +++ b/arch/arc/Kconfig | |||
@@ -249,10 +249,6 @@ source "arch/arc/plat-arcfpga/Kconfig" | |||
249 | 249 | ||
250 | #New platform adds here | 250 | #New platform adds here |
251 | 251 | ||
252 | config ARC_PLAT_CLK | ||
253 | int "Clk speed in Hz" | ||
254 | default "80000000" | ||
255 | |||
256 | config LINUX_LINK_BASE | 252 | config LINUX_LINK_BASE |
257 | hex "Linux Link Address" | 253 | hex "Linux Link Address" |
258 | default "0x80000000" | 254 | default "0x80000000" |
@@ -266,14 +262,6 @@ config LINUX_LINK_BASE | |||
266 | Linux needs to be scooted a bit. | 262 | Linux needs to be scooted a bit. |
267 | If you don't know what the above means, leave this setting alone. | 263 | If you don't know what the above means, leave this setting alone. |
268 | 264 | ||
269 | config ARC_PLAT_SDRAM_SIZE | ||
270 | hex "SD RAM Size" | ||
271 | default "0x10000000" | ||
272 | help | ||
273 | Implies the amount of SDRAM/DRAM Linux is going to claim/own. | ||
274 | The actual memory itself could be larger than this number. But for | ||
275 | all software purposes, this is the amt of memory. | ||
276 | |||
277 | endmenu # "Platform Board Configuration" | 265 | endmenu # "Platform Board Configuration" |
278 | 266 | ||
279 | config ARC_STACK_NONEXEC | 267 | config ARC_STACK_NONEXEC |
diff --git a/arch/arc/boot/dts/skeleton.dtsi b/arch/arc/boot/dts/skeleton.dtsi index 9b357d802a1..eb8b7736735 100644 --- a/arch/arc/boot/dts/skeleton.dtsi +++ b/arch/arc/boot/dts/skeleton.dtsi | |||
@@ -13,9 +13,13 @@ | |||
13 | 13 | ||
14 | / { | 14 | / { |
15 | compatible = "snps,arc"; | 15 | compatible = "snps,arc"; |
16 | clock-frequency = <80000000>; /* 80 MHZ */ | ||
16 | #address-cells = <1>; | 17 | #address-cells = <1>; |
17 | #size-cells = <1>; | 18 | #size-cells = <1>; |
18 | chosen { }; | 19 | chosen { }; |
19 | aliases { }; | 20 | aliases { }; |
20 | memory { device_type = "memory"; reg = <0 0>; }; | 21 | memory { |
22 | device_type = "memory"; | ||
23 | reg = <0x00000000 0x10000000>; /* 256M */ | ||
24 | }; | ||
21 | }; | 25 | }; |
diff --git a/arch/arc/include/asm/clk.h b/arch/arc/include/asm/clk.h index 61956436c75..bf9d29f5bd5 100644 --- a/arch/arc/include/asm/clk.h +++ b/arch/arc/include/asm/clk.h | |||
@@ -17,4 +17,6 @@ static inline unsigned long arc_get_core_freq(void) | |||
17 | return core_freq; | 17 | return core_freq; |
18 | } | 18 | } |
19 | 19 | ||
20 | extern int arc_set_core_freq(unsigned long); | ||
21 | |||
20 | #endif | 22 | #endif |
diff --git a/arch/arc/kernel/clk.c b/arch/arc/kernel/clk.c index 64925db9eb5..66ce0dc917f 100644 --- a/arch/arc/kernel/clk.c +++ b/arch/arc/kernel/clk.c | |||
@@ -8,4 +8,14 @@ | |||
8 | 8 | ||
9 | #include <asm/clk.h> | 9 | #include <asm/clk.h> |
10 | 10 | ||
11 | unsigned long core_freq = CONFIG_ARC_PLAT_CLK; | 11 | unsigned long core_freq = 800000000; |
12 | |||
13 | /* | ||
14 | * As of now we default to device-tree provided clock | ||
15 | * In future we can determine this in early boot | ||
16 | */ | ||
17 | int arc_set_core_freq(unsigned long freq) | ||
18 | { | ||
19 | core_freq = freq; | ||
20 | return 0; | ||
21 | } | ||
diff --git a/arch/arc/kernel/devtree.c b/arch/arc/kernel/devtree.c index 48e157efad1..c8166dc02c3 100644 --- a/arch/arc/kernel/devtree.c +++ b/arch/arc/kernel/devtree.c | |||
@@ -15,6 +15,7 @@ | |||
15 | #include <linux/of.h> | 15 | #include <linux/of.h> |
16 | #include <linux/of_fdt.h> | 16 | #include <linux/of_fdt.h> |
17 | #include <asm/prom.h> | 17 | #include <asm/prom.h> |
18 | #include <asm/clk.h> | ||
18 | 19 | ||
19 | /* called from unflatten_device_tree() to bootstrap devicetree itself */ | 20 | /* called from unflatten_device_tree() to bootstrap devicetree itself */ |
20 | void * __init early_init_dt_alloc_memory_arch(u64 size, u64 align) | 21 | void * __init early_init_dt_alloc_memory_arch(u64 size, u64 align) |
@@ -34,7 +35,9 @@ int __init setup_machine_fdt(void *dt) | |||
34 | struct boot_param_header *devtree = dt; | 35 | struct boot_param_header *devtree = dt; |
35 | unsigned long dt_root; | 36 | unsigned long dt_root; |
36 | char *model, *compat; | 37 | char *model, *compat; |
38 | void *clk; | ||
37 | char manufacturer[16]; | 39 | char manufacturer[16]; |
40 | unsigned long len; | ||
38 | 41 | ||
39 | /* check device tree validity */ | 42 | /* check device tree validity */ |
40 | if (be32_to_cpu(devtree->magic) != OF_DT_HEADER) | 43 | if (be32_to_cpu(devtree->magic) != OF_DT_HEADER) |
@@ -60,5 +63,15 @@ int __init setup_machine_fdt(void *dt) | |||
60 | /* Retrieve various information from the /chosen node */ | 63 | /* Retrieve various information from the /chosen node */ |
61 | of_scan_flat_dt(early_init_dt_scan_chosen, boot_command_line); | 64 | of_scan_flat_dt(early_init_dt_scan_chosen, boot_command_line); |
62 | 65 | ||
66 | /* Initialize {size,address}-cells info */ | ||
67 | of_scan_flat_dt(early_init_dt_scan_root, NULL); | ||
68 | |||
69 | /* Setup memory, calling early_init_dt_add_memory_arch */ | ||
70 | of_scan_flat_dt(early_init_dt_scan_memory, NULL); | ||
71 | |||
72 | clk = of_get_flat_dt_prop(dt_root, "clock-frequency", &len); | ||
73 | if (clk) | ||
74 | arc_set_core_freq(of_read_ulong(clk, len/4)); | ||
75 | |||
63 | return 0; | 76 | return 0; |
64 | } | 77 | } |
diff --git a/arch/arc/mm/init.c b/arch/arc/mm/init.c index 682cf574048..caf797de23f 100644 --- a/arch/arc/mm/init.c +++ b/arch/arc/mm/init.c | |||
@@ -25,7 +25,7 @@ char empty_zero_page[PAGE_SIZE] __aligned(PAGE_SIZE); | |||
25 | EXPORT_SYMBOL(empty_zero_page); | 25 | EXPORT_SYMBOL(empty_zero_page); |
26 | 26 | ||
27 | /* Default tot mem from .config */ | 27 | /* Default tot mem from .config */ |
28 | static unsigned long arc_mem_sz = CONFIG_ARC_PLAT_SDRAM_SIZE; | 28 | static unsigned long arc_mem_sz = 0x20000000; /* some default */ |
29 | 29 | ||
30 | /* User can over-ride above with "mem=nnn[KkMm]" in cmdline */ | 30 | /* User can over-ride above with "mem=nnn[KkMm]" in cmdline */ |
31 | static int __init setup_mem_sz(char *str) | 31 | static int __init setup_mem_sz(char *str) |
@@ -41,7 +41,8 @@ early_param("mem", setup_mem_sz); | |||
41 | 41 | ||
42 | void __init early_init_dt_add_memory_arch(u64 base, u64 size) | 42 | void __init early_init_dt_add_memory_arch(u64 base, u64 size) |
43 | { | 43 | { |
44 | pr_err("%s(%llx, %llx)\n", __func__, base, size); | 44 | arc_mem_sz = size & PAGE_MASK; |
45 | pr_info("Memory size set via devicetree %ldM\n", TO_MB(arc_mem_sz)); | ||
45 | } | 46 | } |
46 | 47 | ||
47 | /* | 48 | /* |
@@ -62,7 +63,9 @@ void __init setup_arch_memory(void) | |||
62 | 63 | ||
63 | /* | 64 | /* |
64 | * We do it here, so that memory is correctly instantiated | 65 | * We do it here, so that memory is correctly instantiated |
65 | * even if "mem=xxx" cmline over-ride is not given | 66 | * even if "mem=xxx" cmline over-ride is given and/or |
67 | * DT has memory node. Each causes an update to @arc_mem_sz | ||
68 | * and we finally add memory one here | ||
66 | */ | 69 | */ |
67 | memblock_add(CONFIG_LINUX_LINK_BASE, arc_mem_sz); | 70 | memblock_add(CONFIG_LINUX_LINK_BASE, arc_mem_sz); |
68 | 71 | ||