diff options
author | David Howells | 2012-10-04 06:10:18 -0500 |
---|---|---|
committer | David Howells | 2012-10-04 06:10:18 -0500 |
commit | 890139529d45ebd3c60d541f4eddc60e042fdf98 (patch) | |
tree | b5a6bc076ca22ce95269544db5c9033496df8b95 /arch/hexagon | |
parent | 612a9aab56a93533e76e3ad91642db7033e03b69 (diff) | |
download | am43-linux-kernel-890139529d45ebd3c60d541f4eddc60e042fdf98.tar.gz am43-linux-kernel-890139529d45ebd3c60d541f4eddc60e042fdf98.tar.xz am43-linux-kernel-890139529d45ebd3c60d541f4eddc60e042fdf98.zip |
UAPI: Fix the guards on various asm/unistd.h files
asm-generic/unistd.h and a number of asm/unistd.h files have been given
reinclusion guards that allow the guard to be overridden if __SYSCALL is
defined. Unfortunately, these files define __SYSCALL and don't undefine it
when they've finished with it, thus rendering the guard ineffective.
The reason for this override is to allow the file to be #included multiple
times with different settings on __SYSCALL for purposes like generating syscall
tables.
The following guards are problematic:
arch/arm64/include/asm/unistd.h:#if !defined(__ASM_UNISTD_H) || defined(__SYSCALL)
arch/arm64/include/asm/unistd32.h:#if !defined(__ASM_UNISTD32_H) || defined(__SYSCALL)
arch/c6x/include/asm/unistd.h:#if !defined(_ASM_C6X_UNISTD_H) || defined(__SYSCALL)
arch/hexagon/include/asm/unistd.h:#if !defined(_ASM_HEXAGON_UNISTD_H) || defined(__SYSCALL)
arch/openrisc/include/asm/unistd.h:#if !defined(__ASM_OPENRISC_UNISTD_H) || defined(__SYSCALL)
arch/score/include/asm/unistd.h:#if !defined(_ASM_SCORE_UNISTD_H) || defined(__SYSCALL)
arch/tile/include/asm/unistd.h:#if !defined(_ASM_TILE_UNISTD_H) || defined(__SYSCALL)
arch/unicore32/include/asm/unistd.h:#if !defined(__UNICORE_UNISTD_H__) || defined(__SYSCALL)
include/asm-generic/unistd.h:#if !defined(_ASM_GENERIC_UNISTD_H) || defined(__SYSCALL)
On the assumption that the guards' ineffectiveness has passed unnoticed, just
remove these guards entirely.
Signed-off-by: David Howells <dhowells@redhat.com>
Acked-by: Arnd Bergmann <arnd@arndb.de>
Acked-by: Catalin Marinas <catalin.marinas@arm.com>
Diffstat (limited to 'arch/hexagon')
-rw-r--r-- | arch/hexagon/include/asm/unistd.h | 5 |
1 files changed, 0 insertions, 5 deletions
diff --git a/arch/hexagon/include/asm/unistd.h b/arch/hexagon/include/asm/unistd.h index 4d0ecde3665..c0d5565030a 100644 --- a/arch/hexagon/include/asm/unistd.h +++ b/arch/hexagon/include/asm/unistd.h | |||
@@ -18,9 +18,6 @@ | |||
18 | * 02110-1301, USA. | 18 | * 02110-1301, USA. |
19 | */ | 19 | */ |
20 | 20 | ||
21 | #if !defined(_ASM_HEXAGON_UNISTD_H) || defined(__SYSCALL) | ||
22 | #define _ASM_HEXAGON_UNISTD_H | ||
23 | |||
24 | /* | 21 | /* |
25 | * The kernel pulls this unistd.h in three different ways: | 22 | * The kernel pulls this unistd.h in three different ways: |
26 | * 1. the "normal" way which gets all the __NR defines | 23 | * 1. the "normal" way which gets all the __NR defines |
@@ -32,5 +29,3 @@ | |||
32 | #define sys_mmap2 sys_mmap_pgoff | 29 | #define sys_mmap2 sys_mmap_pgoff |
33 | 30 | ||
34 | #include <asm-generic/unistd.h> | 31 | #include <asm-generic/unistd.h> |
35 | |||
36 | #endif | ||