diff options
author | Al Viro | 2012-06-01 13:22:01 -0500 |
---|---|---|
committer | Al Viro | 2012-10-01 08:58:13 -0500 |
commit | 16a8016372c42c7628eb4a39d75386a461e8c5d0 (patch) | |
tree | 94ed1fab5b073d66be50a876ad81104eeb73c732 /arch/m32r | |
parent | 8af4efac26e1805c76144ad44118157239308d35 (diff) | |
download | am43-linux-kernel-16a8016372c42c7628eb4a39d75386a461e8c5d0.tar.gz am43-linux-kernel-16a8016372c42c7628eb4a39d75386a461e8c5d0.tar.xz am43-linux-kernel-16a8016372c42c7628eb4a39d75386a461e8c5d0.zip |
sanitize tsk_is_polling()
Make default just return 0. The current default (checking
TIF_POLLING_NRFLAG) is taken to architectures that need it;
ones that don't do polling in their idle threads don't need
to defined TIF_POLLING_NRFLAG at all.
ia64 defined both TS_POLLING (used by its tsk_is_polling())
and TIF_POLLING_NRFLAG (not used at all). Killed the latter...
Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
Diffstat (limited to 'arch/m32r')
-rw-r--r-- | arch/m32r/include/asm/thread_info.h | 2 |
1 files changed, 0 insertions, 2 deletions
diff --git a/arch/m32r/include/asm/thread_info.h b/arch/m32r/include/asm/thread_info.h index 18b058457d3..763e8aec5ea 100644 --- a/arch/m32r/include/asm/thread_info.h +++ b/arch/m32r/include/asm/thread_info.h | |||
@@ -123,7 +123,6 @@ static inline unsigned int get_thread_fault_code(void) | |||
123 | #define TIF_NOTIFY_RESUME 5 /* callback before returning to user */ | 123 | #define TIF_NOTIFY_RESUME 5 /* callback before returning to user */ |
124 | #define TIF_RESTORE_SIGMASK 8 /* restore signal mask in do_signal() */ | 124 | #define TIF_RESTORE_SIGMASK 8 /* restore signal mask in do_signal() */ |
125 | #define TIF_USEDFPU 16 /* FPU was used by this task this quantum (SMP) */ | 125 | #define TIF_USEDFPU 16 /* FPU was used by this task this quantum (SMP) */ |
126 | #define TIF_POLLING_NRFLAG 17 /* true if poll_idle() is polling TIF_NEED_RESCHED */ | ||
127 | #define TIF_MEMDIE 18 /* is terminating due to OOM killer */ | 126 | #define TIF_MEMDIE 18 /* is terminating due to OOM killer */ |
128 | 127 | ||
129 | #define _TIF_SYSCALL_TRACE (1<<TIF_SYSCALL_TRACE) | 128 | #define _TIF_SYSCALL_TRACE (1<<TIF_SYSCALL_TRACE) |
@@ -133,7 +132,6 @@ static inline unsigned int get_thread_fault_code(void) | |||
133 | #define _TIF_IRET (1<<TIF_IRET) | 132 | #define _TIF_IRET (1<<TIF_IRET) |
134 | #define _TIF_NOTIFY_RESUME (1<<TIF_NOTIFY_RESUME) | 133 | #define _TIF_NOTIFY_RESUME (1<<TIF_NOTIFY_RESUME) |
135 | #define _TIF_USEDFPU (1<<TIF_USEDFPU) | 134 | #define _TIF_USEDFPU (1<<TIF_USEDFPU) |
136 | #define _TIF_POLLING_NRFLAG (1<<TIF_POLLING_NRFLAG) | ||
137 | 135 | ||
138 | #define _TIF_WORK_MASK 0x0000FFFE /* work to do on interrupt/exception return */ | 136 | #define _TIF_WORK_MASK 0x0000FFFE /* work to do on interrupt/exception return */ |
139 | #define _TIF_ALLWORK_MASK 0x0000FFFF /* work to do on any return to u-space */ | 137 | #define _TIF_ALLWORK_MASK 0x0000FFFF /* work to do on any return to u-space */ |