diff options
author | Linus Torvalds | 2012-10-09 01:58:38 -0500 |
---|---|---|
committer | Linus Torvalds | 2012-10-09 01:58:38 -0500 |
commit | 50e0d10232db05c6776afcf6098459bff47e8b15 (patch) | |
tree | 0e89971de6d960c8946cc9351d73b297347a0260 /arch/m32r | |
parent | 8711798772641b2f593beebebcab5b1ec2309f0c (diff) | |
parent | c37d6154c0b9163c27e53cc1d0be3867b4abd760 (diff) | |
download | am43-linux-kernel-50e0d10232db05c6776afcf6098459bff47e8b15.tar.gz am43-linux-kernel-50e0d10232db05c6776afcf6098459bff47e8b15.tar.xz am43-linux-kernel-50e0d10232db05c6776afcf6098459bff47e8b15.zip |
Merge tag 'asm-generic' of git://git.kernel.org/pub/scm/linux/kernel/git/arnd/asm-generic
Pull asm-generic updates from Arnd Bergmann:
"This has three changes for asm-generic that did not really fit into
any other branch as normal asm-generic changes do. One is a fix for a
build warning, the other two are more interesting:
* A patch from Mark Brown to allow using the common clock
infrastructure on all architectures, so we can use the clock API in
architecture independent device drivers.
* The UAPI split patches from David Howells for the asm-generic
files. There are other architecture specific series that are going
through the arch maintainer tree and that depend on this one.
There may be a few small merge conflicts between Mark's patch and the
following arch header file split patches. In each case the solution
will be to keep the new "generic-y += clkdev.h" line, even if it ends
up being the only line in the Kbuild file."
* tag 'asm-generic' of git://git.kernel.org/pub/scm/linux/kernel/git/arnd/asm-generic:
UAPI: (Scripted) Disintegrate include/asm-generic
asm-generic: Add default clkdev.h
asm-generic: xor: mark static functions as __maybe_unused
Diffstat (limited to 'arch/m32r')
-rw-r--r-- | arch/m32r/include/asm/Kbuild | 2 |
1 files changed, 2 insertions, 0 deletions
diff --git a/arch/m32r/include/asm/Kbuild b/arch/m32r/include/asm/Kbuild index c68e1680da0..0e152a93c12 100644 --- a/arch/m32r/include/asm/Kbuild +++ b/arch/m32r/include/asm/Kbuild | |||
@@ -1 +1,3 @@ | |||
1 | include include/asm-generic/Kbuild.asm | 1 | include include/asm-generic/Kbuild.asm |
2 | |||
3 | generic-y += clkdev.h | ||