diff options
author | Al Viro | 2012-05-02 08:59:21 -0500 |
---|---|---|
committer | Al Viro | 2012-06-01 11:58:48 -0500 |
commit | b7f9a11a6cf1ea9ee6be3eb2b90d91327a09ad14 (patch) | |
tree | 7d5a5f469aea8ac2b3e1ab41e05a6abafcb2b694 /arch/score | |
parent | 51a7b448d4134e3e8eec633435e3e8faee14a828 (diff) | |
download | am43-linux-kernel-b7f9a11a6cf1ea9ee6be3eb2b90d91327a09ad14.tar.gz am43-linux-kernel-b7f9a11a6cf1ea9ee6be3eb2b90d91327a09ad14.tar.xz am43-linux-kernel-b7f9a11a6cf1ea9ee6be3eb2b90d91327a09ad14.zip |
new helper: sigmask_to_save()
replace boilerplate "should we use ->saved_sigmask or ->blocked?"
with calls of obvious inlined helper...
Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
Diffstat (limited to 'arch/score')
-rw-r--r-- | arch/score/kernel/signal.c | 12 |
1 files changed, 3 insertions, 9 deletions
diff --git a/arch/score/kernel/signal.c b/arch/score/kernel/signal.c index 9e751559375..b24dfaf2462 100644 --- a/arch/score/kernel/signal.c +++ b/arch/score/kernel/signal.c | |||
@@ -242,7 +242,7 @@ give_sigsegv: | |||
242 | } | 242 | } |
243 | 243 | ||
244 | static int handle_signal(unsigned long sig, siginfo_t *info, | 244 | static int handle_signal(unsigned long sig, siginfo_t *info, |
245 | struct k_sigaction *ka, sigset_t *oldset, struct pt_regs *regs) | 245 | struct k_sigaction *ka, struct pt_regs *regs) |
246 | { | 246 | { |
247 | int ret; | 247 | int ret; |
248 | 248 | ||
@@ -269,7 +269,7 @@ static int handle_signal(unsigned long sig, siginfo_t *info, | |||
269 | /* | 269 | /* |
270 | * Set up the stack frame | 270 | * Set up the stack frame |
271 | */ | 271 | */ |
272 | ret = setup_rt_frame(ka, regs, sig, oldset, info); | 272 | ret = setup_rt_frame(ka, regs, sig, sigmask_to_save(), info); |
273 | 273 | ||
274 | if (ret == 0) | 274 | if (ret == 0) |
275 | block_sigmask(ka, sig); | 275 | block_sigmask(ka, sig); |
@@ -280,7 +280,6 @@ static int handle_signal(unsigned long sig, siginfo_t *info, | |||
280 | static void do_signal(struct pt_regs *regs) | 280 | static void do_signal(struct pt_regs *regs) |
281 | { | 281 | { |
282 | struct k_sigaction ka; | 282 | struct k_sigaction ka; |
283 | sigset_t *oldset; | ||
284 | siginfo_t info; | 283 | siginfo_t info; |
285 | int signr; | 284 | int signr; |
286 | 285 | ||
@@ -292,15 +291,10 @@ static void do_signal(struct pt_regs *regs) | |||
292 | if (!user_mode(regs)) | 291 | if (!user_mode(regs)) |
293 | return; | 292 | return; |
294 | 293 | ||
295 | if (test_thread_flag(TIF_RESTORE_SIGMASK)) | ||
296 | oldset = ¤t->saved_sigmask; | ||
297 | else | ||
298 | oldset = ¤t->blocked; | ||
299 | |||
300 | signr = get_signal_to_deliver(&info, &ka, regs, NULL); | 294 | signr = get_signal_to_deliver(&info, &ka, regs, NULL); |
301 | if (signr > 0) { | 295 | if (signr > 0) { |
302 | /* Actually deliver the signal. */ | 296 | /* Actually deliver the signal. */ |
303 | if (handle_signal(signr, &info, &ka, oldset, regs) == 0) { | 297 | if (handle_signal(signr, &info, &ka, regs) == 0) { |
304 | /* | 298 | /* |
305 | * A signal was successfully delivered; the saved | 299 | * A signal was successfully delivered; the saved |
306 | * sigmask will have been stored in the signal frame, | 300 | * sigmask will have been stored in the signal frame, |