diff options
author | Linus Torvalds | 2013-02-23 20:50:11 -0600 |
---|---|---|
committer | Linus Torvalds | 2013-02-23 20:50:11 -0600 |
commit | 9e2d59ad580d590134285f361a0e80f0e98c0207 (patch) | |
tree | f3232be75781484193413f32ec82c21f6d8eb76e /arch/sh | |
parent | 5ce1a70e2f00f0bce0cab57f798ca354b9496169 (diff) | |
parent | 235b80226b986dabcbba844968f7807866bd0bfe (diff) | |
download | am43-linux-kernel-9e2d59ad580d590134285f361a0e80f0e98c0207.tar.gz am43-linux-kernel-9e2d59ad580d590134285f361a0e80f0e98c0207.tar.xz am43-linux-kernel-9e2d59ad580d590134285f361a0e80f0e98c0207.zip |
Merge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/signal
Pull signal handling cleanups from Al Viro:
"This is the first pile; another one will come a bit later and will
contain SYSCALL_DEFINE-related patches.
- a bunch of signal-related syscalls (both native and compat)
unified.
- a bunch of compat syscalls switched to COMPAT_SYSCALL_DEFINE
(fixing several potential problems with missing argument
validation, while we are at it)
- a lot of now-pointless wrappers killed
- a couple of architectures (cris and hexagon) forgot to save
altstack settings into sigframe, even though they used the
(uninitialized) values in sigreturn; fixed.
- microblaze fixes for delivery of multiple signals arriving at once
- saner set of helpers for signal delivery introduced, several
architectures switched to using those."
* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/signal: (143 commits)
x86: convert to ksignal
sparc: convert to ksignal
arm: switch to struct ksignal * passing
alpha: pass k_sigaction and siginfo_t using ksignal pointer
burying unused conditionals
make do_sigaltstack() static
arm64: switch to generic old sigaction() (compat-only)
arm64: switch to generic compat rt_sigaction()
arm64: switch compat to generic old sigsuspend
arm64: switch to generic compat rt_sigqueueinfo()
arm64: switch to generic compat rt_sigpending()
arm64: switch to generic compat rt_sigprocmask()
arm64: switch to generic sigaltstack
sparc: switch to generic old sigsuspend
sparc: COMPAT_SYSCALL_DEFINE does all sign-extension as well as SYSCALL_DEFINE
sparc: kill sign-extending wrappers for native syscalls
kill sparc32_open()
sparc: switch to use of generic old sigaction
sparc: switch sys_compat_rt_sigaction() to COMPAT_SYSCALL_DEFINE
mips: switch to generic sys_fork() and sys_clone()
...
Diffstat (limited to 'arch/sh')
-rw-r--r-- | arch/sh/Kconfig | 2 | ||||
-rw-r--r-- | arch/sh/include/asm/syscalls_32.h | 6 | ||||
-rw-r--r-- | arch/sh/include/asm/unistd.h | 2 | ||||
-rw-r--r-- | arch/sh/include/uapi/asm/signal.h | 2 | ||||
-rw-r--r-- | arch/sh/kernel/signal_32.c | 63 | ||||
-rw-r--r-- | arch/sh/kernel/signal_64.c | 62 |
6 files changed, 8 insertions, 129 deletions
diff --git a/arch/sh/Kconfig b/arch/sh/Kconfig index 479146c180c..ef6717a64bc 100644 --- a/arch/sh/Kconfig +++ b/arch/sh/Kconfig | |||
@@ -39,6 +39,8 @@ config SUPERH | |||
39 | select GENERIC_STRNLEN_USER | 39 | select GENERIC_STRNLEN_USER |
40 | select HAVE_MOD_ARCH_SPECIFIC if DWARF_UNWINDER | 40 | select HAVE_MOD_ARCH_SPECIFIC if DWARF_UNWINDER |
41 | select MODULES_USE_ELF_RELA | 41 | select MODULES_USE_ELF_RELA |
42 | select OLD_SIGSUSPEND | ||
43 | select OLD_SIGACTION | ||
42 | help | 44 | help |
43 | The SuperH is a RISC processor targeted for use in embedded systems | 45 | The SuperH is a RISC processor targeted for use in embedded systems |
44 | and consumer electronics; it was also used in the Sega Dreamcast | 46 | and consumer electronics; it was also used in the Sega Dreamcast |
diff --git a/arch/sh/include/asm/syscalls_32.h b/arch/sh/include/asm/syscalls_32.h index cc25485996b..4f97df87d7d 100644 --- a/arch/sh/include/asm/syscalls_32.h +++ b/arch/sh/include/asm/syscalls_32.h | |||
@@ -9,12 +9,6 @@ | |||
9 | 9 | ||
10 | struct pt_regs; | 10 | struct pt_regs; |
11 | 11 | ||
12 | asmlinkage int sys_sigsuspend(old_sigset_t mask); | ||
13 | asmlinkage int sys_sigaction(int sig, const struct old_sigaction __user *act, | ||
14 | struct old_sigaction __user *oact); | ||
15 | asmlinkage int sys_sigaltstack(const stack_t __user *uss, stack_t __user *uoss, | ||
16 | unsigned long r6, unsigned long r7, | ||
17 | struct pt_regs __regs); | ||
18 | asmlinkage int sys_sigreturn(unsigned long r4, unsigned long r5, | 12 | asmlinkage int sys_sigreturn(unsigned long r4, unsigned long r5, |
19 | unsigned long r6, unsigned long r7, | 13 | unsigned long r6, unsigned long r7, |
20 | struct pt_regs __regs); | 14 | struct pt_regs __regs); |
diff --git a/arch/sh/include/asm/unistd.h b/arch/sh/include/asm/unistd.h index 012004ed333..5e90fa2b7ee 100644 --- a/arch/sh/include/asm/unistd.h +++ b/arch/sh/include/asm/unistd.h | |||
@@ -4,7 +4,6 @@ | |||
4 | # include <asm/unistd_64.h> | 4 | # include <asm/unistd_64.h> |
5 | # endif | 5 | # endif |
6 | 6 | ||
7 | # define __ARCH_WANT_SYS_RT_SIGSUSPEND | ||
8 | # define __ARCH_WANT_OLD_READDIR | 7 | # define __ARCH_WANT_OLD_READDIR |
9 | # define __ARCH_WANT_OLD_STAT | 8 | # define __ARCH_WANT_OLD_STAT |
10 | # define __ARCH_WANT_STAT64 | 9 | # define __ARCH_WANT_STAT64 |
@@ -27,7 +26,6 @@ | |||
27 | # define __ARCH_WANT_SYS_OLDUMOUNT | 26 | # define __ARCH_WANT_SYS_OLDUMOUNT |
28 | # define __ARCH_WANT_SYS_SIGPENDING | 27 | # define __ARCH_WANT_SYS_SIGPENDING |
29 | # define __ARCH_WANT_SYS_SIGPROCMASK | 28 | # define __ARCH_WANT_SYS_SIGPROCMASK |
30 | # define __ARCH_WANT_SYS_RT_SIGACTION | ||
31 | # define __ARCH_WANT_SYS_FORK | 29 | # define __ARCH_WANT_SYS_FORK |
32 | # define __ARCH_WANT_SYS_VFORK | 30 | # define __ARCH_WANT_SYS_VFORK |
33 | # define __ARCH_WANT_SYS_CLONE | 31 | # define __ARCH_WANT_SYS_CLONE |
diff --git a/arch/sh/include/uapi/asm/signal.h b/arch/sh/include/uapi/asm/signal.h index 9ac530a90bc..cb96d02f55a 100644 --- a/arch/sh/include/uapi/asm/signal.h +++ b/arch/sh/include/uapi/asm/signal.h | |||
@@ -5,11 +5,13 @@ | |||
5 | 5 | ||
6 | #include <asm-generic/signal.h> | 6 | #include <asm-generic/signal.h> |
7 | 7 | ||
8 | #ifndef __KERNEL__ | ||
8 | struct old_sigaction { | 9 | struct old_sigaction { |
9 | __sighandler_t sa_handler; | 10 | __sighandler_t sa_handler; |
10 | old_sigset_t sa_mask; | 11 | old_sigset_t sa_mask; |
11 | unsigned long sa_flags; | 12 | unsigned long sa_flags; |
12 | void (*sa_restorer)(void); | 13 | void (*sa_restorer)(void); |
13 | }; | 14 | }; |
15 | #endif | ||
14 | 16 | ||
15 | #endif /* __ASM_SH_SIGNAL_H */ | 17 | #endif /* __ASM_SH_SIGNAL_H */ |
diff --git a/arch/sh/kernel/signal_32.c b/arch/sh/kernel/signal_32.c index 2f1f65356c0..6af6e7c5cac 100644 --- a/arch/sh/kernel/signal_32.c +++ b/arch/sh/kernel/signal_32.c | |||
@@ -47,60 +47,6 @@ struct fdpic_func_descriptor { | |||
47 | #define UNWINDGUARD 64 | 47 | #define UNWINDGUARD 64 |
48 | 48 | ||
49 | /* | 49 | /* |
50 | * Atomically swap in the new signal mask, and wait for a signal. | ||
51 | */ | ||
52 | asmlinkage int | ||
53 | sys_sigsuspend(old_sigset_t mask) | ||
54 | { | ||
55 | sigset_t blocked; | ||
56 | siginitset(&blocked, mask); | ||
57 | return sigsuspend(&blocked); | ||
58 | } | ||
59 | |||
60 | asmlinkage int | ||
61 | sys_sigaction(int sig, const struct old_sigaction __user *act, | ||
62 | struct old_sigaction __user *oact) | ||
63 | { | ||
64 | struct k_sigaction new_ka, old_ka; | ||
65 | int ret; | ||
66 | |||
67 | if (act) { | ||
68 | old_sigset_t mask; | ||
69 | if (!access_ok(VERIFY_READ, act, sizeof(*act)) || | ||
70 | __get_user(new_ka.sa.sa_handler, &act->sa_handler) || | ||
71 | __get_user(new_ka.sa.sa_restorer, &act->sa_restorer) || | ||
72 | __get_user(new_ka.sa.sa_flags, &act->sa_flags) || | ||
73 | __get_user(mask, &act->sa_mask)) | ||
74 | return -EFAULT; | ||
75 | siginitset(&new_ka.sa.sa_mask, mask); | ||
76 | } | ||
77 | |||
78 | ret = do_sigaction(sig, act ? &new_ka : NULL, oact ? &old_ka : NULL); | ||
79 | |||
80 | if (!ret && oact) { | ||
81 | if (!access_ok(VERIFY_WRITE, oact, sizeof(*oact)) || | ||
82 | __put_user(old_ka.sa.sa_handler, &oact->sa_handler) || | ||
83 | __put_user(old_ka.sa.sa_restorer, &oact->sa_restorer) || | ||
84 | __put_user(old_ka.sa.sa_flags, &oact->sa_flags) || | ||
85 | __put_user(old_ka.sa.sa_mask.sig[0], &oact->sa_mask)) | ||
86 | return -EFAULT; | ||
87 | } | ||
88 | |||
89 | return ret; | ||
90 | } | ||
91 | |||
92 | asmlinkage int | ||
93 | sys_sigaltstack(const stack_t __user *uss, stack_t __user *uoss, | ||
94 | unsigned long r6, unsigned long r7, | ||
95 | struct pt_regs __regs) | ||
96 | { | ||
97 | struct pt_regs *regs = RELOC_HIDE(&__regs, 0); | ||
98 | |||
99 | return do_sigaltstack(uss, uoss, regs->regs[15]); | ||
100 | } | ||
101 | |||
102 | |||
103 | /* | ||
104 | * Do a signal return; undo the signal stack. | 50 | * Do a signal return; undo the signal stack. |
105 | */ | 51 | */ |
106 | 52 | ||
@@ -257,8 +203,7 @@ asmlinkage int sys_rt_sigreturn(unsigned long r4, unsigned long r5, | |||
257 | if (restore_sigcontext(regs, &frame->uc.uc_mcontext, &r0)) | 203 | if (restore_sigcontext(regs, &frame->uc.uc_mcontext, &r0)) |
258 | goto badframe; | 204 | goto badframe; |
259 | 205 | ||
260 | if (do_sigaltstack(&frame->uc.uc_stack, NULL, | 206 | if (restore_altstack(&frame->uc.uc_stack)) |
261 | regs->regs[15]) == -EFAULT) | ||
262 | goto badframe; | 207 | goto badframe; |
263 | 208 | ||
264 | return r0; | 209 | return r0; |
@@ -423,11 +368,7 @@ static int setup_rt_frame(int sig, struct k_sigaction *ka, siginfo_t *info, | |||
423 | /* Create the ucontext. */ | 368 | /* Create the ucontext. */ |
424 | err |= __put_user(0, &frame->uc.uc_flags); | 369 | err |= __put_user(0, &frame->uc.uc_flags); |
425 | err |= __put_user(NULL, &frame->uc.uc_link); | 370 | err |= __put_user(NULL, &frame->uc.uc_link); |
426 | err |= __put_user((void *)current->sas_ss_sp, | 371 | err |= __save_altstack(&frame->uc.uc_stack, regs->regs[15]); |
427 | &frame->uc.uc_stack.ss_sp); | ||
428 | err |= __put_user(sas_ss_flags(regs->regs[15]), | ||
429 | &frame->uc.uc_stack.ss_flags); | ||
430 | err |= __put_user(current->sas_ss_size, &frame->uc.uc_stack.ss_size); | ||
431 | err |= setup_sigcontext(&frame->uc.uc_mcontext, | 372 | err |= setup_sigcontext(&frame->uc.uc_mcontext, |
432 | regs, set->sig[0]); | 373 | regs, set->sig[0]); |
433 | err |= __copy_to_user(&frame->uc.uc_sigmask, set, sizeof(*set)); | 374 | err |= __copy_to_user(&frame->uc.uc_sigmask, set, sizeof(*set)); |
diff --git a/arch/sh/kernel/signal_64.c b/arch/sh/kernel/signal_64.c index d867cd95a62..23d4c71c91a 100644 --- a/arch/sh/kernel/signal_64.c +++ b/arch/sh/kernel/signal_64.c | |||
@@ -128,58 +128,6 @@ static void do_signal(struct pt_regs *regs) | |||
128 | } | 128 | } |
129 | 129 | ||
130 | /* | 130 | /* |
131 | * Atomically swap in the new signal mask, and wait for a signal. | ||
132 | */ | ||
133 | asmlinkage int | ||
134 | sys_sigsuspend(old_sigset_t mask) | ||
135 | { | ||
136 | sigset_t blocked; | ||
137 | siginitset(&blocked, mask); | ||
138 | return sigsuspend(&blocked); | ||
139 | } | ||
140 | |||
141 | asmlinkage int | ||
142 | sys_sigaction(int sig, const struct old_sigaction __user *act, | ||
143 | struct old_sigaction __user *oact) | ||
144 | { | ||
145 | struct k_sigaction new_ka, old_ka; | ||
146 | int ret; | ||
147 | |||
148 | if (act) { | ||
149 | old_sigset_t mask; | ||
150 | if (!access_ok(VERIFY_READ, act, sizeof(*act)) || | ||
151 | __get_user(new_ka.sa.sa_handler, &act->sa_handler) || | ||
152 | __get_user(new_ka.sa.sa_restorer, &act->sa_restorer) || | ||
153 | __get_user(new_ka.sa.sa_flags, &act->sa_flags) || | ||
154 | __get_user(mask, &act->sa_mask)) | ||
155 | return -EFAULT; | ||
156 | siginitset(&new_ka.sa.sa_mask, mask); | ||
157 | } | ||
158 | |||
159 | ret = do_sigaction(sig, act ? &new_ka : NULL, oact ? &old_ka : NULL); | ||
160 | |||
161 | if (!ret && oact) { | ||
162 | if (!access_ok(VERIFY_WRITE, oact, sizeof(*oact)) || | ||
163 | __put_user(old_ka.sa.sa_handler, &oact->sa_handler) || | ||
164 | __put_user(old_ka.sa.sa_restorer, &oact->sa_restorer) || | ||
165 | __put_user(old_ka.sa.sa_flags, &oact->sa_flags) || | ||
166 | __put_user(old_ka.sa.sa_mask.sig[0], &oact->sa_mask)) | ||
167 | return -EFAULT; | ||
168 | } | ||
169 | |||
170 | return ret; | ||
171 | } | ||
172 | |||
173 | asmlinkage int | ||
174 | sys_sigaltstack(const stack_t __user *uss, stack_t __user *uoss, | ||
175 | unsigned long r4, unsigned long r5, unsigned long r6, | ||
176 | unsigned long r7, | ||
177 | struct pt_regs * regs) | ||
178 | { | ||
179 | return do_sigaltstack(uss, uoss, REF_REG_SP); | ||
180 | } | ||
181 | |||
182 | /* | ||
183 | * Do a signal return; undo the signal stack. | 131 | * Do a signal return; undo the signal stack. |
184 | */ | 132 | */ |
185 | struct sigframe { | 133 | struct sigframe { |
@@ -364,9 +312,7 @@ asmlinkage int sys_rt_sigreturn(unsigned long r2, unsigned long r3, | |||
364 | goto badframe; | 312 | goto badframe; |
365 | regs->pc -= 4; | 313 | regs->pc -= 4; |
366 | 314 | ||
367 | /* It is more difficult to avoid calling this function than to | 315 | if (restore_altstack(&frame->uc.uc_stack)) |
368 | call it and ignore errors. */ | ||
369 | if (do_sigaltstack(&frame->uc.uc_stack, NULL, REF_REG_SP) == -EFAULT) | ||
370 | goto badframe; | 316 | goto badframe; |
371 | 317 | ||
372 | return (int) ret; | 318 | return (int) ret; |
@@ -560,11 +506,7 @@ static int setup_rt_frame(int sig, struct k_sigaction *ka, siginfo_t *info, | |||
560 | /* Create the ucontext. */ | 506 | /* Create the ucontext. */ |
561 | err |= __put_user(0, &frame->uc.uc_flags); | 507 | err |= __put_user(0, &frame->uc.uc_flags); |
562 | err |= __put_user(0, &frame->uc.uc_link); | 508 | err |= __put_user(0, &frame->uc.uc_link); |
563 | err |= __put_user((void *)current->sas_ss_sp, | 509 | err |= __save_altstack(&frame->uc.uc_stack, regs->regs[REG_SP]); |
564 | &frame->uc.uc_stack.ss_sp); | ||
565 | err |= __put_user(sas_ss_flags(regs->regs[REG_SP]), | ||
566 | &frame->uc.uc_stack.ss_flags); | ||
567 | err |= __put_user(current->sas_ss_size, &frame->uc.uc_stack.ss_size); | ||
568 | err |= setup_sigcontext(&frame->uc.uc_mcontext, | 510 | err |= setup_sigcontext(&frame->uc.uc_mcontext, |
569 | regs, set->sig[0]); | 511 | regs, set->sig[0]); |
570 | err |= __copy_to_user(&frame->uc.uc_sigmask, set, sizeof(*set)); | 512 | err |= __copy_to_user(&frame->uc.uc_sigmask, set, sizeof(*set)); |