diff options
author | Petr Malat | 2013-02-27 19:01:52 -0600 |
---|---|---|
committer | David S. Miller | 2013-02-28 14:37:30 -0600 |
commit | b2a431915d19893f047e0dd149d0c1b9d2a0b960 (patch) | |
tree | e3e507b869479b8ba8b09667b159c3dbc606cf4c /drivers | |
parent | d521de04a73abb5e662c12eafa8c839aaaa6ae4f (diff) | |
download | am43-linux-kernel-b2a431915d19893f047e0dd149d0c1b9d2a0b960.tar.gz am43-linux-kernel-b2a431915d19893f047e0dd149d0c1b9d2a0b960.tar.xz am43-linux-kernel-b2a431915d19893f047e0dd149d0c1b9d2a0b960.zip |
phy: Fix phy_device_free memory leak
Fix memory leak in phy_device_free() for the case when phy_device*
returned by phy_device_create() is not registered in the system.
Bug description:
phy_device_create() sets name of kobject using dev_set_name(), which
allocates memory using kvasprintf(), but this memory isn't freed if
the underlying device isn't registered properly, because kobject_cleanup()
is not called in that case. This can happen (and actually is happening on
our machines) if phy_device_register(), called by mdiobus_scan(), fails.
Patch description:
Embedded struct device is initialized in phy_device_create() and it
counterpart phy_device_free() just drops one reference to the device,
which leads to proper deinitialization including releasing the kobject
name memory.
Signed-off-by: Petr Malat <oss@malat.biz>
Signed-off-by: David S. Miller <davem@davemloft.net>
Diffstat (limited to 'drivers')
-rw-r--r-- | drivers/net/phy/phy_device.c | 10 |
1 files changed, 6 insertions, 4 deletions
diff --git a/drivers/net/phy/phy_device.c b/drivers/net/phy/phy_device.c index 9930f999956..3657b4a2912 100644 --- a/drivers/net/phy/phy_device.c +++ b/drivers/net/phy/phy_device.c | |||
@@ -44,13 +44,13 @@ MODULE_LICENSE("GPL"); | |||
44 | 44 | ||
45 | void phy_device_free(struct phy_device *phydev) | 45 | void phy_device_free(struct phy_device *phydev) |
46 | { | 46 | { |
47 | kfree(phydev); | 47 | put_device(&phydev->dev); |
48 | } | 48 | } |
49 | EXPORT_SYMBOL(phy_device_free); | 49 | EXPORT_SYMBOL(phy_device_free); |
50 | 50 | ||
51 | static void phy_device_release(struct device *dev) | 51 | static void phy_device_release(struct device *dev) |
52 | { | 52 | { |
53 | phy_device_free(to_phy_device(dev)); | 53 | kfree(to_phy_device(dev)); |
54 | } | 54 | } |
55 | 55 | ||
56 | static struct phy_driver genphy_driver; | 56 | static struct phy_driver genphy_driver; |
@@ -201,6 +201,8 @@ struct phy_device *phy_device_create(struct mii_bus *bus, int addr, int phy_id, | |||
201 | there's no driver _already_ loaded. */ | 201 | there's no driver _already_ loaded. */ |
202 | request_module(MDIO_MODULE_PREFIX MDIO_ID_FMT, MDIO_ID_ARGS(phy_id)); | 202 | request_module(MDIO_MODULE_PREFIX MDIO_ID_FMT, MDIO_ID_ARGS(phy_id)); |
203 | 203 | ||
204 | device_initialize(&dev->dev); | ||
205 | |||
204 | return dev; | 206 | return dev; |
205 | } | 207 | } |
206 | EXPORT_SYMBOL(phy_device_create); | 208 | EXPORT_SYMBOL(phy_device_create); |
@@ -363,9 +365,9 @@ int phy_device_register(struct phy_device *phydev) | |||
363 | /* Run all of the fixups for this PHY */ | 365 | /* Run all of the fixups for this PHY */ |
364 | phy_scan_fixups(phydev); | 366 | phy_scan_fixups(phydev); |
365 | 367 | ||
366 | err = device_register(&phydev->dev); | 368 | err = device_add(&phydev->dev); |
367 | if (err) { | 369 | if (err) { |
368 | pr_err("phy %d failed to register\n", phydev->addr); | 370 | pr_err("PHY %d failed to add\n", phydev->addr); |
369 | goto out; | 371 | goto out; |
370 | } | 372 | } |
371 | 373 | ||