aboutsummaryrefslogtreecommitdiffstats
path: root/kernel
diff options
context:
space:
mode:
authorLinus Torvalds2013-03-03 15:23:02 -0600
committerLinus Torvalds2013-03-03 15:23:03 -0600
commit56a79b7b021bf1b08334e63c2c14b280e2dbf47a (patch)
tree0419233e6194f4f12073c9284852885aa8984bec /kernel
parent1c82315a12144cde732636e259d39e3ee81b3c5b (diff)
parentdcf787f39162ce32ca325b3e784aba2d2444619a (diff)
downloadam43-linux-kernel-56a79b7b021bf1b08334e63c2c14b280e2dbf47a.tar.gz
am43-linux-kernel-56a79b7b021bf1b08334e63c2c14b280e2dbf47a.tar.xz
am43-linux-kernel-56a79b7b021bf1b08334e63c2c14b280e2dbf47a.zip
Merge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/vfs
Pull more VFS bits from Al Viro: "Unfortunately, it looks like xattr series will have to wait until the next cycle ;-/ This pile contains 9p cleanups and fixes (races in v9fs_fid_add() etc), fixup for nommu breakage in shmem.c, several cleanups and a bit more file_inode() work" * 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/vfs: constify path_get/path_put and fs_struct.c stuff fix nommu breakage in shmem.c cache the value of file_inode() in struct file 9p: if v9fs_fid_lookup() gets to asking server, it'd better have hashed dentry 9p: make sure ->lookup() adds fid to the right dentry 9p: untangle ->lookup() a bit 9p: double iput() in ->lookup() if d_materialise_unique() fails 9p: v9fs_fid_add() can't fail now v9fs: get rid of v9fs_dentry 9p: turn fid->dlist into hlist 9p: don't bother with private lock in ->d_fsdata; dentry->d_lock will do just fine more file_inode() open-coded instances selinux: opened file can't have NULL or negative ->f_path.dentry (In the meantime, the hlist traversal macros have changed, so this required a semantic conflict fixup for the newly hlistified fid->dlist)
Diffstat (limited to 'kernel')
-rw-r--r--kernel/futex.c2
1 files changed, 1 insertions, 1 deletions
diff --git a/kernel/futex.c b/kernel/futex.c
index fbc07a29ec5..f0090a993da 100644
--- a/kernel/futex.c
+++ b/kernel/futex.c
@@ -226,7 +226,7 @@ static void drop_futex_key_refs(union futex_key *key)
226 * Returns a negative error code or 0 226 * Returns a negative error code or 0
227 * The key words are stored in *key on success. 227 * The key words are stored in *key on success.
228 * 228 *
229 * For shared mappings, it's (page->index, vma->vm_file->f_path.dentry->d_inode, 229 * For shared mappings, it's (page->index, file_inode(vma->vm_file),
230 * offset_within_page). For private mappings, it's (uaddr, current->mm). 230 * offset_within_page). For private mappings, it's (uaddr, current->mm).
231 * We can usually work out the index without swapping in the page. 231 * We can usually work out the index without swapping in the page.
232 * 232 *