diff options
author | Tejun Heo | 2013-02-27 19:04:56 -0600 |
---|---|---|
committer | Linus Torvalds | 2013-02-27 21:10:19 -0600 |
commit | ee94d523bf92d3b8b2de166943d48ac7fd695e10 (patch) | |
tree | 841fc7212003a43da67a7da6eee05dbe7556b742 /kernel | |
parent | 0e9c3be20d88aa5ed13fde4ece50f45eb96824ad (diff) | |
download | am43-linux-kernel-ee94d523bf92d3b8b2de166943d48ac7fd695e10.tar.gz am43-linux-kernel-ee94d523bf92d3b8b2de166943d48ac7fd695e10.tar.xz am43-linux-kernel-ee94d523bf92d3b8b2de166943d48ac7fd695e10.zip |
posix-timers: convert to idr_alloc()
Convert to the much saner new idr interface.
Signed-off-by: Tejun Heo <tj@kernel.org>
Cc: Thomas Gleixner <tglx@linutronix.de>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Diffstat (limited to 'kernel')
-rw-r--r-- | kernel/posix-timers.c | 18 |
1 files changed, 8 insertions, 10 deletions
diff --git a/kernel/posix-timers.c b/kernel/posix-timers.c index 7edfe4b901e..6edbb2c55c2 100644 --- a/kernel/posix-timers.c +++ b/kernel/posix-timers.c | |||
@@ -552,24 +552,22 @@ SYSCALL_DEFINE3(timer_create, const clockid_t, which_clock, | |||
552 | return -EAGAIN; | 552 | return -EAGAIN; |
553 | 553 | ||
554 | spin_lock_init(&new_timer->it_lock); | 554 | spin_lock_init(&new_timer->it_lock); |
555 | retry: | 555 | |
556 | if (unlikely(!idr_pre_get(&posix_timers_id, GFP_KERNEL))) { | 556 | idr_preload(GFP_KERNEL); |
557 | error = -EAGAIN; | ||
558 | goto out; | ||
559 | } | ||
560 | spin_lock_irq(&idr_lock); | 557 | spin_lock_irq(&idr_lock); |
561 | error = idr_get_new(&posix_timers_id, new_timer, &new_timer_id); | 558 | error = idr_alloc(&posix_timers_id, new_timer, 0, 0, GFP_NOWAIT); |
562 | spin_unlock_irq(&idr_lock); | 559 | spin_unlock_irq(&idr_lock); |
563 | if (error) { | 560 | idr_preload_end(); |
564 | if (error == -EAGAIN) | 561 | if (error < 0) { |
565 | goto retry; | ||
566 | /* | 562 | /* |
567 | * Weird looking, but we return EAGAIN if the IDR is | 563 | * Weird looking, but we return EAGAIN if the IDR is |
568 | * full (proper POSIX return value for this) | 564 | * full (proper POSIX return value for this) |
569 | */ | 565 | */ |
570 | error = -EAGAIN; | 566 | if (error == -ENOSPC) |
567 | error = -EAGAIN; | ||
571 | goto out; | 568 | goto out; |
572 | } | 569 | } |
570 | new_timer_id = error; | ||
573 | 571 | ||
574 | it_id_set = IT_ID_SET; | 572 | it_id_set = IT_ID_SET; |
575 | new_timer->it_id = (timer_t) new_timer_id; | 573 | new_timer->it_id = (timer_t) new_timer_id; |