diff options
author | Yinghai Lu | 2013-01-24 14:20:16 -0600 |
---|---|---|
committer | H. Peter Anvin | 2013-01-29 21:36:53 -0600 |
commit | ac2cbab21f318e19bc176a7f38a120cec835220f (patch) | |
tree | 1348f7e5a7e50b85bf56a9e1155bed70be13cd51 /lib | |
parent | 38fa4175e60d98fb1c9815fb14f8057576dade73 (diff) | |
download | am43-linux-kernel-ac2cbab21f318e19bc176a7f38a120cec835220f.tar.gz am43-linux-kernel-ac2cbab21f318e19bc176a7f38a120cec835220f.tar.xz am43-linux-kernel-ac2cbab21f318e19bc176a7f38a120cec835220f.zip |
x86: Don't panic if can not alloc buffer for swiotlb
Normal boot path on system with iommu support:
swiotlb buffer will be allocated early at first and then try to initialize
iommu, if iommu for intel or AMD could setup properly, swiotlb buffer
will be freed.
The early allocating is with bootmem, and could panic when we try to use
kdump with buffer above 4G only, or with memmap to limit mem under 4G.
for example: memmap=4095M$1M to remove memory under 4G.
According to Eric, add _nopanic version and no_iotlb_memory to fail
map single later if swiotlb is still needed.
-v2: don't pass nopanic, and use -ENOMEM return value according to Eric.
panic early instead of using swiotlb_full to panic...according to Eric/Konrad.
-v3: make swiotlb_init to be notpanic, but will affect:
arm64, ia64, powerpc, tile, unicore32, x86.
-v4: cleanup swiotlb_init by removing swiotlb_init_with_default_size.
Suggested-by: Eric W. Biederman <ebiederm@xmission.com>
Signed-off-by: Yinghai Lu <yinghai@kernel.org>
Link: http://lkml.kernel.org/r/1359058816-7615-36-git-send-email-yinghai@kernel.org
Reviewed-and-tested-by: Konrad Rzeszutek Wilk <konrad.wilk@oracle.com>
Cc: Joerg Roedel <joro@8bytes.org>
Cc: Ralf Baechle <ralf@linux-mips.org>
Cc: Jeremy Fitzhardinge <jeremy@goop.org>
Cc: Kyungmin Park <kyungmin.park@samsung.com>
Cc: Marek Szyprowski <m.szyprowski@samsung.com>
Cc: Arnd Bergmann <arnd@arndb.de>
Cc: Andrzej Pietrasiewicz <andrzej.p@samsung.com>
Cc: linux-mips@linux-mips.org
Cc: xen-devel@lists.xensource.com
Cc: virtualization@lists.linux-foundation.org
Cc: Shuah Khan <shuahkhan@gmail.com>
Signed-off-by: H. Peter Anvin <hpa@linux.intel.com>
Diffstat (limited to 'lib')
-rw-r--r-- | lib/swiotlb.c | 47 |
1 files changed, 29 insertions, 18 deletions
diff --git a/lib/swiotlb.c b/lib/swiotlb.c index 196b06984de..bfe02b8fc55 100644 --- a/lib/swiotlb.c +++ b/lib/swiotlb.c | |||
@@ -122,11 +122,18 @@ static dma_addr_t swiotlb_virt_to_bus(struct device *hwdev, | |||
122 | return phys_to_dma(hwdev, virt_to_phys(address)); | 122 | return phys_to_dma(hwdev, virt_to_phys(address)); |
123 | } | 123 | } |
124 | 124 | ||
125 | static bool no_iotlb_memory; | ||
126 | |||
125 | void swiotlb_print_info(void) | 127 | void swiotlb_print_info(void) |
126 | { | 128 | { |
127 | unsigned long bytes = io_tlb_nslabs << IO_TLB_SHIFT; | 129 | unsigned long bytes = io_tlb_nslabs << IO_TLB_SHIFT; |
128 | unsigned char *vstart, *vend; | 130 | unsigned char *vstart, *vend; |
129 | 131 | ||
132 | if (no_iotlb_memory) { | ||
133 | pr_warn("software IO TLB: No low mem\n"); | ||
134 | return; | ||
135 | } | ||
136 | |||
130 | vstart = phys_to_virt(io_tlb_start); | 137 | vstart = phys_to_virt(io_tlb_start); |
131 | vend = phys_to_virt(io_tlb_end); | 138 | vend = phys_to_virt(io_tlb_end); |
132 | 139 | ||
@@ -136,7 +143,7 @@ void swiotlb_print_info(void) | |||
136 | bytes >> 20, vstart, vend - 1); | 143 | bytes >> 20, vstart, vend - 1); |
137 | } | 144 | } |
138 | 145 | ||
139 | void __init swiotlb_init_with_tbl(char *tlb, unsigned long nslabs, int verbose) | 146 | int __init swiotlb_init_with_tbl(char *tlb, unsigned long nslabs, int verbose) |
140 | { | 147 | { |
141 | void *v_overflow_buffer; | 148 | void *v_overflow_buffer; |
142 | unsigned long i, bytes; | 149 | unsigned long i, bytes; |
@@ -150,9 +157,10 @@ void __init swiotlb_init_with_tbl(char *tlb, unsigned long nslabs, int verbose) | |||
150 | /* | 157 | /* |
151 | * Get the overflow emergency buffer | 158 | * Get the overflow emergency buffer |
152 | */ | 159 | */ |
153 | v_overflow_buffer = alloc_bootmem_low_pages(PAGE_ALIGN(io_tlb_overflow)); | 160 | v_overflow_buffer = alloc_bootmem_low_pages_nopanic( |
161 | PAGE_ALIGN(io_tlb_overflow)); | ||
154 | if (!v_overflow_buffer) | 162 | if (!v_overflow_buffer) |
155 | panic("Cannot allocate SWIOTLB overflow buffer!\n"); | 163 | return -ENOMEM; |
156 | 164 | ||
157 | io_tlb_overflow_buffer = __pa(v_overflow_buffer); | 165 | io_tlb_overflow_buffer = __pa(v_overflow_buffer); |
158 | 166 | ||
@@ -169,15 +177,19 @@ void __init swiotlb_init_with_tbl(char *tlb, unsigned long nslabs, int verbose) | |||
169 | 177 | ||
170 | if (verbose) | 178 | if (verbose) |
171 | swiotlb_print_info(); | 179 | swiotlb_print_info(); |
180 | |||
181 | return 0; | ||
172 | } | 182 | } |
173 | 183 | ||
174 | /* | 184 | /* |
175 | * Statically reserve bounce buffer space and initialize bounce buffer data | 185 | * Statically reserve bounce buffer space and initialize bounce buffer data |
176 | * structures for the software IO TLB used to implement the DMA API. | 186 | * structures for the software IO TLB used to implement the DMA API. |
177 | */ | 187 | */ |
178 | static void __init | 188 | void __init |
179 | swiotlb_init_with_default_size(size_t default_size, int verbose) | 189 | swiotlb_init(int verbose) |
180 | { | 190 | { |
191 | /* default to 64MB */ | ||
192 | size_t default_size = 64UL<<20; | ||
181 | unsigned char *vstart; | 193 | unsigned char *vstart; |
182 | unsigned long bytes; | 194 | unsigned long bytes; |
183 | 195 | ||
@@ -188,20 +200,16 @@ swiotlb_init_with_default_size(size_t default_size, int verbose) | |||
188 | 200 | ||
189 | bytes = io_tlb_nslabs << IO_TLB_SHIFT; | 201 | bytes = io_tlb_nslabs << IO_TLB_SHIFT; |
190 | 202 | ||
191 | /* | 203 | /* Get IO TLB memory from the low pages */ |
192 | * Get IO TLB memory from the low pages | 204 | vstart = alloc_bootmem_low_pages_nopanic(PAGE_ALIGN(bytes)); |
193 | */ | 205 | if (vstart && !swiotlb_init_with_tbl(vstart, io_tlb_nslabs, verbose)) |
194 | vstart = alloc_bootmem_low_pages(PAGE_ALIGN(bytes)); | 206 | return; |
195 | if (!vstart) | ||
196 | panic("Cannot allocate SWIOTLB buffer"); | ||
197 | |||
198 | swiotlb_init_with_tbl(vstart, io_tlb_nslabs, verbose); | ||
199 | } | ||
200 | 207 | ||
201 | void __init | 208 | if (io_tlb_start) |
202 | swiotlb_init(int verbose) | 209 | free_bootmem(io_tlb_start, |
203 | { | 210 | PAGE_ALIGN(io_tlb_nslabs << IO_TLB_SHIFT)); |
204 | swiotlb_init_with_default_size(64 * (1<<20), verbose); /* default to 64MB */ | 211 | pr_warn("Cannot allocate SWIOTLB buffer"); |
212 | no_iotlb_memory = true; | ||
205 | } | 213 | } |
206 | 214 | ||
207 | /* | 215 | /* |
@@ -405,6 +413,9 @@ phys_addr_t swiotlb_tbl_map_single(struct device *hwdev, | |||
405 | unsigned long offset_slots; | 413 | unsigned long offset_slots; |
406 | unsigned long max_slots; | 414 | unsigned long max_slots; |
407 | 415 | ||
416 | if (no_iotlb_memory) | ||
417 | panic("Can not allocate SWIOTLB buffer earlier and can't now provide you with the DMA bounce buffer"); | ||
418 | |||
408 | mask = dma_get_seg_boundary(hwdev); | 419 | mask = dma_get_seg_boundary(hwdev); |
409 | 420 | ||
410 | tbl_dma_addr &= mask; | 421 | tbl_dma_addr &= mask; |