diff options
author | Hugh Dickins | 2013-02-22 18:36:03 -0600 |
---|---|---|
committer | Linus Torvalds | 2013-02-23 19:50:23 -0600 |
commit | 8fdb3dbf02335d96bf170321381522709ba63a0c (patch) | |
tree | 5c81a212ef5960298ec4d284640c38f707f5dad6 /mm | |
parent | 49cd0a5c290f99deca3463d16c3c1c7240107889 (diff) | |
download | am43-linux-kernel-8fdb3dbf02335d96bf170321381522709ba63a0c.tar.gz am43-linux-kernel-8fdb3dbf02335d96bf170321381522709ba63a0c.tar.xz am43-linux-kernel-8fdb3dbf02335d96bf170321381522709ba63a0c.zip |
ksm: add some comments
Added slightly more detail to the Documentation of merge_across_nodes, a
few comments in areas indicated by review, and renamed get_ksm_page()'s
argument from "locked" to "lock_it". No functional change.
Signed-off-by: Hugh Dickins <hughd@google.com>
Cc: Mel Gorman <mgorman@suse.de>
Cc: Petr Holasek <pholasek@redhat.com>
Cc: Andrea Arcangeli <aarcange@redhat.com>
Cc: Izik Eidus <izik.eidus@ravellosystems.com>
Cc: Johannes Weiner <hannes@cmpxchg.org>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Diffstat (limited to 'mm')
-rw-r--r-- | mm/ksm.c | 18 |
1 files changed, 14 insertions, 4 deletions
@@ -87,6 +87,9 @@ | |||
87 | * take 10 attempts to find a page in the unstable tree, once it is found, | 87 | * take 10 attempts to find a page in the unstable tree, once it is found, |
88 | * it is secured in the stable tree. (When we scan a new page, we first | 88 | * it is secured in the stable tree. (When we scan a new page, we first |
89 | * compare it against the stable tree, and then against the unstable tree.) | 89 | * compare it against the stable tree, and then against the unstable tree.) |
90 | * | ||
91 | * If the merge_across_nodes tunable is unset, then KSM maintains multiple | ||
92 | * stable trees and multiple unstable trees: one of each for each NUMA node. | ||
90 | */ | 93 | */ |
91 | 94 | ||
92 | /** | 95 | /** |
@@ -526,7 +529,7 @@ static void remove_node_from_stable_tree(struct stable_node *stable_node) | |||
526 | * a page to put something that might look like our key in page->mapping. | 529 | * a page to put something that might look like our key in page->mapping. |
527 | * is on its way to being freed; but it is an anomaly to bear in mind. | 530 | * is on its way to being freed; but it is an anomaly to bear in mind. |
528 | */ | 531 | */ |
529 | static struct page *get_ksm_page(struct stable_node *stable_node, bool locked) | 532 | static struct page *get_ksm_page(struct stable_node *stable_node, bool lock_it) |
530 | { | 533 | { |
531 | struct page *page; | 534 | struct page *page; |
532 | void *expected_mapping; | 535 | void *expected_mapping; |
@@ -575,7 +578,7 @@ again: | |||
575 | goto stale; | 578 | goto stale; |
576 | } | 579 | } |
577 | 580 | ||
578 | if (locked) { | 581 | if (lock_it) { |
579 | lock_page(page); | 582 | lock_page(page); |
580 | if (ACCESS_ONCE(page->mapping) != expected_mapping) { | 583 | if (ACCESS_ONCE(page->mapping) != expected_mapping) { |
581 | unlock_page(page); | 584 | unlock_page(page); |
@@ -705,10 +708,17 @@ static int remove_stable_node(struct stable_node *stable_node) | |||
705 | return 0; | 708 | return 0; |
706 | } | 709 | } |
707 | 710 | ||
708 | if (WARN_ON_ONCE(page_mapped(page))) | 711 | if (WARN_ON_ONCE(page_mapped(page))) { |
712 | /* | ||
713 | * This should not happen: but if it does, just refuse to let | ||
714 | * merge_across_nodes be switched - there is no need to panic. | ||
715 | */ | ||
709 | err = -EBUSY; | 716 | err = -EBUSY; |
710 | else { | 717 | } else { |
711 | /* | 718 | /* |
719 | * The stable node did not yet appear stale to get_ksm_page(), | ||
720 | * since that allows for an unmapped ksm page to be recognized | ||
721 | * right up until it is freed; but the node is safe to remove. | ||
712 | * This page might be in a pagevec waiting to be freed, | 722 | * This page might be in a pagevec waiting to be freed, |
713 | * or it might be PageSwapCache (perhaps under writeback), | 723 | * or it might be PageSwapCache (perhaps under writeback), |
714 | * or it might have been removed from swapcache a moment ago. | 724 | * or it might have been removed from swapcache a moment ago. |