diff options
author | Serge E. Hallyn | 2011-03-23 18:43:20 -0500 |
---|---|---|
committer | Linus Torvalds | 2011-03-23 21:47:05 -0500 |
commit | 8409cca7056113bee3236cb6a8e4d8d4d1eef102 (patch) | |
tree | d9f1ced0d47070fcdf8b399021f33770c150b1ec /security/commoncap.c | |
parent | 39fd33933b0209e4b6254743f2cede07c5ad4c52 (diff) | |
download | am43-linux-kernel-8409cca7056113bee3236cb6a8e4d8d4d1eef102.tar.gz am43-linux-kernel-8409cca7056113bee3236cb6a8e4d8d4d1eef102.tar.xz am43-linux-kernel-8409cca7056113bee3236cb6a8e4d8d4d1eef102.zip |
userns: allow ptrace from non-init user namespaces
ptrace is allowed to tasks in the same user namespace according to the
usual rules (i.e. the same rules as for two tasks in the init user
namespace). ptrace is also allowed to a user namespace to which the
current task the has CAP_SYS_PTRACE capability.
Changelog:
Dec 31: Address feedback by Eric:
. Correct ptrace uid check
. Rename may_ptrace_ns to ptrace_capable
. Also fix the cap_ptrace checks.
Jan 1: Use const cred struct
Jan 11: use task_ns_capable() in place of ptrace_capable().
Feb 23: same_or_ancestore_user_ns() was not an appropriate
check to constrain cap_issubset. Rather, cap_issubset()
only is meaningful when both capsets are in the same
user_ns.
Signed-off-by: Serge E. Hallyn <serge.hallyn@canonical.com>
Cc: "Eric W. Biederman" <ebiederm@xmission.com>
Acked-by: Daniel Lezcano <daniel.lezcano@free.fr>
Acked-by: David Howells <dhowells@redhat.com>
Cc: James Morris <jmorris@namei.org>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Diffstat (limited to 'security/commoncap.c')
-rw-r--r-- | security/commoncap.c | 40 |
1 files changed, 32 insertions, 8 deletions
diff --git a/security/commoncap.c b/security/commoncap.c index 43a205bc7d7..f20e984ccfb 100644 --- a/security/commoncap.c +++ b/security/commoncap.c | |||
@@ -127,18 +127,30 @@ int cap_settime(const struct timespec *ts, const struct timezone *tz) | |||
127 | * @child: The process to be accessed | 127 | * @child: The process to be accessed |
128 | * @mode: The mode of attachment. | 128 | * @mode: The mode of attachment. |
129 | * | 129 | * |
130 | * If we are in the same or an ancestor user_ns and have all the target | ||
131 | * task's capabilities, then ptrace access is allowed. | ||
132 | * If we have the ptrace capability to the target user_ns, then ptrace | ||
133 | * access is allowed. | ||
134 | * Else denied. | ||
135 | * | ||
130 | * Determine whether a process may access another, returning 0 if permission | 136 | * Determine whether a process may access another, returning 0 if permission |
131 | * granted, -ve if denied. | 137 | * granted, -ve if denied. |
132 | */ | 138 | */ |
133 | int cap_ptrace_access_check(struct task_struct *child, unsigned int mode) | 139 | int cap_ptrace_access_check(struct task_struct *child, unsigned int mode) |
134 | { | 140 | { |
135 | int ret = 0; | 141 | int ret = 0; |
142 | const struct cred *cred, *child_cred; | ||
136 | 143 | ||
137 | rcu_read_lock(); | 144 | rcu_read_lock(); |
138 | if (!cap_issubset(__task_cred(child)->cap_permitted, | 145 | cred = current_cred(); |
139 | current_cred()->cap_permitted) && | 146 | child_cred = __task_cred(child); |
140 | !capable(CAP_SYS_PTRACE)) | 147 | if (cred->user->user_ns == child_cred->user->user_ns && |
141 | ret = -EPERM; | 148 | cap_issubset(child_cred->cap_permitted, cred->cap_permitted)) |
149 | goto out; | ||
150 | if (ns_capable(child_cred->user->user_ns, CAP_SYS_PTRACE)) | ||
151 | goto out; | ||
152 | ret = -EPERM; | ||
153 | out: | ||
142 | rcu_read_unlock(); | 154 | rcu_read_unlock(); |
143 | return ret; | 155 | return ret; |
144 | } | 156 | } |
@@ -147,18 +159,30 @@ int cap_ptrace_access_check(struct task_struct *child, unsigned int mode) | |||
147 | * cap_ptrace_traceme - Determine whether another process may trace the current | 159 | * cap_ptrace_traceme - Determine whether another process may trace the current |
148 | * @parent: The task proposed to be the tracer | 160 | * @parent: The task proposed to be the tracer |
149 | * | 161 | * |
162 | * If parent is in the same or an ancestor user_ns and has all current's | ||
163 | * capabilities, then ptrace access is allowed. | ||
164 | * If parent has the ptrace capability to current's user_ns, then ptrace | ||
165 | * access is allowed. | ||
166 | * Else denied. | ||
167 | * | ||
150 | * Determine whether the nominated task is permitted to trace the current | 168 | * Determine whether the nominated task is permitted to trace the current |
151 | * process, returning 0 if permission is granted, -ve if denied. | 169 | * process, returning 0 if permission is granted, -ve if denied. |
152 | */ | 170 | */ |
153 | int cap_ptrace_traceme(struct task_struct *parent) | 171 | int cap_ptrace_traceme(struct task_struct *parent) |
154 | { | 172 | { |
155 | int ret = 0; | 173 | int ret = 0; |
174 | const struct cred *cred, *child_cred; | ||
156 | 175 | ||
157 | rcu_read_lock(); | 176 | rcu_read_lock(); |
158 | if (!cap_issubset(current_cred()->cap_permitted, | 177 | cred = __task_cred(parent); |
159 | __task_cred(parent)->cap_permitted) && | 178 | child_cred = current_cred(); |
160 | !has_capability(parent, CAP_SYS_PTRACE)) | 179 | if (cred->user->user_ns == child_cred->user->user_ns && |
161 | ret = -EPERM; | 180 | cap_issubset(child_cred->cap_permitted, cred->cap_permitted)) |
181 | goto out; | ||
182 | if (has_ns_capability(parent, child_cred->user->user_ns, CAP_SYS_PTRACE)) | ||
183 | goto out; | ||
184 | ret = -EPERM; | ||
185 | out: | ||
162 | rcu_read_unlock(); | 186 | rcu_read_unlock(); |
163 | return ret; | 187 | return ret; |
164 | } | 188 | } |