diff options
author | Linus Torvalds | 2012-01-14 20:36:33 -0600 |
---|---|---|
committer | Linus Torvalds | 2012-01-14 20:36:33 -0600 |
commit | c49c41a4134679cecb77362e7f6b59acb6320aa7 (patch) | |
tree | 45e690c036ca5846a48c8be67945d1d841b2d96d /security/commoncap.c | |
parent | 892d208bcf79e4e1058707786a7b6d486697cd78 (diff) | |
parent | f423e5ba76e7e4a6fcb4836b4f072d1fdebba8b5 (diff) | |
download | am43-linux-kernel-c49c41a4134679cecb77362e7f6b59acb6320aa7.tar.gz am43-linux-kernel-c49c41a4134679cecb77362e7f6b59acb6320aa7.tar.xz am43-linux-kernel-c49c41a4134679cecb77362e7f6b59acb6320aa7.zip |
Merge branch 'for-linus' of git://selinuxproject.org/~jmorris/linux-security
* 'for-linus' of git://selinuxproject.org/~jmorris/linux-security:
capabilities: remove __cap_full_set definition
security: remove the security_netlink_recv hook as it is equivalent to capable()
ptrace: do not audit capability check when outputing /proc/pid/stat
capabilities: remove task_ns_* functions
capabitlies: ns_capable can use the cap helpers rather than lsm call
capabilities: style only - move capable below ns_capable
capabilites: introduce new has_ns_capabilities_noaudit
capabilities: call has_ns_capability from has_capability
capabilities: remove all _real_ interfaces
capabilities: introduce security_capable_noaudit
capabilities: reverse arguments to security_capable
capabilities: remove the task from capable LSM hook entirely
selinux: sparse fix: fix several warnings in the security server cod
selinux: sparse fix: fix warnings in netlink code
selinux: sparse fix: eliminate warnings for selinuxfs
selinux: sparse fix: declare selinux_disable() in security.h
selinux: sparse fix: move selinux_complete_init
selinux: sparse fix: make selinux_secmark_refcount static
SELinux: Fix RCU deref check warning in sel_netport_insert()
Manually fix up a semantic mis-merge wrt security_netlink_recv():
- the interface was removed in commit fd7784615248 ("security: remove
the security_netlink_recv hook as it is equivalent to capable()")
- a new user of it appeared in commit a38f7907b926 ("crypto: Add
userspace configuration API")
causing no automatic merge conflict, but Eric Paris pointed out the
issue.
Diffstat (limited to 'security/commoncap.c')
-rw-r--r-- | security/commoncap.c | 24 |
1 files changed, 7 insertions, 17 deletions
diff --git a/security/commoncap.c b/security/commoncap.c index ee4f8486e5f..7ce191ea29a 100644 --- a/security/commoncap.c +++ b/security/commoncap.c | |||
@@ -56,17 +56,8 @@ int cap_netlink_send(struct sock *sk, struct sk_buff *skb) | |||
56 | return 0; | 56 | return 0; |
57 | } | 57 | } |
58 | 58 | ||
59 | int cap_netlink_recv(struct sk_buff *skb, int cap) | ||
60 | { | ||
61 | if (!cap_raised(current_cap(), cap)) | ||
62 | return -EPERM; | ||
63 | return 0; | ||
64 | } | ||
65 | EXPORT_SYMBOL(cap_netlink_recv); | ||
66 | |||
67 | /** | 59 | /** |
68 | * cap_capable - Determine whether a task has a particular effective capability | 60 | * cap_capable - Determine whether a task has a particular effective capability |
69 | * @tsk: The task to query | ||
70 | * @cred: The credentials to use | 61 | * @cred: The credentials to use |
71 | * @ns: The user namespace in which we need the capability | 62 | * @ns: The user namespace in which we need the capability |
72 | * @cap: The capability to check for | 63 | * @cap: The capability to check for |
@@ -80,8 +71,8 @@ EXPORT_SYMBOL(cap_netlink_recv); | |||
80 | * cap_has_capability() returns 0 when a task has a capability, but the | 71 | * cap_has_capability() returns 0 when a task has a capability, but the |
81 | * kernel's capable() and has_capability() returns 1 for this case. | 72 | * kernel's capable() and has_capability() returns 1 for this case. |
82 | */ | 73 | */ |
83 | int cap_capable(struct task_struct *tsk, const struct cred *cred, | 74 | int cap_capable(const struct cred *cred, struct user_namespace *targ_ns, |
84 | struct user_namespace *targ_ns, int cap, int audit) | 75 | int cap, int audit) |
85 | { | 76 | { |
86 | for (;;) { | 77 | for (;;) { |
87 | /* The creator of the user namespace has all caps. */ | 78 | /* The creator of the user namespace has all caps. */ |
@@ -222,9 +213,8 @@ static inline int cap_inh_is_capped(void) | |||
222 | /* they are so limited unless the current task has the CAP_SETPCAP | 213 | /* they are so limited unless the current task has the CAP_SETPCAP |
223 | * capability | 214 | * capability |
224 | */ | 215 | */ |
225 | if (cap_capable(current, current_cred(), | 216 | if (cap_capable(current_cred(), current_cred()->user->user_ns, |
226 | current_cred()->user->user_ns, CAP_SETPCAP, | 217 | CAP_SETPCAP, SECURITY_CAP_AUDIT) == 0) |
227 | SECURITY_CAP_AUDIT) == 0) | ||
228 | return 0; | 218 | return 0; |
229 | return 1; | 219 | return 1; |
230 | } | 220 | } |
@@ -874,7 +864,7 @@ int cap_task_prctl(int option, unsigned long arg2, unsigned long arg3, | |||
874 | & (new->securebits ^ arg2)) /*[1]*/ | 864 | & (new->securebits ^ arg2)) /*[1]*/ |
875 | || ((new->securebits & SECURE_ALL_LOCKS & ~arg2)) /*[2]*/ | 865 | || ((new->securebits & SECURE_ALL_LOCKS & ~arg2)) /*[2]*/ |
876 | || (arg2 & ~(SECURE_ALL_LOCKS | SECURE_ALL_BITS)) /*[3]*/ | 866 | || (arg2 & ~(SECURE_ALL_LOCKS | SECURE_ALL_BITS)) /*[3]*/ |
877 | || (cap_capable(current, current_cred(), | 867 | || (cap_capable(current_cred(), |
878 | current_cred()->user->user_ns, CAP_SETPCAP, | 868 | current_cred()->user->user_ns, CAP_SETPCAP, |
879 | SECURITY_CAP_AUDIT) != 0) /*[4]*/ | 869 | SECURITY_CAP_AUDIT) != 0) /*[4]*/ |
880 | /* | 870 | /* |
@@ -940,7 +930,7 @@ int cap_vm_enough_memory(struct mm_struct *mm, long pages) | |||
940 | { | 930 | { |
941 | int cap_sys_admin = 0; | 931 | int cap_sys_admin = 0; |
942 | 932 | ||
943 | if (cap_capable(current, current_cred(), &init_user_ns, CAP_SYS_ADMIN, | 933 | if (cap_capable(current_cred(), &init_user_ns, CAP_SYS_ADMIN, |
944 | SECURITY_CAP_NOAUDIT) == 0) | 934 | SECURITY_CAP_NOAUDIT) == 0) |
945 | cap_sys_admin = 1; | 935 | cap_sys_admin = 1; |
946 | return __vm_enough_memory(mm, pages, cap_sys_admin); | 936 | return __vm_enough_memory(mm, pages, cap_sys_admin); |
@@ -967,7 +957,7 @@ int cap_file_mmap(struct file *file, unsigned long reqprot, | |||
967 | int ret = 0; | 957 | int ret = 0; |
968 | 958 | ||
969 | if (addr < dac_mmap_min_addr) { | 959 | if (addr < dac_mmap_min_addr) { |
970 | ret = cap_capable(current, current_cred(), &init_user_ns, CAP_SYS_RAWIO, | 960 | ret = cap_capable(current_cred(), &init_user_ns, CAP_SYS_RAWIO, |
971 | SECURITY_CAP_AUDIT); | 961 | SECURITY_CAP_AUDIT); |
972 | /* set PF_SUPERPRIV if it turns out we allow the low mmap */ | 962 | /* set PF_SUPERPRIV if it turns out we allow the low mmap */ |
973 | if (ret == 0) | 963 | if (ret == 0) |