aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorLinus Torvalds2012-10-02 13:11:09 -0500
committerLinus Torvalds2012-10-02 13:11:09 -0500
commit437589a74b6a590d175f86cf9f7b2efcee7765e7 (patch)
tree37bf8635b1356d80ef002b00e84f3faf3d555a63 /security/selinux
parent68d47a137c3bef754923bccf73fb639c9b0bbd5e (diff)
parent72235465864d84cedb2d9f26f8e1de824ee20339 (diff)
downloadam43-linux-kernel-437589a74b6a590d175f86cf9f7b2efcee7765e7.tar.gz
am43-linux-kernel-437589a74b6a590d175f86cf9f7b2efcee7765e7.tar.xz
am43-linux-kernel-437589a74b6a590d175f86cf9f7b2efcee7765e7.zip
Merge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/ebiederm/user-namespace
Pull user namespace changes from Eric Biederman: "This is a mostly modest set of changes to enable basic user namespace support. This allows the code to code to compile with user namespaces enabled and removes the assumption there is only the initial user namespace. Everything is converted except for the most complex of the filesystems: autofs4, 9p, afs, ceph, cifs, coda, fuse, gfs2, ncpfs, nfs, ocfs2 and xfs as those patches need a bit more review. The strategy is to push kuid_t and kgid_t values are far down into subsystems and filesystems as reasonable. Leaving the make_kuid and from_kuid operations to happen at the edge of userspace, as the values come off the disk, and as the values come in from the network. Letting compile type incompatible compile errors (present when user namespaces are enabled) guide me to find the issues. The most tricky areas have been the places where we had an implicit union of uid and gid values and were storing them in an unsigned int. Those places were converted into explicit unions. I made certain to handle those places with simple trivial patches. Out of that work I discovered we have generic interfaces for storing quota by projid. I had never heard of the project identifiers before. Adding full user namespace support for project identifiers accounts for most of the code size growth in my git tree. Ultimately there will be work to relax privlige checks from "capable(FOO)" to "ns_capable(user_ns, FOO)" where it is safe allowing root in a user names to do those things that today we only forbid to non-root users because it will confuse suid root applications. While I was pushing kuid_t and kgid_t changes deep into the audit code I made a few other cleanups. I capitalized on the fact we process netlink messages in the context of the message sender. I removed usage of NETLINK_CRED, and started directly using current->tty. Some of these patches have also made it into maintainer trees, with no problems from identical code from different trees showing up in linux-next. After reading through all of this code I feel like I might be able to win a game of kernel trivial pursuit." Fix up some fairly trivial conflicts in netfilter uid/git logging code. * 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/ebiederm/user-namespace: (107 commits) userns: Convert the ufs filesystem to use kuid/kgid where appropriate userns: Convert the udf filesystem to use kuid/kgid where appropriate userns: Convert ubifs to use kuid/kgid userns: Convert squashfs to use kuid/kgid where appropriate userns: Convert reiserfs to use kuid and kgid where appropriate userns: Convert jfs to use kuid/kgid where appropriate userns: Convert jffs2 to use kuid and kgid where appropriate userns: Convert hpfs to use kuid and kgid where appropriate userns: Convert btrfs to use kuid/kgid where appropriate userns: Convert bfs to use kuid/kgid where appropriate userns: Convert affs to use kuid/kgid wherwe appropriate userns: On alpha modify linux_to_osf_stat to use convert from kuids and kgids userns: On ia64 deal with current_uid and current_gid being kuid and kgid userns: On ppc convert current_uid from a kuid before printing. userns: Convert s390 getting uid and gid system calls to use kuid and kgid userns: Convert s390 hypfs to use kuid and kgid where appropriate userns: Convert binder ipc to use kuids userns: Teach security_path_chown to take kuids and kgids userns: Add user namespace support to IMA userns: Convert EVM to deal with kuids and kgids in it's hmac computation ...
Diffstat (limited to 'security/selinux')
-rw-r--r--security/selinux/selinuxfs.c6
-rw-r--r--security/selinux/ss/services.c2
2 files changed, 4 insertions, 4 deletions
diff --git a/security/selinux/selinuxfs.c b/security/selinux/selinuxfs.c
index 298e695d682..55af8c5b57e 100644
--- a/security/selinux/selinuxfs.c
+++ b/security/selinux/selinuxfs.c
@@ -174,7 +174,7 @@ static ssize_t sel_write_enforce(struct file *file, const char __user *buf,
174 audit_log(current->audit_context, GFP_KERNEL, AUDIT_MAC_STATUS, 174 audit_log(current->audit_context, GFP_KERNEL, AUDIT_MAC_STATUS,
175 "enforcing=%d old_enforcing=%d auid=%u ses=%u", 175 "enforcing=%d old_enforcing=%d auid=%u ses=%u",
176 new_value, selinux_enforcing, 176 new_value, selinux_enforcing,
177 audit_get_loginuid(current), 177 from_kuid(&init_user_ns, audit_get_loginuid(current)),
178 audit_get_sessionid(current)); 178 audit_get_sessionid(current));
179 selinux_enforcing = new_value; 179 selinux_enforcing = new_value;
180 if (selinux_enforcing) 180 if (selinux_enforcing)
@@ -305,7 +305,7 @@ static ssize_t sel_write_disable(struct file *file, const char __user *buf,
305 goto out; 305 goto out;
306 audit_log(current->audit_context, GFP_KERNEL, AUDIT_MAC_STATUS, 306 audit_log(current->audit_context, GFP_KERNEL, AUDIT_MAC_STATUS,
307 "selinux=0 auid=%u ses=%u", 307 "selinux=0 auid=%u ses=%u",
308 audit_get_loginuid(current), 308 from_kuid(&init_user_ns, audit_get_loginuid(current)),
309 audit_get_sessionid(current)); 309 audit_get_sessionid(current));
310 } 310 }
311 311
@@ -551,7 +551,7 @@ static ssize_t sel_write_load(struct file *file, const char __user *buf,
551out1: 551out1:
552 audit_log(current->audit_context, GFP_KERNEL, AUDIT_MAC_POLICY_LOAD, 552 audit_log(current->audit_context, GFP_KERNEL, AUDIT_MAC_POLICY_LOAD,
553 "policy loaded auid=%u ses=%u", 553 "policy loaded auid=%u ses=%u",
554 audit_get_loginuid(current), 554 from_kuid(&init_user_ns, audit_get_loginuid(current)),
555 audit_get_sessionid(current)); 555 audit_get_sessionid(current));
556out: 556out:
557 mutex_unlock(&sel_mutex); 557 mutex_unlock(&sel_mutex);
diff --git a/security/selinux/ss/services.c b/security/selinux/ss/services.c
index 4321b8fc886..b4feecc3fe0 100644
--- a/security/selinux/ss/services.c
+++ b/security/selinux/ss/services.c
@@ -2440,7 +2440,7 @@ int security_set_bools(int len, int *values)
2440 sym_name(&policydb, SYM_BOOLS, i), 2440 sym_name(&policydb, SYM_BOOLS, i),
2441 !!values[i], 2441 !!values[i],
2442 policydb.bool_val_to_struct[i]->state, 2442 policydb.bool_val_to_struct[i]->state,
2443 audit_get_loginuid(current), 2443 from_kuid(&init_user_ns, audit_get_loginuid(current)),
2444 audit_get_sessionid(current)); 2444 audit_get_sessionid(current));
2445 } 2445 }
2446 if (values[i]) 2446 if (values[i])