diff options
-rw-r--r-- | Documentation/keys-trusted-encrypted.txt | 145 | ||||
-rw-r--r-- | include/keys/trusted-type.h | 31 | ||||
-rw-r--r-- | include/linux/tpm_command.h | 28 | ||||
-rw-r--r-- | security/Kconfig | 15 | ||||
-rw-r--r-- | security/keys/Makefile | 1 | ||||
-rw-r--r-- | security/keys/trusted_defined.c | 1151 | ||||
-rw-r--r-- | security/keys/trusted_defined.h | 134 |
7 files changed, 1505 insertions, 0 deletions
diff --git a/Documentation/keys-trusted-encrypted.txt b/Documentation/keys-trusted-encrypted.txt new file mode 100644 index 00000000000..8fb79bc1ac4 --- /dev/null +++ b/Documentation/keys-trusted-encrypted.txt | |||
@@ -0,0 +1,145 @@ | |||
1 | Trusted and Encrypted Keys | ||
2 | |||
3 | Trusted and Encrypted Keys are two new key types added to the existing kernel | ||
4 | key ring service. Both of these new types are variable length symmetic keys, | ||
5 | and in both cases all keys are created in the kernel, and user space sees, | ||
6 | stores, and loads only encrypted blobs. Trusted Keys require the availability | ||
7 | of a Trusted Platform Module (TPM) chip for greater security, while Encrypted | ||
8 | Keys can be used on any system. All user level blobs, are displayed and loaded | ||
9 | in hex ascii for convenience, and are integrity verified. | ||
10 | |||
11 | Trusted Keys use a TPM both to generate and to seal the keys. Keys are sealed | ||
12 | under a 2048 bit RSA key in the TPM, and optionally sealed to specified PCR | ||
13 | (integrity measurement) values, and only unsealed by the TPM, if PCRs and blob | ||
14 | integrity verifications match. A loaded Trusted Key can be updated with new | ||
15 | (future) PCR values, so keys are easily migrated to new pcr values, such as | ||
16 | when the kernel and initramfs are updated. The same key can have many saved | ||
17 | blobs under different PCR values, so multiple boots are easily supported. | ||
18 | |||
19 | By default, trusted keys are sealed under the SRK, which has the default | ||
20 | authorization value (20 zeros). This can be set at takeownership time with the | ||
21 | trouser's utility: "tpm_takeownership -u -z". | ||
22 | |||
23 | Usage: | ||
24 | keyctl add trusted name "new keylen [options]" ring | ||
25 | keyctl add trusted name "load hex_blob [pcrlock=pcrnum]" ring | ||
26 | keyctl update key "update [options]" | ||
27 | keyctl print keyid | ||
28 | |||
29 | options: | ||
30 | keyhandle= ascii hex value of sealing key default 0x40000000 (SRK) | ||
31 | keyauth= ascii hex auth for sealing key default 0x00...i | ||
32 | (40 ascii zeros) | ||
33 | blobauth= ascii hex auth for sealed data default 0x00... | ||
34 | (40 ascii zeros) | ||
35 | blobauth= ascii hex auth for sealed data default 0x00... | ||
36 | (40 ascii zeros) | ||
37 | pcrinfo= ascii hex of PCR_INFO or PCR_INFO_LONG (no default) | ||
38 | pcrlock= pcr number to be extended to "lock" blob | ||
39 | migratable= 0|1 indicating permission to reseal to new PCR values, | ||
40 | default 1 (resealing allowed) | ||
41 | |||
42 | "keyctl print" returns an ascii hex copy of the sealed key, which is in standard | ||
43 | TPM_STORED_DATA format. The key length for new keys are always in bytes. | ||
44 | Trusted Keys can be 32 - 128 bytes (256 - 1024 bits), the upper limit is to fit | ||
45 | within the 2048 bit SRK (RSA) keylength, with all necessary structure/padding. | ||
46 | |||
47 | Encrypted keys do not depend on a TPM, and are faster, as they use AES for | ||
48 | encryption/decryption. New keys are created from kernel generated random | ||
49 | numbers, and are encrypted/decrypted using a specified 'master' key. The | ||
50 | 'master' key can either be a trusted-key or user-key type. The main | ||
51 | disadvantage of encrypted keys is that if they are not rooted in a trusted key, | ||
52 | they are only as secure as the user key encrypting them. The master user key | ||
53 | should therefore be loaded in as secure a way as possible, preferably early in | ||
54 | boot. | ||
55 | |||
56 | Usage: | ||
57 | keyctl add encrypted name "new key-type:master-key-name keylen" ring | ||
58 | keyctl add encrypted name "load hex_blob" ring | ||
59 | keyctl update keyid "update key-type:master-key-name" | ||
60 | |||
61 | where 'key-type' is either 'trusted' or 'user'. | ||
62 | |||
63 | Examples of trusted and encrypted key usage: | ||
64 | |||
65 | Create and save a trusted key named "kmk" of length 32 bytes: | ||
66 | |||
67 | $ keyctl add trusted kmk "new 32" @u | ||
68 | 440502848 | ||
69 | |||
70 | $ keyctl show | ||
71 | Session Keyring | ||
72 | -3 --alswrv 500 500 keyring: _ses | ||
73 | 97833714 --alswrv 500 -1 \_ keyring: _uid.500 | ||
74 | 440502848 --alswrv 500 500 \_ trusted: kmk | ||
75 | |||
76 | $ keyctl print 440502848 | ||
77 | 0101000000000000000001005d01b7e3f4a6be5709930f3b70a743cbb42e0cc95e18e915 | ||
78 | 3f60da455bbf1144ad12e4f92b452f966929f6105fd29ca28e4d4d5a031d068478bacb0b | ||
79 | 27351119f822911b0a11ba3d3498ba6a32e50dac7f32894dd890eb9ad578e4e292c83722 | ||
80 | a52e56a097e6a68b3f56f7a52ece0cdccba1eb62cad7d817f6dc58898b3ac15f36026fec | ||
81 | d568bd4a706cb60bb37be6d8f1240661199d640b66fb0fe3b079f97f450b9ef9c22c6d5d | ||
82 | dd379f0facd1cd020281dfa3c70ba21a3fa6fc2471dc6d13ecf8298b946f65345faa5ef0 | ||
83 | f1f8fff03ad0acb083725535636addb08d73dedb9832da198081e5deae84bfaf0409c22b | ||
84 | e4a8aea2b607ec96931e6f4d4fe563ba | ||
85 | |||
86 | $ keyctl pipe 440502848 > kmk.blob | ||
87 | |||
88 | Load a trusted key from the saved blob: | ||
89 | |||
90 | $ keyctl add trusted kmk "load `cat kmk.blob`" @u | ||
91 | 268728824 | ||
92 | |||
93 | $ keyctl print 268728824 | ||
94 | 0101000000000000000001005d01b7e3f4a6be5709930f3b70a743cbb42e0cc95e18e915 | ||
95 | 3f60da455bbf1144ad12e4f92b452f966929f6105fd29ca28e4d4d5a031d068478bacb0b | ||
96 | 27351119f822911b0a11ba3d3498ba6a32e50dac7f32894dd890eb9ad578e4e292c83722 | ||
97 | a52e56a097e6a68b3f56f7a52ece0cdccba1eb62cad7d817f6dc58898b3ac15f36026fec | ||
98 | d568bd4a706cb60bb37be6d8f1240661199d640b66fb0fe3b079f97f450b9ef9c22c6d5d | ||
99 | dd379f0facd1cd020281dfa3c70ba21a3fa6fc2471dc6d13ecf8298b946f65345faa5ef0 | ||
100 | f1f8fff03ad0acb083725535636addb08d73dedb9832da198081e5deae84bfaf0409c22b | ||
101 | e4a8aea2b607ec96931e6f4d4fe563ba | ||
102 | |||
103 | Reseal a trusted key under new pcr values: | ||
104 | |||
105 | $ keyctl update 268728824 "update pcrinfo=`cat pcr.blob`" | ||
106 | $ keyctl print 268728824 | ||
107 | 010100000000002c0002800093c35a09b70fff26e7a98ae786c641e678ec6ffb6b46d805 | ||
108 | 77c8a6377aed9d3219c6dfec4b23ffe3000001005d37d472ac8a44023fbb3d18583a4f73 | ||
109 | d3a076c0858f6f1dcaa39ea0f119911ff03f5406df4f7f27f41da8d7194f45c9f4e00f2e | ||
110 | df449f266253aa3f52e55c53de147773e00f0f9aca86c64d94c95382265968c354c5eab4 | ||
111 | 9638c5ae99c89de1e0997242edfb0b501744e11ff9762dfd951cffd93227cc513384e7e6 | ||
112 | e782c29435c7ec2edafaa2f4c1fe6e7a781b59549ff5296371b42133777dcc5b8b971610 | ||
113 | 94bc67ede19e43ddb9dc2baacad374a36feaf0314d700af0a65c164b7082401740e489c9 | ||
114 | 7ef6a24defe4846104209bf0c3eced7fa1a672ed5b125fc9d8cd88b476a658a4434644ef | ||
115 | df8ae9a178e9f83ba9f08d10fa47e4226b98b0702f06b3b8 | ||
116 | |||
117 | Create and save an encrypted key "evm" using the above trusted key "kmk": | ||
118 | |||
119 | $ keyctl add encrypted evm "new trusted:kmk 32" @u | ||
120 | 159771175 | ||
121 | |||
122 | $ keyctl print 159771175 | ||
123 | trusted:kmk 32 2375725ad57798846a9bbd240de8906f006e66c03af53b1b382dbbc55 | ||
124 | be2a44616e4959430436dc4f2a7a9659aa60bb4652aeb2120f149ed197c564e024717c64 | ||
125 | 5972dcb82ab2dde83376d82b2e3c09ffc | ||
126 | |||
127 | $ keyctl pipe 159771175 > evm.blob | ||
128 | |||
129 | Load an encrypted key "evm" from saved blob: | ||
130 | |||
131 | $ keyctl add encrypted evm "load `cat evm.blob`" @u | ||
132 | 831684262 | ||
133 | |||
134 | $ keyctl print 831684262 | ||
135 | trusted:kmk 32 2375725ad57798846a9bbd240de8906f006e66c03af53b1b382dbbc55 | ||
136 | be2a44616e4959430436dc4f2a7a9659aa60bb4652aeb2120f149ed197c564e024717c64 | ||
137 | 5972dcb82ab2dde83376d82b2e3c09ffc | ||
138 | |||
139 | |||
140 | The initial consumer of trusted keys is EVM, which at boot time needs a high | ||
141 | quality symmetric key for HMAC protection of file metadata. The use of a | ||
142 | trusted key provides strong guarantees that the EVM key has not been | ||
143 | compromised by a user level problem, and when sealed to specific boot PCR | ||
144 | values, protects against boot and offline attacks. Other uses for trusted and | ||
145 | encrypted keys, such as for disk and file encryption are anticipated. | ||
diff --git a/include/keys/trusted-type.h b/include/keys/trusted-type.h new file mode 100644 index 00000000000..56f82e5c997 --- /dev/null +++ b/include/keys/trusted-type.h | |||
@@ -0,0 +1,31 @@ | |||
1 | /* | ||
2 | * Copyright (C) 2010 IBM Corporation | ||
3 | * Author: David Safford <safford@us.ibm.com> | ||
4 | * | ||
5 | * This program is free software; you can redistribute it and/or modify | ||
6 | * it under the terms of the GNU General Public License as published by | ||
7 | * the Free Software Foundation, version 2 of the License. | ||
8 | */ | ||
9 | |||
10 | #ifndef _KEYS_TRUSTED_TYPE_H | ||
11 | #define _KEYS_TRUSTED_TYPE_H | ||
12 | |||
13 | #include <linux/key.h> | ||
14 | #include <linux/rcupdate.h> | ||
15 | |||
16 | #define MIN_KEY_SIZE 32 | ||
17 | #define MAX_KEY_SIZE 128 | ||
18 | #define MAX_BLOB_SIZE 320 | ||
19 | |||
20 | struct trusted_key_payload { | ||
21 | struct rcu_head rcu; | ||
22 | unsigned int key_len; | ||
23 | unsigned int blob_len; | ||
24 | unsigned char migratable; | ||
25 | unsigned char key[MAX_KEY_SIZE + 1]; | ||
26 | unsigned char blob[MAX_BLOB_SIZE]; | ||
27 | }; | ||
28 | |||
29 | extern struct key_type key_type_trusted; | ||
30 | |||
31 | #endif /* _KEYS_TRUSTED_TYPE_H */ | ||
diff --git a/include/linux/tpm_command.h b/include/linux/tpm_command.h new file mode 100644 index 00000000000..727512e249b --- /dev/null +++ b/include/linux/tpm_command.h | |||
@@ -0,0 +1,28 @@ | |||
1 | #ifndef __LINUX_TPM_COMMAND_H__ | ||
2 | #define __LINUX_TPM_COMMAND_H__ | ||
3 | |||
4 | /* | ||
5 | * TPM Command constants from specifications at | ||
6 | * http://www.trustedcomputinggroup.org | ||
7 | */ | ||
8 | |||
9 | /* Command TAGS */ | ||
10 | #define TPM_TAG_RQU_COMMAND 193 | ||
11 | #define TPM_TAG_RQU_AUTH1_COMMAND 194 | ||
12 | #define TPM_TAG_RQU_AUTH2_COMMAND 195 | ||
13 | #define TPM_TAG_RSP_COMMAND 196 | ||
14 | #define TPM_TAG_RSP_AUTH1_COMMAND 197 | ||
15 | #define TPM_TAG_RSP_AUTH2_COMMAND 198 | ||
16 | |||
17 | /* Command Ordinals */ | ||
18 | #define TPM_ORD_GETRANDOM 70 | ||
19 | #define TPM_ORD_OSAP 11 | ||
20 | #define TPM_ORD_OIAP 10 | ||
21 | #define TPM_ORD_SEAL 23 | ||
22 | #define TPM_ORD_UNSEAL 24 | ||
23 | |||
24 | /* Other constants */ | ||
25 | #define SRKHANDLE 0x40000000 | ||
26 | #define TPM_NONCE_SIZE 20 | ||
27 | |||
28 | #endif | ||
diff --git a/security/Kconfig b/security/Kconfig index e80da955e68..24b8f9b491b 100644 --- a/security/Kconfig +++ b/security/Kconfig | |||
@@ -21,6 +21,21 @@ config KEYS | |||
21 | 21 | ||
22 | If you are unsure as to whether this is required, answer N. | 22 | If you are unsure as to whether this is required, answer N. |
23 | 23 | ||
24 | config TRUSTED_KEYS | ||
25 | tristate "TRUSTED KEYS" | ||
26 | depends on KEYS && TCG_TPM | ||
27 | select CRYPTO | ||
28 | select CRYPTO_HMAC | ||
29 | select CRYPTO_SHA1 | ||
30 | help | ||
31 | This option provides support for creating, sealing, and unsealing | ||
32 | keys in the kernel. Trusted keys are random number symmetric keys, | ||
33 | generated and RSA-sealed by the TPM. The TPM only unseals the keys, | ||
34 | if the boot PCRs and other criteria match. Userspace will only ever | ||
35 | see encrypted blobs. | ||
36 | |||
37 | If you are unsure as to whether this is required, answer N. | ||
38 | |||
24 | config KEYS_DEBUG_PROC_KEYS | 39 | config KEYS_DEBUG_PROC_KEYS |
25 | bool "Enable the /proc/keys file by which keys may be viewed" | 40 | bool "Enable the /proc/keys file by which keys may be viewed" |
26 | depends on KEYS | 41 | depends on KEYS |
diff --git a/security/keys/Makefile b/security/keys/Makefile index 74d5447d7df..fcb107020b4 100644 --- a/security/keys/Makefile +++ b/security/keys/Makefile | |||
@@ -13,6 +13,7 @@ obj-y := \ | |||
13 | request_key_auth.o \ | 13 | request_key_auth.o \ |
14 | user_defined.o | 14 | user_defined.o |
15 | 15 | ||
16 | obj-$(CONFIG_TRUSTED_KEYS) += trusted_defined.o | ||
16 | obj-$(CONFIG_KEYS_COMPAT) += compat.o | 17 | obj-$(CONFIG_KEYS_COMPAT) += compat.o |
17 | obj-$(CONFIG_PROC_FS) += proc.o | 18 | obj-$(CONFIG_PROC_FS) += proc.o |
18 | obj-$(CONFIG_SYSCTL) += sysctl.o | 19 | obj-$(CONFIG_SYSCTL) += sysctl.o |
diff --git a/security/keys/trusted_defined.c b/security/keys/trusted_defined.c new file mode 100644 index 00000000000..1bec72e7596 --- /dev/null +++ b/security/keys/trusted_defined.c | |||
@@ -0,0 +1,1151 @@ | |||
1 | /* | ||
2 | * Copyright (C) 2010 IBM Corporation | ||
3 | * | ||
4 | * Author: | ||
5 | * David Safford <safford@us.ibm.com> | ||
6 | * | ||
7 | * This program is free software; you can redistribute it and/or modify | ||
8 | * it under the terms of the GNU General Public License as published by | ||
9 | * the Free Software Foundation, version 2 of the License. | ||
10 | * | ||
11 | * See Documentation/keys-trusted-encrypted.txt | ||
12 | */ | ||
13 | |||
14 | #include <linux/uaccess.h> | ||
15 | #include <linux/module.h> | ||
16 | #include <linux/init.h> | ||
17 | #include <linux/slab.h> | ||
18 | #include <linux/parser.h> | ||
19 | #include <linux/string.h> | ||
20 | #include <keys/user-type.h> | ||
21 | #include <keys/trusted-type.h> | ||
22 | #include <linux/key-type.h> | ||
23 | #include <linux/rcupdate.h> | ||
24 | #include <linux/crypto.h> | ||
25 | #include <crypto/hash.h> | ||
26 | #include <crypto/sha.h> | ||
27 | #include <linux/capability.h> | ||
28 | #include <linux/tpm.h> | ||
29 | #include <linux/tpm_command.h> | ||
30 | |||
31 | #include "trusted_defined.h" | ||
32 | |||
33 | static const char hmac_alg[] = "hmac(sha1)"; | ||
34 | static const char hash_alg[] = "sha1"; | ||
35 | |||
36 | struct sdesc { | ||
37 | struct shash_desc shash; | ||
38 | char ctx[]; | ||
39 | }; | ||
40 | |||
41 | static struct crypto_shash *hashalg; | ||
42 | static struct crypto_shash *hmacalg; | ||
43 | |||
44 | static struct sdesc *init_sdesc(struct crypto_shash *alg) | ||
45 | { | ||
46 | struct sdesc *sdesc; | ||
47 | int size; | ||
48 | |||
49 | size = sizeof(struct shash_desc) + crypto_shash_descsize(alg); | ||
50 | sdesc = kmalloc(size, GFP_KERNEL); | ||
51 | if (!sdesc) | ||
52 | return ERR_PTR(-ENOMEM); | ||
53 | sdesc->shash.tfm = alg; | ||
54 | sdesc->shash.flags = 0x0; | ||
55 | return sdesc; | ||
56 | } | ||
57 | |||
58 | static int TSS_sha1(const unsigned char *data, const unsigned int datalen, | ||
59 | unsigned char *digest) | ||
60 | { | ||
61 | struct sdesc *sdesc; | ||
62 | int ret; | ||
63 | |||
64 | sdesc = init_sdesc(hashalg); | ||
65 | if (IS_ERR(sdesc)) { | ||
66 | pr_info("trusted_key: can't alloc %s\n", hash_alg); | ||
67 | return PTR_ERR(sdesc); | ||
68 | } | ||
69 | |||
70 | ret = crypto_shash_digest(&sdesc->shash, data, datalen, digest); | ||
71 | kfree(sdesc); | ||
72 | return ret; | ||
73 | } | ||
74 | |||
75 | static int TSS_rawhmac(unsigned char *digest, const unsigned char *key, | ||
76 | const unsigned int keylen, ...) | ||
77 | { | ||
78 | struct sdesc *sdesc; | ||
79 | va_list argp; | ||
80 | unsigned int dlen; | ||
81 | unsigned char *data; | ||
82 | int ret; | ||
83 | |||
84 | sdesc = init_sdesc(hmacalg); | ||
85 | if (IS_ERR(sdesc)) { | ||
86 | pr_info("trusted_key: can't alloc %s\n", hmac_alg); | ||
87 | return PTR_ERR(sdesc); | ||
88 | } | ||
89 | |||
90 | ret = crypto_shash_setkey(hmacalg, key, keylen); | ||
91 | if (ret < 0) | ||
92 | goto out; | ||
93 | ret = crypto_shash_init(&sdesc->shash); | ||
94 | if (ret < 0) | ||
95 | goto out; | ||
96 | |||
97 | va_start(argp, keylen); | ||
98 | for (;;) { | ||
99 | dlen = va_arg(argp, unsigned int); | ||
100 | if (dlen == 0) | ||
101 | break; | ||
102 | data = va_arg(argp, unsigned char *); | ||
103 | if (data == NULL) | ||
104 | return -EINVAL; | ||
105 | ret = crypto_shash_update(&sdesc->shash, data, dlen); | ||
106 | if (ret < 0) | ||
107 | goto out; | ||
108 | } | ||
109 | va_end(argp); | ||
110 | ret = crypto_shash_final(&sdesc->shash, digest); | ||
111 | out: | ||
112 | kfree(sdesc); | ||
113 | return ret; | ||
114 | } | ||
115 | |||
116 | /* | ||
117 | * calculate authorization info fields to send to TPM | ||
118 | */ | ||
119 | static uint32_t TSS_authhmac(unsigned char *digest, const unsigned char *key, | ||
120 | const unsigned int keylen, unsigned char *h1, | ||
121 | unsigned char *h2, unsigned char h3, ...) | ||
122 | { | ||
123 | unsigned char paramdigest[SHA1_DIGEST_SIZE]; | ||
124 | struct sdesc *sdesc; | ||
125 | unsigned int dlen; | ||
126 | unsigned char *data; | ||
127 | unsigned char c; | ||
128 | int ret; | ||
129 | va_list argp; | ||
130 | |||
131 | sdesc = init_sdesc(hashalg); | ||
132 | if (IS_ERR(sdesc)) { | ||
133 | pr_info("trusted_key: can't alloc %s\n", hash_alg); | ||
134 | return PTR_ERR(sdesc); | ||
135 | } | ||
136 | |||
137 | c = h3; | ||
138 | ret = crypto_shash_init(&sdesc->shash); | ||
139 | if (ret < 0) | ||
140 | goto out; | ||
141 | va_start(argp, h3); | ||
142 | for (;;) { | ||
143 | dlen = va_arg(argp, unsigned int); | ||
144 | if (dlen == 0) | ||
145 | break; | ||
146 | data = va_arg(argp, unsigned char *); | ||
147 | ret = crypto_shash_update(&sdesc->shash, data, dlen); | ||
148 | if (ret < 0) | ||
149 | goto out; | ||
150 | } | ||
151 | va_end(argp); | ||
152 | ret = crypto_shash_final(&sdesc->shash, paramdigest); | ||
153 | if (!ret) | ||
154 | TSS_rawhmac(digest, key, keylen, SHA1_DIGEST_SIZE, | ||
155 | paramdigest, TPM_NONCE_SIZE, h1, | ||
156 | TPM_NONCE_SIZE, h2, 1, &c, 0, 0); | ||
157 | out: | ||
158 | kfree(sdesc); | ||
159 | return ret; | ||
160 | } | ||
161 | |||
162 | /* | ||
163 | * verify the AUTH1_COMMAND (Seal) result from TPM | ||
164 | */ | ||
165 | static uint32_t TSS_checkhmac1(unsigned char *buffer, | ||
166 | const uint32_t command, | ||
167 | const unsigned char *ononce, | ||
168 | const unsigned char *key, | ||
169 | const unsigned int keylen, ...) | ||
170 | { | ||
171 | uint32_t bufsize; | ||
172 | uint16_t tag; | ||
173 | uint32_t ordinal; | ||
174 | uint32_t result; | ||
175 | unsigned char *enonce; | ||
176 | unsigned char *continueflag; | ||
177 | unsigned char *authdata; | ||
178 | unsigned char testhmac[SHA1_DIGEST_SIZE]; | ||
179 | unsigned char paramdigest[SHA1_DIGEST_SIZE]; | ||
180 | struct sdesc *sdesc; | ||
181 | unsigned int dlen; | ||
182 | unsigned int dpos; | ||
183 | va_list argp; | ||
184 | int ret; | ||
185 | |||
186 | bufsize = LOAD32(buffer, TPM_SIZE_OFFSET); | ||
187 | tag = LOAD16(buffer, 0); | ||
188 | ordinal = command; | ||
189 | result = LOAD32N(buffer, TPM_RETURN_OFFSET); | ||
190 | if (tag == TPM_TAG_RSP_COMMAND) | ||
191 | return 0; | ||
192 | if (tag != TPM_TAG_RSP_AUTH1_COMMAND) | ||
193 | return -EINVAL; | ||
194 | authdata = buffer + bufsize - SHA1_DIGEST_SIZE; | ||
195 | continueflag = authdata - 1; | ||
196 | enonce = continueflag - TPM_NONCE_SIZE; | ||
197 | |||
198 | sdesc = init_sdesc(hashalg); | ||
199 | if (IS_ERR(sdesc)) { | ||
200 | pr_info("trusted_key: can't alloc %s\n", hash_alg); | ||
201 | return PTR_ERR(sdesc); | ||
202 | } | ||
203 | ret = crypto_shash_init(&sdesc->shash); | ||
204 | if (ret < 0) | ||
205 | goto out; | ||
206 | ret = crypto_shash_update(&sdesc->shash, (const u8 *)&result, | ||
207 | sizeof result); | ||
208 | if (ret < 0) | ||
209 | goto out; | ||
210 | ret = crypto_shash_update(&sdesc->shash, (const u8 *)&ordinal, | ||
211 | sizeof ordinal); | ||
212 | if (ret < 0) | ||
213 | goto out; | ||
214 | va_start(argp, keylen); | ||
215 | for (;;) { | ||
216 | dlen = va_arg(argp, unsigned int); | ||
217 | if (dlen == 0) | ||
218 | break; | ||
219 | dpos = va_arg(argp, unsigned int); | ||
220 | ret = crypto_shash_update(&sdesc->shash, buffer + dpos, dlen); | ||
221 | if (ret < 0) | ||
222 | goto out; | ||
223 | } | ||
224 | va_end(argp); | ||
225 | ret = crypto_shash_final(&sdesc->shash, paramdigest); | ||
226 | if (ret < 0) | ||
227 | goto out; | ||
228 | ret = TSS_rawhmac(testhmac, key, keylen, SHA1_DIGEST_SIZE, paramdigest, | ||
229 | TPM_NONCE_SIZE, enonce, TPM_NONCE_SIZE, ononce, | ||
230 | 1, continueflag, 0, 0); | ||
231 | if (ret < 0) | ||
232 | goto out; | ||
233 | if (memcmp(testhmac, authdata, SHA1_DIGEST_SIZE)) | ||
234 | ret = -EINVAL; | ||
235 | out: | ||
236 | kfree(sdesc); | ||
237 | return ret; | ||
238 | } | ||
239 | |||
240 | /* | ||
241 | * verify the AUTH2_COMMAND (unseal) result from TPM | ||
242 | */ | ||
243 | static uint32_t TSS_checkhmac2(unsigned char *buffer, | ||
244 | const uint32_t command, | ||
245 | const unsigned char *ononce, | ||
246 | const unsigned char *key1, | ||
247 | const unsigned int keylen1, | ||
248 | const unsigned char *key2, | ||
249 | const unsigned int keylen2, ...) | ||
250 | { | ||
251 | uint32_t bufsize; | ||
252 | uint16_t tag; | ||
253 | uint32_t ordinal; | ||
254 | uint32_t result; | ||
255 | unsigned char *enonce1; | ||
256 | unsigned char *continueflag1; | ||
257 | unsigned char *authdata1; | ||
258 | unsigned char *enonce2; | ||
259 | unsigned char *continueflag2; | ||
260 | unsigned char *authdata2; | ||
261 | unsigned char testhmac1[SHA1_DIGEST_SIZE]; | ||
262 | unsigned char testhmac2[SHA1_DIGEST_SIZE]; | ||
263 | unsigned char paramdigest[SHA1_DIGEST_SIZE]; | ||
264 | struct sdesc *sdesc; | ||
265 | unsigned int dlen; | ||
266 | unsigned int dpos; | ||
267 | va_list argp; | ||
268 | int ret; | ||
269 | |||
270 | bufsize = LOAD32(buffer, TPM_SIZE_OFFSET); | ||
271 | tag = LOAD16(buffer, 0); | ||
272 | ordinal = command; | ||
273 | result = LOAD32N(buffer, TPM_RETURN_OFFSET); | ||
274 | |||
275 | if (tag == TPM_TAG_RSP_COMMAND) | ||
276 | return 0; | ||
277 | if (tag != TPM_TAG_RSP_AUTH2_COMMAND) | ||
278 | return -EINVAL; | ||
279 | authdata1 = buffer + bufsize - (SHA1_DIGEST_SIZE + 1 | ||
280 | + SHA1_DIGEST_SIZE + SHA1_DIGEST_SIZE); | ||
281 | authdata2 = buffer + bufsize - (SHA1_DIGEST_SIZE); | ||
282 | continueflag1 = authdata1 - 1; | ||
283 | continueflag2 = authdata2 - 1; | ||
284 | enonce1 = continueflag1 - TPM_NONCE_SIZE; | ||
285 | enonce2 = continueflag2 - TPM_NONCE_SIZE; | ||
286 | |||
287 | sdesc = init_sdesc(hashalg); | ||
288 | if (IS_ERR(sdesc)) { | ||
289 | pr_info("trusted_key: can't alloc %s\n", hash_alg); | ||
290 | return PTR_ERR(sdesc); | ||
291 | } | ||
292 | ret = crypto_shash_init(&sdesc->shash); | ||
293 | if (ret < 0) | ||
294 | goto out; | ||
295 | ret = crypto_shash_update(&sdesc->shash, (const u8 *)&result, | ||
296 | sizeof result); | ||
297 | if (ret < 0) | ||
298 | goto out; | ||
299 | ret = crypto_shash_update(&sdesc->shash, (const u8 *)&ordinal, | ||
300 | sizeof ordinal); | ||
301 | if (ret < 0) | ||
302 | goto out; | ||
303 | |||
304 | va_start(argp, keylen2); | ||
305 | for (;;) { | ||
306 | dlen = va_arg(argp, unsigned int); | ||
307 | if (dlen == 0) | ||
308 | break; | ||
309 | dpos = va_arg(argp, unsigned int); | ||
310 | ret = crypto_shash_update(&sdesc->shash, buffer + dpos, dlen); | ||
311 | if (ret < 0) | ||
312 | goto out; | ||
313 | } | ||
314 | ret = crypto_shash_final(&sdesc->shash, paramdigest); | ||
315 | if (ret < 0) | ||
316 | goto out; | ||
317 | |||
318 | ret = TSS_rawhmac(testhmac1, key1, keylen1, SHA1_DIGEST_SIZE, | ||
319 | paramdigest, TPM_NONCE_SIZE, enonce1, | ||
320 | TPM_NONCE_SIZE, ononce, 1, continueflag1, 0, 0); | ||
321 | if (memcmp(testhmac1, authdata1, SHA1_DIGEST_SIZE)) { | ||
322 | ret = -EINVAL; | ||
323 | goto out; | ||
324 | } | ||
325 | ret = TSS_rawhmac(testhmac2, key2, keylen2, SHA1_DIGEST_SIZE, | ||
326 | paramdigest, TPM_NONCE_SIZE, enonce2, | ||
327 | TPM_NONCE_SIZE, ononce, 1, continueflag2, 0, 0); | ||
328 | if (memcmp(testhmac2, authdata2, SHA1_DIGEST_SIZE)) | ||
329 | ret = -EINVAL; | ||
330 | out: | ||
331 | kfree(sdesc); | ||
332 | return ret; | ||
333 | } | ||
334 | |||
335 | /* | ||
336 | * For key specific tpm requests, we will generate and send our | ||
337 | * own TPM command packets using the drivers send function. | ||
338 | */ | ||
339 | static int trusted_tpm_send(const u32 chip_num, unsigned char *cmd, | ||
340 | size_t buflen) | ||
341 | { | ||
342 | int rc; | ||
343 | |||
344 | dump_tpm_buf(cmd); | ||
345 | rc = tpm_send(chip_num, cmd, buflen); | ||
346 | dump_tpm_buf(cmd); | ||
347 | if (rc > 0) | ||
348 | /* Can't return positive return codes values to keyctl */ | ||
349 | rc = -EPERM; | ||
350 | return rc; | ||
351 | } | ||
352 | |||
353 | /* | ||
354 | * get a random value from TPM | ||
355 | */ | ||
356 | static int tpm_get_random(struct tpm_buf *tb, unsigned char *buf, uint32_t len) | ||
357 | { | ||
358 | int ret; | ||
359 | |||
360 | INIT_BUF(tb); | ||
361 | store16(tb, TPM_TAG_RQU_COMMAND); | ||
362 | store32(tb, TPM_GETRANDOM_SIZE); | ||
363 | store32(tb, TPM_ORD_GETRANDOM); | ||
364 | store32(tb, len); | ||
365 | ret = trusted_tpm_send(TPM_ANY_NUM, tb->data, sizeof tb->data); | ||
366 | memcpy(buf, tb->data + TPM_GETRANDOM_SIZE, len); | ||
367 | |||
368 | return ret; | ||
369 | } | ||
370 | |||
371 | static int my_get_random(unsigned char *buf, int len) | ||
372 | { | ||
373 | struct tpm_buf *tb; | ||
374 | int ret; | ||
375 | |||
376 | tb = kzalloc(sizeof *tb, GFP_KERNEL); | ||
377 | if (!tb) | ||
378 | return -ENOMEM; | ||
379 | ret = tpm_get_random(tb, buf, len); | ||
380 | |||
381 | kfree(tb); | ||
382 | return ret; | ||
383 | } | ||
384 | |||
385 | /* | ||
386 | * Lock a trusted key, by extending a selected PCR. | ||
387 | * | ||
388 | * Prevents a trusted key that is sealed to PCRs from being accessed. | ||
389 | * This uses the tpm driver's extend function. | ||
390 | */ | ||
391 | static int pcrlock(const int pcrnum) | ||
392 | { | ||
393 | unsigned char hash[SHA1_DIGEST_SIZE]; | ||
394 | |||
395 | if (!capable(CAP_SYS_ADMIN)) | ||
396 | return -EPERM; | ||
397 | my_get_random(hash, SHA1_DIGEST_SIZE); | ||
398 | return tpm_pcr_extend(TPM_ANY_NUM, pcrnum, hash) ? -EINVAL : 0; | ||
399 | } | ||
400 | |||
401 | /* | ||
402 | * Create an object specific authorisation protocol (OSAP) session | ||
403 | */ | ||
404 | static int osap(struct tpm_buf *tb, struct osapsess *s, | ||
405 | const unsigned char *key, const uint16_t type, | ||
406 | const uint32_t handle) | ||
407 | { | ||
408 | unsigned char enonce[TPM_NONCE_SIZE]; | ||
409 | unsigned char ononce[TPM_NONCE_SIZE]; | ||
410 | int ret; | ||
411 | |||
412 | ret = tpm_get_random(tb, ononce, TPM_NONCE_SIZE); | ||
413 | if (ret < 0) | ||
414 | return ret; | ||
415 | |||
416 | INIT_BUF(tb); | ||
417 | store16(tb, TPM_TAG_RQU_COMMAND); | ||
418 | store32(tb, TPM_OSAP_SIZE); | ||
419 | store32(tb, TPM_ORD_OSAP); | ||
420 | store16(tb, type); | ||
421 | store32(tb, handle); | ||
422 | storebytes(tb, ononce, TPM_NONCE_SIZE); | ||
423 | |||
424 | ret = trusted_tpm_send(TPM_ANY_NUM, tb->data, MAX_BUF_SIZE); | ||
425 | if (ret < 0) | ||
426 | return ret; | ||
427 | |||
428 | s->handle = LOAD32(tb->data, TPM_DATA_OFFSET); | ||
429 | memcpy(s->enonce, &(tb->data[TPM_DATA_OFFSET + sizeof(uint32_t)]), | ||
430 | TPM_NONCE_SIZE); | ||
431 | memcpy(enonce, &(tb->data[TPM_DATA_OFFSET + sizeof(uint32_t) + | ||
432 | TPM_NONCE_SIZE]), TPM_NONCE_SIZE); | ||
433 | ret = TSS_rawhmac(s->secret, key, SHA1_DIGEST_SIZE, TPM_NONCE_SIZE, | ||
434 | enonce, TPM_NONCE_SIZE, ononce, 0, 0); | ||
435 | return ret; | ||
436 | } | ||
437 | |||
438 | /* | ||
439 | * Create an object independent authorisation protocol (oiap) session | ||
440 | */ | ||
441 | static int oiap(struct tpm_buf *tb, uint32_t *handle, unsigned char *nonce) | ||
442 | { | ||
443 | int ret; | ||
444 | |||
445 | INIT_BUF(tb); | ||
446 | store16(tb, TPM_TAG_RQU_COMMAND); | ||
447 | store32(tb, TPM_OIAP_SIZE); | ||
448 | store32(tb, TPM_ORD_OIAP); | ||
449 | ret = trusted_tpm_send(TPM_ANY_NUM, tb->data, MAX_BUF_SIZE); | ||
450 | if (ret < 0) | ||
451 | return ret; | ||
452 | |||
453 | *handle = LOAD32(tb->data, TPM_DATA_OFFSET); | ||
454 | memcpy(nonce, &tb->data[TPM_DATA_OFFSET + sizeof(uint32_t)], | ||
455 | TPM_NONCE_SIZE); | ||
456 | return ret; | ||
457 | } | ||
458 | |||
459 | struct tpm_digests { | ||
460 | unsigned char encauth[SHA1_DIGEST_SIZE]; | ||
461 | unsigned char pubauth[SHA1_DIGEST_SIZE]; | ||
462 | unsigned char xorwork[SHA1_DIGEST_SIZE * 2]; | ||
463 | unsigned char xorhash[SHA1_DIGEST_SIZE]; | ||
464 | unsigned char nonceodd[TPM_NONCE_SIZE]; | ||
465 | }; | ||
466 | |||
467 | /* | ||
468 | * Have the TPM seal(encrypt) the trusted key, possibly based on | ||
469 | * Platform Configuration Registers (PCRs). AUTH1 for sealing key. | ||
470 | */ | ||
471 | static int tpm_seal(struct tpm_buf *tb, const uint16_t keytype, | ||
472 | const uint32_t keyhandle, const unsigned char *keyauth, | ||
473 | const unsigned char *data, const uint32_t datalen, | ||
474 | unsigned char *blob, uint32_t *bloblen, | ||
475 | const unsigned char *blobauth, | ||
476 | const unsigned char *pcrinfo, const uint32_t pcrinfosize) | ||
477 | { | ||
478 | struct osapsess sess; | ||
479 | struct tpm_digests *td; | ||
480 | unsigned char cont; | ||
481 | uint32_t ordinal; | ||
482 | uint32_t pcrsize; | ||
483 | uint32_t datsize; | ||
484 | int sealinfosize; | ||
485 | int encdatasize; | ||
486 | int storedsize; | ||
487 | int ret; | ||
488 | int i; | ||
489 | |||
490 | /* alloc some work space for all the hashes */ | ||
491 | td = kmalloc(sizeof *td, GFP_KERNEL); | ||
492 | if (!td) | ||
493 | return -ENOMEM; | ||
494 | |||
495 | /* get session for sealing key */ | ||
496 | ret = osap(tb, &sess, keyauth, keytype, keyhandle); | ||
497 | if (ret < 0) | ||
498 | return ret; | ||
499 | dump_sess(&sess); | ||
500 | |||
501 | /* calculate encrypted authorization value */ | ||
502 | memcpy(td->xorwork, sess.secret, SHA1_DIGEST_SIZE); | ||
503 | memcpy(td->xorwork + SHA1_DIGEST_SIZE, sess.enonce, SHA1_DIGEST_SIZE); | ||
504 | ret = TSS_sha1(td->xorwork, SHA1_DIGEST_SIZE * 2, td->xorhash); | ||
505 | if (ret < 0) | ||
506 | return ret; | ||
507 | |||
508 | ret = tpm_get_random(tb, td->nonceodd, TPM_NONCE_SIZE); | ||
509 | if (ret < 0) | ||
510 | return ret; | ||
511 | ordinal = htonl(TPM_ORD_SEAL); | ||
512 | datsize = htonl(datalen); | ||
513 | pcrsize = htonl(pcrinfosize); | ||
514 | cont = 0; | ||
515 | |||
516 | /* encrypt data authorization key */ | ||
517 | for (i = 0; i < SHA1_DIGEST_SIZE; ++i) | ||
518 | td->encauth[i] = td->xorhash[i] ^ blobauth[i]; | ||
519 | |||
520 | /* calculate authorization HMAC value */ | ||
521 | if (pcrinfosize == 0) { | ||
522 | /* no pcr info specified */ | ||
523 | TSS_authhmac(td->pubauth, sess.secret, SHA1_DIGEST_SIZE, | ||
524 | sess.enonce, td->nonceodd, cont, sizeof(uint32_t), | ||
525 | &ordinal, SHA1_DIGEST_SIZE, td->encauth, | ||
526 | sizeof(uint32_t), &pcrsize, sizeof(uint32_t), | ||
527 | &datsize, datalen, data, 0, 0); | ||
528 | } else { | ||
529 | /* pcr info specified */ | ||
530 | TSS_authhmac(td->pubauth, sess.secret, SHA1_DIGEST_SIZE, | ||
531 | sess.enonce, td->nonceodd, cont, sizeof(uint32_t), | ||
532 | &ordinal, SHA1_DIGEST_SIZE, td->encauth, | ||
533 | sizeof(uint32_t), &pcrsize, pcrinfosize, | ||
534 | pcrinfo, sizeof(uint32_t), &datsize, datalen, | ||
535 | data, 0, 0); | ||
536 | } | ||
537 | |||
538 | /* build and send the TPM request packet */ | ||
539 | INIT_BUF(tb); | ||
540 | store16(tb, TPM_TAG_RQU_AUTH1_COMMAND); | ||
541 | store32(tb, TPM_SEAL_SIZE + pcrinfosize + datalen); | ||
542 | store32(tb, TPM_ORD_SEAL); | ||
543 | store32(tb, keyhandle); | ||
544 | storebytes(tb, td->encauth, SHA1_DIGEST_SIZE); | ||
545 | store32(tb, pcrinfosize); | ||
546 | storebytes(tb, pcrinfo, pcrinfosize); | ||
547 | store32(tb, datalen); | ||
548 | storebytes(tb, data, datalen); | ||
549 | store32(tb, sess.handle); | ||
550 | storebytes(tb, td->nonceodd, TPM_NONCE_SIZE); | ||
551 | store8(tb, cont); | ||
552 | storebytes(tb, td->pubauth, SHA1_DIGEST_SIZE); | ||
553 | |||
554 | ret = trusted_tpm_send(TPM_ANY_NUM, tb->data, MAX_BUF_SIZE); | ||
555 | if (ret < 0) | ||
556 | return ret; | ||
557 | |||
558 | /* calculate the size of the returned Blob */ | ||
559 | sealinfosize = LOAD32(tb->data, TPM_DATA_OFFSET + sizeof(uint32_t)); | ||
560 | encdatasize = LOAD32(tb->data, TPM_DATA_OFFSET + sizeof(uint32_t) + | ||
561 | sizeof(uint32_t) + sealinfosize); | ||
562 | storedsize = sizeof(uint32_t) + sizeof(uint32_t) + sealinfosize + | ||
563 | sizeof(uint32_t) + encdatasize; | ||
564 | |||
565 | /* check the HMAC in the response */ | ||
566 | ret = TSS_checkhmac1(tb->data, ordinal, td->nonceodd, sess.secret, | ||
567 | SHA1_DIGEST_SIZE, storedsize, TPM_DATA_OFFSET, 0, | ||
568 | 0); | ||
569 | |||
570 | /* copy the returned blob to caller */ | ||
571 | memcpy(blob, tb->data + TPM_DATA_OFFSET, storedsize); | ||
572 | *bloblen = storedsize; | ||
573 | return ret; | ||
574 | } | ||
575 | |||
576 | /* | ||
577 | * use the AUTH2_COMMAND form of unseal, to authorize both key and blob | ||
578 | */ | ||
579 | static int tpm_unseal(struct tpm_buf *tb, | ||
580 | const uint32_t keyhandle, const unsigned char *keyauth, | ||
581 | const unsigned char *blob, const int bloblen, | ||
582 | const unsigned char *blobauth, | ||
583 | unsigned char *data, unsigned int *datalen) | ||
584 | { | ||
585 | unsigned char nonceodd[TPM_NONCE_SIZE]; | ||
586 | unsigned char enonce1[TPM_NONCE_SIZE]; | ||
587 | unsigned char enonce2[TPM_NONCE_SIZE]; | ||
588 | unsigned char authdata1[SHA1_DIGEST_SIZE]; | ||
589 | unsigned char authdata2[SHA1_DIGEST_SIZE]; | ||
590 | uint32_t authhandle1 = 0; | ||
591 | uint32_t authhandle2 = 0; | ||
592 | unsigned char cont = 0; | ||
593 | uint32_t ordinal; | ||
594 | uint32_t keyhndl; | ||
595 | int ret; | ||
596 | |||
597 | /* sessions for unsealing key and data */ | ||
598 | ret = oiap(tb, &authhandle1, enonce1); | ||
599 | if (ret < 0) { | ||
600 | pr_info("trusted_key: oiap failed (%d)\n", ret); | ||
601 | return ret; | ||
602 | } | ||
603 | ret = oiap(tb, &authhandle2, enonce2); | ||
604 | if (ret < 0) { | ||
605 | pr_info("trusted_key: oiap failed (%d)\n", ret); | ||
606 | return ret; | ||
607 | } | ||
608 | |||
609 | ordinal = htonl(TPM_ORD_UNSEAL); | ||
610 | keyhndl = htonl(SRKHANDLE); | ||
611 | ret = tpm_get_random(tb, nonceodd, TPM_NONCE_SIZE); | ||
612 | if (ret < 0) { | ||
613 | pr_info("trusted_key: tpm_get_random failed (%d)\n", ret); | ||
614 | return ret; | ||
615 | } | ||
616 | TSS_authhmac(authdata1, keyauth, TPM_NONCE_SIZE, | ||
617 | enonce1, nonceodd, cont, sizeof(uint32_t), | ||
618 | &ordinal, bloblen, blob, 0, 0); | ||
619 | TSS_authhmac(authdata2, blobauth, TPM_NONCE_SIZE, | ||
620 | enonce2, nonceodd, cont, sizeof(uint32_t), | ||
621 | &ordinal, bloblen, blob, 0, 0); | ||
622 | |||
623 | /* build and send TPM request packet */ | ||
624 | INIT_BUF(tb); | ||
625 | store16(tb, TPM_TAG_RQU_AUTH2_COMMAND); | ||
626 | store32(tb, TPM_UNSEAL_SIZE + bloblen); | ||
627 | store32(tb, TPM_ORD_UNSEAL); | ||
628 | store32(tb, keyhandle); | ||
629 | storebytes(tb, blob, bloblen); | ||
630 | store32(tb, authhandle1); | ||
631 | storebytes(tb, nonceodd, TPM_NONCE_SIZE); | ||
632 | store8(tb, cont); | ||
633 | storebytes(tb, authdata1, SHA1_DIGEST_SIZE); | ||
634 | store32(tb, authhandle2); | ||
635 | storebytes(tb, nonceodd, TPM_NONCE_SIZE); | ||
636 | store8(tb, cont); | ||
637 | storebytes(tb, authdata2, SHA1_DIGEST_SIZE); | ||
638 | |||
639 | ret = trusted_tpm_send(TPM_ANY_NUM, tb->data, MAX_BUF_SIZE); | ||
640 | if (ret < 0) { | ||
641 | pr_info("trusted_key: authhmac failed (%d)\n", ret); | ||
642 | return ret; | ||
643 | } | ||
644 | |||
645 | *datalen = LOAD32(tb->data, TPM_DATA_OFFSET); | ||
646 | ret = TSS_checkhmac2(tb->data, ordinal, nonceodd, | ||
647 | keyauth, SHA1_DIGEST_SIZE, | ||
648 | blobauth, SHA1_DIGEST_SIZE, | ||
649 | sizeof(uint32_t), TPM_DATA_OFFSET, | ||
650 | *datalen, TPM_DATA_OFFSET + sizeof(uint32_t), 0, | ||
651 | 0); | ||
652 | if (ret < 0) | ||
653 | pr_info("trusted_key: TSS_checkhmac2 failed (%d)\n", ret); | ||
654 | memcpy(data, tb->data + TPM_DATA_OFFSET + sizeof(uint32_t), *datalen); | ||
655 | return ret; | ||
656 | } | ||
657 | |||
658 | /* | ||
659 | * Have the TPM seal(encrypt) the symmetric key | ||
660 | */ | ||
661 | static int key_seal(struct trusted_key_payload *p, | ||
662 | struct trusted_key_options *o) | ||
663 | { | ||
664 | struct tpm_buf *tb; | ||
665 | int ret; | ||
666 | |||
667 | tb = kzalloc(sizeof *tb, GFP_KERNEL); | ||
668 | if (!tb) | ||
669 | return -ENOMEM; | ||
670 | |||
671 | /* include migratable flag at end of sealed key */ | ||
672 | p->key[p->key_len] = p->migratable; | ||
673 | |||
674 | ret = tpm_seal(tb, o->keytype, o->keyhandle, o->keyauth, | ||
675 | p->key, p->key_len + 1, p->blob, &p->blob_len, | ||
676 | o->blobauth, o->pcrinfo, o->pcrinfo_len); | ||
677 | if (ret < 0) | ||
678 | pr_info("trusted_key: srkseal failed (%d)\n", ret); | ||
679 | |||
680 | kfree(tb); | ||
681 | return ret; | ||
682 | } | ||
683 | |||
684 | /* | ||
685 | * Have the TPM unseal(decrypt) the symmetric key | ||
686 | */ | ||
687 | static int key_unseal(struct trusted_key_payload *p, | ||
688 | struct trusted_key_options *o) | ||
689 | { | ||
690 | struct tpm_buf *tb; | ||
691 | int ret; | ||
692 | |||
693 | tb = kzalloc(sizeof *tb, GFP_KERNEL); | ||
694 | if (!tb) | ||
695 | return -ENOMEM; | ||
696 | |||
697 | ret = tpm_unseal(tb, o->keyhandle, o->keyauth, p->blob, p->blob_len, | ||
698 | o->blobauth, p->key, &p->key_len); | ||
699 | /* pull migratable flag out of sealed key */ | ||
700 | p->migratable = p->key[--p->key_len]; | ||
701 | |||
702 | if (ret < 0) | ||
703 | pr_info("trusted_key: srkunseal failed (%d)\n", ret); | ||
704 | |||
705 | kfree(tb); | ||
706 | return ret; | ||
707 | } | ||
708 | |||
709 | enum { | ||
710 | Opt_err = -1, | ||
711 | Opt_new, Opt_load, Opt_update, | ||
712 | Opt_keyhandle, Opt_keyauth, Opt_blobauth, | ||
713 | Opt_pcrinfo, Opt_pcrlock, Opt_migratable | ||
714 | }; | ||
715 | |||
716 | static const match_table_t key_tokens = { | ||
717 | {Opt_new, "new"}, | ||
718 | {Opt_load, "load"}, | ||
719 | {Opt_update, "update"}, | ||
720 | {Opt_keyhandle, "keyhandle=%s"}, | ||
721 | {Opt_keyauth, "keyauth=%s"}, | ||
722 | {Opt_blobauth, "blobauth=%s"}, | ||
723 | {Opt_pcrinfo, "pcrinfo=%s"}, | ||
724 | {Opt_pcrlock, "pcrlock=%s"}, | ||
725 | {Opt_migratable, "migratable=%s"}, | ||
726 | {Opt_err, NULL} | ||
727 | }; | ||
728 | |||
729 | /* can have zero or more token= options */ | ||
730 | static int getoptions(char *c, struct trusted_key_payload *pay, | ||
731 | struct trusted_key_options *opt) | ||
732 | { | ||
733 | substring_t args[MAX_OPT_ARGS]; | ||
734 | char *p = c; | ||
735 | int token; | ||
736 | int res; | ||
737 | unsigned long handle; | ||
738 | unsigned long lock; | ||
739 | |||
740 | while ((p = strsep(&c, " \t"))) { | ||
741 | if (*p == '\0' || *p == ' ' || *p == '\t') | ||
742 | continue; | ||
743 | token = match_token(p, key_tokens, args); | ||
744 | |||
745 | switch (token) { | ||
746 | case Opt_pcrinfo: | ||
747 | opt->pcrinfo_len = strlen(args[0].from) / 2; | ||
748 | if (opt->pcrinfo_len > MAX_PCRINFO_SIZE) | ||
749 | return -EINVAL; | ||
750 | hex2bin(opt->pcrinfo, args[0].from, opt->pcrinfo_len); | ||
751 | break; | ||
752 | case Opt_keyhandle: | ||
753 | res = strict_strtoul(args[0].from, 16, &handle); | ||
754 | if (res < 0) | ||
755 | return -EINVAL; | ||
756 | opt->keytype = SEAL_keytype; | ||
757 | opt->keyhandle = handle; | ||
758 | break; | ||
759 | case Opt_keyauth: | ||
760 | if (strlen(args[0].from) != 2 * SHA1_DIGEST_SIZE) | ||
761 | return -EINVAL; | ||
762 | hex2bin(opt->keyauth, args[0].from, SHA1_DIGEST_SIZE); | ||
763 | break; | ||
764 | case Opt_blobauth: | ||
765 | if (strlen(args[0].from) != 2 * SHA1_DIGEST_SIZE) | ||
766 | return -EINVAL; | ||
767 | hex2bin(opt->blobauth, args[0].from, SHA1_DIGEST_SIZE); | ||
768 | break; | ||
769 | case Opt_migratable: | ||
770 | if (*args[0].from == '0') | ||
771 | pay->migratable = 0; | ||
772 | else | ||
773 | return -EINVAL; | ||
774 | break; | ||
775 | case Opt_pcrlock: | ||
776 | res = strict_strtoul(args[0].from, 10, &lock); | ||
777 | if (res < 0) | ||
778 | return -EINVAL; | ||
779 | opt->pcrlock = lock; | ||
780 | break; | ||
781 | default: | ||
782 | return -EINVAL; | ||
783 | } | ||
784 | } | ||
785 | return 0; | ||
786 | } | ||
787 | |||
788 | /* | ||
789 | * datablob_parse - parse the keyctl data and fill in the | ||
790 | * payload and options structures | ||
791 | * | ||
792 | * On success returns 0, otherwise -EINVAL. | ||
793 | */ | ||
794 | static int datablob_parse(char *datablob, struct trusted_key_payload *p, | ||
795 | struct trusted_key_options *o) | ||
796 | { | ||
797 | substring_t args[MAX_OPT_ARGS]; | ||
798 | long keylen; | ||
799 | int ret = -EINVAL; | ||
800 | int key_cmd; | ||
801 | char *c; | ||
802 | |||
803 | /* main command */ | ||
804 | c = strsep(&datablob, " \t"); | ||
805 | if (!c) | ||
806 | return -EINVAL; | ||
807 | key_cmd = match_token(c, key_tokens, args); | ||
808 | switch (key_cmd) { | ||
809 | case Opt_new: | ||
810 | /* first argument is key size */ | ||
811 | c = strsep(&datablob, " \t"); | ||
812 | if (!c) | ||
813 | return -EINVAL; | ||
814 | ret = strict_strtol(c, 10, &keylen); | ||
815 | if (ret < 0 || keylen < MIN_KEY_SIZE || keylen > MAX_KEY_SIZE) | ||
816 | return -EINVAL; | ||
817 | p->key_len = keylen; | ||
818 | ret = getoptions(datablob, p, o); | ||
819 | if (ret < 0) | ||
820 | return ret; | ||
821 | ret = Opt_new; | ||
822 | break; | ||
823 | case Opt_load: | ||
824 | /* first argument is sealed blob */ | ||
825 | c = strsep(&datablob, " \t"); | ||
826 | if (!c) | ||
827 | return -EINVAL; | ||
828 | p->blob_len = strlen(c) / 2; | ||
829 | if (p->blob_len > MAX_BLOB_SIZE) | ||
830 | return -EINVAL; | ||
831 | hex2bin(p->blob, c, p->blob_len); | ||
832 | ret = getoptions(datablob, p, o); | ||
833 | if (ret < 0) | ||
834 | return ret; | ||
835 | ret = Opt_load; | ||
836 | break; | ||
837 | case Opt_update: | ||
838 | /* all arguments are options */ | ||
839 | ret = getoptions(datablob, p, o); | ||
840 | if (ret < 0) | ||
841 | return ret; | ||
842 | ret = Opt_update; | ||
843 | break; | ||
844 | case Opt_err: | ||
845 | return -EINVAL; | ||
846 | break; | ||
847 | } | ||
848 | return ret; | ||
849 | } | ||
850 | |||
851 | static struct trusted_key_options *trusted_options_alloc(void) | ||
852 | { | ||
853 | struct trusted_key_options *options; | ||
854 | |||
855 | options = kzalloc(sizeof *options, GFP_KERNEL); | ||
856 | if (!options) | ||
857 | return options; | ||
858 | |||
859 | /* set any non-zero defaults */ | ||
860 | options->keytype = SRK_keytype; | ||
861 | options->keyhandle = SRKHANDLE; | ||
862 | return options; | ||
863 | } | ||
864 | |||
865 | static struct trusted_key_payload *trusted_payload_alloc(struct key *key) | ||
866 | { | ||
867 | struct trusted_key_payload *p = NULL; | ||
868 | int ret; | ||
869 | |||
870 | ret = key_payload_reserve(key, sizeof *p); | ||
871 | if (ret < 0) | ||
872 | return p; | ||
873 | p = kzalloc(sizeof *p, GFP_KERNEL); | ||
874 | |||
875 | /* migratable by default */ | ||
876 | p->migratable = 1; | ||
877 | return p; | ||
878 | } | ||
879 | |||
880 | /* | ||
881 | * trusted_instantiate - create a new trusted key | ||
882 | * | ||
883 | * Unseal an existing trusted blob or, for a new key, get a | ||
884 | * random key, then seal and create a trusted key-type key, | ||
885 | * adding it to the specified keyring. | ||
886 | * | ||
887 | * On success, return 0. Otherwise return errno. | ||
888 | */ | ||
889 | static int trusted_instantiate(struct key *key, const void *data, | ||
890 | const size_t datalen) | ||
891 | { | ||
892 | struct trusted_key_payload *payload = NULL; | ||
893 | struct trusted_key_options *options = NULL; | ||
894 | char *datablob; | ||
895 | int ret = 0; | ||
896 | int key_cmd; | ||
897 | |||
898 | if (datalen <= 0 || datalen > 32767 || !data) | ||
899 | return -EINVAL; | ||
900 | |||
901 | datablob = kmalloc(datalen + 1, GFP_KERNEL); | ||
902 | if (!datablob) | ||
903 | return -ENOMEM; | ||
904 | memcpy(datablob, data, datalen); | ||
905 | datablob[datalen] = '\0'; | ||
906 | |||
907 | options = trusted_options_alloc(); | ||
908 | if (!options) { | ||
909 | ret = -ENOMEM; | ||
910 | goto out; | ||
911 | } | ||
912 | payload = trusted_payload_alloc(key); | ||
913 | if (!payload) { | ||
914 | ret = -ENOMEM; | ||
915 | goto out; | ||
916 | } | ||
917 | |||
918 | key_cmd = datablob_parse(datablob, payload, options); | ||
919 | if (key_cmd < 0) { | ||
920 | ret = key_cmd; | ||
921 | goto out; | ||
922 | } | ||
923 | |||
924 | dump_payload(payload); | ||
925 | dump_options(options); | ||
926 | |||
927 | switch (key_cmd) { | ||
928 | case Opt_load: | ||
929 | ret = key_unseal(payload, options); | ||
930 | dump_payload(payload); | ||
931 | dump_options(options); | ||
932 | if (ret < 0) | ||
933 | pr_info("trusted_key: key_unseal failed (%d)\n", ret); | ||
934 | break; | ||
935 | case Opt_new: | ||
936 | ret = my_get_random(payload->key, payload->key_len); | ||
937 | if (ret < 0) { | ||
938 | pr_info("trusted_key: key_create failed (%d)\n", ret); | ||
939 | goto out; | ||
940 | } | ||
941 | ret = key_seal(payload, options); | ||
942 | if (ret < 0) | ||
943 | pr_info("trusted_key: key_seal failed (%d)\n", ret); | ||
944 | break; | ||
945 | default: | ||
946 | ret = -EINVAL; | ||
947 | goto out; | ||
948 | } | ||
949 | if (!ret && options->pcrlock) | ||
950 | ret = pcrlock(options->pcrlock); | ||
951 | out: | ||
952 | kfree(datablob); | ||
953 | kfree(options); | ||
954 | if (!ret) | ||
955 | rcu_assign_pointer(key->payload.data, payload); | ||
956 | else | ||
957 | kfree(payload); | ||
958 | return ret; | ||
959 | } | ||
960 | |||
961 | static void trusted_rcu_free(struct rcu_head *rcu) | ||
962 | { | ||
963 | struct trusted_key_payload *p; | ||
964 | |||
965 | p = container_of(rcu, struct trusted_key_payload, rcu); | ||
966 | memset(p->key, 0, p->key_len); | ||
967 | kfree(p); | ||
968 | } | ||
969 | |||
970 | /* | ||
971 | * trusted_update - reseal an existing key with new PCR values | ||
972 | */ | ||
973 | static int trusted_update(struct key *key, const void *data, | ||
974 | const size_t datalen) | ||
975 | { | ||
976 | struct trusted_key_payload *p = key->payload.data; | ||
977 | struct trusted_key_payload *new_p; | ||
978 | struct trusted_key_options *new_o; | ||
979 | char *datablob; | ||
980 | int ret = 0; | ||
981 | |||
982 | if (!p->migratable) | ||
983 | return -EPERM; | ||
984 | if (datalen <= 0 || datalen > 32767 || !data) | ||
985 | return -EINVAL; | ||
986 | |||
987 | datablob = kmalloc(datalen + 1, GFP_KERNEL); | ||
988 | if (!datablob) | ||
989 | return -ENOMEM; | ||
990 | new_o = trusted_options_alloc(); | ||
991 | if (!new_o) { | ||
992 | ret = -ENOMEM; | ||
993 | goto out; | ||
994 | } | ||
995 | new_p = trusted_payload_alloc(key); | ||
996 | if (!new_p) { | ||
997 | ret = -ENOMEM; | ||
998 | goto out; | ||
999 | } | ||
1000 | |||
1001 | memcpy(datablob, data, datalen); | ||
1002 | datablob[datalen] = '\0'; | ||
1003 | ret = datablob_parse(datablob, new_p, new_o); | ||
1004 | if (ret != Opt_update) { | ||
1005 | ret = -EINVAL; | ||
1006 | goto out; | ||
1007 | } | ||
1008 | /* copy old key values, and reseal with new pcrs */ | ||
1009 | new_p->migratable = p->migratable; | ||
1010 | new_p->key_len = p->key_len; | ||
1011 | memcpy(new_p->key, p->key, p->key_len); | ||
1012 | dump_payload(p); | ||
1013 | dump_payload(new_p); | ||
1014 | |||
1015 | ret = key_seal(new_p, new_o); | ||
1016 | if (ret < 0) { | ||
1017 | pr_info("trusted_key: key_seal failed (%d)\n", ret); | ||
1018 | kfree(new_p); | ||
1019 | goto out; | ||
1020 | } | ||
1021 | if (new_o->pcrlock) { | ||
1022 | ret = pcrlock(new_o->pcrlock); | ||
1023 | if (ret < 0) { | ||
1024 | pr_info("trusted_key: pcrlock failed (%d)\n", ret); | ||
1025 | kfree(new_p); | ||
1026 | goto out; | ||
1027 | } | ||
1028 | } | ||
1029 | rcu_assign_pointer(key->payload.data, new_p); | ||
1030 | call_rcu(&p->rcu, trusted_rcu_free); | ||
1031 | out: | ||
1032 | kfree(datablob); | ||
1033 | kfree(new_o); | ||
1034 | return ret; | ||
1035 | } | ||
1036 | |||
1037 | /* | ||
1038 | * trusted_read - copy the sealed blob data to userspace in hex. | ||
1039 | * On success, return to userspace the trusted key datablob size. | ||
1040 | */ | ||
1041 | static long trusted_read(const struct key *key, char __user *buffer, | ||
1042 | size_t buflen) | ||
1043 | { | ||
1044 | struct trusted_key_payload *p; | ||
1045 | char *ascii_buf; | ||
1046 | char *bufp; | ||
1047 | int i; | ||
1048 | |||
1049 | p = rcu_dereference_protected(key->payload.data, | ||
1050 | rwsem_is_locked(&((struct key *)key)->sem)); | ||
1051 | if (!p) | ||
1052 | return -EINVAL; | ||
1053 | if (!buffer || buflen <= 0) | ||
1054 | return 2 * p->blob_len; | ||
1055 | ascii_buf = kmalloc(2 * p->blob_len, GFP_KERNEL); | ||
1056 | if (!ascii_buf) | ||
1057 | return -ENOMEM; | ||
1058 | |||
1059 | bufp = ascii_buf; | ||
1060 | for (i = 0; i < p->blob_len; i++) | ||
1061 | bufp = pack_hex_byte(bufp, p->blob[i]); | ||
1062 | if ((copy_to_user(buffer, ascii_buf, 2 * p->blob_len)) != 0) { | ||
1063 | kfree(ascii_buf); | ||
1064 | return -EFAULT; | ||
1065 | } | ||
1066 | kfree(ascii_buf); | ||
1067 | return 2 * p->blob_len; | ||
1068 | } | ||
1069 | |||
1070 | /* | ||
1071 | * trusted_destroy - before freeing the key, clear the decrypted data | ||
1072 | */ | ||
1073 | static void trusted_destroy(struct key *key) | ||
1074 | { | ||
1075 | struct trusted_key_payload *p = key->payload.data; | ||
1076 | |||
1077 | if (!p) | ||
1078 | return; | ||
1079 | memset(p->key, 0, p->key_len); | ||
1080 | kfree(key->payload.data); | ||
1081 | } | ||
1082 | |||
1083 | struct key_type key_type_trusted = { | ||
1084 | .name = "trusted", | ||
1085 | .instantiate = trusted_instantiate, | ||
1086 | .update = trusted_update, | ||
1087 | .match = user_match, | ||
1088 | .destroy = trusted_destroy, | ||
1089 | .describe = user_describe, | ||
1090 | .read = trusted_read, | ||
1091 | }; | ||
1092 | |||
1093 | EXPORT_SYMBOL_GPL(key_type_trusted); | ||
1094 | |||
1095 | static void trusted_shash_release(void) | ||
1096 | { | ||
1097 | if (hashalg) | ||
1098 | crypto_free_shash(hashalg); | ||
1099 | if (hmacalg) | ||
1100 | crypto_free_shash(hmacalg); | ||
1101 | } | ||
1102 | |||
1103 | static int __init trusted_shash_alloc(void) | ||
1104 | { | ||
1105 | int ret; | ||
1106 | |||
1107 | hmacalg = crypto_alloc_shash(hmac_alg, 0, CRYPTO_ALG_ASYNC); | ||
1108 | if (IS_ERR(hmacalg)) { | ||
1109 | pr_info("trusted_key: could not allocate crypto %s\n", | ||
1110 | hmac_alg); | ||
1111 | return PTR_ERR(hmacalg); | ||
1112 | } | ||
1113 | |||
1114 | hashalg = crypto_alloc_shash(hash_alg, 0, CRYPTO_ALG_ASYNC); | ||
1115 | if (IS_ERR(hashalg)) { | ||
1116 | pr_info("trusted_key: could not allocate crypto %s\n", | ||
1117 | hash_alg); | ||
1118 | ret = PTR_ERR(hashalg); | ||
1119 | goto hashalg_fail; | ||
1120 | } | ||
1121 | |||
1122 | return 0; | ||
1123 | |||
1124 | hashalg_fail: | ||
1125 | crypto_free_shash(hmacalg); | ||
1126 | return ret; | ||
1127 | } | ||
1128 | |||
1129 | static int __init init_trusted(void) | ||
1130 | { | ||
1131 | int ret; | ||
1132 | |||
1133 | ret = trusted_shash_alloc(); | ||
1134 | if (ret < 0) | ||
1135 | return ret; | ||
1136 | ret = register_key_type(&key_type_trusted); | ||
1137 | if (ret < 0) | ||
1138 | trusted_shash_release(); | ||
1139 | return ret; | ||
1140 | } | ||
1141 | |||
1142 | static void __exit cleanup_trusted(void) | ||
1143 | { | ||
1144 | trusted_shash_release(); | ||
1145 | unregister_key_type(&key_type_trusted); | ||
1146 | } | ||
1147 | |||
1148 | late_initcall(init_trusted); | ||
1149 | module_exit(cleanup_trusted); | ||
1150 | |||
1151 | MODULE_LICENSE("GPL"); | ||
diff --git a/security/keys/trusted_defined.h b/security/keys/trusted_defined.h new file mode 100644 index 00000000000..3249fbd2b65 --- /dev/null +++ b/security/keys/trusted_defined.h | |||
@@ -0,0 +1,134 @@ | |||
1 | #ifndef __TRUSTED_KEY_H | ||
2 | #define __TRUSTED_KEY_H | ||
3 | |||
4 | /* implementation specific TPM constants */ | ||
5 | #define MAX_PCRINFO_SIZE 64 | ||
6 | #define MAX_BUF_SIZE 512 | ||
7 | #define TPM_GETRANDOM_SIZE 14 | ||
8 | #define TPM_OSAP_SIZE 36 | ||
9 | #define TPM_OIAP_SIZE 10 | ||
10 | #define TPM_SEAL_SIZE 87 | ||
11 | #define TPM_UNSEAL_SIZE 104 | ||
12 | #define TPM_SIZE_OFFSET 2 | ||
13 | #define TPM_RETURN_OFFSET 6 | ||
14 | #define TPM_DATA_OFFSET 10 | ||
15 | |||
16 | #define LOAD32(buffer, offset) (ntohl(*(uint32_t *)&buffer[offset])) | ||
17 | #define LOAD32N(buffer, offset) (*(uint32_t *)&buffer[offset]) | ||
18 | #define LOAD16(buffer, offset) (ntohs(*(uint16_t *)&buffer[offset])) | ||
19 | |||
20 | struct tpm_buf { | ||
21 | int len; | ||
22 | unsigned char data[MAX_BUF_SIZE]; | ||
23 | }; | ||
24 | |||
25 | #define INIT_BUF(tb) (tb->len = 0) | ||
26 | |||
27 | struct osapsess { | ||
28 | uint32_t handle; | ||
29 | unsigned char secret[SHA1_DIGEST_SIZE]; | ||
30 | unsigned char enonce[TPM_NONCE_SIZE]; | ||
31 | }; | ||
32 | |||
33 | /* discrete values, but have to store in uint16_t for TPM use */ | ||
34 | enum { | ||
35 | SEAL_keytype = 1, | ||
36 | SRK_keytype = 4 | ||
37 | }; | ||
38 | |||
39 | struct trusted_key_options { | ||
40 | uint16_t keytype; | ||
41 | uint32_t keyhandle; | ||
42 | unsigned char keyauth[SHA1_DIGEST_SIZE]; | ||
43 | unsigned char blobauth[SHA1_DIGEST_SIZE]; | ||
44 | uint32_t pcrinfo_len; | ||
45 | unsigned char pcrinfo[MAX_PCRINFO_SIZE]; | ||
46 | int pcrlock; | ||
47 | }; | ||
48 | |||
49 | #define TPM_DEBUG 0 | ||
50 | |||
51 | #if TPM_DEBUG | ||
52 | static inline void dump_options(struct trusted_key_options *o) | ||
53 | { | ||
54 | pr_info("trusted_key: sealing key type %d\n", o->keytype); | ||
55 | pr_info("trusted_key: sealing key handle %0X\n", o->keyhandle); | ||
56 | pr_info("trusted_key: pcrlock %d\n", o->pcrlock); | ||
57 | pr_info("trusted_key: pcrinfo %d\n", o->pcrinfo_len); | ||
58 | print_hex_dump(KERN_INFO, "pcrinfo ", DUMP_PREFIX_NONE, | ||
59 | 16, 1, o->pcrinfo, o->pcrinfo_len, 0); | ||
60 | } | ||
61 | |||
62 | static inline void dump_payload(struct trusted_key_payload *p) | ||
63 | { | ||
64 | pr_info("trusted_key: key_len %d\n", p->key_len); | ||
65 | print_hex_dump(KERN_INFO, "key ", DUMP_PREFIX_NONE, | ||
66 | 16, 1, p->key, p->key_len, 0); | ||
67 | pr_info("trusted_key: bloblen %d\n", p->blob_len); | ||
68 | print_hex_dump(KERN_INFO, "blob ", DUMP_PREFIX_NONE, | ||
69 | 16, 1, p->blob, p->blob_len, 0); | ||
70 | pr_info("trusted_key: migratable %d\n", p->migratable); | ||
71 | } | ||
72 | |||
73 | static inline void dump_sess(struct osapsess *s) | ||
74 | { | ||
75 | print_hex_dump(KERN_INFO, "trusted-key: handle ", DUMP_PREFIX_NONE, | ||
76 | 16, 1, &s->handle, 4, 0); | ||
77 | pr_info("trusted-key: secret:\n"); | ||
78 | print_hex_dump(KERN_INFO, "", DUMP_PREFIX_NONE, | ||
79 | 16, 1, &s->secret, SHA1_DIGEST_SIZE, 0); | ||
80 | pr_info("trusted-key: enonce:\n"); | ||
81 | print_hex_dump(KERN_INFO, "", DUMP_PREFIX_NONE, | ||
82 | 16, 1, &s->enonce, SHA1_DIGEST_SIZE, 0); | ||
83 | } | ||
84 | |||
85 | static inline void dump_tpm_buf(unsigned char *buf) | ||
86 | { | ||
87 | int len; | ||
88 | |||
89 | pr_info("\ntrusted-key: tpm buffer\n"); | ||
90 | len = LOAD32(buf, TPM_SIZE_OFFSET); | ||
91 | print_hex_dump(KERN_INFO, "", DUMP_PREFIX_NONE, 16, 1, buf, len, 0); | ||
92 | } | ||
93 | #else | ||
94 | static inline void dump_options(struct trusted_key_options *o) | ||
95 | { | ||
96 | } | ||
97 | |||
98 | static inline void dump_payload(struct trusted_key_payload *p) | ||
99 | { | ||
100 | } | ||
101 | |||
102 | static inline void dump_sess(struct osapsess *s) | ||
103 | { | ||
104 | } | ||
105 | |||
106 | static inline void dump_tpm_buf(unsigned char *buf) | ||
107 | { | ||
108 | } | ||
109 | #endif | ||
110 | |||
111 | static inline void store8(struct tpm_buf *buf, const unsigned char value) | ||
112 | { | ||
113 | buf->data[buf->len++] = value; | ||
114 | } | ||
115 | |||
116 | static inline void store16(struct tpm_buf *buf, const uint16_t value) | ||
117 | { | ||
118 | *(uint16_t *) & buf->data[buf->len] = htons(value); | ||
119 | buf->len += sizeof value; | ||
120 | } | ||
121 | |||
122 | static inline void store32(struct tpm_buf *buf, const uint32_t value) | ||
123 | { | ||
124 | *(uint32_t *) & buf->data[buf->len] = htonl(value); | ||
125 | buf->len += sizeof value; | ||
126 | } | ||
127 | |||
128 | static inline void storebytes(struct tpm_buf *buf, const unsigned char *in, | ||
129 | const int len) | ||
130 | { | ||
131 | memcpy(buf->data + buf->len, in, len); | ||
132 | buf->len += len; | ||
133 | } | ||
134 | #endif | ||