aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* .gitignore: remove stale entry for generated version.hJonathan Austin2012-12-171-1/+0
| | | | | | | | | | | | | | | | Since userspace headers were moved to generated/uapi it possible to have a stale copy of linux/version.h at that file's old location. This causes confusion after building an older kernel version, then checking out and building a new one; the old (stale) version header will still get picked up until it is manually removed. This upsets the C library. Since the uapi changes, include/linux/version.h is no longer generated and should not be ignored, so this patch removes it from .gitignore. Signed-off-by: Jonathan Austin <jonathan.austin@arm.com> Reported-by: Kevin Petit <kevin.petit@arm.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* MODSIGN: Cleanup .gitignoreDavid Howells2012-10-191-6/+0
| | | | | | | | The module build process no longer creates intermediate files for module signing, so remove them from .gitignore. Signed-off-by: David Howells <dhowells@redhat.com> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* MODSIGN: Provide gitignore and make clean rules for extra filesDavid Howells2012-10-101-0/+14
| | | | | | | | | | Provide gitignore and make clean rules for extra files to hide and clean up the extra files produced by module signing stuff once it is added. Also add a clean up rule for the module content extractor program used to extract the data to be signed. Signed-off-by: David Howells <dhowells@redhat.com> Signed-off-by: Rusty Russell <rusty@rustcorp.com.au>
* gitignore: ignore debian build directoryGreg Dietsche2011-07-011-0/+5
| | | | | | | | Have git ignore the Debian directory created when running: make deb-pkg Signed-off-by: Greg Dietsche <Gregory.Dietsche@cuw.edu> Signed-off-by: Michal Marek <mmarek@suse.cz>
* kbuild: asm-generic supportSam Ravnborg2011-04-281-0/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | There is an increasing amount of header files shared between individual architectures in asm-generic. To avoid a lot of dummy wrapper files that just include the corresponding file in asm-generic provide some basic support in kbuild for this. With the following patch an architecture can maintain a list of files in the file arch/$(ARCH)/include/asm/Kbuild To use a generic file just add: generic-y += <name-of-header-file.h> For each file listed kbuild will generate the necessary wrapper in arch/$(ARCH)/include/generated/asm. When installing userspace headers a wrapper is likewise created. The original inspiration for this came from the unicore32 patchset - although a different method is used. The patch includes several improvements from Arnd Bergmann. Michael Marek contributed Makefile.asm-generic. Remis Baima did an intial implementation along to achive the same - see https://patchwork.kernel.org/patch/13352/ Signed-off-by: Sam Ravnborg <sam@ravnborg.org> Acked-by: Guan Xuetao <guanxuetao@mprc.pku.edu.cn> Tested-by: Guan Xuetao <guanxuetao@mprc.pku.edu.cn> Acked-by: Arnd Bergmann <arnd@arndb.de> Cc: Remis Lima Baima <remis.developer@googlemail.com> Signed-off-by: Michal Marek <mmarek@suse.cz>
* .gitignore: ignore *.xz filesRomain Francoise2011-02-221-0/+1
| | | | | | | | | | | | | | | Building with CONFIG_KERNEL_XZ results in the following: # Untracked files: # (use "git add <file>..." to include in what will be committed) # # arch/x86/boot/compressed/vmlinux.bin.xz So ignore xz-compressed files at the top level like we already do for other compression types. Signed-off-by: Romain Francoise <romain@orebokech.com> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* Merge branch 'for-35' of git://repo.or.cz/linux-kbuildLinus Torvalds2010-06-011-0/+1
|\ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | * 'for-35' of git://repo.or.cz/linux-kbuild: (81 commits) kbuild: Revert part of e8d400a to resolve a conflict kbuild: Fix checking of scm-identifier variable gconfig: add support to show hidden options that have prompts menuconfig: add support to show hidden options which have prompts gconfig: remove show_debug option gconfig: remove dbg_print_ptype() and dbg_print_stype() kconfig: fix zconfdump() kconfig: some small fixes add random binaries to .gitignore kbuild: Include gen_initramfs_list.sh and the file list in the .d file kconfig: recalc symbol value before showing search results .gitignore: ignore *.lzo files headerdep: perlcritic warning scripts/Makefile.lib: Align the output of LZO kbuild: Generate modules.builtin in make modules_install Revert "kbuild: specify absolute paths for cscope" kbuild: Do not unnecessarily regenerate modules.builtin headers_install: use local file handles headers_check: fix perl warnings export_report: fix perl warnings ...
| * .gitignore: ignore *.lzo filesPhilipp Kohlbecher2010-03-231-0/+1
| | | | | | | | | | | | | | Ignore files compressed with lzop. Signed-off-by: Philipp Kohlbecher <xt28@gmx.de> Signed-off-by: Michal Marek <mmarek@suse.cz>
* | Fix up .gitignore for top-level file patternsLinus Torvalds2010-03-121-8/+12
| | | | | | | | | | | | | | | | | | | | | | | | Some of the gitignore file patters were explicitly meant to be only for the top level, but weren't marked that way, so they would trigger recursively in subdirectories too. Normally that was harmless, but at least "linux" happened to trigger elsewhere too. Fix it up. And other patterns in that section weren't necessarily top-level at all. Reported-by: Jiri Slaby <jirislaby@gmail.com> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | um: tell git to ignore generated filesWANG Cong2010-03-061-0/+1
|/ | | | | | | | | | | | | | | Tell git to ignore the generated files under um, except: include/shared/kern_constants.h include/shared/user_constants.h which will be moved to include/generated. Signed-off-by: WANG Cong <xiyou.wangcong@gmail.com> Cc: Al Viro <viro@zeniv.linux.org.uk> Cc: Jeff Dike <jdike@addtoit.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* .gitignore: ignore vmlinuzFlorian Fainelli2010-01-111-0/+1
| | | | | | | | | | | MIPS compressed kernels output a vmlinuz file in the top-level directory (maybe others do). Add vmlinuz to the list of files to ignore by git. Signed-off-by: Florian Fainelli <ffainelli@freebox.fr> Cc: Ralf Baechle <ralf@linux-mips.org> Cc: Maxime Bizon <mbizon@freebox.fr> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* kbuild: generate modules.builtinMichal Marek2009-12-121-0/+1
| | | | | | | | | | | To make it easier for module-init-tools and scripts like mkinitrd to distinguish builtin and missing modules, install a modules.builtin file listing all builtin modules. This is done by generating an additional config file (tristate.conf) with tristate options set to uppercase 'Y' or 'M'. If we source that config file, the builtin modules appear in obj-Y. Signed-off-by: Michal Marek <mmarek@suse.cz>
* kbuild: move utsrelease.h to include/generatedSam Ravnborg2009-12-121-1/+0
| | | | | | | Fix up all users of utsrelease.h Signed-off-by: Sam Ravnborg <sam@ravnborg.org> Signed-off-by: Michal Marek <mmarek@suse.cz>
* kbuild: move autoconf.h to include/generatedSam Ravnborg2009-12-121-1/+0
| | | | | Signed-off-by: Sam Ravnborg <sam@ravnborg.org> Signed-off-by: Michal Marek <mmarek@suse.cz>
* kbuild: move compile.h to include/generatedSam Ravnborg2009-12-121-1/+0
| | | | | Signed-off-by: Sam Ravnborg <sam@ravnborg.org> Signed-off-by: Michal Marek <mmarek@suse.cz>
* kbuild: drop include/asmSam Ravnborg2009-12-121-1/+0
| | | | | | | | | | | | | | | We no longer use this directory for generated files and all architectures has moved their header files so no symlink tricks are needed either. Drop the symlink and drop the ARCH check. If we really need to check that the SRCARCH has not changed when we build a kernel we can add this check back - but then we will find a more convenient way to store the info. Signed-off-by: Sam Ravnborg <sam@ravnborg.org> Signed-off-by: Michal Marek <mmarek@suse.cz>
* kbuild: move asm-offsets.h to include/generatedSam Ravnborg2009-12-121-1/+0
| | | | | | | | | | | | | The simplest method was to add an extra asm-offsets.h file in arch/$ARCH/include/asm that references the generated file. We can now migrate the architectures one-by-one to reference the generated file direct - and when done we can delete the temporary arch/$ARCH/include/asm/asm-offsets.h file. Signed-off-by: Sam Ravnborg <sam@ravnborg.org> Cc: Al Viro <viro@zeniv.linux.org.uk> Signed-off-by: Michal Marek <mmarek@suse.cz>
* kbuild: move bounds.h to include/generatedSam Ravnborg2009-12-121-1/+0
| | | | | | Signed-off-by: Sam Ravnborg <sam@ravnborg.org> Cc: Al Viro <viro@zeniv.linux.org.uk> Signed-off-by: Michal Marek <mmarek@suse.cz>
* .gitignore: Add bzip2 compressed filesGertjan van Wingerde2009-11-301-0/+1
| | | | | | | We can have bzip2 compressed images nowadays. Signed-off-by: Gertjan van Wingerde <gwingerde@gmail.com> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* gitignore: ignore gcov output filesAmerigo Wang2009-06-261-0/+1
| | | | | | | Ignore *.gcno files which are generated by gcov. Signed-off-by: WANG Cong <xiyou.wangcong@gmail.com> Signed-off-by: Sam Ravnborg <sam@ravnborg.org>
* Merge branch 'master' of ↵Linus Torvalds2009-06-141-0/+8
|\ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/sam/kbuild-next * 'master' of git://git.kernel.org/pub/scm/linux/kernel/git/sam/kbuild-next: (53 commits) .gitignore: ignore *.lzma files kbuild: add generic --set-str option to scripts/config kbuild: simplify argument loop in scripts/config kbuild: handle non-existing options in scripts/config kallsyms: generalize text region handling kallsyms: support kernel symbols in Blackfin on-chip memory documentation: make version fix kbuild: fix a compile warning gitignore: Add GNU GLOBAL files to top .gitignore kbuild: fix delay in setlocalversion on readonly source README: fix misleading pointer to the defconf directory vmlinux.lds.h update kernel-doc: cleanup perl script Improve vmlinux.lds.h support for arch specific linker scripts kbuild: fix headers_exports with boolean expression kbuild/headers_check: refine extern check kbuild: fix "Argument list too long" error for "make headers_check", ignore *.patch files Remove bashisms from scripts menu: fix embedded menu presentation ...
| * .gitignore: ignore *.lzma filesArne Janbu2009-06-141-0/+1
| | | | | | | | Signed-off-by: Sam Ravnborg <sam@ravnborg.org>
| * gitignore: Add GNU GLOBAL files to top .gitignoreJani Nikula2009-06-141-0/+6
| | | | | | | | | | | | | | Ignore GPATH, GRTAGS, GSYMS, and GTAGS generated by GNU GLOBAL. Signed-off-by: Jani Nikula <ext-jani.1.nikula@nokia.com> Signed-off-by: Sam Ravnborg <sam@ravnborg.org>
| * ignore *.patch filesMike Frysinger2009-06-091-0/+1
| | | | | | | | | | Signed-off-by: Mike Frysinger <vapier@gentoo.org> Signed-off-by: Sam Ravnborg <sam@ravnborg.org>
* | trivial: Remove the hyphen from git commandsMatt Kraai2009-06-121-1/+1
|/ | | | | Signed-off-by: Matt Kraai <kraai@ftbfs.org> Signed-off-by: Jiri Kosina <jkosina@suse.cz>
* kbuild: support include/generatedSam Ravnborg2009-04-191-0/+1
| | | | | | | | | | | | | | | | | | | | | | | | We need a location for generated files. Today they are spread over several places and bringing them together to a common place makes it obvious hat is generated and what isreal files. Al Viro originally suggested: include/gen Linus suggested to spell it out. This patch implement support for include/generated All files in include/generated are ignored by git. include/generated is removed during "make mrproper". With this we are ready to implement support for include/generated in the various architctures and in the base kernel. Signed-off-by: Sam Ravnborg <sam@ravnborg.org> Cc: Al Viro <viro@ZenIV.linux.org.uk> Cc: Linus Torvalds <torvalds@linux-foundation.org>
* Fix and clean top .gitignoreEduard - Gabriel Munteanu2008-06-291-3/+9
| | | | | | | | | | Removed vmlinux* rule because it matches too many useful files, replacing it with rules matching filetype by filename (e.g. *.gz). Also unignored .mailmap from the top directory. Added a comment telling the user how to check for tracked files being ignored. Signed-off-by: Eduard - Gabriel Munteanu <eduard.munteanu@linux360.ro> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* Unignore vmlinux.lds.h from Git.Eduard - Gabriel Munteanu2008-06-171-0/+1
| | | | | | | | Added !vmlinux.lds.h to .gitignore because it would otherwise be ignored. Signed-off-by: Eduard - Gabriel Munteanu <eduard.munteanu@linux360.ro> Acked-by: Mathieu Desnoyers <mathieu.desnoyers@polymtl.ca> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* .gitignore: match ncscope.outJike Song2008-05-251-0/+1
| | | | | | | | | | | | | | | | | | | Sometimes I got this: $ git-status {snip} # On branch master # Untracked files: # (use "git add <file>..." to include in what will be committed) # # ncscope.out nothing added to commit but untracked files present (use "git add" to track) Fix it. Signed-off-by: Jike Song <albcamus@gmail.com> Signed-off-by: Sam Ravnborg <sam@ravnborg.org>
* Remove *.rej pattern from .gitignoreS.Çağlar Onur2008-05-111-1/+0
| | | | | | | | | | | | | | | | | | With commit 3f1b0e1f287547903f11fa1e6de7d2765597766e ".gitignore update" Linus's current git tree starts to ignore any "*.rej" files. So "git status" no longer shows these files, but the ones who works with quilt patchsets, this not makes life easier as expected. Because sometimes a work flow (at least for me) requires "quilt push -f" followed by "git status" to see unresolved merge conflicts, work on these conflicts to correct them and finalize the patch with "quilt refresh". And if there are some "*.rej" files exists in tree, for whatever reason, this means something goes really wrong there and i think this situation not deserves to be ignored. Signed-off-by: S.Çağlar Onur <caglar@pardus.org.tr> Signed-off-by: Sam Ravnborg <sam@ravnborg.org>
* Update .gitignore to include include/linux/bounds.hTheodore Ts'o2008-04-301-0/+1
| | | | | | | (which is autogenerated by kbuild) Signed-off-by: "Theodore Ts'o" <tytso@mit.edu> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* Update .gitignore filesMatthew Wilcox2008-04-251-0/+1
| | | | | | | Add some autogenerated files to various .gitignore files Signed-off-by: Matthew Wilcox <willy@linux.intel.com> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* .gitignore: ignore emacs backup and temporary files.Chris Dearman2008-03-041-0/+2
| | | | | | | Signed-off-by: Chris Dearman <chris@mips.com> Signed-off-by: Ralf Baechle <ralf@linux-mips.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* kbuild: ignore *.order filesSam Ravnborg2008-01-281-0/+1
| | | | | | | | Introducing the new modules.order patch created a number of additional files. Teach git to ignore them. Signed-off-by: Sam Ravnborg <sam@ravnborg.org> Acked-by: Tejun Heo <htejun@gmail.com>
* x86: update .gitignore entriesThomas Gleixner2007-10-191-0/+1
| | | | | | | | | | | vdso / vsycall create .so.dbg files now. Add *.so.dbg to the main .ignore file Exclude the compile time created boot directory in arch/x86_64 as well Signed-off-by: Thomas Gleixner <tglx@linutronix.de> Signed-off-by: Ingo Molnar <mingo@elte.hu>
* .gitignore update for x86 archDenis V. Lunev2007-10-171-0/+1
| | | | | | | | | This patch: - makes .gitignore files visible to git - makes arch/x86/kernel/vsyscall_32.lds and arch/i386/boot invisible Signed-off-by: Denis V. Lunev <den@openvz.org> Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
* .gitignore updateAlexey Dobriyan2007-07-311-0/+1
| | | | | | | | | | | | | | | | | | Somehow I ended up with the following in tree: $ git status ... # Untracked files: # (use "git add <file>..." to include in what will be committed) # # fs/proc/root.o.FuMxJQ # net/ipv4/tcp_minisocks.o.geCDYR These are presumably temporary gcc files, which aren't interesting. Signed-off-by: Alexey Dobriyan <adobriyan@sw.ru> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* Un-ignore "vmlinux.lds.S" in .gitignoreLinus Torvalds2007-07-201-0/+1
| | | | | | | | | | | | | We ignore all the generated files called "vmlinux*" from the top-level gitignore, but that also ends up catching a few files that we track, and that people do edit. Notably the "vmlinux.lds.S" file, that each architecture has. You can always use "git add -f" to override the ignore file, but we might as well just make it explicit for this file. Bitten-by-and-tested-by: Ingo Molnar <mingo@elte.hu> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* .gitignore updateAlexey Dobriyan2007-07-161-0/+3
| | | | | | | | | | | | headers_install by default puts headers into usr/include/ . They're auto-generated, so should be ignored. Same for *.orig, *.rej . Signed-off-by: Alexey Dobriyan <adobriyan@sw.ru> Cc: David Woodhouse <dwmw2@infradead.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* [PATCH] Add cscope generated files to .gitignoreTobias Klauser2006-12-221-0/+3
| | | | | | | | Ignore files generated by 'make cscope' Signed-off-by: Tobias Klauser <tklauser@distanz.ch> Signed-off-by: Andrew Morton <akpm@osdl.org> Signed-off-by: Linus Torvalds <torvalds@osdl.org>
* [PATCH] .gitignore: add miscellaneous filesFranck Bui-Huu2006-11-131-0/+1
| | | | | | | | | | | | | | | | | Prevent git from reporting this useless status: On branch refs/heads/master Untracked files: (use "git add" to add to commit) TAGS scripts/kconfig/lkc_defs.h scripts/kconfig/qconf.moc nothing to commit Signed-off-by: Franck Bui-Huu <fbuihuu@gmail.com> Signed-off-by: Andrew Morton <akpm@osdl.org> Signed-off-by: Linus Torvalds <torvalds@osdl.org>
* [PATCH] Add symbol type files (*.symtypes) to .gitignoreJosh Triplett2006-09-161-0/+1
| | | | | | | | | The kernel build system supports making symbol type files (*.symtypes) from C source files. Add these files to .gitignore. Signed-off-by: Josh Triplett <josh@freedesktop.org> Signed-off-by: Andrew Morton <akpm@osdl.org> Signed-off-by: Linus Torvalds <torvalds@osdl.org>
* [PATCH] Add mixed source and assembly listings (*.lst) to .gitignoreJosh Triplett2006-09-161-0/+1
| | | | | | | | | The kernel build system supports making mixed source and assembly listings (*.lst) from C source files. Add these files to .gitignore. Signed-off-by: Josh Triplett <josh@freedesktop.org> Signed-off-by: Andrew Morton <akpm@osdl.org> Signed-off-by: Linus Torvalds <torvalds@osdl.org>
* [PATCH] Add preprocessed files (*.i) to .gitignoreJosh Triplett2006-09-161-0/+1
| | | | | | | | | The kernel build system supports making preprocessed files (*.i) from C source files. Add these files to .gitignore. Signed-off-by: Josh Triplett <josh@freedesktop.org> Signed-off-by: Andrew Morton <akpm@osdl.org> Signed-off-by: Linus Torvalds <torvalds@osdl.org>
* gitignore: gitignore quilt's filesQi Yong2006-08-011-0/+4
| | | | | | | gitignore: ignore quilt's files. Signed-off-by: Qi Yong <qiyong@fc-cn.com> Signed-off-by: Sam Ravnborg <sam@ravnborg.org>
* kbuild: .gitignore utsrelease.hSam Ravnborg2006-08-011-0/+1
| | | | Signed-off-by: Sam Ravnborg <sam@ravnborg.org>
* add "tags" to .gitignoreUwe Zeisberger2006-03-211-0/+1
| | | | | Signed-off-by: Uwe Zeisberger <Uwe_Zeisberger@digi.com> Signed-off-by: Adrian Bunk <bunk@stusta.de>
* V4L/DVB (3300b): .gitignore should also ignore StGit generated dirsMauro Carvalho Chehab2006-02-261-0/+2
| | | | | | | StGit genreates patches-* when you run stg export command. It makes no sense to show such directories as changes on git status. Signed-off-by: Mauro Carvalho Chehab <mchehab@infradead.org>
* gitignore: ignore shared objectsBrian Gerst2006-01-061-0/+1
| | | | | | | Many arches make shared objects for VDSOs. Generally exclude them. Signed-off-by: Brian Gerst <bgerst@didntduck.org> Signed-off-by: Sam Ravnborg <sam@ravnborg.org>
* gitignore: asm-offsets.hBrian Gerst2006-01-011-0/+1
| | | | | | | Ignore asm-offsets.h for all arches. Signed-off-by: Brian Gerst <bgerst@didntduck.org> Signed-off-by: Sam Ravnborg <sam@ravnborg.org>