aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* Merge branch 'merge' of ↵HEADmasterLinus Torvalds2013-03-0510-19/+17
|\ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/benh/powerpc Pull powerpc fixes from Ben Herrenschmidt: "Here are a few powerpc bits & fixes for rc1. A couple of str*cpy fixes, some fixes in handling the FSCR register on Power8 (controls the enabling of processor features), a 32-bit build fix and a couple more nits." * 'merge' of git://git.kernel.org/pub/scm/linux/kernel/git/benh/powerpc: powerpc: Set DSCR bit in FSCR setup powerpc: Add DSCR FSCR register bit definition powerpc: Fix setting FSCR for HV=0 and on secondary CPUs powerpc: Wireup the kcmp syscall to sys_ni powerpc: Remove unused BITOP_LE_SWIZZLE macro powerpc: Avoid link stack corruption in MMU on syscall entry path drivers/tty/hvc: Use strlcpy instead of strncpy powerpc/pseries/hvcserver: Fix strncpy buffer limit in location code powerpc: Fix compile of sha1-powerpc-asm.S on 32-bit
| * powerpc: Set DSCR bit in FSCR setupMichael Neuling2013-03-041-1/+1
| | | | | | | | | | | | | | | | | | | | We support DSCR (Data Stream Control Register) so we should make sure we set it in the FSCR (Facility Status & Control Register) incase some firmwares don't set it. If we don't set this, we'll take a facility unavailable exception when using the DSCR. Signed-off-by: Michael Neuling <mikey@neuling.org> Signed-off-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
| * powerpc: Add DSCR FSCR register bit definitionMichael Neuling2013-03-041-1/+2
| | | | | | | | | | | | | | | | | | | | This sets the DSCR (Data Stream Control Register) in the FSCR (Facility Status & Control Register). Also harmonise TAR (Target Address Register) FSCR bit definition too. Signed-off-by: Michael Neuling <mikey@neuling.org> Signed-off-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
| * powerpc: Fix setting FSCR for HV=0 and on secondary CPUsMichael Neuling2013-03-041-1/+2
| | | | | | | | | | | | | | | | | | | | | | | | Currently we only set the FSCR (Facility Status and Control Register) when HV=1 but this feature is available when HV=0 also. This patch sets FSCR when HV=0. Also, we currently only set the FSCR on the master CPU. This patch also sets the FSCR on secondary CPUs. Signed-off-by: Michael Neuling <mikey@neuling.org> cc: Ian Munsie <imunsie@au1.ibm.com> Signed-off-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
| * powerpc: Wireup the kcmp syscall to sys_niTony Breeds2013-03-043-1/+3
| | | | | | | | | | | | | | | | | | Since kmp takes 2 unsigned long args there should be a compat wrapper. Since one isn't provided I think it's safer just to hook this up to not implemented. If we need it later we can do it properly then. Signed-off-by: Tony Breeds <tony@bakeyournoodle.com> Signed-off-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
| * powerpc: Remove unused BITOP_LE_SWIZZLE macroAkinobu Mita2013-03-041-2/+0
| | | | | | | | | | | | | | | | | | | | | | | | The BITOP_LE_SWIZZLE macro was used in the little-endian bitops functions for powerpc. But these functions were converted to generic bitops and the BITOP_LE_SWIZZLE is not used anymore. Signed-off-by: Akinobu Mita <akinobu.mita@gmail.com> Cc: Benjamin Herrenschmidt <benh@kernel.crashing.org> Cc: Paul Mackerras <paulus@samba.org> Cc: linuxppc-dev@lists.ozlabs.org Signed-off-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
| * powerpc: Avoid link stack corruption in MMU on syscall entry pathMichael Neuling2013-03-041-2/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Currently we use the link register to branch up high in the early MMU on syscall entry path. Unfortunately, this trashes the link stack as the address we are going to is not associated with the earlier mflr. This patch simply converts us to used the count register (volatile over syscalls anyway) instead. This is much better at predicting in this scenario and doesn't trash link stack causing a bunch of additional branch mispredicts later. Benchmarking this on POWER8 saves a bunch of cycles on Anton's null syscall benchmark here: http://ozlabs.org/~anton/junkcode/null_syscall.c Signed-off-by: Michael Neuling <mikey@neuling.org> Signed-off-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
| * drivers/tty/hvc: Use strlcpy instead of strncpyChen Gang2013-03-041-7/+2
| | | | | | | | | | | | | | | | | | when strlen pi->location_code is larger than HVCS_CLC_LENGTH + 1, original implementation can not let hvcsd->p_location_code NUL terminated. so need fix it (also can simplify the code) Signed-off-by: Chen Gang <gang.chen@asianux.com> Signed-off-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
| * powerpc/pseries/hvcserver: Fix strncpy buffer limit in location codeChen Gang2013-03-041-2/+3
| | | | | | | | | | | | | | | | | | the dest buf len is 80 (HVCS_CLC_LENGTH + 1). the src buf len is PAGE_SIZE. if src buf string len is more than 80, it will cause issue. Signed-off-by: Chen Gang <gang.chen@asianux.com> Signed-off-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
| * powerpc: Fix compile of sha1-powerpc-asm.S on 32-bitTony Breeds2013-03-041-2/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | When building with CRYPTO_SHA1_PPC enabled we fail with: powerpc/crypto/sha1-powerpc-asm.S: Assembler messages: powerpc/crypto/sha1-powerpc-asm.S:116: Error: can't resolve `0' {*ABS* section} - `STACKFRAMESIZE' {*UND* section} powerpc/crypto/sha1-powerpc-asm.S:116: Error: expression too complex powerpc/crypto/sha1-powerpc-asm.S:178: Error: unsupported relocation against STACKFRAMESIZE Use INT_FRAME_SIZE instead of STACKFRAMESIZE. Signed-off-by: Tony Breeds <tony@bakeyournoodle.com> Tested-by: Christian Kujau <lists@nerdbynature.de> Signed-off-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
* | Merge tag 'fixes-for-linus' of ↵Linus Torvalds2013-03-051-3/+16
|\ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/rusty/linux Pull virtio hwrng fix from Rusty Russell: "Nasty side-effect of vmalloc'ing modules: their static vars cannot be put into scatterlists. Jens has a check queued for this, so it shouldn't happen again. We could fix this in virtio_rng, but it's actually far easier to just do it in the core" * tag 'fixes-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/rusty/linux: hw_random: make buffer usable in scatterlist.
| * | hw_random: make buffer usable in scatterlist.Rusty Russell2013-03-041-3/+16
| |/ | | | | | | | | | | | | | | | | | | | | | | | | | | | | virtio_rng feeds the randomness buffer handed by the core directly into the scatterlist, since commit bb347d98079a547e80bd4722dee1de61e4dca0e8. However, if CONFIG_HW_RANDOM=m, the static buffer isn't a linear address (at least on most archs). We could fix this in virtio_rng, but it's actually far easier to just do it in the core as virtio_rng would have to allocate a buffer every time (it doesn't know how much the core will want to read). Reported-by: Aurelien Jarno <aurelien@aurel32.net> Tested-by: Aurelien Jarno <aurelien@aurel32.net> Signed-off-by: Rusty Russell <rusty@rustcorp.com.au> Cc: stable@kernel.org
* | Merge git://git.kernel.org/pub/scm/linux/kernel/git/davem/netLinus Torvalds2013-03-0559-334/+2083
|\ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Pull networking fixes from David Miller: "A moderately sized pile of fixes, some specifically for merge window introduced regressions although others are for longer standing items and have been queued up for -stable. I'm kind of tired of all the RDS protocol bugs over the years, to be honest, it's way out of proportion to the number of people who actually use it. 1) Fix missing range initialization in netfilter IPSET, from Jozsef Kadlecsik. 2) ieee80211_local->tim_lock needs to use BH disabling, from Johannes Berg. 3) Fix DMA syncing in SFC driver, from Ben Hutchings. 4) Fix regression in BOND device MAC address setting, from Jiri Pirko. 5) Missing usb_free_urb in ISDN Hisax driver, from Marina Makienko. 6) Fix UDP checksumming in bnx2x driver for 57710 and 57711 chips, fix from Dmitry Kravkov. 7) Missing cfgspace_lock initialization in BCMA driver. 8) Validate parameter size for SCTP assoc stats getsockopt(), from Guenter Roeck. 9) Fix SCTP association hangs, from Lee A Roberts. 10) Fix jumbo frame handling in r8169, from Francois Romieu. 11) Fix phy_device memory leak, from Petr Malat. 12) Omit trailing FCS from frames received in BGMAC driver, from Hauke Mehrtens. 13) Missing socket refcount release in L2TP, from Guillaume Nault. 14) sctp_endpoint_init should respect passed in gfp_t, rather than use GFP_KERNEL unconditionally. From Dan Carpenter. 15) Add AISX AX88179 USB driver, from Freddy Xin. 16) Remove MAINTAINERS entries for drivers deleted during the merge window, from Cesar Eduardo Barros. 17) RDS protocol can try to allocate huge amounts of memory, check that the user's request length makes sense, from Cong Wang. 18) SCTP should use the provided KMALLOC_MAX_SIZE instead of it's own, bogus, definition. From Cong Wang. 19) Fix deadlocks in FEC driver by moving TX reclaim into NAPI poll, from Frank Li. Also, fix a build error introduced in the merge window. 20) Fix bogus purging of default routes in ipv6, from Lorenzo Colitti. 21) Don't double count RTT measurements when we leave the TCP receive fast path, from Neal Cardwell." * git://git.kernel.org/pub/scm/linux/kernel/git/davem/net: (61 commits) tcp: fix double-counted receiver RTT when leaving receiver fast path CAIF: fix sparse warning for caif_usb rds: simplify a warning message net: fec: fix build error in no MXC platform net: ipv6: Don't purge default router if accept_ra=2 net: fec: put tx to napi poll function to fix dead lock sctp: use KMALLOC_MAX_SIZE instead of its own MAX_KMALLOC_SIZE rds: limit the size allocated by rds_message_alloc() MAINTAINERS: remove eexpress MAINTAINERS: remove drivers/net/wan/cycx* MAINTAINERS: remove 3c505 caif_dev: fix sparse warnings for caif_flow_cb ax88179_178a: ASIX AX88179_178A USB 3.0/2.0 to gigabit ethernet adapter driver sctp: use the passed in gfp flags instead GFP_KERNEL ipv[4|6]: correct dropwatch false positive in local_deliver_finish l2tp: Restore socket refcount when sendmsg succeeds net/phy: micrel: Disable asymmetric pause for KSZ9021 bgmac: omit the fcs phy: Fix phy_device_free memory leak bnx2x: Fix KR2 work-around condition ...
| * | tcp: fix double-counted receiver RTT when leaving receiver fast pathNeal Cardwell2013-03-041-3/+3
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | We should not update ts_recent and call tcp_rcv_rtt_measure_ts() both before and after going to step5. That wastes CPU and double-counts the receiver-side RTT sample. Signed-off-by: Neal Cardwell <ncardwell@google.com> Acked-by: Eric Dumazet <edumazet@google.com> Signed-off-by: David S. Miller <davem@davemloft.net>
| * | CAIF: fix sparse warning for caif_usbSilviu-Mihai Popescu2013-03-041-2/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | This fixes the following sparse warning: net/caif/caif_usb.c:84:16: warning: symbol 'cfusbl_create' was not declared. Should it be static? Signed-off-by: Silviu-Mihai Popescu <silviupopescu1990@gmail.com> Signed-off-by: David S. Miller <davem@davemloft.net>
| * | rds: simplify a warning messageCong Wang2013-03-041-4/+1
| | | | | | | | | | | | | | | | | | | | | Cc: David S. Miller <davem@davemloft.net> Cc: Venkat Venkatsubra <venkat.x.venkatsubra@oracle.com> Signed-off-by: Cong Wang <amwang@redhat.com> Signed-off-by: David S. Miller <davem@davemloft.net>
| * | net: fec: fix build error in no MXC platformFrank Li2013-03-041-8/+7
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | build error cause by Commit ff43da86c69d76a726ffe7d1666148960dc1d108 ("NET: FEC: dynamtic check DMA desc buff type") drivers/net/ethernet/freescale/fec.c: In function ‘fec_enet_get_nextdesc’: drivers/net/ethernet/freescale/fec.c:215:18: error: invalid use of undefined type ‘struct bufdesc_ex’ drivers/net/ethernet/freescale/fec.c: In function ‘fec_enet_get_prevdesc’: drivers/net/ethernet/freescale/fec.c:224:18: error: invalid use of undefined type ‘struct bufdesc_ex’ drivers/net/ethernet/freescale/fec.c: In function ‘fec_enet_start_xmit’: drivers/net/ethernet/freescale/fec.c:286:37: error: arithmetic on pointer to an incomplete type drivers/net/ethernet/freescale/fec.c:287:13: error: arithmetic on pointer to an incomplete type drivers/net/ethernet/freescale/fec.c:324:7: error: dereferencing pointer to incomplete type etc.... Signed-off-by: Frank Li <Frank.Li@freescale.com> Signed-off-by: David S. Miller <davem@davemloft.net>
| * | net: ipv6: Don't purge default router if accept_ra=2Lorenzo Colitti2013-03-041-1/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Setting net.ipv6.conf.<interface>.accept_ra=2 causes the kernel to accept RAs even when forwarding is enabled. However, enabling forwarding purges all default routes on the system, breaking connectivity until the next RA is received. Fix this by not purging default routes on interfaces that have accept_ra=2. Signed-off-by: Lorenzo Colitti <lorenzo@google.com> Acked-by: YOSHIFUJI Hideaki <yoshfuji@linux-ipv6.org> Acked-by: Eric Dumazet <edumazet@google.com> Signed-off-by: David S. Miller <davem@davemloft.net>
| * | net: fec: put tx to napi poll function to fix dead lockFrank Li2013-03-042-47/+41
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | up stack ndo_start_xmit already hold lock. fec_enet_start_xmit needn't spin lock. stat_xmit just update fep->cur_tx fec_enet_tx just update fep->dirty_tx Reserve a empty bdb to check full or empty cur_tx == dirty_tx means full cur_tx == dirty_tx +1 means empty So needn't is_full variable. Fix spin lock deadlock ================================= [ INFO: inconsistent lock state ] 3.8.0-rc5+ #107 Not tainted --------------------------------- inconsistent {HARDIRQ-ON-W} -> {IN-HARDIRQ-W} usage. ptp4l/615 [HC1[1]:SC0[0]:HE0:SE1] takes: (&(&list->lock)->rlock#3){?.-...}, at: [<8042c3c4>] skb_queue_tail+0x20/0x50 {HARDIRQ-ON-W} state was registered at: [<80067250>] mark_lock+0x154/0x4e8 [<800676f4>] mark_irqflags+0x110/0x1a4 [<80069208>] __lock_acquire+0x494/0x9c0 [<80069ce8>] lock_acquire+0x90/0xa4 [<80527ad0>] _raw_spin_lock_bh+0x44/0x54 [<804877e0>] first_packet_length+0x38/0x1f0 [<804879e4>] udp_poll+0x4c/0x5c [<804231f8>] sock_poll+0x24/0x28 [<800d27f0>] do_poll.isra.10+0x120/0x254 [<800d36e4>] do_sys_poll+0x15c/0x1e8 [<800d3828>] sys_poll+0x60/0xc8 [<8000e780>] ret_fast_syscall+0x0/0x3c *** DEADLOCK *** 1 lock held by ptp4l/615: #0: (&(&fep->hw_lock)->rlock){-.-...}, at: [<80355f9c>] fec_enet_tx+0x24/0x268 stack backtrace: Backtrace: [<800121e0>] (dump_backtrace+0x0/0x10c) from [<80516210>] (dump_stack+0x18/0x1c) r6:8063b1fc r5:bf38b2f8 r4:bf38b000 r3:bf38b000 [<805161f8>] (dump_stack+0x0/0x1c) from [<805189d0>] (print_usage_bug.part.34+0x164/0x1a4) [<8051886c>] (print_usage_bug.part.34+0x0/0x1a4) from [<80518a88>] (print_usage_bug+0x78/0x88) r8:80065664 r7:bf38b2f8 r6:00000002 r5:00000000 r4:bf38b000 [<80518a10>] (print_usage_bug+0x0/0x88) from [<80518b58>] (mark_lock_irq+0xc0/0x270) r7:bf38b000 r6:00000002 r5:bf38b2f8 r4:00000000 [<80518a98>] (mark_lock_irq+0x0/0x270) from [<80067270>] (mark_lock+0x174/0x4e8) [<800670fc>] (mark_lock+0x0/0x4e8) from [<80067744>] (mark_irqflags+0x160/0x1a4) [<800675e4>] (mark_irqflags+0x0/0x1a4) from [<80069208>] (__lock_acquire+0x494/0x9c0) r5:00000002 r4:bf38b2f8 [<80068d74>] (__lock_acquire+0x0/0x9c0) from [<80069ce8>] (lock_acquire+0x90/0xa4) [<80069c58>] (lock_acquire+0x0/0xa4) from [<805278d8>] (_raw_spin_lock_irqsave+0x4c/0x60) [<8052788c>] (_raw_spin_lock_irqsave+0x0/0x60) from [<8042c3c4>] (skb_queue_tail+0x20/0x50) r6:bfbb2180 r5:bf1d0190 r4:bf1d0184 [<8042c3a4>] (skb_queue_tail+0x0/0x50) from [<8042c4cc>] (sock_queue_err_skb+0xd8/0x188) r6:00000056 r5:bfbb2180 r4:bf1d0000 r3:00000000 [<8042c3f4>] (sock_queue_err_skb+0x0/0x188) from [<8042d15c>] (skb_tstamp_tx+0x70/0xa0) r6:bf0dddb0 r5:bf1d0000 r4:bfbb2180 r3:00000004 [<8042d0ec>] (skb_tstamp_tx+0x0/0xa0) from [<803561d0>] (fec_enet_tx+0x258/0x268) r6:c089d260 r5:00001c00 r4:bfbd0000 [<80355f78>] (fec_enet_tx+0x0/0x268) from [<803562cc>] (fec_enet_interrupt+0xec/0xf8) [<803561e0>] (fec_enet_interrupt+0x0/0xf8) from [<8007d5b0>] (handle_irq_event_percpu+0x54/0x1a0) [<8007d55c>] (handle_irq_event_percpu+0x0/0x1a0) from [<8007d740>] (handle_irq_event+0x44/0x64) [<8007d6fc>] (handle_irq_event+0x0/0x64) from [<80080690>] (handle_fasteoi_irq+0xc4/0x15c) r6:bf0dc000 r5:bf811290 r4:bf811240 r3:00000000 [<800805cc>] (handle_fasteoi_irq+0x0/0x15c) from [<8007ceec>] (generic_handle_irq+0x28/0x38) r5:807130c8 r4:00000096 [<8007cec4>] (generic_handle_irq+0x0/0x38) from [<8000f16c>] (handle_IRQ+0x54/0xb4) r4:8071d280 r3:00000180 [<8000f118>] (handle_IRQ+0x0/0xb4) from [<80008544>] (gic_handle_irq+0x30/0x64) r8:8000e924 r7:f4000100 r6:bf0ddef8 r5:8071c974 r4:f400010c r3:00000000 [<80008514>] (gic_handle_irq+0x0/0x64) from [<8000e2e4>] (__irq_svc+0x44/0x5c) Exception stack(0xbf0ddef8 to 0xbf0ddf40) Signed-off-by: Frank Li <Frank.Li@freescale.com> Signed-off-by: David S. Miller <davem@davemloft.net>
| * | sctp: use KMALLOC_MAX_SIZE instead of its own MAX_KMALLOC_SIZECong Wang2013-03-041-5/+3
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Don't definite its own MAX_KMALLOC_SIZE, use the one defined in mm. Cc: Vlad Yasevich <vyasevich@gmail.com> Cc: Sridhar Samudrala <sri@us.ibm.com> Cc: Neil Horman <nhorman@tuxdriver.com> Cc: David S. Miller <davem@davemloft.net> Signed-off-by: Cong Wang <amwang@redhat.com> Acked-by: Neil Horman <nhorman@tuxdriver.com> Signed-off-by: David S. Miller <davem@davemloft.net>
| * | rds: limit the size allocated by rds_message_alloc()Cong Wang2013-03-041-0/+3
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Dave Jones reported the following bug: "When fed mangled socket data, rds will trust what userspace gives it, and tries to allocate enormous amounts of memory larger than what kmalloc can satisfy." WARNING: at mm/page_alloc.c:2393 __alloc_pages_nodemask+0xa0d/0xbe0() Hardware name: GA-MA78GM-S2H Modules linked in: vmw_vsock_vmci_transport vmw_vmci vsock fuse bnep dlci bridge 8021q garp stp mrp binfmt_misc l2tp_ppp l2tp_core rfcomm s Pid: 24652, comm: trinity-child2 Not tainted 3.8.0+ #65 Call Trace: [<ffffffff81044155>] warn_slowpath_common+0x75/0xa0 [<ffffffff8104419a>] warn_slowpath_null+0x1a/0x20 [<ffffffff811444ad>] __alloc_pages_nodemask+0xa0d/0xbe0 [<ffffffff8100a196>] ? native_sched_clock+0x26/0x90 [<ffffffff810b2128>] ? trace_hardirqs_off_caller+0x28/0xc0 [<ffffffff810b21cd>] ? trace_hardirqs_off+0xd/0x10 [<ffffffff811861f8>] alloc_pages_current+0xb8/0x180 [<ffffffff8113eaaa>] __get_free_pages+0x2a/0x80 [<ffffffff811934fe>] kmalloc_order_trace+0x3e/0x1a0 [<ffffffff81193955>] __kmalloc+0x2f5/0x3a0 [<ffffffff8104df0c>] ? local_bh_enable_ip+0x7c/0xf0 [<ffffffffa0401ab3>] rds_message_alloc+0x23/0xb0 [rds] [<ffffffffa04043a1>] rds_sendmsg+0x2b1/0x990 [rds] [<ffffffff810b21cd>] ? trace_hardirqs_off+0xd/0x10 [<ffffffff81564620>] sock_sendmsg+0xb0/0xe0 [<ffffffff810b2052>] ? get_lock_stats+0x22/0x70 [<ffffffff810b24be>] ? put_lock_stats.isra.23+0xe/0x40 [<ffffffff81567f30>] sys_sendto+0x130/0x180 [<ffffffff810b872d>] ? trace_hardirqs_on+0xd/0x10 [<ffffffff816c547b>] ? _raw_spin_unlock_irq+0x3b/0x60 [<ffffffff816cd767>] ? sysret_check+0x1b/0x56 [<ffffffff810b8695>] ? trace_hardirqs_on_caller+0x115/0x1a0 [<ffffffff81341d8e>] ? trace_hardirqs_on_thunk+0x3a/0x3f [<ffffffff816cd742>] system_call_fastpath+0x16/0x1b ---[ end trace eed6ae990d018c8b ]--- Reported-by: Dave Jones <davej@redhat.com> Cc: Dave Jones <davej@redhat.com> Cc: David S. Miller <davem@davemloft.net> Cc: Venkat Venkatsubra <venkat.x.venkatsubra@oracle.com> Signed-off-by: Cong Wang <amwang@redhat.com> Acked-by: Venkat Venkatsubra <venkat.x.venkatsubra@oracle.com> Signed-off-by: David S. Miller <davem@davemloft.net>
| * | MAINTAINERS: remove eexpressCesar Eduardo Barros2013-03-031-6/+0
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | This driver was removed by commit f84932d (drivers/net: delete ISA intel eexpress and eepro i825xx drivers). Cc: Paul Gortmaker <paul.gortmaker@windriver.com> Cc: Philip Blundell <philb@gnu.org> Cc: netdev@vger.kernel.org Signed-off-by: Cesar Eduardo Barros <cesarb@cesarb.net> Signed-off-by: David S. Miller <davem@davemloft.net>
| * | MAINTAINERS: remove drivers/net/wan/cycx*Cesar Eduardo Barros2013-03-031-6/+0
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | This driver was removed by commit 6fcdf4f (wanrouter: delete now orphaned header content, files/drivers). Cc: Paul Gortmaker <paul.gortmaker@windriver.com> Cc: Arnaldo Carvalho de Melo <acme@redhat.com> Cc: netdev@vger.kernel.org Signed-off-by: Cesar Eduardo Barros <cesarb@cesarb.net> Signed-off-by: David S. Miller <davem@davemloft.net>
| * | MAINTAINERS: remove 3c505Cesar Eduardo Barros2013-03-031-6/+0
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | This driver was removed by commit 0e245db (drivers/net: delete the 3Com 3c505/3c507 intel i825xx support). Cc: Paul Gortmaker <paul.gortmaker@windriver.com> Cc: Philip Blundell <philb@gnu.org> Cc: netdev@vger.kernel.org Signed-off-by: Cesar Eduardo Barros <cesarb@cesarb.net> Signed-off-by: David S. Miller <davem@davemloft.net>
| * | caif_dev: fix sparse warnings for caif_flow_cbSilviu-Mihai Popescu2013-03-031-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | This fixed the following sparse warning: net/caif/caif_dev.c:121:6: warning: symbol 'caif_flow_cb' was not declared. Should it be static? Signed-off-by: Silviu-Mihai Popescu <silviupopescu1990@gmail.com> Signed-off-by: David S. Miller <davem@davemloft.net>
| * | ax88179_178a: ASIX AX88179_178A USB 3.0/2.0 to gigabit ethernet adapter driverFreddy Xin2013-03-033-0/+1467
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | This is a resubmission. Added kfree() in ax88179_get_eeprom to prevent memory leakage. Modified "__le16 rxctl" to "u16 rxctl" in "struct ax88179_data" and removed pointless casts. Removed asix_init and asix_exit functions and added "module_usb_driver(ax88179_178a_driver)". Fixed endianness issue on big endian systems and verified this driver on iBook G4. Removed steps that change net->features in ax88179_set_features function. Added "const" to ethtool_ops structure and fixed the coding style of AX88179_BULKIN_SIZE array. Fixed the issue that the default MTU is not 1500. Added ax88179_change_mtu function and enabled the hardware jumbo frame function to support an MTU higher than 1500. Fixed indentation and empty line coding style errors. The _nopm version usb functions were added to access register in suspend and resume functions. Serveral variables allocted dynamically were removed and replaced by stack variables. ax88179_get_eeprom were modified from asix_get_eeprom in asix_common. This patch adds a driver for ASIX's AX88179 family of USB 3.0/2.0 to gigabit ethernet adapters. It's based on the AX88xxx driver but the usb commands used to access registers for AX88179 are completely different. This driver had been verified on x86 system with AX88179/AX88178A and Sitcomm LN-032 USB dongles. Signed-off-by: Freddy Xin <freddy@asix.com.tw> Signed-off-by: David S. Miller <davem@davemloft.net>
| * | sctp: use the passed in gfp flags instead GFP_KERNELDan Carpenter2013-03-011-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | This patch doesn't change how the code works because in the current kernel gfp is always GFP_KERNEL. But gfp was obviously intended instead of GFP_KERNEL. Signed-off-by: Dan Carpenter <dan.carpenter@oracle.com> Acked-by: Neil Horman <nhorman@tuxdriver.com> Signed-off-by: David S. Miller <davem@davemloft.net>
| * | ipv[4|6]: correct dropwatch false positive in local_deliver_finishNeil Horman2013-03-012-4/+8
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | I had a report recently of a user trying to use dropwatch to localise some frame loss, and they were getting false positives. Turned out they were using a user space SCTP stack that used raw sockets to grab frames. When we don't have a registered protocol for a given packet, we record it as a drop, even if a raw socket receieves the frame. We should only record the drop in the event a raw socket doesnt exist to receive the frames Tested by the reported successfully Signed-off-by: Neil Horman <nhorman@tuxdriver.com> Reported-by: William Reich <reich@ulticom.com> Tested-by: William Reich <reich@ulticom.com> CC: "David S. Miller" <davem@davemloft.net> CC: William Reich <reich@ulticom.com> CC: eric.dumazet@gmail.com Acked-by: Eric Dumazet <edumazet@google.com> Signed-off-by: David S. Miller <davem@davemloft.net>
| * | Merge branch 'for-davem' of ↵David S. Miller2013-03-0119-174/+258
| |\ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/linville/wireless John W. Linville says: ==================== This is another flurry of fixes intended for the 3.9 stream... A mac80211 pull from Johannes: "Seth fixes a stupid bug I introduced into one of his earlier patches, Chun-Yeow fixes mesh forwarding and Felix fixes monitor mode. I myself fixed a small locking issue and, the biggest change here, removed some nl80211 information with which sometimes the per wiphy information was getting too large for the typical 4k-minus-overhead. In my -next tree I have a patch to allow splitting that and add back the information removed now." An iwlwifi pull from Johannes: "I have a fix for a pretty important bug regarding DMA mapping, that could cause the DMA engine to overwrite data we wanted to send to it, so that the next time we send it it would be bad. This particularly affects calibration results. Other than that, three little fixes for the MVM driver." But wait, there's more! Avinash Patil fixes an incorrectly timed delay in mwifiex. Bing Zhao prevents a crash in SD8688 caused by failing to properly set a flag before issuing a command. Felix Fietkau is the big here this time, providing a trio of minor ath9k fixes and correcting the advertised interface combinations for rt2x00 when mesh support is disabled. Finally, Hauke Mehrtens gives us a patch that correctlin initializes a spin lock in the bcma code. Please let me know if there are problems! ==================== Signed-off-by: David S. Miller <davem@davemloft.net>
| | * \ Merge branch 'master' of ↵John W. Linville2013-03-0119-174/+258
| | |\ \ | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/linville/wireless into for-davem
| | | * | libertas: fix crash for SD8688Bing Zhao2013-02-271-1/+5
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | For SD8688, FUNC_INIT command is queued before fw_ready flag is set. This causes the following crash as lbs_thread blocks any command if fw_ready is not set. [ 209.338953] [<c0502248>] (__schedule+0x610/0x764) from [<bf20ae24>] (__lbs_cmd+0xb8/0x130 [libertas]) [ 209.348340] [<bf20ae24>] (__lbs_cmd+0xb8/0x130 [libertas]) from [<bf222474>] (if_sdio_finish_power_on+0xec/0x1b0 [libertas_sdio]) [ 209.360136] [<bf222474>] (if_sdio_finish_power_on+0xec/0x1b0 [libertas_sdio]) from [<bf2226c4>] (if_sdio_power_on+0x18c/0x20c [libertas_sdio]) [ 209.373052] [<bf2226c4>] (if_sdio_power_on+0x18c/0x20c [libertas_sdio]) from [<bf222944>] (if_sdio_probe+0x200/0x31c [libertas_sdio]) [ 209.385316] [<bf222944>] (if_sdio_probe+0x200/0x31c [libertas_sdio]) from [<bf01d820>] (sdio_bus_probe+0x94/0xfc [mmc_core]) [ 209.396748] [<bf01d820>] (sdio_bus_probe+0x94/0xfc [mmc_core]) from [<c02e729c>] (driver_probe_device+0x12c/0x348) [ 209.407214] [<c02e729c>] (driver_probe_device+0x12c/0x348) from [<c02e7530>] (__driver_attach+0x78/0x9c) [ 209.416798] [<c02e7530>] (__driver_attach+0x78/0x9c) from [<c02e5658>] (bus_for_each_dev+0x50/0x88) [ 209.425946] [<c02e5658>] (bus_for_each_dev+0x50/0x88) from [<c02e6810>] (bus_add_driver+0x108/0x268) [ 209.435180] [<c02e6810>] (bus_add_driver+0x108/0x268) from [<c02e782c>] (driver_register+0xa4/0x134) [ 209.444426] [<c02e782c>] (driver_register+0xa4/0x134) from [<bf22601c>] (if_sdio_init_module+0x1c/0x3c [libertas_sdio]) [ 209.455339] [<bf22601c>] (if_sdio_init_module+0x1c/0x3c [libertas_sdio]) from [<c00085b8>] (do_one_initcall+0x98/0x174) [ 209.466236] [<c00085b8>] (do_one_initcall+0x98/0x174) from [<c0076504>] (load_module+0x1c5c/0x1f80) [ 209.475390] [<c0076504>] (load_module+0x1c5c/0x1f80) from [<c007692c>] (sys_init_module+0x104/0x128) [ 209.484632] [<c007692c>] (sys_init_module+0x104/0x128) from [<c0008c40>] (ret_fast_syscall+0x0/0x38) Fix it by setting fw_ready flag prior to queuing FUNC_INIT command. Cc: <stable@vger.kernel.org> # 3.5+ Reported-by: Lubomir Rintel <lkundrak@v3.sk> Tested-by: Lubomir Rintel <lkundrak@v3.sk> Signed-off-by: Bing Zhao <bzhao@marvell.com> Signed-off-by: John W. Linville <linville@tuxdriver.com>
| | | * | rt2x00: error in configurations with mesh support disabledFelix Fietkau2013-02-271-2/+6
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | If CONFIG_MAC80211_MESH is not set, cfg80211 will now allow advertising interface combinations with NL80211_IFTYPE_MESH_POINT present. Add appropriate ifdefs to avoid running into errors. Cc: stable@vger.kernel.org Signed-off-by: Felix Fietkau <nbd@openwrt.org> Acked-by: Gertjan van Wingerde <gwingerde@gmail.com> Signed-off-by: John W. Linville <linville@tuxdriver.com>
| | | * | mwifiex: correct sleep delay counterAvinash Patil2013-02-271-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Maximum delay for waking up card is 50 ms. Because of typo in counter, this delay goes to 500ms. This patch fixes the bug. Cc: <stable@vger.kernel.org> # 3.2+ Signed-off-by: Avinash Patil <patila@marvell.com> Signed-off-by: Amitkumar Karwar <akarwar@marvell.com> Signed-off-by: Yogesh Ashok Powar <yogeshp@marvell.com> Signed-off-by: Bing Zhao <bzhao@marvell.com> Signed-off-by: John W. Linville <linville@tuxdriver.com>
| | | * | ath9k_hw: improve reset reliability after errorsFelix Fietkau2013-02-271-1/+3
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | On many different chips, important aspects of the MAC state are not fully cleared by a warm reset. This can show up as tx/rx hangs, those annoying "DMA failed to stop in 10 ms..." messages or other quirks. On AR933x, the chip can occasionally get stuck in a way that only a driver unload/reload or a reboot would bring it back to life. With this patch, a full reset is issued when bringing the chip out of FULL-SLEEP state (after idle), or if either Rx or Tx was not shut down properly. This makes the DMA related error messages disappear completely in my tests on AR933x, and the chip does not get stuck anymore. Cc: stable@vger.kernel.org Signed-off-by: Felix Fietkau <nbd@openwrt.org> Signed-off-by: John W. Linville <linville@tuxdriver.com>
| | | * | bcma: init spin lockHauke Mehrtens2013-02-271-0/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | This spin lock was not initialized. Signed-off-by: Hauke Mehrtens <hauke@hauke-m.de> Signed-off-by: John W. Linville <linville@tuxdriver.com>
| | | * | ath9k_htc: fix signal strength handling issuesFelix Fietkau2013-02-272-7/+12
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The ath9k commit 2ef167557c0a26c88162ecffb017bfcc51eb7b29 (ath9k: fix signal strength reporting issues) fixed an issue where the reported per-frame signal strength reported to mac80211 was being overwritten with an internal average. The same issue is also present in ath9k_htc. In addition to preventing the driver from overwriting the value, this commit also ensures that the internal average (which is used for ANI) only tracks beacons of the AP that we're connected to. Signed-off-by: Felix Fietkau <nbd@openwrt.org> Cc: stable@vger.kernel.org Signed-off-by: John W. Linville <linville@tuxdriver.com>
| | | * | ath9k: fix RSSI dummy marker valueFelix Fietkau2013-02-271-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | RSSI is being stored internally as s8 in several places. The indication of an unset RSSI value, ATH_RSSI_DUMMY_MARKER, was supposed to have been set to 127, but ended up being set to 0x127 because of a code cleanup mistake. This could lead to invalid signal strength values in a few places. Signed-off-by: Felix Fietkau <nbd@openwrt.org> Cc: stable@vger.kernel.org Signed-off-by: John W. Linville <linville@tuxdriver.com>
| | | * | Merge branch 'for-john' of ↵John W. Linville2013-02-277-71/+166
| | | |\ \ | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/iwlwifi/iwlwifi-fixes
| | | | * | iwlwifi: mvm: Remove testing of static PIC in PhyDBDor Shaish2013-02-271-16/+0
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The PIC was supposed to be a small signature appended to the PhyDB data, but the signature isn't really static and thus attempting to check it just causes the warnings spuriously so remove them. Signed-off-by: Dor Shaish <dor.shaish@intel.com> Reviewed-by: Emmanuel Grumbach <emmanuel.grumbach@intel.com> Signed-off-by: Johannes Berg <johannes.berg@intel.com>
| | | | * | iwlwifi: fix wakeup status query and packet reportingJohannes Berg2013-02-272-27/+81
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The wakeup packet in the status response is padded out to a multiple of 4 bytes by the firmware for transfer to the host, take that into account when checking the length of the command. Also, the reported wakeup packet includes the FCS but the userspace API doesn't, so remove that. If it is a data packet it is reported as an 802.3 packet but I forgot to take into account and remove the encryption head/tail, fix all of that as well. Reviewed-by: Emmanuel Grumbach <emmanuel.grumbach@intel.com> Signed-off-by: Johannes Berg <johannes.berg@intel.com>
| | | | * | iwlwifi: mvm: fix AP/GO mode station removalJohannes Berg2013-02-261-5/+14
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | When stations are removed while packets are in the queue, we drain the queues first, and then remove the stations. If this happens in AP mode while the interface is removed the MAC context might be removed from the firmware before we removed the station(s), resulting in a SYSASSERT 3421. This is because we remove the MAC context from the FW in stop_ap(), but only flush the station drain work later in remove_interface(). Refactor the code a bit to have a common MAC context removal preparation first to solve this. Reviewed-by: Emmanuel Grumbach <emmanuel.grumbach@intel.com> Signed-off-by: Johannes Berg <johannes.berg@intel.com>
| | | | * | iwlwifi: always copy first 16 bytes of commandsJohannes Berg2013-02-263-23/+71
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The FH hardware will always write back to the scratch field in commands, even host commands not just TX commands, which can overwrite parts of the command. This is problematic if the command is re-used (with IWL_HCMD_DFL_NOCOPY) and can cause calibration issues. Address this problem by always putting at least the first 16 bytes into the buffer we also use for the command header and therefore make the DMA engine write back into this. For commands that are smaller than 16 bytes also always map enough memory for the DMA engine to write back to. Cc: stable@vger.kernel.org Reviewed-by: Emmanuel Grumbach <emmanuel.grumbach@intel.com> Signed-off-by: Johannes Berg <johannes.berg@intel.com>
| | | * | | mac80211: fix monitor mode channel reportingFelix Fietkau2013-02-261-3/+9
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | When not using channel contexts with only monitor mode interfaces being active, report local->monitor_chandef to userspace. Signed-off-by: Felix Fietkau <nbd@openwrt.org> Signed-off-by: Johannes Berg <johannes.berg@intel.com>
| | | * | | mac80211: fix idle handling in monitor modeFelix Fietkau2013-02-261-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | When the driver does not want a monitor mode VIF, no channel context is allocated for it. This causes ieee80211_recalc_idle to put the hardware into idle mode if only a monitor mode is active, breaking injection. Fix this by checking local->monitors in addition to active channel contexts. Signed-off-by: Felix Fietkau <nbd@openwrt.org> Signed-off-by: Johannes Berg <johannes.berg@intel.com>
| | | * | | mac80211: Ensure off-channel frames don't get queuedSeth Forshee2013-02-261-25/+31
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Commit 6c17b77b67587b9f9e3070fb89fe98cef3187131 (mac80211: Fix tx queue handling during scans) contains a bug that causes off-channel frames to get queued when they should be handed down to the driver for transmit. Prevent this from happening. Reported-by: Fabio Rossi <rossi.f@inwind.it> Signed-off-by: Seth Forshee <seth.forshee@canonical.com> Signed-off-by: Johannes Berg <johannes.berg@intel.com>
| | | * | | mac80211: fix the problem of forwarding from DS to DS in MeshChun-Yeow Yeoh2013-02-251-1/+16
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Unicast frame with unknown forwarding information always trigger the path discovery assuming destination is always located inside the MBSS. This patch allows the forwarding to look for mesh gate if path discovery inside the MBSS has failed. Reported-by: Cedric Voncken <cedric.voncken@acksys.fr> Signed-off-by: Chun-Yeow Yeoh <yeohchunyeow@gmail.com> Signed-off-by: Johannes Berg <johannes.berg@intel.com>
| | | * | | nl80211: remove TCP WoWLAN informationJohannes Berg2013-02-251-45/+0
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Just like the radar information, the TCP WoWLAN capability data can increase the wiphy information and make it too big. Remove the TCP WoWLAN information; no driver supports it and new userspace tools will be required as well. Signed-off-by: Johannes Berg <johannes.berg@intel.com>
| | | * | | nl80211: remove radar informationJohannes Berg2013-02-251-13/+3
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The wiphy information is getting very close to being too much for a typical netlink dump message and adding the radar attributes to channels and interface combinations can push it over the limit, which means userspace gets no information whatsoever. Therefore, remove these again for now, no driver actually supports radar detection anyway and a modified userspace is required as well. We're working on a solution that will allow userspace to request splitting the information across multiple netlink messages, which will allow us to add this back. Cc: Simon Wunderlich <simon.wunderlich@s2003.tu-chemnitz.de> Signed-off-by: Johannes Berg <johannes.berg@intel.com>
| | | * | | mac80211: fix tim_lock lockingJohannes Berg2013-02-251-2/+2
| | | |/ / | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The ieee80211_beacon_add_tim() function might be called by drivers with BHs enabled, which causes a potential deadlock if TX happens at the same time and attempts to lock the tim_lock as well. Use spin_lock_bh to fix it. Signed-off-by: Johannes Berg <johannes.berg@intel.com>
| * | / / l2tp: Restore socket refcount when sendmsg succeedsGuillaume Nault2013-03-011-0/+1
| |/ / / | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The sendmsg() syscall handler for PPPoL2TP doesn't decrease the socket reference counter after successful transmissions. Any successful sendmsg() call from userspace will then increase the reference counter forever, thus preventing the kernel's session and tunnel data from being freed later on. The problem only happens when writing directly on L2TP sockets. PPP sockets attached to L2TP are unaffected as the PPP subsystem uses pppol2tp_xmit() which symmetrically increase/decrease reference counters. This patch adds the missing call to sock_put() before returning from pppol2tp_sendmsg(). Signed-off-by: Guillaume Nault <g.nault@alphalink.fr> Signed-off-by: David S. Miller <davem@davemloft.net>