aboutsummaryrefslogtreecommitdiffstats
path: root/lib
Commit message (Collapse)AuthorAgeFilesLines
* Merge tag 'metag-v3.9-rc1-v4' of ↵Linus Torvalds2013-03-031-2/+2
|\ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/jhogan/metag Pull new ImgTec Meta architecture from James Hogan: "This adds core architecture support for Imagination's Meta processor cores, followed by some later miscellaneous arch/metag cleanups and fixes which I kept separate to ease review: - Support for basic Meta 1 (ATP) and Meta 2 (HTP) core architecture - A few fixes all over, particularly for symbol prefixes - A few privilege protection fixes - Several cleanups (setup.c includes, split out a lot of metag_ksyms.c) - Fix some missing exports - Convert hugetlb to use vm_unmapped_area() - Copy device tree to non-init memory - Provide dma_get_sgtable()" * tag 'metag-v3.9-rc1-v4' of git://git.kernel.org/pub/scm/linux/kernel/git/jhogan/metag: (61 commits) metag: Provide dma_get_sgtable() metag: prom.h: remove declaration of metag_dt_memblock_reserve() metag: copy devicetree to non-init memory metag: cleanup metag_ksyms.c includes metag: move mm/init.c exports out of metag_ksyms.c metag: move usercopy.c exports out of metag_ksyms.c metag: move setup.c exports out of metag_ksyms.c metag: move kick.c exports out of metag_ksyms.c metag: move traps.c exports out of metag_ksyms.c metag: move irq enable out of irqflags.h on SMP genksyms: fix metag symbol prefix on crc symbols metag: hugetlb: convert to vm_unmapped_area() metag: export clear_page and copy_page metag: export metag_code_cache_flush_all metag: protect more non-MMU memory regions metag: make TXPRIVEXT bits explicit metag: kernel/setup.c: sort includes perf: Enable building perf tools for Meta metag: add boot time LNKGET/LNKSET check metag: add __init to metag_cache_probe() ...
| * Kconfig.debug: add METAG to dependency listsJames Hogan2013-03-021-2/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | Add [!]METAG to a couple of Kconfig dependencies in lib/Kconfig.debug. Don't allow stack utilization instrumentation on metag, and allow building with frame pointers. Signed-off-by: James Hogan <james.hogan@imgtec.com> Cc: Andrew Morton <akpm@linux-foundation.org> Cc: "Paul E. McKenney" <paul.mckenney@linaro.org> Cc: Akinobu Mita <akinobu.mita@gmail.com> Cc: Michel Lespinasse <walken@google.com> Cc: Catalin Marinas <catalin.marinas@arm.com>
* | Merge tag 'for_linux-3.9' of ↵Linus Torvalds2013-03-021-0/+18
|\ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/jwessel/kgdb Pull KGDB/KDB fixes and cleanups from Jason Wessel: "For a change we removed more code than we added. If people aren't using it we shouldn't be carrying it. :-) Cleanups: - Remove kdb ssb command - there is no in kernel disassembler to support it - Remove kdb ll command - Always caused a kernel oops and there were no bug reports so no one was using this command - Use kernel ARRAY_SIZE macro instead of array computations Fixes: - Stop oops in kdb if user executes kdb_defcmd with args - kdb help command truncated text - ppc64 support for kgdbts - Add missing kconfig option from original kdb port for dealing with catastrophic kernel crashes such that you can reboot automatically on continue from kdb" * tag 'for_linux-3.9' of git://git.kernel.org/pub/scm/linux/kernel/git/jwessel/kgdb: kdb: Remove unhandled ssb command kdb: Prevent kernel oops with kdb_defcmd kdb: Remove the ll command kdb_main: fix help print kdb: Fix overlap in buffers with strcpy Fixed dead ifdef block by adding missing Kconfig option. kdb: Setup basic kdb state before invoking commands via kgdb kdb: use ARRAY_SIZE where possible kgdb/kgdbts: support ppc64 kdb: A fix for kdb command table expansion
| * | Fixed dead ifdef block by adding missing Kconfig option.Robert Obermeier2013-03-021-0/+18
| |/ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Added missing Kconfig option KDB_CONTINUE_CATASTROPHIC which lead to a dead ifdef block in kernel/debug/kdb/kdb_main.c:73-75. The code using KDB_CONTINUE_CATASTROPHIC was originally introduced in commit '5d5314d6795f3c1c0f415348ff8c51f7de042b77' by Jason Wessel. This patchset ("kdb: core for kgdb back end (1 of 2)") added platform independent part of kdb to the linux kernel. The Kernel option however, even though it had the same options and behaviour on all supported architectures, was part of the x86 and ia64 patchset of KDB and therefore not pulled into the mainline kernel tree. I actually took the originally written Kconfig by Keith Owens <kaos@sgi.com> (2003-06-20 according to KDB changelog) and changed it to reflect the correct behaviour, as the KDUMP patchset is not part of the kernel and the expected functionality is missing from it. Signed-off-by: Robert Obermeier <obbi89@googlemail.com> Signed-off-by: Jason Wessel <jason.wessel@windriver.com>
* | Merge tag 'arc-v3.9-rc1-late' of ↵Linus Torvalds2013-03-021-0/+2
|\ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/vgupta/arc Pull new ARC architecture from Vineet Gupta: "Initial ARC Linux port with some fixes on top for 3.9-rc1: I would like to introduce the Linux port to ARC Processors (from Synopsys) for 3.9-rc1. The patch-set has been discussed on the public lists since Nov and has received a fair bit of review, specially from Arnd, tglx, Al and other subsystem maintainers for DeviceTree, kgdb... The arch bits are in arch/arc, some asm-generic changes (acked by Arnd), a minor change to PARISC (acked by Helge). The series is a touch bigger for a new port for 2 main reasons: 1. It enables a basic kernel in first sub-series and adds ptrace/kgdb/.. later 2. Some of the fallout of review (DeviceTree support, multi-platform- image support) were added on top of orig series, primarily to record the revision history. This updated pull request additionally contains - fixes due to our GNU tools catching up with the new syscall/ptrace ABI - some (minor) cross-arch Kconfig updates." * tag 'arc-v3.9-rc1-late' of git://git.kernel.org/pub/scm/linux/kernel/git/vgupta/arc: (82 commits) ARC: split elf.h into uapi and export it for userspace ARC: Fixup the current ABI version ARC: gdbserver using regset interface possibly broken ARC: Kconfig cleanup tracking cross-arch Kconfig pruning in merge window ARC: make a copy of flat DT ARC: [plat-arcfpga] DT arc-uart bindings change: "baud" => "current-speed" ARC: Ensure CONFIG_VIRT_TO_BUS is not enabled ARC: Fix pt_orig_r8 access ARC: [3.9] Fallout of hlist iterator update ARC: 64bit RTSC timestamp hardware issue ARC: Don't fiddle with non-existent caches ARC: Add self to MAINTAINERS ARC: Provide a default serial.h for uart drivers needing BASE_BAUD ARC: [plat-arcfpga] defconfig for fully loaded ARC Linux ARC: [Review] Multi-platform image #8: platform registers SMP callbacks ARC: [Review] Multi-platform image #7: SMP common code to use callbacks ARC: [Review] Multi-platform image #6: cpu-to-dma-addr optional ARC: [Review] Multi-platform image #5: NR_IRQS defined by ARC core ARC: [Review] Multi-platform image #4: Isolate platform headers ARC: [Review] Multi-platform image #3: switch to board callback ...
| * | asm-generic headers: Allow yet more arch overrides in checksum.hVineet Gupta2013-02-111-0/+2
| | | | | | | | | | | | | | | | | | | | | arches can have more efficient implementation of these routines Acked-by: Arnd Bergmann <arnd@arndb.de> Signed-off-by: Vineet Gupta <vgupta@synopsys.com>
* | | Merge tag 'lzo-update-signature-20130226' of ↵Linus Torvalds2013-02-286-409/+460
|\ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://github.com/markus-oberhumer/linux Pull LZO compression update from Markus Oberhumer: "Summary: ======== Update the Linux kernel LZO compression and decompression code to the current upstream version which features significant performance improvements on modern machines. Some *synthetic* benchmarks: ============================ x86_64 (Sandy Bridge), gcc-4.6 -O3, Silesia test corpus, 256 kB block-size: compression speed decompression speed LZO-2005 : 150 MB/sec 468 MB/sec LZO-2012 : 434 MB/sec 1210 MB/sec i386 (Sandy Bridge), gcc-4.6 -O3, Silesia test corpus, 256 kB block-size: compression speed decompression speed LZO-2005 : 143 MB/sec 409 MB/sec LZO-2012 : 372 MB/sec 1121 MB/sec armv7 (Cortex-A9), Linaro gcc-4.6 -O3, Silesia test corpus, 256 kB block-size: compression speed decompression speed LZO-2005 : 27 MB/sec 84 MB/sec LZO-2012 : 44 MB/sec 117 MB/sec **LZO-2013-UA : 47 MB/sec 167 MB/sec Legend: LZO-2005 : LZO version in current 3.8 kernel (which is based on the LZO 2.02 release from 2005) LZO-2012 : updated LZO version available in linux-next **LZO-2013-UA : updated LZO version available in linux-next plus experimental ARM Unaligned Access patch. This needs approval from some ARM maintainer ist NOT YET INCLUDED." Andrew Morton <akpm@linux-foundation.org> acks it and says: "There's a new LZ4 on the block which is even faster than the sped-up LZO, but various filesystems and things use LZO" * tag 'lzo-update-signature-20130226' of git://github.com/markus-oberhumer/linux: crypto: testmgr - update LZO compression test vectors lib/lzo: Update LZO compression to current upstream version lib/lzo: Rename lzo1x_decompress.c to lzo1x_decompress_safe.c
| * | | lib/lzo: Update LZO compression to current upstream versionMarkus F.X.J. Oberhumer2013-02-203-336/+387
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | This commit updates the kernel LZO code to the current upsteam version which features a significant speed improvement - benchmarking the Calgary and Silesia test corpora typically shows a doubled performance in both compression and decompression on modern i386/x86_64/powerpc machines. Signed-off-by: Markus F.X.J. Oberhumer <markus@oberhumer.com>
| * | | lib/lzo: Rename lzo1x_decompress.c to lzo1x_decompress_safe.cMarkus F.X.J. Oberhumer2013-02-203-2/+2
| | |/ | |/| | | | | | | | | | | | | | | | | | | Rename the source file to match the function name and thereby also make room for a possible future even slightly faster "non-safe" decompressor version. Signed-off-by: Markus F.X.J. Oberhumer <markus@oberhumer.com>
* | | hlist: drop the node parameter from iteratorsSasha Levin2013-02-272-13/+11
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | I'm not sure why, but the hlist for each entry iterators were conceived list_for_each_entry(pos, head, member) The hlist ones were greedy and wanted an extra parameter: hlist_for_each_entry(tpos, pos, head, member) Why did they need an extra pos parameter? I'm not quite sure. Not only they don't really need it, it also prevents the iterator from looking exactly like the list iterator, which is unfortunate. Besides the semantic patch, there was some manual work required: - Fix up the actual hlist iterators in linux/list.h - Fix up the declaration of other iterators based on the hlist ones. - A very small amount of places were using the 'node' parameter, this was modified to use 'obj->member' instead. - Coccinelle didn't handle the hlist_for_each_entry_safe iterator properly, so those had to be fixed up manually. The semantic patch which is mostly the work of Peter Senna Tschudin is here: @@ iterator name hlist_for_each_entry, hlist_for_each_entry_continue, hlist_for_each_entry_from, hlist_for_each_entry_rcu, hlist_for_each_entry_rcu_bh, hlist_for_each_entry_continue_rcu_bh, for_each_busy_worker, ax25_uid_for_each, ax25_for_each, inet_bind_bucket_for_each, sctp_for_each_hentry, sk_for_each, sk_for_each_rcu, sk_for_each_from, sk_for_each_safe, sk_for_each_bound, hlist_for_each_entry_safe, hlist_for_each_entry_continue_rcu, nr_neigh_for_each, nr_neigh_for_each_safe, nr_node_for_each, nr_node_for_each_safe, for_each_gfn_indirect_valid_sp, for_each_gfn_sp, for_each_host; type T; expression a,c,d,e; identifier b; statement S; @@ -T b; <+... when != b ( hlist_for_each_entry(a, - b, c, d) S | hlist_for_each_entry_continue(a, - b, c) S | hlist_for_each_entry_from(a, - b, c) S | hlist_for_each_entry_rcu(a, - b, c, d) S | hlist_for_each_entry_rcu_bh(a, - b, c, d) S | hlist_for_each_entry_continue_rcu_bh(a, - b, c) S | for_each_busy_worker(a, c, - b, d) S | ax25_uid_for_each(a, - b, c) S | ax25_for_each(a, - b, c) S | inet_bind_bucket_for_each(a, - b, c) S | sctp_for_each_hentry(a, - b, c) S | sk_for_each(a, - b, c) S | sk_for_each_rcu(a, - b, c) S | sk_for_each_from -(a, b) +(a) S + sk_for_each_from(a) S | sk_for_each_safe(a, - b, c, d) S | sk_for_each_bound(a, - b, c) S | hlist_for_each_entry_safe(a, - b, c, d, e) S | hlist_for_each_entry_continue_rcu(a, - b, c) S | nr_neigh_for_each(a, - b, c) S | nr_neigh_for_each_safe(a, - b, c, d) S | nr_node_for_each(a, - b, c) S | nr_node_for_each_safe(a, - b, c, d) S | - for_each_gfn_sp(a, c, d, b) S + for_each_gfn_sp(a, c, d) S | - for_each_gfn_indirect_valid_sp(a, c, d, b) S + for_each_gfn_indirect_valid_sp(a, c, d) S | for_each_host(a, - b, c) S | for_each_host_safe(a, - b, c, d) S | for_each_mesh_entry(a, - b, c, d) S ) ...+> [akpm@linux-foundation.org: drop bogus change from net/ipv4/raw.c] [akpm@linux-foundation.org: drop bogus hunk from net/ipv6/raw.c] [akpm@linux-foundation.org: checkpatch fixes] [akpm@linux-foundation.org: fix warnings] [akpm@linux-foudnation.org: redo intrusive kvm changes] Tested-by: Peter Senna Tschudin <peter.senna@gmail.com> Acked-by: Paul E. McKenney <paulmck@linux.vnet.ibm.com> Signed-off-by: Sasha Levin <sasha.levin@oracle.com> Cc: Wu Fengguang <fengguang.wu@intel.com> Cc: Marcelo Tosatti <mtosatti@redhat.com> Cc: Gleb Natapov <gleb@redhat.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | kfifo: fix kfifo_alloc() and kfifo_init()Stefani Seibold2013-02-271-4/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Fix kfifo_alloc() and kfifo_init() to alloc at least the requested number of elements. Since the kfifo operates on power of 2 the request size will be rounded up to the next power of two. Signed-off-by: Stefani Seibold <stefani@seibold.net> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | kfifo: move kfifo.c from kernel/ to lib/Stefani Seibold2013-02-272-1/+610
| | | | | | | | | | | | | | | | | | | | | | | | Move kfifo.c from kernel/ to lib/ Signed-off-by: Stefani Seibold <stefani@seibold.net> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | idr: explain WARN_ON_ONCE() on negative IDs out-of-range IDTejun Heo2013-02-271-0/+10
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Until recently, when an negative ID is specified, idr functions used to ignore the sign bit and proceeded with the operation with the rest of bits, which is bizarre and error-prone. The behavior recently got changed so that negative IDs are treated as invalid but we're triggering WARN_ON_ONCE() on negative IDs just in case somebody was depending on the sign bit being ignored, so that those can be detected and fixed easily. We only need this for a while. Explain why WARN_ON_ONCE()s are there and that they can be removed later. Signed-off-by: Tejun Heo <tj@kernel.org> Acked-by: Thomas Gleixner <tglx@linutronix.de> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | idr: implement lookup hintTejun Heo2013-02-271-22/+16
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | While idr lookup isn't a particularly heavy operation, it still is too substantial to use in hot paths without worrying about the performance implications. With recent changes, each idr_layer covers 256 slots which should be enough to cover most use cases with single idr_layer making lookup hint very attractive. This patch adds idr->hint which points to the idr_layer which allocated an ID most recently and the fast path lookup becomes if (look up target's prefix matches that of the hinted layer) return hint->ary[ID's offset in the leaf layer]; which can be inlined. idr->hint is set to the leaf node on idr_fill_slot() and cleared from free_layer(). [andriy.shevchenko@linux.intel.com: always do slow path when hint is uninitialized] Signed-off-by: Tejun Heo <tj@kernel.org> Cc: Kirill A. Shutemov <kirill.shutemov@linux.intel.com> Cc: Sasha Levin <sasha.levin@oracle.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | idr: add idr_layer->prefixTejun Heo2013-02-271-0/+13
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Add a field which carries the prefix of ID the idr_layer covers. This will be used to implement lookup hint. This patch doesn't make use of the new field and doesn't introduce any behavior difference. Signed-off-by: Tejun Heo <tj@kernel.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | idr: remove length restriction from idr_layer->bitmapTejun Heo2013-02-271-17/+17
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Currently, idr->bitmap is declared as an unsigned long which restricts the number of bits an idr_layer can contain. All bitops can handle arbitrary positive integer bit number and there's no reason for this restriction. Declare idr_layer->bitmap using DECLARE_BITMAP() instead of a single unsigned long. * idr_layer->bitmap is now an array. '&' dropped from params to bitops. * Replaced "== IDR_FULL" tests with bitmap_full() and removed IDR_FULL. * Replaced find_next_bit() on ~bitmap with find_next_zero_bit(). * Replaced "bitmap = 0" with bitmap_clear(). This patch doesn't (or at least shouldn't) introduce any behavior changes. [akpm@linux-foundation.org: checkpatch fixes] Signed-off-by: Tejun Heo <tj@kernel.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | idr: remove MAX_IDR_MASK and move left MAX_IDR_* into idr.cTejun Heo2013-02-271-7/+17
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | MAX_IDR_MASK is another weirdness in the idr interface. As idr covers whole positive integer range, it's defined as 0x7fffffff or INT_MAX. Its usage in idr_find(), idr_replace() and idr_remove() is bizarre. They basically mask off the sign bit and operate on the rest, so if the caller, by accident, passes in a negative number, the sign bit will be masked off and the remaining part will be used as if that was the input, which is worse than crashing. The constant is visible in idr.h and there are several users in the kernel. * drivers/i2c/i2c-core.c:i2c_add_numbered_adapter() Basically used to test if adap->nr is a negative number which isn't -1 and returns -EINVAL if so. idr_alloc() already has negative @start checking (w/ WARN_ON_ONCE), so this can go away. * drivers/infiniband/core/cm.c:cm_alloc_id() drivers/infiniband/hw/mlx4/cm.c:id_map_alloc() Used to wrap cyclic @start. Can be replaced with max(next, 0). Note that this type of cyclic allocation using idr is buggy. These are prone to spurious -ENOSPC failure after the first wraparound. * fs/super.c:get_anon_bdev() The ID allocated from ida is masked off before being tested whether it's inside valid range. ida allocated ID can never be a negative number and the masking is unnecessary. Update idr_*() functions to fail with -EINVAL when negative @id is specified and update other MAX_IDR_MASK users as described above. This leaves MAX_IDR_MASK without any user, remove it and relocate other MAX_IDR_* constants to lib/idr.c. Signed-off-by: Tejun Heo <tj@kernel.org> Cc: Jean Delvare <khali@linux-fr.org> Cc: Roland Dreier <roland@kernel.org> Cc: Sean Hefty <sean.hefty@intel.com> Cc: Hal Rosenstock <hal.rosenstock@gmail.com> Cc: "Marciniszyn, Mike" <mike.marciniszyn@intel.com> Cc: Jack Morgenstein <jackm@dev.mellanox.co.il> Cc: Or Gerlitz <ogerlitz@mellanox.com> Cc: Al Viro <viro@zeniv.linux.org.uk> Acked-by: Wolfram Sang <wolfram@the-dreams.de> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | idr: fix top layer handlingTejun Heo2013-02-271-15/+23
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Most functions in idr fail to deal with the high bits when the idr tree grows to the maximum height. * idr_get_empty_slot() stops growing idr tree once the depth reaches MAX_IDR_LEVEL - 1, which is one depth shallower than necessary to cover the whole range. The function doesn't even notice that it didn't grow the tree enough and ends up allocating the wrong ID given sufficiently high @starting_id. For example, on 64 bit, if the starting id is 0x7fffff01, idr_get_empty_slot() will grow the tree 5 layer deep, which only covers the 30 bits and then proceed to allocate as if the bit 30 wasn't specified. It ends up allocating 0x3fffff01 without the bit 30 but still returns 0x7fffff01. * __idr_remove_all() will not remove anything if the tree is fully grown. * idr_find() can't find anything if the tree is fully grown. * idr_for_each() and idr_get_next() can't iterate anything if the tree is fully grown. Fix it by introducing idr_max() which returns the maximum possible ID given the depth of tree and replacing the id limit checks in all affected places. As the idr_layer pointer array pa[] needs to be 1 larger than the maximum depth, enlarge pa[] arrays by one. While this plugs the discovered issues, the whole code base is horrible and in desparate need of rewrite. It's fragile like hell, Signed-off-by: Tejun Heo <tj@kernel.org> Cc: Rusty Russell <rusty@rustcorp.com.au> Cc: <stable@vger.kernel.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | idr: implement idr_preload[_end]() and idr_alloc()Tejun Heo2013-02-271-8/+166
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The current idr interface is very cumbersome. * For all allocations, two function calls - idr_pre_get() and idr_get_new*() - should be made. * idr_pre_get() doesn't guarantee that the following idr_get_new*() will not fail from memory shortage. If idr_get_new*() returns -EAGAIN, the caller is expected to retry pre_get and allocation. * idr_get_new*() can't enforce upper limit. Upper limit can only be enforced by allocating and then freeing if above limit. * idr_layer buffer is unnecessarily per-idr. Each idr ends up keeping around MAX_IDR_FREE idr_layers. The memory consumed per idr is under two pages but it makes it difficult to make idr_layer larger. This patch implements the following new set of allocation functions. * idr_preload[_end]() - Similar to radix preload but doesn't fail. The first idr_alloc() inside preload section can be treated as if it were called with @gfp_mask used for idr_preload(). * idr_alloc() - Allocate an ID w/ lower and upper limits. Takes @gfp_flags and can be used w/o preloading. When used inside preloaded section, the allocation mask of preloading can be assumed. If idr_alloc() can be called from a context which allows sufficiently relaxed @gfp_mask, it can be used by itself. If, for example, idr_alloc() is called inside spinlock protected region, preloading can be used like the following. idr_preload(GFP_KERNEL); spin_lock(lock); id = idr_alloc(idr, ptr, start, end, GFP_NOWAIT); spin_unlock(lock); idr_preload_end(); if (id < 0) error; which is much simpler and less error-prone than idr_pre_get and idr_get_new*() loop. The new interface uses per-pcu idr_layer buffer and thus the number of idr's in the system doesn't affect the amount of memory used for preloading. idr_layer_alloc() is introduced to handle idr_layer allocations for both old and new ID allocation paths. This is a bit hairy now but the new interface is expected to replace the old and the internal implementation eventually will become simpler. Signed-off-by: Tejun Heo <tj@kernel.org> Cc: Rusty Russell <rusty@rustcorp.com.au> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | idr: refactor idr_get_new_above()Tejun Heo2013-02-271-18/+12
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Move slot filling to idr_fill_slot() from idr_get_new_above_int() and make idr_get_new_above() directly call it. idr_get_new_above_int() is no longer needed and removed. This will be used to implement a new ID allocation interface. Signed-off-by: Tejun Heo <tj@kernel.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | idr: remove _idr_rc_to_errno() hackTejun Heo2013-02-271-12/+23
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | idr uses -1, IDR_NEED_TO_GROW and IDR_NOMORE_SPACE to communicate exception conditions internally. The return value is later translated to errno values using _idr_rc_to_errno(). This is confusing. Drop the custom ones and consistently use -EAGAIN for "tree needs to grow", -ENOMEM for "need more memory" and -ENOSPC for "ran out of ID space". Due to the weird memory preloading mechanism, [ra]_get_new*() return -EAGAIN on memory shortage, so we need to substitute -ENOMEM w/ -EAGAIN on those interface functions. They'll eventually be cleaned up and the translations will go away. This patch doesn't introduce any functional changes. Signed-off-by: Tejun Heo <tj@kernel.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | idr: relocate idr_for_each_entry() and reorganize id[r|a]_get_new()Tejun Heo2013-02-271-49/+0
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | * Move idr_for_each_entry() definition next to other idr related definitions. * Make id[r|a]_get_new() inline wrappers of id[r|a]_get_new_above(). This changes the implementation of idr_get_new() but the new implementation is trivial. This patch doesn't introduce any functional change. Signed-off-by: Tejun Heo <tj@kernel.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | idr: deprecate idr_remove_all()Tejun Heo2013-02-271-7/+3
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | There was only one legitimate use of idr_remove_all() and a lot more of incorrect uses (or lack of it). Now that idr_destroy() implies idr_remove_all() and all the in-kernel users updated not to use it, there's no reason to keep it around. Mark it deprecated so that we can later unexport it. idr_remove_all() is made an inline function calling __idr_remove_all() to avoid triggering deprecated warning on EXPORT_SYMBOL(). Signed-off-by: Tejun Heo <tj@kernel.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | idr: make idr_destroy() imply idr_remove_all()Tejun Heo2013-02-271-9/+11
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | idr is silly in quite a few ways, one of which is how it's supposed to be destroyed - idr_destroy() doesn't release IDs and doesn't even whine if the idr isn't empty. If the caller forgets idr_remove_all(), it simply leaks memory. Even ida gets this wrong and leaks memory on destruction. There is absoltely no reason not to call idr_remove_all() from idr_destroy(). Nobody is abusing idr_destroy() for shrinking free layer buffer and continues to use idr after idr_destroy(), so it's safe to do remove_all from destroy. In the whole kernel, there is only one place where idr_remove_all() is legitimiately used without following idr_destroy() while there are quite a few places where the caller forgets either idr_remove_all() or idr_destroy() leaking memory. This patch makes idr_destroy() call idr_destroy_all() and updates the function description accordingly. Signed-off-by: Tejun Heo <tj@kernel.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | idr: fix a subtle bug in idr_get_next()Tejun Heo2013-02-271-1/+8
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The iteration logic of idr_get_next() is borrowed mostly verbatim from idr_for_each(). It walks down the tree looking for the slot matching the current ID. If the matching slot is not found, the ID is incremented by the distance of single slot at the given level and repeats. The implementation assumes that during the whole iteration id is aligned to the layer boundaries of the level closest to the leaf, which is true for all iterations starting from zero or an existing element and thus is fine for idr_for_each(). However, idr_get_next() may be given any point and if the starting id hits in the middle of a non-existent layer, increment to the next layer will end up skipping the same offset into it. For example, an IDR with IDs filled between [64, 127] would look like the following. [ 0 64 ... ] /----/ | | | NULL [ 64 ... 127 ] If idr_get_next() is called with 63 as the starting point, it will try to follow down the pointer from 0. As it is NULL, it will then try to proceed to the next slot in the same level by adding the slot distance at that level which is 64 - making the next try 127. It goes around the loop and finds and returns 127 skipping [64, 126]. Note that this bug also triggers in idr_for_each_entry() loop which deletes during iteration as deletions can make layers go away leaving the iteration with unaligned ID into missing layers. Fix it by ensuring proceeding to the next slot doesn't carry over the unaligned offset - ie. use round_up(id + 1, slot_distance) instead of id += slot_distance. Signed-off-by: Tejun Heo <tj@kernel.org> Reported-by: David Teigland <teigland@redhat.com> Cc: KAMEZAWA Hiroyuki <kamezawa.hiroyu@jp.fujitsu.com> Cc: <stable@vger.kernel.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | lib/scatterlist: use page iterator in the mapping iteratorImre Deak2013-02-271-25/+23
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | For better code reuse use the newly added page iterator to iterate through the pages. The offset, length within the page is still calculated by the mapping iterator as well as the actual mapping. Idea from Tejun Heo. Signed-off-by: Imre Deak <imre.deak@intel.com> Cc: Maxim Levitsky <maximlevitsky@gmail.com> Cc: Tejun Heo <tj@kernel.org> Cc: Daniel Vetter <daniel.vetter@ffwll.ch> Cc: James Hogan <james.hogan@imgtec.com> Cc: Stephen Warren <swarren@wwwdotorg.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | lib/scatterlist: add simple page iteratorImre Deak2013-02-271-0/+38
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Add an iterator to walk through a scatter list a page at a time starting at a specific page offset. As opposed to the mapping iterator this is meant to be small, performing well even in simple loops like collecting all pages on the scatterlist into an array or setting up an iommu table based on the pages' DMA address. Signed-off-by: Imre Deak <imre.deak@intel.com> Cc: Maxim Levitsky <maximlevitsky@gmail.com> Cc: Tejun Heo <tj@kernel.org> Cc: Daniel Vetter <daniel.vetter@ffwll.ch> Tested-by: Stephen Warren <swarren@wwwdotorg.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | lib/devres.c: fix misplaced #endifJingoo Han2013-02-271-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | A misplaced #endif causes link errors related to pcim_*() functions. This is because pcim_*() functions are related to CONFIG_PCI option, however these are not related to CONFIG_HAS_IOPORT option. Therefore, when CONFIG_PCI is enabled and CONFIG_HAS_IOPORT is not enabled, it makes link errors related to pcim_*() functions as below: drivers/ata/libata-sff.c:3233: undefined reference to `pcim_iomap_regions' drivers/ata/libata-sff.c:3238: undefined reference to `pcim_iomap_table' drivers/built-in.o: In function `ata_pci_sff_init_host': drivers/ata/libata-sff.c:2318: undefined reference to `pcim_iomap_regions' drivers/ata/libata-sff.c:2329: undefined reference to `pcim_iomap_table Signed-off-by: Jingoo Han <jg1.han@samsung.com> Cc: Greg KH <greg@kroah.com> Cc: Tejun Heo <tj@kernel.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | Merge tag 'modules-next-for-linus' of ↵Linus Torvalds2013-02-251-1/+2
|\ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/rusty/linux Pull module update from Rusty Russell: "The sweeping change is to make add_taint() explicitly indicate whether to disable lockdep, but it's a mechanical change." * tag 'modules-next-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/rusty/linux: MODSIGN: Add option to not sign modules during modules_install MODSIGN: Add -s <signature> option to sign-file MODSIGN: Specify the hash algorithm on sign-file command line MODSIGN: Simplify Makefile with a Kconfig helper module: clean up load_module a little more. modpost: Ignore ARC specific non-alloc sections module: constify within_module_* taint: add explicit flag to show whether lock dep is still OK. module: printk message when module signature fail taints kernel.
| * | | taint: add explicit flag to show whether lock dep is still OK.Rusty Russell2013-01-211-1/+2
| | |/ | |/| | | | | | | | | | | | | | | | Fix up all callers as they were before, with make one change: an unsigned module taints the kernel, but doesn't turn off lockdep. Signed-off-by: Rusty Russell <rusty@rustcorp.com.au>
* | | Merge branch 'core-locking-for-linus' of ↵Linus Torvalds2013-02-223-91/+87
|\ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip Pull core locking changes from Ingo Molnar: "The biggest change is the rwsem lock-steal improvements, both to the assembly optimized and the spinlock based variants. The other notable change is the clean up of the seqlock implementation to be based on the seqcount infrastructure. The rest is assorted smaller debuggability, cleanup and continued -rt locking changes." * 'core-locking-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip: rwsem-spinlock: Implement writer lock-stealing for better scalability futex: Revert "futex: Mark get_robust_list as deprecated" generic: Use raw local irq variant for generic cmpxchg lockdep: Selftest: convert spinlock to raw spinlock seqlock: Use seqcount infrastructure seqlock: Remove unused functions ntp: Make ntp_lock raw intel_idle: Convert i7300_idle_lock to raw_spinlock locking: Various static lock initializer fixes lockdep: Print more info when MAX_LOCK_DEPTH is exceeded rwsem: Implement writer lock-stealing for better scalability lockdep: Silence warning if CONFIG_LOCKDEP isn't set watchdog: Use local_clock for get_timestamp() lockdep: Rename print_unlock_inbalance_bug() to print_unlock_imbalance_bug() locking/stat: Fix a typo
| * | | rwsem-spinlock: Implement writer lock-stealing for better scalabilityYuanhan Liu2013-02-191-45/+24
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | We (Linux Kernel Performance project) found a regression introduced by commit: 5a505085f043 mm/rmap: Convert the struct anon_vma::mutex to an rwsem which converted all anon_vma::mutex locks rwsem write locks. The semantics are the same, but the behavioral difference is quite huge in some cases. After investigating it we found the root cause: mutexes support lock stealing while rwsems don't. Here is the link for the detailed regression report: https://lkml.org/lkml/2013/1/29/84 Ingo suggested adding write lock stealing to rwsems: "I think we should allow lock-steal between rwsem writers - that will not hurt fairness as most rwsem fairness concerns relate to reader vs. writer fairness" And here is the rwsem-spinlock version. With this patch, we got a double performance increase in one test box with following aim7 workfile: FILESIZE: 1M POOLSIZE: 10M 10 fork_test /usr/bin/time output w/o patch /usr/bin/time_output with patch -- Percent of CPU this job got: 369% Percent of CPU this job got: 537% Voluntary context switches: 640595016 Voluntary context switches: 157915561 We got a 45% increase in CPU usage and saved about 3/4 voluntary context switches. Reported-by: LKP project <lkp@linux.intel.com> Suggested-by: Ingo Molnar <mingo@kernel.org> Signed-off-by: Yuanhan Liu <yuanhan.liu@linux.intel.com> Cc: Alex Shi <alex.shi@intel.com> Cc: David Howells <dhowells@redhat.com> Cc: Michel Lespinasse <walken@google.com> Cc: Linus Torvalds <torvalds@linux-foundation.org> Cc: Andrew Morton <akpm@linux-foundation.org> Cc: Peter Zijlstra <a.p.zijlstra@chello.nl> Cc: Anton Blanchard <anton@samba.org> Cc: Arjan van de Ven <arjan@linux.intel.com> Cc: paul.gortmaker@windriver.com Link: http://lkml.kernel.org/r/1359716356-23865-1-git-send-email-yuanhan.liu@linux.intel.com Signed-off-by: Ingo Molnar <mingo@kernel.org>
| * | | lockdep: Selftest: convert spinlock to raw spinlockYong Zhang2013-02-191-17/+17
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | To make the lockdep selftest working on RT we need to convert the spinlock tests to a raw spinlock. Otherwise we cannot run the irq context checks. For mainline this is just annotational as spinlocks are mapped to raw_spinlocks anyway. Signed-off-by: Yong Zhang <yong.zhang0@gmail.com> Link: http://lkml.kernel.org/r/1334559716-18447-2-git-send-email-yong.zhang0@gmail.com Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
| * | | rwsem: Implement writer lock-stealing for better scalabilityAlex Shi2013-02-191-29/+46
| | |/ | |/| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Commit 5a505085f043 ("mm/rmap: Convert the struct anon_vma::mutex to an rwsem") changed struct anon_vma::mutex to an rwsem, which caused aim7 fork_test performance to drop by 50%. Yuanhan Liu did the following excellent analysis: https://lkml.org/lkml/2013/1/29/84 and found that the regression is caused by strict, serialized, FIFO sequential write-ownership of rwsems. Ingo suggested implementing opportunistic lock-stealing for the front writer task in the waitqueue. Yuanhan Liu implemented lock-stealing for spinlock-rwsems, which indeed recovered much of the regression - confirming the analysis that the main factor in the regression was the FIFO writer-fairness of rwsems. In this patch we allow lock-stealing to happen when the first waiter is also writer. With that change in place the aim7 fork_test performance is fully recovered on my Intel NHM EP, NHM EX, SNB EP 2S and 4S test-machines. Reported-by: lkp@linux.intel.com Reported-by: Yuanhan Liu <yuanhan.liu@linux.intel.com> Signed-off-by: Alex Shi <alex.shi@intel.com> Cc: David Howells <dhowells@redhat.com> Cc: Michel Lespinasse <walken@google.com> Cc: Linus Torvalds <torvalds@linux-foundation.org> Cc: Andrew Morton <akpm@linux-foundation.org> Cc: Peter Zijlstra <a.p.zijlstra@chello.nl> Cc: Anton Blanchard <anton@samba.org> Cc: Arjan van de Ven <arjan@linux.intel.com> Cc: paul.gortmaker@windriver.com Link: https://lkml.org/lkml/2013/1/29/84 Link: http://lkml.kernel.org/r/1360069915-31619-1-git-send-email-alex.shi@intel.com [ Small stylistic fixes, updated changelog. ] Signed-off-by: Ingo Molnar <mingo@kernel.org>
* | | Merge branch 'x86-mm-for-linus' of ↵Linus Torvalds2013-02-211-18/+29
|\ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip Pull x86 mm changes from Peter Anvin: "This is a huge set of several partly interrelated (and concurrently developed) changes, which is why the branch history is messier than one would like. The *really* big items are two humonguous patchsets mostly developed by Yinghai Lu at my request, which completely revamps the way we create initial page tables. In particular, rather than estimating how much memory we will need for page tables and then build them into that memory -- a calculation that has shown to be incredibly fragile -- we now build them (on 64 bits) with the aid of a "pseudo-linear mode" -- a #PF handler which creates temporary page tables on demand. This has several advantages: 1. It makes it much easier to support things that need access to data very early (a followon patchset uses this to load microcode way early in the kernel startup). 2. It allows the kernel and all the kernel data objects to be invoked from above the 4 GB limit. This allows kdump to work on very large systems. 3. It greatly reduces the difference between Xen and native (Xen's equivalent of the #PF handler are the temporary page tables created by the domain builder), eliminating a bunch of fragile hooks. The patch series also gets us a bit closer to W^X. Additional work in this pull is the 64-bit get_user() work which you were also involved with, and a bunch of cleanups/speedups to __phys_addr()/__pa()." * 'x86-mm-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip: (105 commits) x86, mm: Move reserving low memory later in initialization x86, doc: Clarify the use of asm("%edx") in uaccess.h x86, mm: Redesign get_user with a __builtin_choose_expr hack x86: Be consistent with data size in getuser.S x86, mm: Use a bitfield to mask nuisance get_user() warnings x86/kvm: Fix compile warning in kvm_register_steal_time() x86-32: Add support for 64bit get_user() x86-32, mm: Remove reference to alloc_remap() x86-32, mm: Remove reference to resume_map_numa_kva() x86-32, mm: Rip out x86_32 NUMA remapping code x86/numa: Use __pa_nodebug() instead x86: Don't panic if can not alloc buffer for swiotlb mm: Add alloc_bootmem_low_pages_nopanic() x86, 64bit, mm: hibernate use generic mapping_init x86, 64bit, mm: Mark data/bss/brk to nx x86: Merge early kernel reserve for 32bit and 64bit x86: Add Crash kernel low reservation x86, kdump: Remove crashkernel range find limit for 64bit memblock: Add memblock_mem_size() x86, boot: Not need to check setup_header version for setup_data ...
| * | | x86: Don't panic if can not alloc buffer for swiotlbYinghai Lu2013-01-291-18/+29
| | |/ | |/| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Normal boot path on system with iommu support: swiotlb buffer will be allocated early at first and then try to initialize iommu, if iommu for intel or AMD could setup properly, swiotlb buffer will be freed. The early allocating is with bootmem, and could panic when we try to use kdump with buffer above 4G only, or with memmap to limit mem under 4G. for example: memmap=4095M$1M to remove memory under 4G. According to Eric, add _nopanic version and no_iotlb_memory to fail map single later if swiotlb is still needed. -v2: don't pass nopanic, and use -ENOMEM return value according to Eric. panic early instead of using swiotlb_full to panic...according to Eric/Konrad. -v3: make swiotlb_init to be notpanic, but will affect: arm64, ia64, powerpc, tile, unicore32, x86. -v4: cleanup swiotlb_init by removing swiotlb_init_with_default_size. Suggested-by: Eric W. Biederman <ebiederm@xmission.com> Signed-off-by: Yinghai Lu <yinghai@kernel.org> Link: http://lkml.kernel.org/r/1359058816-7615-36-git-send-email-yinghai@kernel.org Reviewed-and-tested-by: Konrad Rzeszutek Wilk <konrad.wilk@oracle.com> Cc: Joerg Roedel <joro@8bytes.org> Cc: Ralf Baechle <ralf@linux-mips.org> Cc: Jeremy Fitzhardinge <jeremy@goop.org> Cc: Kyungmin Park <kyungmin.park@samsung.com> Cc: Marek Szyprowski <m.szyprowski@samsung.com> Cc: Arnd Bergmann <arnd@arndb.de> Cc: Andrzej Pietrasiewicz <andrzej.p@samsung.com> Cc: linux-mips@linux-mips.org Cc: xen-devel@lists.xensource.com Cc: virtualization@lists.linux-foundation.org Cc: Shuah Khan <shuahkhan@gmail.com> Signed-off-by: H. Peter Anvin <hpa@linux.intel.com>
* | | Merge branch 'akpm' (incoming from Andrew)Linus Torvalds2013-02-214-23/+27
|\ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Merge misc patches from Andrew Morton: - Florian has vanished so I appear to have become fbdev maintainer again :( - Joel and Mark are distracted to welcome to the new OCFS2 maintainer - The backlight queue - Small core kernel changes - lib/ updates - The rtc queue - Various random bits * akpm: (164 commits) rtc: rtc-davinci: use devm_*() functions rtc: rtc-max8997: use devm_request_threaded_irq() rtc: rtc-max8907: use devm_request_threaded_irq() rtc: rtc-da9052: use devm_request_threaded_irq() rtc: rtc-wm831x: use devm_request_threaded_irq() rtc: rtc-tps80031: use devm_request_threaded_irq() rtc: rtc-lp8788: use devm_request_threaded_irq() rtc: rtc-coh901331: use devm_clk_get() rtc: rtc-vt8500: use devm_*() functions rtc: rtc-tps6586x: use devm_request_threaded_irq() rtc: rtc-imxdi: use devm_clk_get() rtc: rtc-cmos: use dev_warn()/dev_dbg() instead of printk()/pr_debug() rtc: rtc-pcf8583: use dev_warn() instead of printk() rtc: rtc-sun4v: use pr_warn() instead of printk() rtc: rtc-vr41xx: use dev_info() instead of printk() rtc: rtc-rs5c313: use pr_err() instead of printk() rtc: rtc-at91rm9200: use dev_dbg()/dev_err() instead of printk()/pr_debug() rtc: rtc-rs5c372: use dev_dbg()/dev_warn() instead of printk()/pr_debug() rtc: rtc-ds2404: use dev_err() instead of printk() rtc: rtc-efi: use dev_err()/dev_warn()/pr_err() instead of printk() ...
| * | | decompressors: make the default XZ_DEC_* config match the selected architectureFlorian Fainelli2013-02-211-6/+6
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Change the defautl XZ_DEC_* config symbol to match the configured architecture. It is perfectly legitimate to support multiple XZ BCJ filters for different architectures (e.g.: to mount foreign squashfs/xz compressed filesystems), it is however more natural not to select them all by default, but only the one matching the configured architecture. Signed-off-by: Florian Fainelli <florian@openwrt.org> Acked-by: Lasse Collin <lasse.collin@tukaani.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
| * | | decompressors: drop dependency on CONFIG_EXPERTFlorian Fainelli2013-02-211-6/+6
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Remove the XZ_DEC_* depedencey on CONFIG_EXPERT as recommended by Lasse Colin. Signed-off-by: Florian Fainelli <florian@openwrt.org> Acked-by: Lasse Collin <lasse.collin@tukaani.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
| * | | decompressors: group XZ_DEC_* symbols under an if XZ_BCJ / endifFlorian Fainelli2013-02-211-6/+4
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Group all architecture-specific BCJ filter configuration symbols under an if XZ_BCJ / endif statement. Signed-off-by: Florian Fainelli <florian@openwrt.org> Acked-by: Lasse Collin <lasse.collin@tukaani.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
| * | | lib/parser.c: fix up comments for valid return values from match_numberNamjae Jeon2013-02-211-3/+3
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | match_number() has return values of -ENOMEM, -EINVAL and -ERANGE. So, for all the functions calling match_number, the return value should include these values. Fix up the comments to reflect the correct values. Signed-off-by: Namjae Jeon <namjae.jeon@samsung.com> Signed-off-by: Amit Sahrawat <a.sahrawat@samsung.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
| * | | lib/vsprintf.c: add %pa format specifier for phys_addr_t typesStepan Moskovchenko2013-02-211-0/+7
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Add the %pa format specifier for printing a phys_addr_t type and its derivative types (such as resource_size_t), since the physical address size on some platforms can vary based on build options, regardless of the native integer type. Signed-off-by: Stepan Moskovchenko <stepanm@codeaurora.org> Cc: Rob Landley <rob@landley.net> Cc: George Spelvin <linux@horizon.com> Cc: Andy Shevchenko <andriy.shevchenko@linux.intel.com> Cc: Stephen Boyd <sboyd@codeaurora.org> Cc: Andrei Emeltchenko <andrei.emeltchenko@intel.com> Cc: Ingo Molnar <mingo@elte.hu> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
| * | | lib/Kconfig.debug: unhide CONFIG_PANIC_ON_OOPSKyle McMartin2013-02-211-2/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | CONFIG_EXPERT doesn't really make sense, and hides it unintentionally. Remove superfluous "default n" pointed out by Ingo as well. Signed-off-by: Kyle McMartin <kyle@redhat.com> Acked-by: Ingo Molnar <mingo@kernel.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | | Merge tag 'tty-3.9-rc1' of ↵Linus Torvalds2013-02-211-0/+1
|\ \ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/gregkh/tty Pull tty/serial patches from Greg Kroah-Hartman: "Here's the big tty/serial driver patches for 3.9-rc1. More tty port rework and fixes from Jiri here, as well as lots of individual serial driver updates and fixes. All of these have been in the linux-next tree for a while." * tag 'tty-3.9-rc1' of git://git.kernel.org/pub/scm/linux/kernel/git/gregkh/tty: (140 commits) tty: mxser: improve error handling in mxser_probe() and mxser_module_init() serial: imx: fix uninitialized variable warning serial: tegra: assume CONFIG_OF TTY: do not update atime/mtime on read/write lguest: select CONFIG_TTY to build properly. ARM defconfigs: add missing inclusions of linux/platform_device.h fb/exynos: include platform_device.h ARM: sa1100/assabet: include platform_device.h directly serial: imx: Fix recursive locking bug pps: Fix build breakage from decoupling pps from tty tty: Remove ancient hardpps() pps: Additional cleanups in uart_handle_dcd_change pps: Move timestamp read into PPS code proper pps: Don't crash the machine when exiting will do pps: Fix a use-after free bug when unregistering a source. pps: Use pps_lookup_dev to reduce ldisc coupling pps: Add pps_lookup_dev() function tty: serial: uartlite: Support uartlite on big and little endian systems tty: serial: uartlite: Fix sparse and checkpatch warnings serial/arc-uart: Miscll DT related updates (Grant's review comments) ... Fix up trivial conflicts, mostly just due to the TTY config option clashing with the EXPERIMENTAL removal.
| * \ \ \ Merge 3.8-rc5 into tty-nextGreg Kroah-Hartman2013-01-253-8/+67
| |\ \ \ \ | | | |/ / | | |/| | | | | | | | | | | | | | | | | This resolves a number of tty driver merge issues found in linux-next Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
| * | | | tty: Added a CONFIG_TTY option to allow removal of TTYJoe Millenbach2013-01-181-0/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The option allows you to remove TTY and compile without errors. This saves space on systems that won't support TTY interfaces anyway. bloat-o-meter output is below. The bulk of this patch consists of Kconfig changes adding "depends on TTY" to various serial devices and similar drivers that require the TTY layer. Ideally, these dependencies would occur on a common intermediate symbol such as SERIO, but most drivers "select SERIO" rather than "depends on SERIO", and "select" does not respect dependencies. bloat-o-meter output comparing our previous minimal to new minimal by removing TTY. The list is filtered to not show removed entries with awk '$3 != "-"' as the list was very long. add/remove: 0/226 grow/shrink: 2/14 up/down: 6/-35356 (-35350) function old new delta chr_dev_init 166 170 +4 allow_signal 80 82 +2 static.__warned 143 142 -1 disallow_signal 63 62 -1 __set_special_pids 95 94 -1 unregister_console 126 121 -5 start_kernel 546 541 -5 register_console 593 588 -5 copy_from_user 45 40 -5 sys_setsid 128 120 -8 sys_vhangup 32 19 -13 do_exit 1543 1526 -17 bitmap_zero 60 40 -20 arch_local_irq_save 137 117 -20 release_task 674 652 -22 static.spin_unlock_irqrestore 308 260 -48 Signed-off-by: Joe Millenbach <jmillenbach@gmail.com> Reviewed-by: Jamey Sharp <jamey@minilop.net> Reviewed-by: Josh Triplett <josh@joshtriplett.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* | | | | Merge tag 'driver-core-3.9-rc1' of ↵Linus Torvalds2013-02-216-85/+148
|\ \ \ \ \ | |_|_|/ / |/| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/gregkh/driver-core Pull driver core patches from Greg Kroah-Hartman: "Here is the big driver core merge for 3.9-rc1 There are two major series here, both of which touch lots of drivers all over the kernel, and will cause you some merge conflicts: - add a new function called devm_ioremap_resource() to properly be able to check return values. - remove CONFIG_EXPERIMENTAL Other than those patches, there's not much here, some minor fixes and updates" Fix up trivial conflicts * tag 'driver-core-3.9-rc1' of git://git.kernel.org/pub/scm/linux/kernel/git/gregkh/driver-core: (221 commits) base: memory: fix soft/hard_offline_page permissions drivercore: Fix ordering between deferred_probe and exiting initcalls backlight: fix class_find_device() arguments TTY: mark tty_get_device call with the proper const values driver-core: constify data for class_find_device() firmware: Ignore abort check when no user-helper is used firmware: Reduce ifdef CONFIG_FW_LOADER_USER_HELPER firmware: Make user-mode helper optional firmware: Refactoring for splitting user-mode helper code Driver core: treat unregistered bus_types as having no devices watchdog: Convert to devm_ioremap_resource() thermal: Convert to devm_ioremap_resource() spi: Convert to devm_ioremap_resource() power: Convert to devm_ioremap_resource() mtd: Convert to devm_ioremap_resource() mmc: Convert to devm_ioremap_resource() mfd: Convert to devm_ioremap_resource() media: Convert to devm_ioremap_resource() iommu: Convert to devm_ioremap_resource() drm: Convert to devm_ioremap_resource() ...
| * | | | Merge 3.8-rc5 into driver-core-nextGreg Kroah-Hartman2013-01-251-0/+1
| |\ \ \ \ | | | |/ / | | |/| | | | | | | | | | | | | | | | | This resolves a gpio driver merge issue pointed out in linux-next. Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
| * | | | lib: devres: Fix build breakageThierry Reding2013-01-221-0/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The ERR_PTR() and IS_ERR() macros used by the devm_ioremap_resource() function are defined in the linux/err.h header. On ARM this seems to be pulled in by one of the other headers but the build fails at least on OpenRISC. Signed-off-by: Thierry Reding <thierry.reding@avionic-design.de> Reported-by: kbuild test robot <fengguang.wu@intel.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
| * | | | lib: devres: Introduce devm_ioremap_resource()Thierry Reding2013-01-221-13/+44
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The devm_request_and_ioremap() function is very useful and helps avoid a whole lot of boilerplate. However, one issue that keeps popping up is its lack of a specific error code to determine which of the steps that it performs failed. Furthermore, while the function gives an example and suggests what error code to return on failure, a wide variety of error codes are used throughout the tree. In an attempt to fix these problems, this patch adds a new function that drivers can transition to. The devm_ioremap_resource() returns a pointer to the remapped I/O memory on success or an ERR_PTR() encoded error code on failure. Callers can check for failure using IS_ERR() and determine its cause by extracting the error code using PTR_ERR(). devm_request_and_ioremap() is implemented as a wrapper around the new API and return NULL on failure as before. This ensures that backwards compatibility is maintained until all users have been converted to the new API, at which point the old devm_request_and_ioremap() function should be removed. A semantic patch is included which can be used to convert from the old devm_request_and_ioremap() API to the new devm_ioremap_resource() API. Some non-trivial cases may require manual intervention, though. Signed-off-by: Thierry Reding <thierry.reding@avionic-design.de> Cc: Arnd Bergmann <arnd@arndb.de> Acked-by: Dmitry Torokhov <dmitry.torokhov@gmail.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>