From 38a12b5b029dec6e6dad1b5d3269b4c356c44c0e Mon Sep 17 00:00:00 2001 From: Johannes Berg Date: Fri, 22 Feb 2013 14:07:56 +0100 Subject: iwlwifi: mvm: fix AP/GO mode station removal When stations are removed while packets are in the queue, we drain the queues first, and then remove the stations. If this happens in AP mode while the interface is removed the MAC context might be removed from the firmware before we removed the station(s), resulting in a SYSASSERT 3421. This is because we remove the MAC context from the FW in stop_ap(), but only flush the station drain work later in remove_interface(). Refactor the code a bit to have a common MAC context removal preparation first to solve this. Reviewed-by: Emmanuel Grumbach Signed-off-by: Johannes Berg --- drivers/net/wireless/iwlwifi/mvm/mac80211.c | 19 ++++++++++++++----- 1 file changed, 14 insertions(+), 5 deletions(-) diff --git a/drivers/net/wireless/iwlwifi/mvm/mac80211.c b/drivers/net/wireless/iwlwifi/mvm/mac80211.c index e8264e11b12..7e169b085af 100644 --- a/drivers/net/wireless/iwlwifi/mvm/mac80211.c +++ b/drivers/net/wireless/iwlwifi/mvm/mac80211.c @@ -557,11 +557,9 @@ static int iwl_mvm_mac_add_interface(struct ieee80211_hw *hw, return ret; } -static void iwl_mvm_mac_remove_interface(struct ieee80211_hw *hw, - struct ieee80211_vif *vif) +static void iwl_mvm_prepare_mac_removal(struct iwl_mvm *mvm, + struct ieee80211_vif *vif) { - struct iwl_mvm *mvm = IWL_MAC80211_GET_MVM(hw); - struct iwl_mvm_vif *mvmvif = iwl_mvm_vif_from_mac80211(vif); u32 tfd_msk = 0, ac; for (ac = 0; ac < IEEE80211_NUM_ACS; ac++) @@ -594,12 +592,21 @@ static void iwl_mvm_mac_remove_interface(struct ieee80211_hw *hw, */ flush_work(&mvm->sta_drained_wk); } +} + +static void iwl_mvm_mac_remove_interface(struct ieee80211_hw *hw, + struct ieee80211_vif *vif) +{ + struct iwl_mvm *mvm = IWL_MAC80211_GET_MVM(hw); + struct iwl_mvm_vif *mvmvif = iwl_mvm_vif_from_mac80211(vif); + + iwl_mvm_prepare_mac_removal(mvm, vif); mutex_lock(&mvm->mutex); /* * For AP/GO interface, the tear down of the resources allocated to the - * interface should be handled as part of the bss_info_changed flow. + * interface is be handled as part of the stop_ap flow. */ if (vif->type == NL80211_IFTYPE_AP) { iwl_mvm_dealloc_int_sta(mvm, &mvmvif->bcast_sta); @@ -763,6 +770,8 @@ static void iwl_mvm_stop_ap(struct ieee80211_hw *hw, struct ieee80211_vif *vif) struct iwl_mvm *mvm = IWL_MAC80211_GET_MVM(hw); struct iwl_mvm_vif *mvmvif = iwl_mvm_vif_from_mac80211(vif); + iwl_mvm_prepare_mac_removal(mvm, vif); + mutex_lock(&mvm->mutex); mvmvif->ap_active = false; -- cgit v1.2.3-54-g00ecf