# This a generic Palo configuration file. For more information about how # it works try 'palo -?'. # # Most people using 'make palo' want a bootable file, usable for # network or tape booting for example. --init-tape=lifimage --recoverykernel=vmlinux ########## Pick your ROOT here! ########## # You need at least one 'root='! # # If you want a root ramdisk, use the next 2 lines # (Edit the ramdisk image name!!!!) --ramdisk=ram-disk-image-file --commandline=0/vmlinux HOME=/ root=/dev/ram initrd=0/ramdisk # If you want NFS root, use the following command line (Edit the HOSTNAME!!!) #--commandline=0/vmlinux HOME=/ root=/dev/nfs nfsroot=HOSTNAME ip=bootp # If you have root on a disk partition, use this (Edit the partition name!!!) #--commandline=0/vmlinux HOME=/ root=/dev/sda1