/* * mm/truncate.c - code for taking down pages from address_spaces * * Copyright (C) 2002, Linus Torvalds * * 10Sep2002 Andrew Morton * Initial version. */ #include #include #include #include #include #include #include #include #include #include #include /* grr. try_to_release_page, do_invalidatepage */ #include #include "internal.h" /** * do_invalidatepage - invalidate part or all of a page * @page: the page which is affected * @offset: the index of the truncation point * * do_invalidatepage() is called when all or part of the page has become * invalidated by a truncate operation. * * do_invalidatepage() does not have to release all buffers, but it must * ensure that no dirty buffer is left outside @offset and that no I/O * is underway against any of the blocks which are outside the truncation * point. Because the caller is about to free (and possibly reuse) those * blocks on-disk. */ void do_invalidatepage(struct page *page, unsigned long offset) { void (*invalidatepage)(struct page *, unsigned long); invalidatepage = page->mapping->a_ops->invalidatepage; #ifdef CONFIG_BLOCK if (!invalidatepage) invalidatepage = block_invalidatepage; #endif if (invalidatepage) (*invalidatepage)(page, offset); } static inline void truncate_partial_page(struct page *page, unsigned partial) { zero_user_segment(page, partial, PAGE_CACHE_SIZE); cleancache_invalidate_page(page->mapping, page); if (page_has_private(page)) do_invalidatepage(page, partial); } /* * This cancels just the dirty bit on the kernel page itself, it * does NOT actually remove dirty bits on any mmap's that may be * around. It also leaves the page tagged dirty, so any sync * activity will still find it on the dirty lists, and in particular, * clear_page_dirty_for_io() will still look at the dirty bits in * the VM. * * Doing this should *normally* only ever be done when a page * is truncated, and is not actually mapped anywhere at all. However, * fs/buffer.c does this when it notices that somebody has cleaned * out all the buffers on a page without actually doing it through * the VM. Can you say "ext3 is horribly ugly"? Tought you could. */ void cancel_dirty_page(struct page *page, unsigned int account_size) { if (TestClearPageDirty(page)) { struct address_space *mapping = page->mapping; if (mapping && mapping_cap_account_dirty(mapping)) { dec_zone_page_state(page, NR_FILE_DIRTY); dec_bdi_stat(mapping->backing_dev_info, BDI_RECLAIMABLE); if (account_size) task_io_account_cancelled_write(account_size); } } } EXPORT_SYMBOL(cancel_dirty_page); /* * If truncate cannot remove the fs-private metadata from the page, the page * becomes orphaned. It will be left on the LRU and may even be mapped into * user pagetables if we're racing with filemap_fault(). * * We need to bale out if page->mapping is no longer equal to the original * mapping. This happens a) when the VM reclaimed the page while we waited on * its lock, b) when a concurrent invalidate_mapping_pages got there first and * c) when tmpfs swizzles a page between a tmpfs inode and swapper_space. */ static int truncate_complete_page(struct address_space *mapping, struct page *page) { if (page->mapping != mapping) return -EIO; if (page_has_private(page)) do_invalidatepage(page, 0); cancel_dirty_page(page, PAGE_CACHE_SIZE); ClearPageMappedToDisk(page); delete_from_page_cache(page); return 0; } /* * This is for invalidate_mapping_pages(). That function can be called at * any time, and is not supposed to throw away dirty pages. But pages can * be marked dirty at any time too, so use remove_mapping which safely * discards clean, unused pages. * * Returns non-zero if the page was successfully invalidated. */ static int invalidate_complete_page(struct address_space *mapping, struct page *page) { int ret; if (page->mapping != mapping) return 0; if (page_has_private(page) && !try_to_release_page(page, 0)) return 0; ret = remove_mapping(mapping, page); return ret; } int truncate_inode_page(struct address_space *mapping, struct page *page) { if (page_mapped(page)) { unmap_mapping_range(mapping, (loff_t)page->index << PAGE_CACHE_SHIFT, PAGE_CACHE_SIZE, 0); } return truncate_complete_page(mapping, page); } /* * Used to get rid of pages on hardware memory corruption. */ int generic_error_remove_page(struct address_space *mapping, struct page *page) { if (!mapping) return -EINVAL; /* * Only punch for normal data pages for now. * Handling other types like directories would need more auditing. */ if (!S_ISREG(mapping->host->i_mode)) return -EIO; return truncate_inode_page(mapping, page); } EXPORT_SYMBOL(generic_error_remove_page); /* * Safely invalidate one page from its pagecache mapping. * It only drops clean, unused pages. The page must be locked. * * Returns 1 if the page is successfully invalidated, otherwise 0. */ int invalidate_inode_page(struct page *page) { struct address_space *mapping = page_mapping(page); if (!mapping) return 0; if (PageDirty(page) || PageWriteback(page)) return 0; if (page_mapped(page)) return 0; return invalidate_complete_page(mapping, page); } /** * truncate_inode_pages_range - truncate range of pages specified by start & end byte offsets * @mapping: mapping to truncate * @lstart: offset from which to truncate * @lend: offset to which to truncate * * Truncate the page cache, removing the pages that are between * specified offsets (and zeroing out partial page * (if lstart is not page aligned)). * * Truncate takes two passes - the first pass is nonblocking. It will not * block on page locks and it will not block on writeback. The second pass * will wait. This is to prevent as much IO as possible in the affected region. * The first pass will remove most pages, so the search cost of the second pass * is low. * * We pass down the cache-hot hint to the page freeing code. Even if the * mapping is large, it is probably the case that the final pages are the most * recently touched, and freeing happens in ascending file offset order. */ void truncate_inode_pages_range(struct address_space *mapping, loff_t lstart, loff_t lend) { const pgoff_t start = (lstart + PAGE_CACHE_SIZE-1) >> PAGE_CACHE_SHIFT; const unsigned partial = lstart & (PAGE_CACHE_SIZE - 1); struct pagevec pvec; pgoff_t index; pgoff_t end; int i; cleancache_invalidate_inode(mapping); if (mapping->nrpages == 0) return; BUG_ON((lend & (PAGE_CACHE_SIZE - 1)) != (PAGE_CACHE_SIZE - 1)); end = (lend >> PAGE_CACHE_SHIFT); pagevec_init(&pvec, 0); index = start; while (index <= end && pagevec_lookup(&pvec, mapping, index, min(end - index, (pgoff_t)PAGEVEC_SIZE - 1) + 1)) { mem_cgroup_uncharge_start(); for (i = 0; i < pagevec_count(&pvec); i++) { struct page *page = pvec.pages[i]; /* We rely upon deletion not changing page->index */ index = page->index; if (index > end) break; if (!trylock_page(page)) continue; WARN_ON(page->index != index); if (PageWriteback(page)) { unlock_page(page); continue; } truncate_inode_page(mapping, page); unlock_page(page); } pagevec_release(&pvec); mem_cgroup_uncharge_end(); cond_resched(); index++; } if (partial) { struct page *page = find_lock_page(mapping, start - 1); if (page) { wait_on_page_writeback(page); truncate_partial_page(page, partial); unlock_page(page); page_cache_release(page); } } index = start; for ( ; ; ) { cond_resched(); if (!pagevec_lookup(&pvec, mapping, index, min(end - index, (pgoff_t)PAGEVEC_SIZE - 1) + 1)) { if (index == start) break; index = start; continue; } if (index == start && pvec.pages[0]->index > end) { pagevec_release(&pvec); break; } mem_cgroup_uncharge_start(); for (i = 0; i < pagevec_count(&pvec); i++) { struct page *page = pvec.pages[i]; /* We rely upon deletion not changing page->index */ index = page->index; if (index > end) break; lock_page(page); WARN_ON(page->index != index); wait_on_page_writeback(page); truncate_inode_page(mapping, page); unlock_page(page); } pagevec_release(&pvec); mem_cgroup_uncharge_end(); index++; } cleancache_invalidate_inode(mapping); } EXPORT_SYMBOL(truncate_inode_pages_range); /** * truncate_inode_pages - truncate *all* the pages from an offset * @mapping: mapping to truncate * @lstart: offset from which to truncate * * Called under (and serialised by) inode->i_mutex. * * Note: When this function returns, there can be a page in the process of * deletion (inside __delete_from_page_cache()) in the specified range. Thus * mapping->nrpages can be non-zero when this function returns even after * truncation of the whole mapping. */ void truncate_inode_pages(struct address_space *mapping, loff_t lstart) { truncate_inode_pages_range(mapping, lstart, (loff_t)-1); } EXPORT_SYMBOL(truncate_inode_pages); /** * invalidate_mapping_pages - Invalidate all the unlocked pages of one inode * @mapping: the address_space which holds the pages to invalidate * @start: the offset 'from' which to invalidate * @end: the offset 'to' which to invalidate (inclusive) * * This function only removes the unlocked pages, if you want to * remove all the pages of one inode, you must call truncate_inode_pages. * * invalidate_mapping_pages() will not block on IO activity. It will not * invalidate pages which are dirty, locked, under writeback or mapped into * pagetables. */ unsigned long invalidate_mapping_pages(struct address_space *mapping, pgoff_t start, pgoff_t end) { struct pagevec pvec; pgoff_t index = start; unsigned long ret; unsigned long count = 0; int i; /* * Note: this function may get called on a shmem/tmpfs mapping: * pagevec_lookup() might then return 0 prematurely (because it * got a gangful of swap entries); but it's hardly worth worrying * about - it can rarely have anything to free from such a mapping * (most pages are dirty), and already skips over any difficulties. */ pagevec_init(&pvec, 0); while (index <= end && pagevec_lookup(&pvec, mapping, index, min(end - index, (pgoff_t)PAGEVEC_SIZE - 1) + 1)) { mem_cgroup_uncharge_start(); for (i = 0; i < pagevec_count(&pvec); i++) { struct page *page = pvec.pages[i]; /* We rely upon deletion not changing page->index */ index = page->index; if (index > end) break; if (!trylock_page(page)) continue; WARN_ON(page->index != index); ret = invalidate_inode_page(page); unlock_page(page); /* * Invalidation is a hint that the page is no longer * of interest and try to speed up its reclaim. */ if (!ret) deactivate_page(page); count += ret; } pagevec_release(&pvec); mem_cgroup_uncharge_end(); cond_resched(); index++; } return count; } EXPORT_SYMBOL(invalidate_mapping_pages); /* * This is like invalidate_complete_page(), except it ignores the page's * refcount. We do this because invalidate_inode_pages2() needs stronger * invalidation guarantees, and cannot afford to leave pages behind because * shrink_page_list() has a temp ref on them, or because they're transiently * sitting in the lru_cache_add() pagevecs. */ static int invalidate_complete_page2(struct address_space *mapping, struct page *page) { if (page->mapping != mapping) return 0; if (page_has_private(page) && !try_to_release_page(page, GFP_KERNEL)) return 0; spin_lock_irq(&mapping->tree_lock); if (PageDirty(page)) goto failed; BUG_ON(page_has_private(page)); __delete_from_page_cache(page); spin_unlock_irq(&mapping->tree_lock); mem_cgroup_uncharge_cache_page(page); if (mapping->a_ops->freepage) mapping->a_ops->freepage(page); page_cache_release(page); /* pagecache ref */ return 1; failed: spin_unlock_irq(&mapping->tree_lock); return 0; } static int do_launder_page(struct address_space *mapping, struct page *page) { if (!PageDirty(page)) return 0; if (page->mapping != mapping || mapping->a_ops->launder_page == NULL) return 0; return mapping->a_ops->launder_page(page); } /** * invalidate_inode_pages2_range - remove range of pages from an address_space * @mapping: the address_space * @start: the page offset 'from' which to invalidate * @end: the page offset 'to' which to invalidate (inclusive) * * Any pages which are found to be mapped into pagetables are unmapped prior to * invalidation. * * Returns -EBUSY if any pages could not be invalidated. */ int invalidate_inode_pages2_range(struct address_space *mapping, pgoff_t start, pgoff_t end) { struct pagevec pvec; pgoff_t index; int i; int ret = 0; int ret2 = 0; int did_range_unmap = 0; cleancache_invalidate_inode(mapping); pagevec_init(&pvec, 0); index = start; while (index <= end && pagevec_lookup(&pvec, mapping, index, min(end - index, (pgoff_t)PAGEVEC_SIZE - 1) + 1)) { mem_cgroup_uncharge_start(); for (i = 0; i < pagevec_count(&pvec); i++) { struct page *page = pvec.pages[i]; /* We rely upon deletion not changing page->index */ index = page->index; if (index > end) break; lock_page(page); WARN_ON(page->index != index); if (page->mapping != mapping) { unlock_page(page); continue; } wait_on_page_writeback(page); if (page_mapped(page)) { if (!did_range_unmap) { /* * Zap the rest of the file in one hit. */ unmap_mapping_range(mapping, (loff_t)index << PAGE_CACHE_SHIFT, (loff_t)(1 + end - index) << PAGE_CACHE_SHIFT, 0); did_range_unmap = 1; } else { /* * Just zap this page */ unmap_mapping_range(mapping, (loff_t)index << PAGE_CACHE_SHIFT, PAGE_CACHE_SIZE, 0); } } BUG_ON(page_mapped(page)); ret2 = do_launder_page(mapping, page); if (ret2 == 0) { if (!invalidate_complete_page2(mapping, page)) ret2 = -EBUSY; } if (ret2 < 0) ret = ret2; unlock_page(page); } pagevec_release(&pvec); mem_cgroup_uncharge_end(); cond_resched(); index++; } cleancache_invalidate_inode(mapping); return ret; } EXPORT_SYMBOL_GPL(invalidate_inode_pages2_range); /** * invalidate_inode_pages2 - remove all pages from an address_space * @mapping: the address_space * * Any pages which are found to be mapped into pagetables are unmapped prior to * invalidation. * * Returns -EBUSY if any pages could not be invalidated. */ int invalidate_inode_pages2(struct address_space *mapping) { return invalidate_inode_pages2_range(mapping, 0, -1); } EXPORT_SYMBOL_GPL(invalidate_inode_pages2); /** * truncate_pagecache - unmap and remove pagecache that has been truncated * @inode: inode * @oldsize: old file size * @newsize: new file size * * inode's new i_size must already be written before truncate_pagecache * is called. * * This function should typically be called before the filesystem * releases resources associated with the freed range (eg. deallocates * blocks). This way, pagecache will always stay logically coherent * with on-disk format, and the filesystem would not have to deal with * situations such as writepage being called for a page that has already * had its underlying blocks deallocated. */ void truncate_pagecache(struct inode *inode, loff_t oldsize, loff_t newsize) { struct address_space *mapping = inode->i_mapping; loff_t holebegin = round_up(newsize, PAGE_SIZE); /* * unmap_mapping_range is called twice, first simply for * efficiency so that truncate_inode_pages does fewer * single-page unmaps. However after this first call, and * before truncate_inode_pages finishes, it is possible for * private pages to be COWed, which remain after * truncate_inode_pages finishes, hence the second * unmap_mapping_range call must be made for correctness. */ unmap_mapping_range(mapping, holebegin, 0, 1); truncate_inode_pages(mapping, newsize); unmap_mapping_range(mapping, holebegin, 0, 1); } EXPORT_SYMBOL(truncate_pagecache); /** * truncate_setsize - update inode and pagecache for a new file size * @inode: inode * @newsize: new file size * * truncate_setsize updates i_size and performs pagecache truncation (if * necessary) to @newsize. It will be typically be called from the filesystem's * setattr function when ATTR_SIZE is passed in. * * Must be called with inode_mutex held and before all filesystem specific * block truncation has been performed. */ void truncate_setsize(struct inode *inode, loff_t newsize) { loff_t oldsize; oldsize = inode->i_size; i_size_write(inode, newsize); truncate_pagecache(inode, oldsize, newsize); } EXPORT_SYMBOL(truncate_setsize); /** * truncate_pagecache_range - unmap and remove pagecache that is hole-punched * @inode: inode * @lstart: offset of beginning of hole * @lend: offset of last byte of hole * * This function should typically be called before the filesystem * releases resources associated with the freed range (eg. deallocates * blocks). This way, pagecache will always stay logically coherent * with on-disk format, and the filesystem would not have to deal with * situations such as writepage being called for a page that has already * had its underlying blocks deallocated. */ void truncate_pagecache_range(struct inode *inode, loff_t lstart, loff_t lend) { struct address_space *mapping = inode->i_mapping; loff_t unmap_start = round_up(lstart, PAGE_SIZE); loff_t unmap_end = round_down(1 + lend, PAGE_SIZE) - 1; /* * This rounding is currently just for example: unmap_mapping_range * expands its hole outwards, whereas we want it to contract the hole * inwards. However, existing callers of truncate_pagecache_range are * doing their own page rounding first; and truncate_inode_pages_range * currently BUGs if lend is not pagealigned-1 (it handles partial * page at start of hole, but not partial page at end of hole). Note * unmap_mapping_range allows holelen 0 for all, and we allow lend -1. */ /* * Unlike in truncate_pagecache, unmap_mapping_range is called only * once (before truncating pagecache), and without "even_cows" flag: * hole-punching should not remove private COWed pages from the hole. */ if ((u64)unmap_end > (u64)unmap_start) unmap_mapping_range(mapping, unmap_start, 1 + unmap_end - unmap_start, 0); truncate_inode_pages_range(mapping, lstart, lend); } EXPORT_SYMBOL(truncate_pagecache_range);