aboutsummaryrefslogtreecommitdiffstats
blob: a462b317f9a0002bb5d35de480f97c8a70b43c3f (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
/*
 * latencytop.c: Latency display infrastructure
 *
 * (C) Copyright 2008 Intel Corporation
 * Author: Arjan van de Ven <arjan@linux.intel.com>
 *
 * This program is free software; you can redistribute it and/or
 * modify it under the terms of the GNU General Public License
 * as published by the Free Software Foundation; version 2
 * of the License.
 */

/*
 * CONFIG_LATENCYTOP enables a kernel latency tracking infrastructure that is
 * used by the "latencytop" userspace tool. The latency that is tracked is not
 * the 'traditional' interrupt latency (which is primarily caused by something
 * else consuming CPU), but instead, it is the latency an application encounters
 * because the kernel sleeps on its behalf for various reasons.
 *
 * This code tracks 2 levels of statistics:
 * 1) System level latency
 * 2) Per process latency
 *
 * The latency is stored in fixed sized data structures in an accumulated form;
 * if the "same" latency cause is hit twice, this will be tracked as one entry
 * in the data structure. Both the count, total accumulated latency and maximum
 * latency are tracked in this data structure. When the fixed size structure is
 * full, no new causes are tracked until the buffer is flushed by writing to
 * the /proc file; the userspace tool does this on a regular basis.
 *
 * A latency cause is identified by a stringified backtrace at the point that
 * the scheduler gets invoked. The userland tool will use this string to
 * identify the cause of the latency in human readable form.
 *
 * The information is exported via /proc/latency_stats and /proc/<pid>/latency.
 * These files look like this:
 *
 * Latency Top version : v0.1
 * 70 59433 4897 i915_irq_wait drm_ioctl vfs_ioctl do_vfs_ioctl sys_ioctl
 * |    |    |    |
 * |    |    |    +----> the stringified backtrace
 * |    |    +---------> The maximum latency for this entry in microseconds
 * |    +--------------> The accumulated latency for this entry (microseconds)
 * +-------------------> The number of times this entry is hit
 *
 * (note: the average latency is the accumulated latency divided by the number
 * of times)
 */

#include <linux/latencytop.h>
#include <linux/kallsyms.h>
#include <linux/seq_file.h>
#include <linux/notifier.h>
#include <linux/spinlock.h>
#include <linux/proc_fs.h>
#include <linux/export.h>
#include <linux/sched.h>
#include <linux/list.h>
#include <linux/stacktrace.h>

static DEFINE_RAW_SPINLOCK(latency_lock);

#define MAXLR 128
static struct latency_record latency_record[MAXLR];

int latencytop_enabled;

void clear_all_latency_tracing(struct task_struct *p)
{
	unsigned long flags;

	if (!latencytop_enabled)
		return;

	raw_spin_lock_irqsave(&latency_lock, flags);
	memset(&p->latency_record, 0, sizeof(p->latency_record));
	p->latency_record_count = 0;
	raw_spin_unlock_irqrestore(&latency_lock, flags);
}

static void clear_global_latency_tracing(void)
{
	unsigned long flags;

	raw_spin_lock_irqsave(&latency_lock, flags);
	memset(&latency_record, 0, sizeof(latency_record));
	raw_spin_unlock_irqrestore(&latency_lock, flags);
}

static void __sched
account_global_scheduler_latency(struct task_struct *tsk, struct latency_record *lat)
{
	int firstnonnull = MAXLR + 1;
	int i;

	if (!latencytop_enabled)
		return;

	/* skip kernel threads for now */
	if (!tsk->mm)
		return;

	for (i = 0; i < MAXLR; i++) {
		int q, same = 1;

		/* Nothing stored: */
		if (!latency_record[i].backtrace[0]) {
			if (firstnonnull > i)
				firstnonnull = i;
			continue;
		}
		for (q = 0; q < LT_BACKTRACEDEPTH; q++) {
			unsigned long record = lat->backtrace[q];

			if (latency_record[i].backtrace[q] != record) {
				same = 0;
				break;
			}

			/* 0 and ULONG_MAX entries mean end of backtrace: */
			if (record == 0 || record == ULONG_MAX)
				break;
		}
		if (same) {
			latency_record[i].count++;
			latency_record[i].time += lat->time;
			if (lat->time > latency_record[i].max)
				latency_record[i].max = lat->time;
			return;
		}
	}

	i = firstnonnull;
	if (i >= MAXLR - 1)
		return;

	/* Allocted a new one: */
	memcpy(&latency_record[i], lat, sizeof(struct latency_record));
}

/*
 * Iterator to store a backtrace into a latency record entry
 */
static inline void store_stacktrace(struct task_struct *tsk,
					struct latency_record *lat)
{
	struct stack_trace trace;

	memset(&trace, 0, sizeof(trace));
	trace.max_entries = LT_BACKTRACEDEPTH;
	trace.entries = &lat->backtrace[0];
	save_stack_trace_tsk(tsk, &trace);
}

/**
 * __account_scheduler_latency - record an occurred latency
 * @tsk - the task struct of the task hitting the latency
 * @usecs - the duration of the latency in microseconds
 * @inter - 1 if the sleep was interruptible, 0 if uninterruptible
 *
 * This function is the main entry point for recording latency entries
 * as called by the scheduler.
 *
 * This function has a few special cases to deal with normal 'non-latency'
 * sleeps: specifically, interruptible sleep longer than 5 msec is skipped
 * since this usually is caused by waiting for events via select() and co.
 *
 * Negative latencies (caused by time going backwards) are also explicitly
 * skipped.
 */
void __sched
__account_scheduler_latency(struct task_struct *tsk, int usecs, int inter)
{
	unsigned long flags;
	int i, q;
	struct latency_record lat;

	/* Long interruptible waits are generally user requested... */
	if (inter && usecs > 5000)
		return;

	/* Negative sleeps are time going backwards */
	/* Zero-time sleeps are non-interesting */
	if (usecs <= 0)
		return;

	memset(&lat, 0, sizeof(lat));
	lat.count = 1;
	lat.time = usecs;
	lat.max = usecs;
	store_stacktrace(tsk, &lat);

	raw_spin_lock_irqsave(&latency_lock, flags);

	account_global_scheduler_latency(tsk, &lat);

	for (i = 0; i < tsk->latency_record_count; i++) {
		struct latency_record *mylat;
		int same = 1;

		mylat = &tsk->latency_record[i];
		for (q = 0; q < LT_BACKTRACEDEPTH; q++) {
			unsigned long record = lat.backtrace[q];

			if (mylat->backtrace[q] != record) {
				same = 0;
				break;
			}

			/* 0 and ULONG_MAX entries mean end of backtrace: */
			if (record == 0 || record == ULONG_MAX)
				break;
		}
		if (same) {
			mylat->count++;
			mylat->time += lat.time;
			if (lat.time > mylat->max)
				mylat->max = lat.time;
			goto out_unlock;
		}
	}

	/*
	 * short term hack; if we're > 32 we stop; future we recycle:
	 */
	if (tsk->latency_record_count >= LT_SAVECOUNT)
		goto out_unlock;

	/* Allocated a new one: */
	i = tsk->latency_record_count++;
	memcpy(&tsk->latency_record[i], &lat, sizeof(struct latency_record));

out_unlock:
	raw_spin_unlock_irqrestore(&latency_lock, flags);
}

static int lstats_show(struct seq_file *m, void *v)
{
	int i;

	seq_puts(m, "Latency Top version : v0.1\n");

	for (i = 0; i < MAXLR; i++) {
		struct latency_record *lr = &latency_record[i];

		if (lr->backtrace[0]) {
			int q;
			seq_printf(m, "%i %lu %lu",
				   lr->count, lr->time, lr->max);
			for (q = 0; q < LT_BACKTRACEDEPTH; q++) {
				unsigned long bt = lr->backtrace[q];
				if (!bt)
					break;
				if (bt == ULONG_MAX)
					break;
				seq_printf(m, " %ps", (void *)bt);
			}
			seq_printf(m, "\n");
		}
	}
	return 0;
}

static ssize_t
lstats_write(struct file *file, const char __user *buf, size_t count,
	     loff_t *offs)
{
	clear_global_latency_tracing();

	return count;
}

static int lstats_open(struct inode *inode, struct file *filp)
{
	return single_open(filp, lstats_show, NULL);
}

static const struct file_operations lstats_fops = {
	.open		= lstats_open,
	.read		= seq_read,
	.write		= lstats_write,
	.llseek		= seq_lseek,
	.release	= single_release,
};

static int __init init_lstats_procfs(void)
{
	proc_create("latency_stats", 0644, NULL, &lstats_fops);
	return 0;
}
device_initcall(init_lstats_procfs);