aboutsummaryrefslogtreecommitdiffstats
blob: 87abd3e2bd329d7ee3630cbc3ed4770d35e6370e (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
/*
 * INET		An implementation of the TCP/IP protocol suite for the LINUX
 *		operating system.  INET is implemented using the  BSD Socket
 *		interface as the means of communication with the user level.
 *
 *		The Internet Protocol (IP) module.
 *
 * Authors:	Ross Biro
 *		Fred N. van Kempen, <waltje@uWalt.NL.Mugnet.ORG>
 *		Donald Becker, <becker@super.org>
 *		Alan Cox, <alan@lxorguk.ukuu.org.uk>
 *		Richard Underwood
 *		Stefan Becker, <stefanb@yello.ping.de>
 *		Jorge Cwik, <jorge@laser.satlink.net>
 *		Arnt Gulbrandsen, <agulbra@nvg.unit.no>
 *
 *
 * Fixes:
 *		Alan Cox	:	Commented a couple of minor bits of surplus code
 *		Alan Cox	:	Undefining IP_FORWARD doesn't include the code
 *					(just stops a compiler warning).
 *		Alan Cox	:	Frames with >=MAX_ROUTE record routes, strict routes or loose routes
 *					are junked rather than corrupting things.
 *		Alan Cox	:	Frames to bad broadcast subnets are dumped
 *					We used to process them non broadcast and
 *					boy could that cause havoc.
 *		Alan Cox	:	ip_forward sets the free flag on the
 *					new frame it queues. Still crap because
 *					it copies the frame but at least it
 *					doesn't eat memory too.
 *		Alan Cox	:	Generic queue code and memory fixes.
 *		Fred Van Kempen :	IP fragment support (borrowed from NET2E)
 *		Gerhard Koerting:	Forward fragmented frames correctly.
 *		Gerhard Koerting: 	Fixes to my fix of the above 8-).
 *		Gerhard Koerting:	IP interface addressing fix.
 *		Linus Torvalds	:	More robustness checks
 *		Alan Cox	:	Even more checks: Still not as robust as it ought to be
 *		Alan Cox	:	Save IP header pointer for later
 *		Alan Cox	:	ip option setting
 *		Alan Cox	:	Use ip_tos/ip_ttl settings
 *		Alan Cox	:	Fragmentation bogosity removed
 *					(Thanks to Mark.Bush@prg.ox.ac.uk)
 *		Dmitry Gorodchanin :	Send of a raw packet crash fix.
 *		Alan Cox	:	Silly ip bug when an overlength
 *					fragment turns up. Now frees the
 *					queue.
 *		Linus Torvalds/ :	Memory leakage on fragmentation
 *		Alan Cox	:	handling.
 *		Gerhard Koerting:	Forwarding uses IP priority hints
 *		Teemu Rantanen	:	Fragment problems.
 *		Alan Cox	:	General cleanup, comments and reformat
 *		Alan Cox	:	SNMP statistics
 *		Alan Cox	:	BSD address rule semantics. Also see
 *					UDP as there is a nasty checksum issue
 *					if you do things the wrong way.
 *		Alan Cox	:	Always defrag, moved IP_FORWARD to the config.in file
 *		Alan Cox	: 	IP options adjust sk->priority.
 *		Pedro Roque	:	Fix mtu/length error in ip_forward.
 *		Alan Cox	:	Avoid ip_chk_addr when possible.
 *	Richard Underwood	:	IP multicasting.
 *		Alan Cox	:	Cleaned up multicast handlers.
 *		Alan Cox	:	RAW sockets demultiplex in the BSD style.
 *		Gunther Mayer	:	Fix the SNMP reporting typo
 *		Alan Cox	:	Always in group 224.0.0.1
 *	Pauline Middelink	:	Fast ip_checksum update when forwarding
 *					Masquerading support.
 *		Alan Cox	:	Multicast loopback error for 224.0.0.1
 *		Alan Cox	:	IP_MULTICAST_LOOP option.
 *		Alan Cox	:	Use notifiers.
 *		Bjorn Ekwall	:	Removed ip_csum (from slhc.c too)
 *		Bjorn Ekwall	:	Moved ip_fast_csum to ip.h (inline!)
 *		Stefan Becker   :       Send out ICMP HOST REDIRECT
 *	Arnt Gulbrandsen	:	ip_build_xmit
 *		Alan Cox	:	Per socket routing cache
 *		Alan Cox	:	Fixed routing cache, added header cache.
 *		Alan Cox	:	Loopback didn't work right in original ip_build_xmit - fixed it.
 *		Alan Cox	:	Only send ICMP_REDIRECT if src/dest are the same net.
 *		Alan Cox	:	Incoming IP option handling.
 *		Alan Cox	:	Set saddr on raw output frames as per BSD.
 *		Alan Cox	:	Stopped broadcast source route explosions.
 *		Alan Cox	:	Can disable source routing
 *		Takeshi Sone    :	Masquerading didn't work.
 *	Dave Bonn,Alan Cox	:	Faster IP forwarding whenever possible.
 *		Alan Cox	:	Memory leaks, tramples, misc debugging.
 *		Alan Cox	:	Fixed multicast (by popular demand 8))
 *		Alan Cox	:	Fixed forwarding (by even more popular demand 8))
 *		Alan Cox	:	Fixed SNMP statistics [I think]
 *	Gerhard Koerting	:	IP fragmentation forwarding fix
 *		Alan Cox	:	Device lock against page fault.
 *		Alan Cox	:	IP_HDRINCL facility.
 *	Werner Almesberger	:	Zero fragment bug
 *		Alan Cox	:	RAW IP frame length bug
 *		Alan Cox	:	Outgoing firewall on build_xmit
 *		A.N.Kuznetsov	:	IP_OPTIONS support throughout the kernel
 *		Alan Cox	:	Multicast routing hooks
 *		Jos Vos		:	Do accounting *before* call_in_firewall
 *	Willy Konynenberg	:	Transparent proxying support
 *
 *
 *
 * To Fix:
 *		IP fragmentation wants rewriting cleanly. The RFC815 algorithm is much more efficient
 *		and could be made very efficient with the addition of some virtual memory hacks to permit
 *		the allocation of a buffer that can then be 'grown' by twiddling page tables.
 *		Output fragmentation wants updating along with the buffer management to use a single
 *		interleaved copy algorithm so that fragmenting has a one copy overhead. Actual packet
 *		output should probably do its own fragmentation at the UDP/RAW layer. TCP shouldn't cause
 *		fragmentation anyway.
 *
 *		This program is free software; you can redistribute it and/or
 *		modify it under the terms of the GNU General Public License
 *		as published by the Free Software Foundation; either version
 *		2 of the License, or (at your option) any later version.
 */

#define pr_fmt(fmt) "IPv4: " fmt

#include <linux/module.h>
#include <linux/types.h>
#include <linux/kernel.h>
#include <linux/string.h>
#include <linux/errno.h>
#include <linux/slab.h>

#include <linux/net.h>
#include <linux/socket.h>
#include <linux/sockios.h>
#include <linux/in.h>
#include <linux/inet.h>
#include <linux/inetdevice.h>
#include <linux/netdevice.h>
#include <linux/etherdevice.h>

#include <net/snmp.h>
#include <net/ip.h>
#include <net/protocol.h>
#include <net/route.h>
#include <linux/skbuff.h>
#include <net/sock.h>
#include <net/arp.h>
#include <net/icmp.h>
#include <net/raw.h>
#include <net/checksum.h>
#include <linux/netfilter_ipv4.h>
#include <net/xfrm.h>
#include <linux/mroute.h>
#include <linux/netlink.h>

/*
 *	Process Router Attention IP option (RFC 2113)
 */
bool ip_call_ra_chain(struct sk_buff *skb)
{
	struct ip_ra_chain *ra;
	u8 protocol = ip_hdr(skb)->protocol;
	struct sock *last = NULL;
	struct net_device *dev = skb->dev;

	for (ra = rcu_dereference(ip_ra_chain); ra; ra = rcu_dereference(ra->next)) {
		struct sock *sk = ra->sk;

		/* If socket is bound to an interface, only report
		 * the packet if it came  from that interface.
		 */
		if (sk && inet_sk(sk)->inet_num == protocol &&
		    (!sk->sk_bound_dev_if ||
		     sk->sk_bound_dev_if == dev->ifindex) &&
		    net_eq(sock_net(sk), dev_net(dev))) {
			if (ip_is_fragment(ip_hdr(skb))) {
				if (ip_defrag(skb, IP_DEFRAG_CALL_RA_CHAIN))
					return true;
			}
			if (last) {
				struct sk_buff *skb2 = skb_clone(skb, GFP_ATOMIC);
				if (skb2)
					raw_rcv(last, skb2);
			}
			last = sk;
		}
	}

	if (last) {
		raw_rcv(last, skb);
		return true;
	}
	return false;
}

static int ip_local_deliver_finish(struct sk_buff *skb)
{
	struct net *net = dev_net(skb->dev);

	__skb_pull(skb, ip_hdrlen(skb));

	/* Point into the IP datagram, just past the header. */
	skb_reset_transport_header(skb);

	rcu_read_lock();
	{
		int protocol = ip_hdr(skb)->protocol;
		const struct net_protocol *ipprot;
		int raw;

	resubmit:
		raw = raw_local_deliver(skb, protocol);

		ipprot = rcu_dereference(inet_protos[protocol]);
		if (ipprot != NULL) {
			int ret;

			if (!ipprot->no_policy) {
				if (!xfrm4_policy_check(NULL, XFRM_POLICY_IN, skb)) {
					kfree_skb(skb);
					goto out;
				}
				nf_reset(skb);
			}
			ret = ipprot->handler(skb);
			if (ret < 0) {
				protocol = -ret;
				goto resubmit;
			}
			IP_INC_STATS_BH(net, IPSTATS_MIB_INDELIVERS);
		} else {
			if (!raw) {
				if (xfrm4_policy_check(NULL, XFRM_POLICY_IN, skb)) {
					IP_INC_STATS_BH(net, IPSTATS_MIB_INUNKNOWNPROTOS);
					icmp_send(skb, ICMP_DEST_UNREACH,
						  ICMP_PROT_UNREACH, 0);
				}
			} else
				IP_INC_STATS_BH(net, IPSTATS_MIB_INDELIVERS);
			kfree_skb(skb);
		}
	}
 out:
	rcu_read_unlock();

	return 0;
}

/*
 * 	Deliver IP Packets to the higher protocol layers.
 */
int ip_local_deliver(struct sk_buff *skb)
{
	/*
	 *	Reassemble IP fragments.
	 */

	if (ip_is_fragment(ip_hdr(skb))) {
		if (ip_defrag(skb, IP_DEFRAG_LOCAL_DELIVER))
			return 0;
	}

	return NF_HOOK(NFPROTO_IPV4, NF_INET_LOCAL_IN, skb, skb->dev, NULL,
		       ip_local_deliver_finish);
}

static inline bool ip_rcv_options(struct sk_buff *skb)
{
	struct ip_options *opt;
	const struct iphdr *iph;
	struct net_device *dev = skb->dev;

	/* It looks as overkill, because not all
	   IP options require packet mangling.
	   But it is the easiest for now, especially taking
	   into account that combination of IP options
	   and running sniffer is extremely rare condition.
					      --ANK (980813)
	*/
	if (skb_cow(skb, skb_headroom(skb))) {
		IP_INC_STATS_BH(dev_net(dev), IPSTATS_MIB_INDISCARDS);
		goto drop;
	}

	iph = ip_hdr(skb);
	opt = &(IPCB(skb)->opt);
	opt->optlen = iph->ihl*4 - sizeof(struct iphdr);

	if (ip_options_compile(dev_net(dev), opt, skb)) {
		IP_INC_STATS_BH(dev_net(dev), IPSTATS_MIB_INHDRERRORS);
		goto drop;
	}

	if (unlikely(opt->srr)) {
		struct in_device *in_dev = __in_dev_get_rcu(dev);

		if (in_dev) {
			if (!IN_DEV_SOURCE_ROUTE(in_dev)) {
				if (IN_DEV_LOG_MARTIANS(in_dev))
					net_info_ratelimited("source route option %pI4 -> %pI4\n",
							     &iph->saddr,
							     &iph->daddr);
				goto drop;
			}
		}

		if (ip_options_rcv_srr(skb))
			goto drop;
	}

	return false;
drop:
	return true;
}

int sysctl_ip_early_demux __read_mostly = 1;
EXPORT_SYMBOL(sysctl_ip_early_demux);

static int ip_rcv_finish(struct sk_buff *skb)
{
	const struct iphdr *iph = ip_hdr(skb);
	struct rtable *rt;

	if (sysctl_ip_early_demux && !skb_dst(skb)) {
		const struct net_protocol *ipprot;
		int protocol = iph->protocol;

		ipprot = rcu_dereference(inet_protos[protocol]);
		if (ipprot && ipprot->early_demux) {
			ipprot->early_demux(skb);
			/* must reload iph, skb->head might have changed */
			iph = ip_hdr(skb);
		}
	}

	/*
	 *	Initialise the virtual path cache for the packet. It describes
	 *	how the packet travels inside Linux networking.
	 */
	if (!skb_dst(skb)) {
		int err = ip_route_input_noref(skb, iph->daddr, iph->saddr,
					       iph->tos, skb->dev);
		if (unlikely(err)) {
			if (err == -EXDEV)
				NET_INC_STATS_BH(dev_net(skb->dev),
						 LINUX_MIB_IPRPFILTER);
			goto drop;
		}
	}

#ifdef CONFIG_IP_ROUTE_CLASSID
	if (unlikely(skb_dst(skb)->tclassid)) {
		struct ip_rt_acct *st = this_cpu_ptr(ip_rt_acct);
		u32 idx = skb_dst(skb)->tclassid;
		st[idx&0xFF].o_packets++;
		st[idx&0xFF].o_bytes += skb->len;
		st[(idx>>16)&0xFF].i_packets++;
		st[(idx>>16)&0xFF].i_bytes += skb->len;
	}
#endif

	if (iph->ihl > 5 && ip_rcv_options(skb))
		goto drop;

	rt = skb_rtable(skb);
	if (rt->rt_type == RTN_MULTICAST) {
		IP_UPD_PO_STATS_BH(dev_net(rt->dst.dev), IPSTATS_MIB_INMCAST,
				skb->len);
	} else if (rt->rt_type == RTN_BROADCAST)
		IP_UPD_PO_STATS_BH(dev_net(rt->dst.dev), IPSTATS_MIB_INBCAST,
				skb->len);

	return dst_input(skb);

drop:
	kfree_skb(skb);
	return NET_RX_DROP;
}

/*
 * 	Main IP Receive routine.
 */
int ip_rcv(struct sk_buff *skb, struct net_device *dev, struct packet_type *pt, struct net_device *orig_dev)
{
	const struct iphdr *iph;
	u32 len;

	/* When the interface is in promisc. mode, drop all the crap
	 * that it receives, do not try to analyse it.
	 */
	if (skb->pkt_type == PACKET_OTHERHOST)
		goto drop;


	IP_UPD_PO_STATS_BH(dev_net(dev), IPSTATS_MIB_IN, skb->len);

	if ((skb = skb_share_check(skb, GFP_ATOMIC)) == NULL) {
		IP_INC_STATS_BH(dev_net(dev), IPSTATS_MIB_INDISCARDS);
		goto out;
	}

	if (!pskb_may_pull(skb, sizeof(struct iphdr)))
		goto inhdr_error;

	iph = ip_hdr(skb);

	/*
	 *	RFC1122: 3.2.1.2 MUST silently discard any IP frame that fails the checksum.
	 *
	 *	Is the datagram acceptable?
	 *
	 *	1.	Length at least the size of an ip header
	 *	2.	Version of 4
	 *	3.	Checksums correctly. [Speed optimisation for later, skip loopback checksums]
	 *	4.	Doesn't have a bogus length
	 */

	if (iph->ihl < 5 || iph->version != 4)
		goto inhdr_error;

	if (!pskb_may_pull(skb, iph->ihl*4))
		goto inhdr_error;

	iph = ip_hdr(skb);

	if (unlikely(ip_fast_csum((u8 *)iph, iph->ihl)))
		goto inhdr_error;

	len = ntohs(iph->tot_len);
	if (skb->len < len) {
		IP_INC_STATS_BH(dev_net(dev), IPSTATS_MIB_INTRUNCATEDPKTS);
		goto drop;
	} else if (len < (iph->ihl*4))
		goto inhdr_error;

	/* Our transport medium may have padded the buffer out. Now we know it
	 * is IP we can trim to the true length of the frame.
	 * Note this now means skb->len holds ntohs(iph->tot_len).
	 */
	if (pskb_trim_rcsum(skb, len)) {
		IP_INC_STATS_BH(dev_net(dev), IPSTATS_MIB_INDISCARDS);
		goto drop;
	}

	/* Remove any debris in the socket control block */
	memset(IPCB(skb), 0, sizeof(struct inet_skb_parm));

	/* Must drop socket now because of tproxy. */
	skb_orphan(skb);

	return NF_HOOK(NFPROTO_IPV4, NF_INET_PRE_ROUTING, skb, dev, NULL,
		       ip_rcv_finish);

inhdr_error:
	IP_INC_STATS_BH(dev_net(dev), IPSTATS_MIB_INHDRERRORS);
drop:
	kfree_skb(skb);
out:
	return NET_RX_DROP;
}