/**
* Copyright (C) ARM Limited 2013-2014. All rights reserved.
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*/
#include "Buffer.h"
#include "Logging.h"
#include "Sender.h"
#include "SessionData.h"
#define mask (mSize - 1)
enum {
CODE_PEA = 1,
CODE_KEYS = 2,
CODE_FORMAT = 3,
CODE_MAPS = 4,
CODE_COMM = 5,
CODE_KEYS_OLD = 6,
};
// Summary Frame Messages
enum {
MESSAGE_SUMMARY = 1,
MESSAGE_CORE_NAME = 3,
};
// From gator_marshaling.c
#define NEWLINE_CANARY \
/* Unix */ \
"1\n" \
/* Windows */ \
"2\r\n" \
/* Mac OS */ \
"3\r" \
/* RISC OS */ \
"4\n\r" \
/* Add another character so the length isn't 0x0a bytes */ \
"5"
Buffer::Buffer(const int32_t core, const int32_t buftype, const int size, sem_t *const readerSem) : mCore(core), mBufType(buftype), mSize(size), mReadPos(0), mWritePos(0), mCommitPos(0), mAvailable(true), mIsDone(false), mBuf(new char[mSize]), mCommitTime(gSessionData->mLiveRate), mReaderSem(readerSem) {
if ((mSize & mask) != 0) {
logg->logError(__FILE__, __LINE__, "Buffer size is not a power of 2");
handleException();
}
frame();
}
Buffer::~Buffer() {
delete [] mBuf;
}
void Buffer::write(Sender *const sender) {
if (!commitReady()) {
return;
}
// determine the size of two halves
int length1 = mCommitPos - mReadPos;
char *buffer1 = mBuf + mReadPos;
int length2 = 0;
char *buffer2 = mBuf;
if (length1 < 0) {
length1 = mSize - mReadPos;
length2 = mCommitPos;
}
logg->logMessage("Sending data length1: %i length2: %i", length1, length2);
// start, middle or end
if (length1 > 0) {
sender->writeData(buffer1, length1, RESPONSE_APC_DATA);
}
// possible wrap around
if (length2 > 0) {
sender->writeData(buffer2, length2, RESPONSE_APC_DATA);
}
mReadPos = mCommitPos;
}
bool Buffer::commitReady() const {
return mCommitPos != mReadPos;
}
int Buffer::bytesAvailable() const {
int filled = mWritePos - mReadPos;
if (filled < 0) {
filled += mSize;
}
int remaining = mSize - filled;
if (mAvailable) {
// Give some extra room; also allows space to insert the overflow error packet
remaining -= 200;
} else {
// Hysteresis, prevents multiple overflow messages
remaining -= 2000;
}
return remaining;
}
bool Buffer::checkSpace(const int bytes) {
const int remaining = bytesAvailable();
if (remaining < bytes) {
mAvailable = false;
} else {
mAvailable = true;
}
return mAvailable;
}
int Buffer::contiguousSpaceAvailable() const {
int remaining = bytesAvailable();
int contiguous = mSize - mWritePos;
if (remaining < contiguous) {
return remaining;
} else {
return contiguous;
}
}
void Buffer::commit(const uint64_t time) {
// post-populate the length, which does not include the response type length nor the length itself, i.e. only the length of the payload
const int typeLength = gSessionData->mLocalCapture ? 0 : 1;
int length = mWritePos - mCommitPos;
if (length < 0) {
length += mSize;
}
length = length - typeLength - sizeof(int32_t);
for (size_t byte = 0; byte < sizeof(int32_t); byte++) {
mBuf[(mCommitPos + typeLength + byte) & mask] = (length >> byte * 8) & 0xFF;
}
logg->logMessage("Committing data mReadPos: %i mWritePos: %i mCommitPos: %i", mReadPos, mWritePos, mCommitPos);
mCommitPos = mWritePos;
if (gSessionData->mLiveRate > 0) {
while (time > mCommitTime) {
mCommitTime += gSessionData->mLiveRate;
}
}
if (!mIsDone) {
frame();
}
// send a notification that data is ready
sem_post(mReaderSem);
}
void Buffer::check(const uint64_t time) {
int filled = mWritePos - mCommitPos;
if (filled < 0) {
filled += mSize;
}
if (filled >= ((mSize * 3) / 4) || (gSessionData->mLiveRate > 0 && time >= mCommitTime)) {
commit(time);
}
}
void Buffer::packInt(char *const buf, const int size, int &writePos, int32_t x) {
int packedBytes = 0;
int more = true;
while (more) {
// low order 7 bits of x
char b = x & 0x7f;
x >>= 7;
if ((x == 0 && (b & 0x40) == 0) || (x == -1 && (b & 0x40) != 0)) {
more = false;
} else {
b |= 0x80;
}
buf[(writePos + packedBytes) & /*mask*/(size - 1)] = b;
packedBytes++;
}
writePos = (writePos + packedBytes) & /*mask*/(size - 1);
}
void Buffer::packInt(int32_t x) {
packInt(mBuf, mSize, mWritePos, x);
}
void Buffer::packInt64(int64_t x) {
int packedBytes = 0;
int more = true;
while (more) {
// low order 7 bits of x
char b = x & 0x7f;
x >>= 7;
if ((x == 0 && (b & 0x40) == 0) || (x == -1 && (b & 0x40) != 0)) {
more = false;
} else {
b |= 0x80;
}
mBuf[(mWritePos + packedBytes) & mask] = b;
packedBytes++;
}
mWritePos = (mWritePos + packedBytes) & mask;
}
void Buffer::writeBytes(const void *const data, size_t count) {
size_t i;
for (i = 0; i < count; ++i) {
mBuf[(mWritePos + i) & mask] = static_cast<const char *>(data)[i];
}
mWritePos = (mWritePos + i) & mask;
}
void Buffer::writeString(const char *const str) {
const int len = strlen(str);
packInt(len);
writeBytes(str, len);
}
void Buffer::frame() {
if (!gSessionData->mLocalCapture) {
packInt(RESPONSE_APC_DATA);
}
// Reserve space for the length
mWritePos += sizeof(int32_t);
packInt(mBufType);
packInt(mCore);
}
void Buffer::summary(const int64_t timestamp, const int64_t uptime, const int64_t monotonicDelta, const char *const uname) {
packInt(MESSAGE_SUMMARY);
writeString(NEWLINE_CANARY);
packInt64(timestamp);
packInt64(uptime);
packInt64(monotonicDelta);
writeString("uname");
writeString(uname);
writeString("");
check(1);
}
void Buffer::coreName(const int core, const int cpuid, const char *const name) {
if (checkSpace(3 * MAXSIZE_PACK32 + 0x100)) {
packInt(MESSAGE_CORE_NAME);
packInt(core);
packInt(cpuid);
writeString(name);
}
check(1);
}
bool Buffer::eventHeader(const uint64_t curr_time) {
bool retval = false;
if (checkSpace(MAXSIZE_PACK32 + MAXSIZE_PACK64)) {
packInt(0); // key of zero indicates a timestamp
packInt64(curr_time);
retval = true;
}
return retval;
}
bool Buffer::eventTid(const int tid) {
bool retval = false;
if (checkSpace(2 * MAXSIZE_PACK32)) {
packInt(1); // key of 1 indicates a tid
packInt(tid);
retval = true;
}
return retval;
}
void Buffer::event(const int32_t key, const int32_t value) {
if (checkSpace(2 * MAXSIZE_PACK32)) {
packInt(key);
packInt(value);
}
}
void Buffer::event64(const int64_t key, const int64_t value) {
if (checkSpace(2 * MAXSIZE_PACK64)) {
packInt64(key);
packInt64(value);
}
}
void Buffer::pea(const struct perf_event_attr *const pea, int key) {
if (checkSpace(2 * MAXSIZE_PACK32 + pea->size)) {
packInt(CODE_PEA);
writeBytes(pea, pea->size);
packInt(key);
} else {
logg->logError(__FILE__, __LINE__, "Ran out of buffer space for perf attrs");
handleException();
}
// Don't know the real perf time so use 1 as it will work for now
check(1);
}
void Buffer::keys(const int count, const __u64 *const ids, const int *const keys) {
if (checkSpace(2 * MAXSIZE_PACK32 + count * (MAXSIZE_PACK32 + MAXSIZE_PACK64))) {
packInt(CODE_KEYS);
packInt(count);
for (int i = 0; i < count; ++i) {
packInt64(ids[i]);
packInt(keys[i]);
}
} else {
logg->logError(__FILE__, __LINE__, "Ran out of buffer space for perf attrs");
handleException();
}
check(1);
}
void Buffer::keysOld(const int keyCount, const int *const keys, const int bytes, const char *const buf) {
if (checkSpace((2 + keyCount) * MAXSIZE_PACK32 + bytes)) {
packInt(CODE_KEYS_OLD);
packInt(keyCount);
for (int i = 0; i < keyCount; ++i) {
packInt(keys[i]);
}
writeBytes(buf, bytes);
} else {
logg->logError(__FILE__, __LINE__, "Ran out of buffer space for perf attrs");
handleException();
}
check(1);
}
void Buffer::format(const int length, const char *const format) {
if (checkSpace(MAXSIZE_PACK32 + length + 1)) {
packInt(CODE_FORMAT);
writeBytes(format, length + 1);
} else {
logg->logError(__FILE__, __LINE__, "Ran out of buffer space for perf attrs");
handleException();
}
check(1);
}
void Buffer::maps(const int pid, const int tid, const char *const maps) {
const int mapsLen = strlen(maps) + 1;
if (checkSpace(3 * MAXSIZE_PACK32 + mapsLen)) {
packInt(CODE_MAPS);
packInt(pid);
packInt(tid);
writeBytes(maps, mapsLen);
} else {
logg->logError(__FILE__, __LINE__, "Ran out of buffer space for perf attrs");
handleException();
}
check(1);
}
void Buffer::comm(const int pid, const int tid, const char *const image, const char *const comm) {
const int imageLen = strlen(image) + 1;
const int commLen = strlen(comm) + 1;
if (checkSpace(3 * MAXSIZE_PACK32 + imageLen + commLen)) {
packInt(CODE_COMM);
packInt(pid);
packInt(tid);
writeBytes(image, imageLen);
writeBytes(comm, commLen);
} else {
logg->logError(__FILE__, __LINE__, "Ran out of buffer space for perf attrs");
handleException();
}
check(1);
}
void Buffer::setDone() {
mIsDone = true;
commit(0);
}
bool Buffer::isDone() const {
return mIsDone && mReadPos == mCommitPos && mCommitPos == mWritePos;
}