blob: 90d5c47706c73fb4e74f5a8be82d26948099ca29 (
plain) (
tree)
|
|
/**
* Copyright (C) ARM Limited 2013-2014. All rights reserved.
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*/
#include "Monitor.h"
#include <errno.h>
#include <string.h>
#include <unistd.h>
#include "Logging.h"
Monitor::Monitor() : mFd(-1) {
}
Monitor::~Monitor() {
if (mFd >= -1) {
close(mFd);
}
}
bool Monitor::init() {
mFd = epoll_create(16);
if (mFd < 0) {
logg->logMessage("%s(%s:%i): epoll_create1 failed", __FUNCTION__, __FILE__, __LINE__);
return false;
}
return true;
}
bool Monitor::add(const int fd) {
struct epoll_event event;
memset(&event, 0, sizeof(event));
event.data.fd = fd;
event.events = EPOLLIN;
if (epoll_ctl(mFd, EPOLL_CTL_ADD, fd, &event) != 0) {
logg->logMessage("%s(%s:%i): epoll_ctl failed", __FUNCTION__, __FILE__, __LINE__);
return false;
}
return true;
}
int Monitor::wait(struct epoll_event *const events, int maxevents, int timeout) {
int result = epoll_wait(mFd, events, maxevents, timeout);
if (result < 0) {
// Ignore if the call was interrupted as this will happen when SIGINT is received
if (errno == EINTR) {
result = 0;
} else {
logg->logMessage("%s(%s:%i): epoll_wait failed", __FUNCTION__, __FILE__, __LINE__);
}
}
return result;
}
|