/**
* Copyright (C) ARM Limited 2013-2014. All rights reserved.
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*/
#include "PerfGroup.h"
#include <errno.h>
#include <string.h>
#include <sys/ioctl.h>
#include <sys/syscall.h>
#include <unistd.h>
#include "Buffer.h"
#include "Logging.h"
#include "Monitor.h"
#include "PerfBuffer.h"
#include "SessionData.h"
#define DEFAULT_PEA_ARGS(pea, additionalSampleType) \
pea.size = sizeof(pea); \
/* Emit time, read_format below, group leader id, and raw tracepoint info */ \
pea.sample_type = (gSessionData->perf.getLegacySupport() \
? PERF_SAMPLE_TID | PERF_SAMPLE_IP | PERF_SAMPLE_TIME | PERF_SAMPLE_READ | PERF_SAMPLE_ID \
: PERF_SAMPLE_TIME | PERF_SAMPLE_READ | PERF_SAMPLE_IDENTIFIER ) | additionalSampleType; \
/* Emit emit value in group format */ \
pea.read_format = PERF_FORMAT_ID | PERF_FORMAT_GROUP; \
/* start out disabled */ \
pea.disabled = 1; \
/* have a sampling interrupt happen when we cross the wakeup_watermark boundary */ \
pea.watermark = 1; \
/* Be conservative in flush size as only one buffer set is monitored */ \
pea.wakeup_watermark = 3 * BUF_SIZE / 4
static int sys_perf_event_open(struct perf_event_attr *const attr, const pid_t pid, const int cpu, const int group_fd, const unsigned long flags) {
return syscall(__NR_perf_event_open, attr, pid, cpu, group_fd, flags);
}
PerfGroup::PerfGroup(PerfBuffer *const pb) : mPb(pb) {
memset(&mAttrs, 0, sizeof(mAttrs));
memset(&mPerCpu, 0, sizeof(mPerCpu));
memset(&mKeys, -1, sizeof(mKeys));
memset(&mFds, -1, sizeof(mFds));
}
PerfGroup::~PerfGroup() {
for (int pos = ARRAY_LENGTH(mFds) - 1; pos >= 0; --pos) {
if (mFds[pos] >= 0) {
close(mFds[pos]);
}
}
}
bool PerfGroup::add(Buffer *const buffer, const int key, const __u32 type, const __u64 config, const __u64 sample, const __u64 sampleType, const int flags) {
int i;
for (i = 0; i < ARRAY_LENGTH(mKeys); ++i) {
if (mKeys[i] < 0) {
break;
}
}
if (i >= ARRAY_LENGTH(mKeys)) {
logg->logMessage("%s(%s:%i): Too many counters", __FUNCTION__, __FILE__, __LINE__);
return false;
}
DEFAULT_PEA_ARGS(mAttrs[i], sampleType);
mAttrs[i].type = type;
mAttrs[i].config = config;
mAttrs[i].sample_period = sample;
// always be on the CPU but only a group leader can be pinned
mAttrs[i].pinned = (i == 0 ? 1 : 0);
mAttrs[i].mmap = (flags & PERF_GROUP_MMAP ? 1 : 0);
mAttrs[i].comm = (flags & PERF_GROUP_COMM ? 1 : 0);
mAttrs[i].freq = (flags & PERF_GROUP_FREQ ? 1 : 0);
mAttrs[i].task = (flags & PERF_GROUP_TASK ? 1 : 0);
mAttrs[i].sample_id_all = (flags & PERF_GROUP_SAMPLE_ID_ALL ? 1 : 0);
mPerCpu[i] = (flags & PERF_GROUP_PER_CPU);
mKeys[i] = key;
buffer->pea(&mAttrs[i], key);
return true;
}
bool PerfGroup::prepareCPU(const int cpu) {
logg->logMessage("%s(%s:%i): Onlining cpu %i", __FUNCTION__, __FILE__, __LINE__, cpu);
for (int i = 0; i < ARRAY_LENGTH(mKeys); ++i) {
if (mKeys[i] < 0) {
continue;
}
if ((cpu != 0) && !mPerCpu[i]) {
continue;
}
const int offset = i * gSessionData->mCores;
if (mFds[cpu + offset] >= 0) {
logg->logMessage("%s(%s:%i): cpu already online or not correctly cleaned up", __FUNCTION__, __FILE__, __LINE__);
return false;
}
logg->logMessage("%s(%s:%i): perf_event_open cpu: %i type: %lli config: %lli sample: %lli sample_type: 0x%llx pinned: %i mmap: %i comm: %i freq: %i task: %i sample_id_all: %i", __FUNCTION__, __FILE__, __LINE__, cpu, (long long)mAttrs[i].type, (long long)mAttrs[i].config, (long long)mAttrs[i].sample_period, (long long)mAttrs[i].sample_type, mAttrs[i].pinned, mAttrs[i].mmap, mAttrs[i].comm, mAttrs[i].freq, mAttrs[i].task, mAttrs[i].sample_id_all);
mFds[cpu + offset] = sys_perf_event_open(&mAttrs[i], -1, cpu, i == 0 ? -1 : mFds[cpu], i == 0 ? 0 : PERF_FLAG_FD_OUTPUT);
if (mFds[cpu + offset] < 0) {
logg->logMessage("%s(%s:%i): failed %s", __FUNCTION__, __FILE__, __LINE__, strerror(errno));
continue;
}
if (!mPb->useFd(cpu, mFds[cpu + offset], mFds[cpu])) {
logg->logMessage("%s(%s:%i): PerfBuffer::useFd failed", __FUNCTION__, __FILE__, __LINE__);
return false;
}
}
return true;
}
int PerfGroup::onlineCPU(const int cpu, const bool start, Buffer *const buffer, Monitor *const monitor) {
__u64 ids[ARRAY_LENGTH(mKeys)];
int coreKeys[ARRAY_LENGTH(mKeys)];
int idCount = 0;
for (int i = 0; i < ARRAY_LENGTH(mKeys); ++i) {
const int fd = mFds[cpu + i * gSessionData->mCores];
if (fd < 0) {
continue;
}
coreKeys[idCount] = mKeys[i];
if (!gSessionData->perf.getLegacySupport() && ioctl(fd, PERF_EVENT_IOC_ID, &ids[idCount]) != 0 &&
// Workaround for running 32-bit gatord on 64-bit systems, kernel patch in the works
ioctl(fd, (PERF_EVENT_IOC_ID & ~IOCSIZE_MASK) | (8 << _IOC_SIZESHIFT), &ids[idCount]) != 0) {
logg->logMessage("%s(%s:%i): ioctl failed", __FUNCTION__, __FILE__, __LINE__);
return false;
}
++idCount;
}
if (!monitor->add(mFds[cpu])) {
logg->logMessage("%s(%s:%i): Monitor::add failed", __FUNCTION__, __FILE__, __LINE__);
return false;
}
if (!gSessionData->perf.getLegacySupport()) {
buffer->keys(idCount, ids, coreKeys);
} else {
char buf[1024];
ssize_t bytes = read(mFds[cpu], buf, sizeof(buf));
if (bytes < 0) {
logg->logMessage("read failed");
return false;
}
buffer->keysOld(idCount, coreKeys, bytes, buf);
}
if (start) {
for (int i = 0; i < ARRAY_LENGTH(mKeys); ++i) {
int offset = i * gSessionData->mCores + cpu;
if (mFds[offset] >= 0 && ioctl(mFds[offset], PERF_EVENT_IOC_ENABLE) < 0) {
logg->logMessage("%s(%s:%i): ioctl failed", __FUNCTION__, __FILE__, __LINE__);
return false;
}
}
}
return idCount;
}
bool PerfGroup::offlineCPU(const int cpu) {
logg->logMessage("%s(%s:%i): Offlining cpu %i", __FUNCTION__, __FILE__, __LINE__, cpu);
for (int i = 0; i < ARRAY_LENGTH(mKeys); ++i) {
int offset = i * gSessionData->mCores + cpu;
if (mFds[offset] >= 0 && ioctl(mFds[offset], PERF_EVENT_IOC_DISABLE) < 0) {
logg->logMessage("%s(%s:%i): ioctl failed", __FUNCTION__, __FILE__, __LINE__);
return false;
}
}
// Mark the buffer so that it will be released next time it's read
mPb->discard(cpu);
for (int i = 0; i < ARRAY_LENGTH(mKeys); ++i) {
if (mKeys[i] < 0) {
continue;
}
int offset = i * gSessionData->mCores + cpu;
if (mFds[offset] >= 0) {
close(mFds[offset]);
mFds[offset] = -1;
}
}
return true;
}
bool PerfGroup::start() {
for (int pos = 0; pos < ARRAY_LENGTH(mFds); ++pos) {
if (mFds[pos] >= 0 && ioctl(mFds[pos], PERF_EVENT_IOC_ENABLE) < 0) {
logg->logMessage("%s(%s:%i): ioctl failed", __FUNCTION__, __FILE__, __LINE__);
goto fail;
}
}
return true;
fail:
stop();
return false;
}
void PerfGroup::stop() {
for (int pos = ARRAY_LENGTH(mFds) - 1; pos >= 0; --pos) {
if (mFds[pos] >= 0) {
ioctl(mFds[pos], PERF_EVENT_IOC_DISABLE);
}
}
}