/**
* Copyright (C) ARM Limited 2010-2013. All rights reserved.
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*
*/
#define COOKIEMAP_ENTRIES 1024 /* must be power of 2 */
#define TRANSLATE_SIZE 256
#define MAX_COLLISIONS 2
static uint32_t *gator_crc32_table;
static unsigned int translate_buffer_mask;
static DEFINE_PER_CPU(char *, translate_text);
static DEFINE_PER_CPU(uint32_t, cookie_next_key);
static DEFINE_PER_CPU(uint64_t *, cookie_keys);
static DEFINE_PER_CPU(uint32_t *, cookie_values);
static DEFINE_PER_CPU(int, translate_buffer_read);
static DEFINE_PER_CPU(int, translate_buffer_write);
static DEFINE_PER_CPU(void **, translate_buffer);
static inline uint32_t get_cookie(int cpu, struct task_struct *task, const char *text, bool from_wq);
static void wq_cookie_handler(struct work_struct *unused);
DECLARE_WORK(cookie_work, wq_cookie_handler);
static struct timer_list app_process_wake_up_timer;
static void app_process_wake_up_handler(unsigned long unused_data);
static uint32_t cookiemap_code(uint64_t value64)
{
uint32_t value = (uint32_t)((value64 >> 32) + value64);
uint32_t cookiecode = (value >> 24) & 0xff;
cookiecode = cookiecode * 31 + ((value >> 16) & 0xff);
cookiecode = cookiecode * 31 + ((value >> 8) & 0xff);
cookiecode = cookiecode * 31 + ((value >> 0) & 0xff);
cookiecode &= (COOKIEMAP_ENTRIES - 1);
return cookiecode * MAX_COLLISIONS;
}
static uint32_t gator_chksum_crc32(const char *data)
{
register unsigned long crc;
const unsigned char *block = data;
int i, length = strlen(data);
crc = 0xFFFFFFFF;
for (i = 0; i < length; i++) {
crc = ((crc >> 8) & 0x00FFFFFF) ^ gator_crc32_table[(crc ^ *block++) & 0xFF];
}
return (crc ^ 0xFFFFFFFF);
}
/*
* Exists
* Pre: [0][1][v][3]..[n-1]
* Post: [v][0][1][3]..[n-1]
*/
static uint32_t cookiemap_exists(uint64_t key)
{
unsigned long x, flags, retval = 0;
int cpu = get_physical_cpu();
uint32_t cookiecode = cookiemap_code(key);
uint64_t *keys = &(per_cpu(cookie_keys, cpu)[cookiecode]);
uint32_t *values = &(per_cpu(cookie_values, cpu)[cookiecode]);
// Can be called from interrupt handler or from work queue
local_irq_save(flags);
for (x = 0; x < MAX_COLLISIONS; x++) {
if (keys[x] == key) {
uint32_t value = values[x];
for (; x > 0; x--) {
keys[x] = keys[x - 1];
values[x] = values[x - 1];
}
keys[0] = key;
values[0] = value;
retval = value;
break;
}
}
local_irq_restore(flags);
return retval;
}
/*
* Add
* Pre: [0][1][2][3]..[n-1]
* Post: [v][0][1][2]..[n-2]
*/
static void cookiemap_add(uint64_t key, uint32_t value)
{
int cpu = get_physical_cpu();
int cookiecode = cookiemap_code(key);
uint64_t *keys = &(per_cpu(cookie_keys, cpu)[cookiecode]);
uint32_t *values = &(per_cpu(cookie_values, cpu)[cookiecode]);
int x;
for (x = MAX_COLLISIONS - 1; x > 0; x--) {
keys[x] = keys[x - 1];
values[x] = values[x - 1];
}
keys[0] = key;
values[0] = value;
}
static void translate_buffer_write_ptr(int cpu, void *x)
{
per_cpu(translate_buffer, cpu)[per_cpu(translate_buffer_write, cpu)++] = x;
per_cpu(translate_buffer_write, cpu) &= translate_buffer_mask;
}
static void *translate_buffer_read_ptr(int cpu)
{
void *value = per_cpu(translate_buffer, cpu)[per_cpu(translate_buffer_read, cpu)++];
per_cpu(translate_buffer_read, cpu) &= translate_buffer_mask;
return value;
}
static void wq_cookie_handler(struct work_struct *unused)
{
struct task_struct *task;
char *text;
int cpu = get_physical_cpu();
unsigned int commit;
mutex_lock(&start_mutex);
if (gator_started != 0) {
commit = per_cpu(translate_buffer_write, cpu);
while (per_cpu(translate_buffer_read, cpu) != commit) {
task = (struct task_struct *)translate_buffer_read_ptr(cpu);
text = (char *)translate_buffer_read_ptr(cpu);
get_cookie(cpu, task, text, true);
}
}
mutex_unlock(&start_mutex);
}
static void app_process_wake_up_handler(unsigned long unused_data)
{
// had to delay scheduling work as attempting to schedule work during the context switch is illegal in kernel versions 3.5 and greater
schedule_work(&cookie_work);
}
// Retrieve full name from proc/pid/cmdline for java processes on Android
static int translate_app_process(const char **text, int cpu, struct task_struct *task, bool from_wq)
{
void *maddr;
unsigned int len;
unsigned long addr;
struct mm_struct *mm;
struct page *page = NULL;
struct vm_area_struct *page_vma;
int bytes, offset, retval = 0, ptr;
char *buf = per_cpu(translate_text, cpu);
// Push work into a work queue if in atomic context as the kernel functions below might sleep
// Rely on the in_interrupt variable rather than in_irq() or in_interrupt() kernel functions, as the value of these functions seems
// inconsistent during a context switch between android/linux versions
if (!from_wq) {
// Check if already in buffer
ptr = per_cpu(translate_buffer_read, cpu);
while (ptr != per_cpu(translate_buffer_write, cpu)) {
if (per_cpu(translate_buffer, cpu)[ptr] == (void *)task)
goto out;
ptr = (ptr + 2) & translate_buffer_mask;
}
translate_buffer_write_ptr(cpu, (void *)task);
translate_buffer_write_ptr(cpu, (void *)*text);
mod_timer(&app_process_wake_up_timer, jiffies + 1);
goto out;
}
mm = get_task_mm(task);
if (!mm)
goto out;
if (!mm->arg_end)
goto outmm;
addr = mm->arg_start;
len = mm->arg_end - mm->arg_start;
if (len > TRANSLATE_SIZE)
len = TRANSLATE_SIZE;
down_read(&mm->mmap_sem);
while (len) {
if (get_user_pages(task, mm, addr, 1, 0, 1, &page, &page_vma) <= 0)
goto outsem;
maddr = kmap(page);
offset = addr & (PAGE_SIZE - 1);
bytes = len;
if (bytes > PAGE_SIZE - offset)
bytes = PAGE_SIZE - offset;
copy_from_user_page(page_vma, page, addr, buf, maddr + offset, bytes);
kunmap(page); // release page allocated by get_user_pages()
page_cache_release(page);
len -= bytes;
buf += bytes;
addr += bytes;
*text = per_cpu(translate_text, cpu);
retval = 1;
}
// On app_process startup, /proc/pid/cmdline is initially "zygote" then "<pre-initialized>" but changes after an initial startup period
if (strcmp(*text, "zygote") == 0 || strcmp(*text, "<pre-initialized>") == 0)
retval = 0;
outsem:
up_read(&mm->mmap_sem);
outmm:
mmput(mm);
out:
return retval;
}
static inline uint32_t get_cookie(int cpu, struct task_struct *task, const char *text, bool from_wq)
{
unsigned long flags, cookie;
uint64_t key;
key = gator_chksum_crc32(text);
key = (key << 32) | (uint32_t)task->tgid;
cookie = cookiemap_exists(key);
if (cookie) {
return cookie;
}
if (strcmp(text, "app_process") == 0) {
if (!translate_app_process(&text, cpu, task, from_wq))
return INVALID_COOKIE;
}
// Can be called from interrupt handler or from work queue or from scheduler trace
local_irq_save(flags);
cookie = INVALID_COOKIE;
if (marshal_cookie_header(text)) {
cookie = per_cpu(cookie_next_key, cpu) += nr_cpu_ids;
cookiemap_add(key, cookie);
marshal_cookie(cookie, text);
}
local_irq_restore(flags);
return cookie;
}
static int get_exec_cookie(int cpu, struct task_struct *task)
{
struct mm_struct *mm = task->mm;
const char *text;
// kernel threads have no address space
if (!mm)
return NO_COOKIE;
if (task && task->mm && task->mm->exe_file) {
text = task->mm->exe_file->f_path.dentry->d_name.name;
return get_cookie(cpu, task, text, false);
}
return INVALID_COOKIE;
}
static unsigned long get_address_cookie(int cpu, struct task_struct *task, unsigned long addr, off_t *offset)
{
unsigned long cookie = NO_COOKIE;
struct mm_struct *mm = task->mm;
struct vm_area_struct *vma;
const char *text;
if (!mm)
return cookie;
for (vma = find_vma(mm, addr); vma; vma = vma->vm_next) {
if (addr < vma->vm_start || addr >= vma->vm_end)
continue;
if (vma->vm_file) {
text = vma->vm_file->f_path.dentry->d_name.name;
cookie = get_cookie(cpu, task, text, false);
*offset = (vma->vm_pgoff << PAGE_SHIFT) + addr - vma->vm_start;
} else {
/* must be an anonymous map */
*offset = addr;
}
break;
}
if (!vma)
cookie = INVALID_COOKIE;
return cookie;
}
static int cookies_initialize(void)
{
uint32_t crc, poly;
int i, j, cpu, size, err = 0;
int translate_buffer_size = 512; // must be a power of 2
translate_buffer_mask = translate_buffer_size / sizeof(per_cpu(translate_buffer, 0)[0]) - 1;
for_each_present_cpu(cpu) {
per_cpu(cookie_next_key, cpu) = nr_cpu_ids + cpu;
size = COOKIEMAP_ENTRIES * MAX_COLLISIONS * sizeof(uint64_t);
per_cpu(cookie_keys, cpu) = (uint64_t *)kmalloc(size, GFP_KERNEL);
if (!per_cpu(cookie_keys, cpu)) {
err = -ENOMEM;
goto cookie_setup_error;
}
memset(per_cpu(cookie_keys, cpu), 0, size);
size = COOKIEMAP_ENTRIES * MAX_COLLISIONS * sizeof(uint32_t);
per_cpu(cookie_values, cpu) = (uint32_t *)kmalloc(size, GFP_KERNEL);
if (!per_cpu(cookie_values, cpu)) {
err = -ENOMEM;
goto cookie_setup_error;
}
memset(per_cpu(cookie_values, cpu), 0, size);
per_cpu(translate_buffer, cpu) = (void **)kmalloc(translate_buffer_size, GFP_KERNEL);
if (!per_cpu(translate_buffer, cpu)) {
err = -ENOMEM;
goto cookie_setup_error;
}
per_cpu(translate_buffer_write, cpu) = 0;
per_cpu(translate_buffer_read, cpu) = 0;
per_cpu(translate_text, cpu) = (char *)kmalloc(TRANSLATE_SIZE, GFP_KERNEL);
if (!per_cpu(translate_text, cpu)) {
err = -ENOMEM;
goto cookie_setup_error;
}
}
// build CRC32 table
poly = 0x04c11db7;
gator_crc32_table = (uint32_t *)kmalloc(256 * sizeof(uint32_t), GFP_KERNEL);
for (i = 0; i < 256; i++) {
crc = i;
for (j = 8; j > 0; j--) {
if (crc & 1) {
crc = (crc >> 1) ^ poly;
} else {
crc >>= 1;
}
}
gator_crc32_table[i] = crc;
}
setup_timer(&app_process_wake_up_timer, app_process_wake_up_handler, 0);
cookie_setup_error:
return err;
}
static void cookies_release(void)
{
int cpu;
for_each_present_cpu(cpu) {
kfree(per_cpu(cookie_keys, cpu));
per_cpu(cookie_keys, cpu) = NULL;
kfree(per_cpu(cookie_values, cpu));
per_cpu(cookie_values, cpu) = NULL;
kfree(per_cpu(translate_buffer, cpu));
per_cpu(translate_buffer, cpu) = NULL;
per_cpu(translate_buffer_read, cpu) = 0;
per_cpu(translate_buffer_write, cpu) = 0;
kfree(per_cpu(translate_text, cpu));
per_cpu(translate_text, cpu) = NULL;
}
del_timer_sync(&app_process_wake_up_timer);
kfree(gator_crc32_table);
gator_crc32_table = NULL;
}