/**
* Copyright (C) ARM Limited 2011-2013. All rights reserved.
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*
*/
#include "gator.h"
#include <linux/module.h>
#include <linux/time.h>
#include <linux/math64.h>
#include <linux/slab.h>
#include <asm/io.h>
#include "linux/mali_linux_trace.h"
#include "gator_events_mali_common.h"
/*
* Check that the MALI_SUPPORT define is set to one of the allowable device codes.
*/
#if (MALI_SUPPORT != MALI_T6xx)
#error MALI_SUPPORT set to an invalid device code: expecting MALI_T6xx
#endif
/* Counters for Mali-T6xx:
*
* - Timeline events
* They are tracepoints, but instead of reporting a number they report a START/STOP event.
* They are reported in Streamline as number of microseconds while that particular counter was active.
*
* - SW counters
* They are tracepoints reporting a particular number.
* They are accumulated in sw_counter_data array until they are passed to Streamline, then they are zeroed.
*
* - Accumulators
* They are the same as software counters but their value is not zeroed.
*/
/* Timeline (start/stop) activity */
static const char *timeline_event_names[] = {
"PM_SHADER_0",
"PM_SHADER_1",
"PM_SHADER_2",
"PM_SHADER_3",
"PM_SHADER_4",
"PM_SHADER_5",
"PM_SHADER_6",
"PM_SHADER_7",
"PM_TILER_0",
"PM_L2_0",
"PM_L2_1",
"MMU_AS_0",
"MMU_AS_1",
"MMU_AS_2",
"MMU_AS_3"
};
enum {
PM_SHADER_0 = 0,
PM_SHADER_1,
PM_SHADER_2,
PM_SHADER_3,
PM_SHADER_4,
PM_SHADER_5,
PM_SHADER_6,
PM_SHADER_7,
PM_TILER_0,
PM_L2_0,
PM_L2_1,
MMU_AS_0,
MMU_AS_1,
MMU_AS_2,
MMU_AS_3
};
/* The number of shader blocks in the enum above */
#define NUM_PM_SHADER (8)
/* Software Counters */
static const char *software_counter_names[] = {
"MMU_PAGE_FAULT_0",
"MMU_PAGE_FAULT_1",
"MMU_PAGE_FAULT_2",
"MMU_PAGE_FAULT_3"
};
enum {
MMU_PAGE_FAULT_0 = 0,
MMU_PAGE_FAULT_1,
MMU_PAGE_FAULT_2,
MMU_PAGE_FAULT_3
};
/* Software Counters */
static const char *accumulators_names[] = {
"TOTAL_ALLOC_PAGES"
};
enum {
TOTAL_ALLOC_PAGES = 0
};
#define FIRST_TIMELINE_EVENT (0)
#define NUMBER_OF_TIMELINE_EVENTS (sizeof(timeline_event_names) / sizeof(timeline_event_names[0]))
#define FIRST_SOFTWARE_COUNTER (FIRST_TIMELINE_EVENT + NUMBER_OF_TIMELINE_EVENTS)
#define NUMBER_OF_SOFTWARE_COUNTERS (sizeof(software_counter_names) / sizeof(software_counter_names[0]))
#define FIRST_ACCUMULATOR (FIRST_SOFTWARE_COUNTER + NUMBER_OF_SOFTWARE_COUNTERS)
#define NUMBER_OF_ACCUMULATORS (sizeof(accumulators_names) / sizeof(accumulators_names[0]))
#define NUMBER_OF_EVENTS (NUMBER_OF_TIMELINE_EVENTS + NUMBER_OF_SOFTWARE_COUNTERS + NUMBER_OF_ACCUMULATORS)
/*
* gatorfs variables for counter enable state
*/
static mali_counter counters[NUMBER_OF_EVENTS];
/* An array used to return the data we recorded
* as key,value pairs hence the *2
*/
static unsigned long counter_dump[NUMBER_OF_EVENTS * 2];
/*
* Array holding counter start times (in ns) for each counter. A zero here
* indicates that the activity monitored by this counter is not running.
*/
static struct timespec timeline_event_starttime[NUMBER_OF_TIMELINE_EVENTS];
/* The data we have recorded */
static unsigned int timeline_data[NUMBER_OF_TIMELINE_EVENTS];
static unsigned int sw_counter_data[NUMBER_OF_SOFTWARE_COUNTERS];
static unsigned int accumulators_data[NUMBER_OF_ACCUMULATORS];
/* Hold the previous timestamp, used to calculate the sample interval. */
static struct timespec prev_timestamp;
/**
* Returns the timespan (in microseconds) between the two specified timestamps.
*
* @param start Ptr to the start timestamp
* @param end Ptr to the end timestamp
*
* @return Number of microseconds between the two timestamps (can be negative if start follows end).
*/
static inline long get_duration_us(const struct timespec *start, const struct timespec *end)
{
long event_duration_us = (end->tv_nsec - start->tv_nsec) / 1000;
event_duration_us += (end->tv_sec - start->tv_sec) * 1000000;
return event_duration_us;
}
static void record_timeline_event(unsigned int timeline_index, unsigned int type)
{
struct timespec event_timestamp;
struct timespec *event_start = &timeline_event_starttime[timeline_index];
switch (type) {
case ACTIVITY_START:
/* Get the event time... */
getnstimeofday(&event_timestamp);
/* Remember the start time if the activity is not already started */
if (event_start->tv_sec == 0) {
*event_start = event_timestamp; /* Structure copy */
}
break;
case ACTIVITY_STOP:
/* if the counter was started... */
if (event_start->tv_sec != 0) {
/* Get the event time... */
getnstimeofday(&event_timestamp);
/* Accumulate the duration in us */
timeline_data[timeline_index] += get_duration_us(event_start, &event_timestamp);
/* Reset the start time to indicate the activity is stopped. */
event_start->tv_sec = 0;
}
break;
default:
/* Other activity events are ignored. */
break;
}
}
/*
* Documentation about the following tracepoints is in mali_linux_trace.h
*/
GATOR_DEFINE_PROBE(mali_pm_status, TP_PROTO(unsigned int event_id, unsigned long long value))
{
#define SHADER_PRESENT_LO 0x100 /* (RO) Shader core present bitmap, low word */
#define TILER_PRESENT_LO 0x110 /* (RO) Tiler core present bitmap, low word */
#define L2_PRESENT_LO 0x120 /* (RO) Level 2 cache present bitmap, low word */
#define BIT_AT(value, pos) ((value >> pos) & 1)
static unsigned long long previous_shader_bitmask = 0;
static unsigned long long previous_tiler_bitmask = 0;
static unsigned long long previous_l2_bitmask = 0;
switch (event_id) {
case SHADER_PRESENT_LO:
{
unsigned long long changed_bitmask = previous_shader_bitmask ^ value;
int pos;
for (pos = 0; pos < NUM_PM_SHADER; ++pos) {
if (BIT_AT(changed_bitmask, pos)) {
record_timeline_event(PM_SHADER_0 + pos, BIT_AT(value, pos) ? ACTIVITY_START : ACTIVITY_STOP);
}
}
previous_shader_bitmask = value;
break;
}
case TILER_PRESENT_LO:
{
unsigned long long changed = previous_tiler_bitmask ^ value;
if (BIT_AT(changed, 0)) {
record_timeline_event(PM_TILER_0, BIT_AT(value, 0) ? ACTIVITY_START : ACTIVITY_STOP);
}
previous_tiler_bitmask = value;
break;
}
case L2_PRESENT_LO:
{
unsigned long long changed = previous_l2_bitmask ^ value;
if (BIT_AT(changed, 0)) {
record_timeline_event(PM_L2_0, BIT_AT(value, 0) ? ACTIVITY_START : ACTIVITY_STOP);
}
if (BIT_AT(changed, 4)) {
record_timeline_event(PM_L2_1, BIT_AT(value, 4) ? ACTIVITY_START : ACTIVITY_STOP);
}
previous_l2_bitmask = value;
break;
}
default:
/* No other blocks are supported at present */
break;
}
#undef SHADER_PRESENT_LO
#undef TILER_PRESENT_LO
#undef L2_PRESENT_LO
#undef BIT_AT
}
GATOR_DEFINE_PROBE(mali_page_fault_insert_pages, TP_PROTO(int event_id, unsigned long value))
{
/* We add to the previous since we may receive many tracepoints in one sample period */
sw_counter_data[MMU_PAGE_FAULT_0 + event_id] += value;
}
GATOR_DEFINE_PROBE(mali_mmu_as_in_use, TP_PROTO(int event_id))
{
record_timeline_event(MMU_AS_0 + event_id, ACTIVITY_START);
}
GATOR_DEFINE_PROBE(mali_mmu_as_released, TP_PROTO(int event_id))
{
record_timeline_event(MMU_AS_0 + event_id, ACTIVITY_STOP);
}
GATOR_DEFINE_PROBE(mali_total_alloc_pages_change, TP_PROTO(long long int event_id))
{
accumulators_data[TOTAL_ALLOC_PAGES] = event_id;
}
static int create_files(struct super_block *sb, struct dentry *root)
{
int event;
/*
* Create the filesystem for all events
*/
int counter_index = 0;
const char *mali_name = gator_mali_get_mali_name();
for (event = FIRST_TIMELINE_EVENT; event < FIRST_TIMELINE_EVENT + NUMBER_OF_TIMELINE_EVENTS; event++) {
if (gator_mali_create_file_system(mali_name, timeline_event_names[counter_index], sb, root, &counters[event]) != 0) {
return -1;
}
counter_index++;
}
counter_index = 0;
for (event = FIRST_SOFTWARE_COUNTER; event < FIRST_SOFTWARE_COUNTER + NUMBER_OF_SOFTWARE_COUNTERS; event++) {
if (gator_mali_create_file_system(mali_name, software_counter_names[counter_index], sb, root, &counters[event]) != 0) {
return -1;
}
counter_index++;
}
counter_index = 0;
for (event = FIRST_ACCUMULATOR; event < FIRST_ACCUMULATOR + NUMBER_OF_ACCUMULATORS; event++) {
if (gator_mali_create_file_system(mali_name, accumulators_names[counter_index], sb, root, &counters[event]) != 0) {
return -1;
}
counter_index++;
}
return 0;
}
static int register_tracepoints(void)
{
if (GATOR_REGISTER_TRACE(mali_pm_status)) {
pr_debug("gator: Mali-T6xx: mali_pm_status tracepoint failed to activate\n");
return 0;
}
if (GATOR_REGISTER_TRACE(mali_page_fault_insert_pages)) {
pr_debug("gator: Mali-T6xx: mali_page_fault_insert_pages tracepoint failed to activate\n");
return 0;
}
if (GATOR_REGISTER_TRACE(mali_mmu_as_in_use)) {
pr_debug("gator: Mali-T6xx: mali_mmu_as_in_use tracepoint failed to activate\n");
return 0;
}
if (GATOR_REGISTER_TRACE(mali_mmu_as_released)) {
pr_debug("gator: Mali-T6xx: mali_mmu_as_released tracepoint failed to activate\n");
return 0;
}
if (GATOR_REGISTER_TRACE(mali_total_alloc_pages_change)) {
pr_debug("gator: Mali-T6xx: mali_total_alloc_pages_change tracepoint failed to activate\n");
return 0;
}
pr_debug("gator: Mali-T6xx: start\n");
pr_debug("gator: Mali-T6xx: mali_pm_status probe is at %p\n", &probe_mali_pm_status);
pr_debug("gator: Mali-T6xx: mali_page_fault_insert_pages probe is at %p\n", &probe_mali_page_fault_insert_pages);
pr_debug("gator: Mali-T6xx: mali_mmu_as_in_use probe is at %p\n", &probe_mali_mmu_as_in_use);
pr_debug("gator: Mali-T6xx: mali_mmu_as_released probe is at %p\n", &probe_mali_mmu_as_released);
pr_debug("gator: Mali-T6xx: mali_total_alloc_pages_change probe is at %p\n", &probe_mali_total_alloc_pages_change);
return 1;
}
static int start(void)
{
unsigned int cnt;
/* Clean all data for the next capture */
for (cnt = 0; cnt < NUMBER_OF_TIMELINE_EVENTS; cnt++) {
timeline_event_starttime[cnt].tv_sec = timeline_event_starttime[cnt].tv_nsec = 0;
timeline_data[cnt] = 0;
}
for (cnt = 0; cnt < NUMBER_OF_SOFTWARE_COUNTERS; cnt++) {
sw_counter_data[cnt] = 0;
}
for (cnt = 0; cnt < NUMBER_OF_ACCUMULATORS; cnt++) {
accumulators_data[cnt] = 0;
}
/* Register tracepoints */
if (register_tracepoints() == 0) {
return -1;
}
/*
* Set the first timestamp for calculating the sample interval. The first interval could be quite long,
* since it will be the time between 'start' and the first 'read'.
* This means that timeline values will be divided by a big number for the first sample.
*/
getnstimeofday(&prev_timestamp);
return 0;
}
static void stop(void)
{
pr_debug("gator: Mali-T6xx: stop\n");
/*
* It is safe to unregister traces even if they were not successfully
* registered, so no need to check.
*/
GATOR_UNREGISTER_TRACE(mali_pm_status);
pr_debug("gator: Mali-T6xx: mali_pm_status tracepoint deactivated\n");
GATOR_UNREGISTER_TRACE(mali_page_fault_insert_pages);
pr_debug("gator: Mali-T6xx: mali_page_fault_insert_pages tracepoint deactivated\n");
GATOR_UNREGISTER_TRACE(mali_mmu_as_in_use);
pr_debug("gator: Mali-T6xx: mali_mmu_as_in_use tracepoint deactivated\n");
GATOR_UNREGISTER_TRACE(mali_mmu_as_released);
pr_debug("gator: Mali-T6xx: mali_mmu_as_released tracepoint deactivated\n");
GATOR_UNREGISTER_TRACE(mali_total_alloc_pages_change);
pr_debug("gator: Mali-T6xx: mali_total_alloc_pages_change tracepoint deactivated\n");
}
static int read(int **buffer)
{
int cnt;
int len = 0;
long sample_interval_us = 0;
struct timespec read_timestamp;
if (!on_primary_core()) {
return 0;
}
/* Get the start of this sample period. */
getnstimeofday(&read_timestamp);
/*
* Calculate the sample interval if the previous sample time is valid.
* We use tv_sec since it will not be 0.
*/
if (prev_timestamp.tv_sec != 0) {
sample_interval_us = get_duration_us(&prev_timestamp, &read_timestamp);
}
/* Structure copy. Update the previous timestamp. */
prev_timestamp = read_timestamp;
/*
* Report the timeline counters (ACTIVITY_START/STOP)
*/
for (cnt = FIRST_TIMELINE_EVENT; cnt < (FIRST_TIMELINE_EVENT + NUMBER_OF_TIMELINE_EVENTS); cnt++) {
mali_counter *counter = &counters[cnt];
if (counter->enabled) {
const int index = cnt - FIRST_TIMELINE_EVENT;
unsigned int value;
/* If the activity is still running, reset its start time to the start of this sample period
* to correct the count. Add the time up to the end of the sample onto the count. */
if (timeline_event_starttime[index].tv_sec != 0) {
const long event_duration = get_duration_us(&timeline_event_starttime[index], &read_timestamp);
timeline_data[index] += event_duration;
timeline_event_starttime[index] = read_timestamp; /* Activity is still running. */
}
if (sample_interval_us != 0) {
/* Convert the counter to a percent-of-sample value */
value = (timeline_data[index] * 100) / sample_interval_us;
} else {
pr_debug("gator: Mali-T6xx: setting value to zero\n");
value = 0;
}
/* Clear the counter value ready for the next sample. */
timeline_data[index] = 0;
counter_dump[len++] = counter->key;
counter_dump[len++] = value;
}
}
/* Report the software counters */
for (cnt = FIRST_SOFTWARE_COUNTER; cnt < (FIRST_SOFTWARE_COUNTER + NUMBER_OF_SOFTWARE_COUNTERS); cnt++) {
const mali_counter *counter = &counters[cnt];
if (counter->enabled) {
const int index = cnt - FIRST_SOFTWARE_COUNTER;
counter_dump[len++] = counter->key;
counter_dump[len++] = sw_counter_data[index];
/* Set the value to zero for the next time */
sw_counter_data[index] = 0;
}
}
/* Report the accumulators */
for (cnt = FIRST_ACCUMULATOR; cnt < (FIRST_ACCUMULATOR + NUMBER_OF_ACCUMULATORS); cnt++) {
const mali_counter *counter = &counters[cnt];
if (counter->enabled) {
const int index = cnt - FIRST_ACCUMULATOR;
counter_dump[len++] = counter->key;
counter_dump[len++] = accumulators_data[index];
/* Do not zero the accumulator */
}
}
/* Update the buffer */
if (buffer) {
*buffer = (int *)counter_dump;
}
return len;
}
static struct gator_interface gator_events_mali_t6xx_interface = {
.create_files = create_files,
.start = start,
.stop = stop,
.read = read
};
extern int gator_events_mali_t6xx_init(void)
{
pr_debug("gator: Mali-T6xx: sw_counters init\n");
gator_mali_initialise_counters(counters, NUMBER_OF_EVENTS);
return gator_events_install(&gator_events_mali_t6xx_interface);
}
gator_events_init(gator_events_mali_t6xx_init);