/*
* Example events provider
*
* Copyright (C) ARM Limited 2010-2014. All rights reserved.
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*
* Similar entries to those below must be present in the events.xml file.
* To add them to the events.xml, create an events-mmap.xml with the
* following contents and rebuild gatord:
*
* <counter_set name="mmapped_cnt" count="3"/>
* <category name="mmapped" counter_set="mmapped_cnt" per_cpu="no">
* <event event="0x0" title="Simulated1" name="Sine" display="maximum" average_selection="yes" description="Sort-of-sine"/>
* <event event="0x1" title="Simulated2" name="Triangle" display="maximum" average_selection="yes" description="Triangular wave"/>
* <event event="0x2" title="Simulated3" name="PWM" display="maximum" average_selection="yes" description="PWM Signal"/>
* </category>
*
* When adding custom events, be sure do the following
* - add any needed .c files to the gator driver Makefile
* - call gator_events_install in the events init function
* - add the init function to GATOR_EVENTS_LIST in gator_main.c
* - add a new events-*.xml file to the gator daemon and rebuild
*/
#include <linux/init.h>
#include <linux/io.h>
#include <linux/ratelimit.h>
#include "gator.h"
#define MMAPPED_COUNTERS_NUM 3
static int mmapped_global_enabled;
static struct {
unsigned long enabled;
unsigned long event;
unsigned long key;
} mmapped_counters[MMAPPED_COUNTERS_NUM];
static int mmapped_buffer[MMAPPED_COUNTERS_NUM * 2];
static s64 prev_time;
/* Adds mmapped_cntX directories and enabled, event, and key files to /dev/gator/events */
static int gator_events_mmapped_create_files(struct super_block *sb,
struct dentry *root)
{
int i;
for (i = 0; i < MMAPPED_COUNTERS_NUM; i++) {
char buf[16];
struct dentry *dir;
snprintf(buf, sizeof(buf), "mmapped_cnt%d", i);
dir = gatorfs_mkdir(sb, root, buf);
if (WARN_ON(!dir))
return -1;
gatorfs_create_ulong(sb, dir, "enabled",
&mmapped_counters[i].enabled);
gatorfs_create_ulong(sb, dir, "event",
&mmapped_counters[i].event);
gatorfs_create_ro_ulong(sb, dir, "key",
&mmapped_counters[i].key);
}
return 0;
}
static int gator_events_mmapped_start(void)
{
int i;
struct timespec ts;
getnstimeofday(&ts);
prev_time = timespec_to_ns(&ts);
mmapped_global_enabled = 0;
for (i = 0; i < MMAPPED_COUNTERS_NUM; i++) {
if (mmapped_counters[i].enabled) {
mmapped_global_enabled = 1;
break;
}
}
return 0;
}
static void gator_events_mmapped_stop(void)
{
}
/* This function "simulates" counters, generating values of fancy
* functions like sine or triangle... */
static int mmapped_simulate(int counter, int delta_in_us)
{
int result = 0;
switch (counter) {
case 0: /* sort-of-sine */
{
static int t = 0;
int x;
t += delta_in_us;
if (t > 2048000)
t = 0;
if (t % 1024000 < 512000)
x = 512000 - (t % 512000);
else
x = t % 512000;
result = 32 * x / 512000;
result = result * result;
if (t < 1024000)
result = 1922 - result;
}
break;
case 1: /* triangle */
{
static int v, d = 1;
v = v + d * delta_in_us;
if (v < 0) {
v = 0;
d = 1;
} else if (v > 1000000) {
v = 1000000;
d = -1;
}
result = v;
}
break;
case 2: /* PWM signal */
{
static int dc, x, t = 0;
t += delta_in_us;
if (t > 1000000)
t = 0;
if (x / 1000000 != (x + delta_in_us) / 1000000)
dc = (dc + 100000) % 1000000;
x += delta_in_us;
result = t < dc ? 0 : 10;
}
break;
}
return result;
}
static int gator_events_mmapped_read(int **buffer)
{
int i;
int len = 0;
int delta_in_us;
struct timespec ts;
s64 time;
/* System wide counters - read from one core only */
if (!on_primary_core() || !mmapped_global_enabled)
return 0;
getnstimeofday(&ts);
time = timespec_to_ns(&ts);
delta_in_us = (int)(time - prev_time) / 1000;
prev_time = time;
for (i = 0; i < MMAPPED_COUNTERS_NUM; i++) {
if (mmapped_counters[i].enabled) {
mmapped_buffer[len++] = mmapped_counters[i].key;
mmapped_buffer[len++] =
mmapped_simulate(mmapped_counters[i].event,
delta_in_us);
}
}
if (buffer)
*buffer = mmapped_buffer;
return len;
}
static struct gator_interface gator_events_mmapped_interface = {
.create_files = gator_events_mmapped_create_files,
.start = gator_events_mmapped_start,
.stop = gator_events_mmapped_stop,
.read = gator_events_mmapped_read,
};
/* Must not be static! */
int __init gator_events_mmapped_init(void)
{
int i;
for (i = 0; i < MMAPPED_COUNTERS_NUM; i++) {
mmapped_counters[i].enabled = 0;
mmapped_counters[i].key = gator_events_get_key();
}
return gator_events_install(&gator_events_mmapped_interface);
}