diff options
author | Wade Cherry | 2012-07-12 10:29:16 -0500 |
---|---|---|
committer | Jon Medhurst | 2012-07-13 04:56:57 -0500 |
commit | 2ccfda6ba471ba1722fe48d23767d9d024bd0750 (patch) | |
tree | c0c548d22ba3f8264d9d958aca29fd52c8ff0863 | |
parent | f7e8a3d4bed65fb0fdb846f53aad7b0a763767c7 (diff) | |
download | arm-ds5-gator-2ccfda6ba471ba1722fe48d23767d9d024bd0750.tar.gz arm-ds5-gator-2ccfda6ba471ba1722fe48d23767d9d024bd0750.tar.xz arm-ds5-gator-2ccfda6ba471ba1722fe48d23767d9d024bd0750.zip |
gator-driver: Move work scheduling to timers
... in order to work around deadlocks in kernel >= 3.5...
Signed-off-by: Wade Cherry <wade.cherry@arm.com>
Signed-off-by: Pawel Moll <pawel.moll@arm.com>
-rw-r--r-- | driver/gator_cookies.c | 15 | ||||
-rw-r--r-- | driver/gator_events_meminfo.c | 19 | ||||
-rw-r--r-- | driver/gator_events_net.c | 18 | ||||
-rw-r--r-- | driver/gator_main.c | 13 |
4 files changed, 51 insertions, 14 deletions
diff --git a/driver/gator_cookies.c b/driver/gator_cookies.c index 7b50916..df14d09 100644 --- a/driver/gator_cookies.c +++ b/driver/gator_cookies.c | |||
@@ -25,6 +25,10 @@ static DEFINE_PER_CPU(unsigned int *, translate_buffer); | |||
25 | static inline uint32_t get_cookie(int cpu, int buftype, struct task_struct *task, struct vm_area_struct *vma, struct module *mod, bool in_interrupt); | 25 | static inline uint32_t get_cookie(int cpu, int buftype, struct task_struct *task, struct vm_area_struct *vma, struct module *mod, bool in_interrupt); |
26 | static void wq_cookie_handler(struct work_struct *unused); | 26 | static void wq_cookie_handler(struct work_struct *unused); |
27 | DECLARE_WORK(cookie_work, wq_cookie_handler); | 27 | DECLARE_WORK(cookie_work, wq_cookie_handler); |
28 | static struct timer_list app_process_wake_up_timer; | ||
29 | static void app_process_wake_up_handler(unsigned long unused_data); | ||
30 | static struct timer_list app_process_wake_up_timer; | ||
31 | static void app_process_wake_up_handler(unsigned long unused_data); | ||
28 | 32 | ||
29 | static uint32_t cookiemap_code(uint64_t value64) { | 33 | static uint32_t cookiemap_code(uint64_t value64) { |
30 | uint32_t value = (uint32_t)((value64 >> 32) + value64); | 34 | uint32_t value = (uint32_t)((value64 >> 32) + value64); |
@@ -136,6 +140,12 @@ static void wq_cookie_handler(struct work_struct *unused) | |||
136 | mutex_unlock(&start_mutex); | 140 | mutex_unlock(&start_mutex); |
137 | } | 141 | } |
138 | 142 | ||
143 | static void app_process_wake_up_handler(unsigned long unused_data) | ||
144 | { | ||
145 | // had to delay scheduling work as attempting to schedule work during the context switch is illegal in kernel versions 3.5 and greater | ||
146 | schedule_work(&cookie_work); | ||
147 | } | ||
148 | |||
139 | // Retrieve full name from proc/pid/cmdline for java processes on Android | 149 | // Retrieve full name from proc/pid/cmdline for java processes on Android |
140 | static int translate_app_process(char** text, int cpu, struct task_struct * task, struct vm_area_struct *vma, bool in_interrupt) | 150 | static int translate_app_process(char** text, int cpu, struct task_struct * task, struct vm_area_struct *vma, bool in_interrupt) |
141 | { | 151 | { |
@@ -162,7 +172,7 @@ static int translate_app_process(char** text, int cpu, struct task_struct * task | |||
162 | 172 | ||
163 | translate_buffer_write_int(cpu, (unsigned int)task); | 173 | translate_buffer_write_int(cpu, (unsigned int)task); |
164 | translate_buffer_write_int(cpu, (unsigned int)vma); | 174 | translate_buffer_write_int(cpu, (unsigned int)vma); |
165 | schedule_work(&cookie_work); | 175 | mod_timer(&app_process_wake_up_timer, jiffies + 1); |
166 | goto out; | 176 | goto out; |
167 | } | 177 | } |
168 | 178 | ||
@@ -372,6 +382,8 @@ static int cookies_initialize(void) | |||
372 | gator_crc32_table[i] = crc; | 382 | gator_crc32_table[i] = crc; |
373 | } | 383 | } |
374 | 384 | ||
385 | setup_timer(&app_process_wake_up_timer, app_process_wake_up_handler, 0); | ||
386 | |||
375 | cookie_setup_error: | 387 | cookie_setup_error: |
376 | return err; | 388 | return err; |
377 | } | 389 | } |
@@ -396,6 +408,7 @@ static void cookies_release(void) | |||
396 | per_cpu(translate_text, cpu) = NULL; | 408 | per_cpu(translate_text, cpu) = NULL; |
397 | } | 409 | } |
398 | 410 | ||
411 | del_timer_sync(&app_process_wake_up_timer); | ||
399 | kfree(gator_crc32_table); | 412 | kfree(gator_crc32_table); |
400 | gator_crc32_table = NULL; | 413 | gator_crc32_table = NULL; |
401 | } | 414 | } |
diff --git a/driver/gator_events_meminfo.c b/driver/gator_events_meminfo.c index ad552ef..f9dfa9a 100644 --- a/driver/gator_events_meminfo.c +++ b/driver/gator_events_meminfo.c | |||
@@ -28,6 +28,8 @@ static bool new_data_avail; | |||
28 | static void wq_sched_handler(struct work_struct *wsptr); | 28 | static void wq_sched_handler(struct work_struct *wsptr); |
29 | 29 | ||
30 | DECLARE_WORK(work, wq_sched_handler); | 30 | DECLARE_WORK(work, wq_sched_handler); |
31 | static struct timer_list meminfo_wake_up_timer; | ||
32 | static void meminfo_wake_up_handler(unsigned long unused_data); | ||
31 | 33 | ||
32 | #if LINUX_VERSION_CODE < KERNEL_VERSION(3, 3, 0) | 34 | #if LINUX_VERSION_CODE < KERNEL_VERSION(3, 3, 0) |
33 | GATOR_DEFINE_PROBE(mm_page_free_direct, TP_PROTO(struct page *page, unsigned int order)) { | 35 | GATOR_DEFINE_PROBE(mm_page_free_direct, TP_PROTO(struct page *page, unsigned int order)) { |
@@ -107,6 +109,7 @@ static int gator_events_meminfo_start(void) | |||
107 | if (GATOR_REGISTER_TRACE(mm_page_alloc)) | 109 | if (GATOR_REGISTER_TRACE(mm_page_alloc)) |
108 | goto mm_page_alloc_exit; | 110 | goto mm_page_alloc_exit; |
109 | 111 | ||
112 | setup_timer(&meminfo_wake_up_timer, meminfo_wake_up_handler, 0); | ||
110 | return 0; | 113 | return 0; |
111 | 114 | ||
112 | mm_page_alloc_exit: | 115 | mm_page_alloc_exit: |
@@ -140,13 +143,15 @@ static void gator_events_meminfo_stop(void) | |||
140 | GATOR_UNREGISTER_TRACE(mm_page_alloc); | 143 | GATOR_UNREGISTER_TRACE(mm_page_alloc); |
141 | } | 144 | } |
142 | 145 | ||
146 | del_timer_sync(&meminfo_wake_up_timer); | ||
147 | |||
143 | meminfo_global_enabled = 0; | 148 | meminfo_global_enabled = 0; |
144 | for (i = 0; i < MEMINFO_TOTAL; i++) { | 149 | for (i = 0; i < MEMINFO_TOTAL; i++) { |
145 | meminfo_enabled[i] = 0; | 150 | meminfo_enabled[i] = 0; |
146 | } | 151 | } |
147 | } | 152 | } |
148 | 153 | ||
149 | // Must be run in process context (work queue) as the kernel function si_meminfo() can sleep | 154 | // Must be run in process context as the kernel function si_meminfo() can sleep |
150 | static void wq_sched_handler(struct work_struct *wsptr) | 155 | static void wq_sched_handler(struct work_struct *wsptr) |
151 | { | 156 | { |
152 | struct sysinfo info; | 157 | struct sysinfo info; |
@@ -181,6 +186,12 @@ static void wq_sched_handler(struct work_struct *wsptr) | |||
181 | new_data_avail = true; | 186 | new_data_avail = true; |
182 | } | 187 | } |
183 | 188 | ||
189 | static void meminfo_wake_up_handler(unsigned long unused_data) | ||
190 | { | ||
191 | // had to delay scheduling work as attempting to schedule work during the context switch is illegal in kernel versions 3.5 and greater | ||
192 | schedule_work(&work); | ||
193 | } | ||
194 | |||
184 | static int gator_events_meminfo_read(long long **buffer) | 195 | static int gator_events_meminfo_read(long long **buffer) |
185 | { | 196 | { |
186 | static unsigned int last_mem_event = 0; | 197 | static unsigned int last_mem_event = 0; |
@@ -190,11 +201,7 @@ static int gator_events_meminfo_read(long long **buffer) | |||
190 | 201 | ||
191 | if (last_mem_event != mem_event) { | 202 | if (last_mem_event != mem_event) { |
192 | last_mem_event = mem_event; | 203 | last_mem_event = mem_event; |
193 | if (in_interrupt()) { | 204 | mod_timer(&meminfo_wake_up_timer, jiffies + 1); |
194 | schedule_work(&work); | ||
195 | } else { | ||
196 | wq_sched_handler(NULL); | ||
197 | } | ||
198 | } | 205 | } |
199 | 206 | ||
200 | if (!new_data_avail) | 207 | if (!new_data_avail) |
diff --git a/driver/gator_events_net.c b/driver/gator_events_net.c index 9298905..a3ae3f0 100644 --- a/driver/gator_events_net.c +++ b/driver/gator_events_net.c | |||
@@ -23,6 +23,8 @@ static int rx_total, tx_total; | |||
23 | static ulong netPrev[TOTALNET]; | 23 | static ulong netPrev[TOTALNET]; |
24 | static int netGet[TOTALNET * 4]; | 24 | static int netGet[TOTALNET * 4]; |
25 | 25 | ||
26 | static struct timer_list net_wake_up_timer; | ||
27 | |||
26 | static void get_network_stats(struct work_struct *wsptr) { | 28 | static void get_network_stats(struct work_struct *wsptr) { |
27 | int rx = 0, tx = 0; | 29 | int rx = 0, tx = 0; |
28 | struct net_device *dev; | 30 | struct net_device *dev; |
@@ -42,6 +44,12 @@ static void get_network_stats(struct work_struct *wsptr) { | |||
42 | } | 44 | } |
43 | DECLARE_WORK(wq_get_stats, get_network_stats); | 45 | DECLARE_WORK(wq_get_stats, get_network_stats); |
44 | 46 | ||
47 | static void net_wake_up_handler(unsigned long unused_data) | ||
48 | { | ||
49 | // had to delay scheduling work as attempting to schedule work during the context switch is illegal in kernel versions 3.5 and greater | ||
50 | schedule_work(&wq_get_stats); | ||
51 | } | ||
52 | |||
45 | static void calculate_delta(int *rx, int *tx) | 53 | static void calculate_delta(int *rx, int *tx) |
46 | { | 54 | { |
47 | int rx_calc, tx_calc; | 55 | int rx_calc, tx_calc; |
@@ -83,14 +91,16 @@ static int gator_events_net_create_files(struct super_block *sb, struct dentry * | |||
83 | 91 | ||
84 | static int gator_events_net_start(void) | 92 | static int gator_events_net_start(void) |
85 | { | 93 | { |
86 | get_network_stats(NULL); | 94 | get_network_stats(0); |
87 | netPrev[NETRX] = rx_total; | 95 | netPrev[NETRX] = rx_total; |
88 | netPrev[NETTX] = tx_total; | 96 | netPrev[NETTX] = tx_total; |
97 | setup_timer(&net_wake_up_timer, net_wake_up_handler, 0); | ||
89 | return 0; | 98 | return 0; |
90 | } | 99 | } |
91 | 100 | ||
92 | static void gator_events_net_stop(void) | 101 | static void gator_events_net_stop(void) |
93 | { | 102 | { |
103 | del_timer_sync(&net_wake_up_timer); | ||
94 | netrx_enabled = 0; | 104 | netrx_enabled = 0; |
95 | nettx_enabled = 0; | 105 | nettx_enabled = 0; |
96 | } | 106 | } |
@@ -106,11 +116,7 @@ static int gator_events_net_read(int **buffer) | |||
106 | if (!netrx_enabled && !nettx_enabled) | 116 | if (!netrx_enabled && !nettx_enabled) |
107 | return 0; | 117 | return 0; |
108 | 118 | ||
109 | if (in_interrupt()){ | 119 | mod_timer(&net_wake_up_timer, jiffies + 1); |
110 | schedule_work(&wq_get_stats); | ||
111 | } else { | ||
112 | get_network_stats(NULL); | ||
113 | } | ||
114 | 120 | ||
115 | calculate_delta(&rx_delta, &tx_delta); | 121 | calculate_delta(&rx_delta, &tx_delta); |
116 | 122 | ||
diff --git a/driver/gator_main.c b/driver/gator_main.c index 988045f..994e35d 100644 --- a/driver/gator_main.c +++ b/driver/gator_main.c | |||
@@ -110,6 +110,7 @@ static DEFINE_MUTEX(gator_buffer_mutex); | |||
110 | bool event_based_sampling; | 110 | bool event_based_sampling; |
111 | 111 | ||
112 | static DECLARE_WAIT_QUEUE_HEAD(gator_buffer_wait); | 112 | static DECLARE_WAIT_QUEUE_HEAD(gator_buffer_wait); |
113 | static struct timer_list gator_buffer_wake_up_timer; | ||
113 | static LIST_HEAD(gator_events); | 114 | static LIST_HEAD(gator_events); |
114 | 115 | ||
115 | /****************************************************************************** | 116 | /****************************************************************************** |
@@ -163,6 +164,11 @@ u32 gator_cpuid(void) | |||
163 | } | 164 | } |
164 | #endif | 165 | #endif |
165 | 166 | ||
167 | static void gator_buffer_wake_up(unsigned long data) | ||
168 | { | ||
169 | wake_up(&gator_buffer_wait); | ||
170 | } | ||
171 | |||
166 | /****************************************************************************** | 172 | /****************************************************************************** |
167 | * Commit interface | 173 | * Commit interface |
168 | ******************************************************************************/ | 174 | ******************************************************************************/ |
@@ -283,7 +289,9 @@ static void gator_commit_buffer(int cpu, int buftype) | |||
283 | 289 | ||
284 | per_cpu(gator_buffer_commit, cpu)[buftype] = per_cpu(gator_buffer_write, cpu)[buftype]; | 290 | per_cpu(gator_buffer_commit, cpu)[buftype] = per_cpu(gator_buffer_write, cpu)[buftype]; |
285 | gator_buffer_header(cpu, buftype); | 291 | gator_buffer_header(cpu, buftype); |
286 | wake_up(&gator_buffer_wait); | 292 | |
293 | // had to delay scheduling work as attempting to schedule work during the context switch is illegal in kernel versions 3.5 and greater | ||
294 | mod_timer(&gator_buffer_wake_up_timer, jiffies + 1); | ||
287 | } | 295 | } |
288 | 296 | ||
289 | static void buffer_check(int cpu, int buftype) | 297 | static void buffer_check(int cpu, int buftype) |
@@ -1069,11 +1077,14 @@ static int __init gator_module_init(void) | |||
1069 | return -1; | 1077 | return -1; |
1070 | } | 1078 | } |
1071 | 1079 | ||
1080 | setup_timer(&gator_buffer_wake_up_timer, gator_buffer_wake_up, 0); | ||
1081 | |||
1072 | return 0; | 1082 | return 0; |
1073 | } | 1083 | } |
1074 | 1084 | ||
1075 | static void __exit gator_module_exit(void) | 1085 | static void __exit gator_module_exit(void) |
1076 | { | 1086 | { |
1087 | del_timer_sync(&gator_buffer_wake_up_timer); | ||
1077 | tracepoint_synchronize_unregister(); | 1088 | tracepoint_synchronize_unregister(); |
1078 | gatorfs_unregister(); | 1089 | gatorfs_unregister(); |
1079 | } | 1090 | } |