diff options
Diffstat (limited to 'daemon/events-Mali-V500.xml')
-rw-r--r-- | daemon/events-Mali-V500.xml | 29 |
1 files changed, 29 insertions, 0 deletions
diff --git a/daemon/events-Mali-V500.xml b/daemon/events-Mali-V500.xml new file mode 100644 index 0000000..d2751e7 --- /dev/null +++ b/daemon/events-Mali-V500.xml | |||
@@ -0,0 +1,29 @@ | |||
1 | <category name="Mali-V500"> | ||
2 | <event counter="ARM_Mali-V500_cnt0" title="Mali Video Engine" name="Samples" class="absolute" description="The number of times we have taken a sample"/> | ||
3 | <event counter="ARM_Mali-V500_cnt1" title="Mali Video Engine" name="Queued input-buffers" class="absolute" description="The number of input-buffers that has been queued for consumption by the MVE"/> | ||
4 | <event counter="ARM_Mali-V500_cnt2" title="Mali Video Engine" name="Consumed input-buffers" class="absolute" description="The number of input-buffers that has been consumed by the MVE and returned to the application"/> | ||
5 | <event counter="ARM_Mali-V500_cnt3" title="Mali Video Engine" name="Queued output-buffers" class="absolute" description="The number of output-buffers that has been queued for usage by the MVE"/> | ||
6 | <event counter="ARM_Mali-V500_cnt4" title="Mali Video Engine" name="Consumed output-buffers" class="absolute" description="The number of output-buffers that has been consumed by the MVE and returned to the application"/> | ||
7 | <event counter="ARM_Mali-V500_cnt5" title="Mali Video Engine" name="Created Sessions" class="absolute" description="The number of created sessions throughout the lifetime of the process"/> | ||
8 | <event counter="ARM_Mali-V500_cnt6" title="Mali Video Engine" name="Active Sessions" description="The number of currently existing sessions"/> | ||
9 | <event counter="ARM_Mali-V500_cnt7" title="Mali Video Engine" name="Processed Frames" class="absolute" description="The number of processed frames. A processed frame is one where the encode or decode is complete for that particular frame. Frames can be processed out of order so this is not the same as the number of output-buffers returned"/> | ||
10 | <event counter="ARM_Mali-V500_cnt8" title="Mali Video Engine" name="Input Flushes Requested" class="absolute" description="The number of requested flushes of the input queue"/> | ||
11 | <event counter="ARM_Mali-V500_cnt9" title="Mali Video Engine" name="Input Flushes Complete" class="absolute" description="The number of completed flushes of the input queue"/> | ||
12 | <event counter="ARM_Mali-V500_cnt10" title="Mali Video Engine" name="Output Flushes Requested" class="absolute" description="The number of requested flushes of the output queue"/> | ||
13 | <event counter="ARM_Mali-V500_cnt11" title="Mali Video Engine" name="Output Flushes Complete" class="absolute" description="The number of completed flushes of the output queue"/> | ||
14 | <event counter="ARM_Mali-V500_cnt12" title="Mali Video Engine" name="Queued Output Buffers (current)" description="The number of output-buffers that are currently queued for usage by the MVE"/> | ||
15 | <event counter="ARM_Mali-V500_cnt13" title="Mali Video Engine" name="Queued Input Buffers (current)" description="The number of input-buffers that are currently queued for consumption by the MVE"/> | ||
16 | <event counter="ARM_Mali-V500_cnt14" title="Mali Video Engine" name="Output Queue Flushes" description="The number of pending flushes for the MVE output-queue"/> | ||
17 | <event counter="ARM_Mali-V500_cnt15" title="Mali Video Engine" name="Input Queue Flushes" description="The number of pending flushes for the MVE input-queue"/> | ||
18 | <event counter="ARM_Mali-V500_cnt16" title="Mali Video Engine" name="Errors encountered" class="absolute" description="The number of errors encountered"/> | ||
19 | <event counter="ARM_Mali-V500_cnt17" title="Mali Video Engine" name="Bits consumed" class="absolute" description="The number of bits consumed during decode"/> | ||
20 | <event counter="ARM_Mali-V500_cnt18" title="Mali Video Engine" name="AFBC bandwidth" class="absolute" description="The amount of AFBC-encoded bytes read or written"/> | ||
21 | <event counter="ARM_Mali-V500_cnt19" title="Mali Video Engine" name="Bandwidth (read)" class="absolute" description="The amount of bytes read over the AXI bus"/> | ||
22 | <event counter="ARM_Mali-V500_cnt20" title="Mali Video Engine" name="Bandwidth (write)" class="absolute" description="The amount of bytes written over the AXI bus"/> | ||
23 | <event counter="ARM_Mali-V500_evn0" title="Mali Video Engine" name="Session created" description="Generated when a session has been created"/> | ||
24 | <event counter="ARM_Mali-V500_evn1" title="Mali Video Engine" name="Session destroyed" description="Generated when a session has been destroyed"/> | ||
25 | <event counter="ARM_Mali-V500_evn2" title="Mali Video Engine" name="Frame Processed" description="Generated when the MVE has finished processing a frame"/> | ||
26 | <event counter="ARM_Mali-V500_evn3" title="Mali Video Engine" name="Output buffer received" description="Generated when an an output buffer is returned to us from the MVE"/> | ||
27 | <event counter="ARM_Mali-V500_evn4" title="Mali Video Engine" name="Input buffer received" description="Generated when we an input buffer is returned to us from the MVE"/> | ||
28 | <!--event counter="ARM_Mali-V500_act" title="VPU" name="Activity" class="activity" activity1="Parsed" activity_color1="0x000000ff" activity2="Piped" activity_color2="0x0000ff00" rendering_type="bar" average_selection="yes" average_cores="yes" percentage="yes" cores="8" description="Mali-V500 Activity"/--> | ||
29 | </category> | ||