/** * Copyright (C) ARM Limited 2010-2014. All rights reserved. * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. */ #include "UserSpaceSource.h" #include #include #include "Child.h" #include "DriverSource.h" #include "Logging.h" #include "SessionData.h" #define NS_PER_US 1000 extern Child *child; UserSpaceSource::UserSpaceSource(sem_t *senderSem) : mBuffer(0, FRAME_BLOCK_COUNTER, gSessionData->mTotalBufferSize*1024*1024, senderSem) { } UserSpaceSource::~UserSpaceSource() { } bool UserSpaceSource::prepare() { return true; } void UserSpaceSource::run() { prctl(PR_SET_NAME, (unsigned long)&"gatord-counters", 0, 0, 0); gSessionData->hwmon.start(); gSessionData->fsDriver.start(); int64_t monotonic_started = 0; while (monotonic_started <= 0) { usleep(10); if (DriverSource::readInt64Driver("/dev/gator/started", &monotonic_started) == -1) { logg->logError(__FILE__, __LINE__, "Error reading gator driver start time"); handleException(); } } uint64_t next_time = 0; while (gSessionData->mSessionIsActive) { const uint64_t curr_time = getTime() - monotonic_started; // Sample ten times a second ignoring gSessionData->mSampleRate next_time += NS_PER_S/10;//gSessionData->mSampleRate; if (next_time < curr_time) { logg->logMessage("Too slow, curr_time: %lli next_time: %lli", curr_time, next_time); next_time = curr_time; } if (mBuffer.eventHeader(curr_time)) { gSessionData->hwmon.read(&mBuffer); gSessionData->fsDriver.read(&mBuffer); // Only check after writing all counters so that time and corresponding counters appear in the same frame mBuffer.check(curr_time); } if (mBuffer.bytesAvailable() <= 0) { logg->logMessage("One shot (counters)"); child->endSession(); } usleep((next_time - curr_time)/NS_PER_US); } mBuffer.setDone(); } void UserSpaceSource::interrupt() { // Do nothing } bool UserSpaceSource::isDone() { return mBuffer.isDone(); } void UserSpaceSource::write(Sender *sender) { if (!mBuffer.isDone()) { mBuffer.write(sender); } }