/** * Copyright (C) ARM Limited 2010-2013. All rights reserved. * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. */ #include "gator.h" #include #include #include #include "linux/mali_linux_trace.h" #include "gator_events_mali_common.h" #include "gator_events_mali_400.h" /* * There are (currently) three different variants of the comms between gator and Mali: * 1 (deprecated): No software counter support * 2 (deprecated): Tracepoint called for each separate s/w counter value as it appears * 3 (default): Single tracepoint for all s/w counters in a bundle. * Interface style 3 is the default if no other is specified. 1 and 2 will be eliminated when * existing Mali DDKs are upgraded. */ #if !defined(GATOR_MALI_INTERFACE_STYLE) #define GATOR_MALI_INTERFACE_STYLE (3) #endif /* * List of possible actions allowing DDK to be controlled by Streamline. * The following numbers are used by DDK to control the frame buffer dumping. */ #define FBDUMP_CONTROL_ENABLE (1) #define FBDUMP_CONTROL_RATE (2) #define SW_EVENTS_ENABLE (3) #define FBDUMP_CONTROL_RESIZE_FACTOR (4) /* * Check that the MALI_SUPPORT define is set to one of the allowable device codes. */ #if (MALI_SUPPORT != MALI_400) #error MALI_SUPPORT set to an invalid device code: expecting MALI_400 #endif /* * The number of fragment processors. Update to suit your hardware implementation. */ #define NUM_FP_UNITS (4) enum counters { /* Timeline activity */ ACTIVITY_VP = 0, ACTIVITY_FP0, ACTIVITY_FP1, ACTIVITY_FP2, ACTIVITY_FP3, /* L2 cache counters */ COUNTER_L2_C0, COUNTER_L2_C1, /* Vertex processor counters */ COUNTER_VP_C0, COUNTER_VP_C1, /* Fragment processor counters */ COUNTER_FP0_C0, COUNTER_FP0_C1, COUNTER_FP1_C0, COUNTER_FP1_C1, COUNTER_FP2_C0, COUNTER_FP2_C1, COUNTER_FP3_C0, COUNTER_FP3_C1, /* EGL Software Counters */ COUNTER_EGL_BLIT_TIME, /* GLES Software Counters */ COUNTER_GLES_DRAW_ELEMENTS_CALLS, COUNTER_GLES_DRAW_ELEMENTS_NUM_INDICES, COUNTER_GLES_DRAW_ELEMENTS_NUM_TRANSFORMED, COUNTER_GLES_DRAW_ARRAYS_CALLS, COUNTER_GLES_DRAW_ARRAYS_NUM_TRANSFORMED, COUNTER_GLES_DRAW_POINTS, COUNTER_GLES_DRAW_LINES, COUNTER_GLES_DRAW_LINE_LOOP, COUNTER_GLES_DRAW_LINE_STRIP, COUNTER_GLES_DRAW_TRIANGLES, COUNTER_GLES_DRAW_TRIANGLE_STRIP, COUNTER_GLES_DRAW_TRIANGLE_FAN, COUNTER_GLES_NON_VBO_DATA_COPY_TIME, COUNTER_GLES_UNIFORM_BYTES_COPIED_TO_MALI, COUNTER_GLES_UPLOAD_TEXTURE_TIME, COUNTER_GLES_UPLOAD_VBO_TIME, COUNTER_GLES_NUM_FLUSHES, COUNTER_GLES_NUM_VSHADERS_GENERATED, COUNTER_GLES_NUM_FSHADERS_GENERATED, COUNTER_GLES_VSHADER_GEN_TIME, COUNTER_GLES_FSHADER_GEN_TIME, COUNTER_GLES_INPUT_TRIANGLES, COUNTER_GLES_VXCACHE_HIT, COUNTER_GLES_VXCACHE_MISS, COUNTER_GLES_VXCACHE_COLLISION, COUNTER_GLES_CULLED_TRIANGLES, COUNTER_GLES_CULLED_LINES, COUNTER_GLES_BACKFACE_TRIANGLES, COUNTER_GLES_GBCLIP_TRIANGLES, COUNTER_GLES_GBCLIP_LINES, COUNTER_GLES_TRIANGLES_DRAWN, COUNTER_GLES_DRAWCALL_TIME, COUNTER_GLES_TRIANGLES_COUNT, COUNTER_GLES_INDEPENDENT_TRIANGLES_COUNT, COUNTER_GLES_STRIP_TRIANGLES_COUNT, COUNTER_GLES_FAN_TRIANGLES_COUNT, COUNTER_GLES_LINES_COUNT, COUNTER_GLES_INDEPENDENT_LINES_COUNT, COUNTER_GLES_STRIP_LINES_COUNT, COUNTER_GLES_LOOP_LINES_COUNT, COUNTER_FILMSTRIP, COUNTER_FREQUENCY, COUNTER_VOLTAGE, NUMBER_OF_EVENTS }; #define FIRST_ACTIVITY_EVENT ACTIVITY_VP #define LAST_ACTIVITY_EVENT ACTIVITY_FP3 #define FIRST_HW_COUNTER COUNTER_L2_C0 #define LAST_HW_COUNTER COUNTER_FP3_C1 #define FIRST_SW_COUNTER COUNTER_EGL_BLIT_TIME #define LAST_SW_COUNTER COUNTER_GLES_LOOP_LINES_COUNT #define FIRST_SPECIAL_COUNTER COUNTER_FILMSTRIP #define LAST_SPECIAL_COUNTER COUNTER_VOLTAGE /* gatorfs variables for counter enable state, * the event the counter should count and the * 'key' (a unique id set by gatord and returned * by gator.ko) */ static unsigned long counter_enabled[NUMBER_OF_EVENTS]; static unsigned long counter_event[NUMBER_OF_EVENTS]; static unsigned long counter_key[NUMBER_OF_EVENTS]; /* The data we have recorded */ static u32 counter_data[NUMBER_OF_EVENTS]; /* The address to sample (or 0 if samples are sent to us) */ static u32 *counter_address[NUMBER_OF_EVENTS]; /* An array used to return the data we recorded * as key,value pairs hence the *2 */ static unsigned long counter_dump[NUMBER_OF_EVENTS * 2]; static unsigned long counter_prev[NUMBER_OF_EVENTS]; /* Note whether tracepoints have been registered */ static int trace_registered; /** * Calculate the difference and handle the overflow. */ static u32 get_difference(u32 start, u32 end) { if (start - end >= 0) { return start - end; } // Mali counters are unsigned 32 bit values that wrap. return (4294967295u - end) + start; } /** * Returns non-zero if the given counter ID is an activity counter. */ static inline int is_activity_counter(unsigned int event_id) { return (event_id >= FIRST_ACTIVITY_EVENT && event_id <= LAST_ACTIVITY_EVENT); } /** * Returns non-zero if the given counter ID is a hardware counter. */ static inline int is_hw_counter(unsigned int event_id) { return (event_id >= FIRST_HW_COUNTER && event_id <= LAST_HW_COUNTER); } #if GATOR_MALI_INTERFACE_STYLE == 2 /** * Returns non-zero if the given counter ID is a software counter. */ static inline int is_sw_counter(unsigned int event_id) { return (event_id >= FIRST_SW_COUNTER && event_id <= LAST_SW_COUNTER); } #endif #if GATOR_MALI_INTERFACE_STYLE == 2 /* * The Mali DDK uses s64 types to contain software counter values, but gator * can only use a maximum of 32 bits. This function scales a software counter * to an appropriate range. */ static u32 scale_sw_counter_value(unsigned int event_id, signed long long value) { u32 scaled_value; switch (event_id) { case COUNTER_GLES_UPLOAD_TEXTURE_TIME: case COUNTER_GLES_UPLOAD_VBO_TIME: scaled_value = (u32)div_s64(value, 1000000); break; default: scaled_value = (u32)value; break; } return scaled_value; } #endif /* Probe for continuously sampled counter */ #if 0 //WE_DONT_CURRENTLY_USE_THIS_SO_SUPPRESS_WARNING GATOR_DEFINE_PROBE(mali_sample_address, TP_PROTO(unsigned int event_id, u32 *addr)) { /* Turning on too many pr_debug statements in frequently called functions * can cause stability and/or performance problems */ //pr_debug("gator: mali_sample_address %d %d\n", event_id, addr); if (event_id >= ACTIVITY_VP && event_id <= COUNTER_FP3_C1) { counter_address[event_id] = addr; } } #endif /* Probe for hardware counter events */ GATOR_DEFINE_PROBE(mali_hw_counter, TP_PROTO(unsigned int event_id, unsigned int value)) { /* Turning on too many pr_debug statements in frequently called functions * can cause stability and/or performance problems */ //pr_debug("gator: mali_hw_counter %d %d\n", event_id, value); if (is_hw_counter(event_id)) { counter_data[event_id] = value; } } #if GATOR_MALI_INTERFACE_STYLE == 2 GATOR_DEFINE_PROBE(mali_sw_counter, TP_PROTO(unsigned int event_id, signed long long value)) { if (is_sw_counter(event_id)) { counter_data[event_id] = scale_sw_counter_value(event_id, value); } } #endif /* GATOR_MALI_INTERFACE_STYLE == 2 */ #if GATOR_MALI_INTERFACE_STYLE == 3 GATOR_DEFINE_PROBE(mali_sw_counters, TP_PROTO(pid_t pid, pid_t tid, void *surface_id, unsigned int *counters)) { u32 i; /* Copy over the values for those counters which are enabled. */ for (i = FIRST_SW_COUNTER; i <= LAST_SW_COUNTER; i++) { if (counter_enabled[i]) { counter_data[i] = (u32)(counters[i - FIRST_SW_COUNTER]); } } } #endif /* GATOR_MALI_INTERFACE_STYLE == 3 */ static int create_files(struct super_block *sb, struct dentry *root) { struct dentry *dir; int event; int n_fp = NUM_FP_UNITS; const char *mali_name = gator_mali_get_mali_name(); /* * Create the filesystem entries for vertex processor, fragment processor * and L2 cache timeline and hardware counters. Software counters get * special handling after this block. */ for (event = FIRST_ACTIVITY_EVENT; event <= LAST_HW_COUNTER; event++) { char buf[40]; /* * We can skip this event if it's for a non-existent fragment * processor. */ if (((event - ACTIVITY_FP0 >= n_fp) && (event < COUNTER_L2_C0)) || (((event - COUNTER_FP0_C0) / 2 >= n_fp))) { continue; } /* Otherwise, set up the filesystem entry for this event. */ switch (event) { case ACTIVITY_VP: snprintf(buf, sizeof buf, "ARM_%s_VP_active", mali_name); break; case ACTIVITY_FP0: case ACTIVITY_FP1: case ACTIVITY_FP2: case ACTIVITY_FP3: snprintf(buf, sizeof buf, "ARM_%s_FP%d_active", mali_name, event - ACTIVITY_FP0); break; case COUNTER_L2_C0: case COUNTER_L2_C1: snprintf(buf, sizeof buf, "ARM_%s_L2_cnt%d", mali_name, event - COUNTER_L2_C0); break; case COUNTER_VP_C0: case COUNTER_VP_C1: snprintf(buf, sizeof buf, "ARM_%s_VP_cnt%d", mali_name, event - COUNTER_VP_C0); break; case COUNTER_FP0_C0: case COUNTER_FP0_C1: case COUNTER_FP1_C0: case COUNTER_FP1_C1: case COUNTER_FP2_C0: case COUNTER_FP2_C1: case COUNTER_FP3_C0: case COUNTER_FP3_C1: snprintf(buf, sizeof buf, "ARM_%s_FP%d_cnt%d", mali_name, (event - COUNTER_FP0_C0) / 2, (event - COUNTER_FP0_C0) % 2); break; default: printk("gator: trying to create file for non-existent counter (%d)\n", event); continue; } dir = gatorfs_mkdir(sb, root, buf); if (!dir) { return -1; } gatorfs_create_ulong(sb, dir, "enabled", &counter_enabled[event]); /* Only create an event node for counters that can change what they count */ if (event >= COUNTER_L2_C0) { gatorfs_create_ulong(sb, dir, "event", &counter_event[event]); } gatorfs_create_ro_ulong(sb, dir, "key", &counter_key[event]); } /* Now set up the software counter entries */ for (event = FIRST_SW_COUNTER; event <= LAST_SW_COUNTER; event++) { char buf[40]; snprintf(buf, sizeof(buf), "ARM_%s_SW_%d", mali_name, event); dir = gatorfs_mkdir(sb, root, buf); if (!dir) { return -1; } gatorfs_create_ulong(sb, dir, "enabled", &counter_enabled[event]); gatorfs_create_ro_ulong(sb, dir, "key", &counter_key[event]); } /* Now set up the special counter entries */ for (event = FIRST_SPECIAL_COUNTER; event <= LAST_SPECIAL_COUNTER; event++) { char buf[40]; switch (event) { case COUNTER_FILMSTRIP: snprintf(buf, sizeof(buf), "ARM_%s_Filmstrip_cnt0", mali_name); break; case COUNTER_FREQUENCY: snprintf(buf, sizeof(buf), "ARM_%s_Frequency", mali_name); break; case COUNTER_VOLTAGE: snprintf(buf, sizeof(buf), "ARM_%s_Voltage", mali_name); break; default: break; } dir = gatorfs_mkdir(sb, root, buf); if (!dir) { return -1; } gatorfs_create_ulong(sb, dir, "event", &counter_event[event]); gatorfs_create_ulong(sb, dir, "enabled", &counter_enabled[event]); gatorfs_create_ro_ulong(sb, dir, "key", &counter_key[event]); } return 0; } /* * Local store for the get_counters entry point into the DDK. * This is stored here since it is used very regularly. */ static mali_profiling_get_counters_type *mali_get_counters = NULL; /* * Examine list of software counters and determine if any one is enabled. * Returns 1 if any counter is enabled, 0 if none is. */ static int is_any_sw_counter_enabled(void) { unsigned int i; for (i = FIRST_SW_COUNTER; i <= LAST_SW_COUNTER; i++) { if (counter_enabled[i]) { return 1; /* At least one counter is enabled */ } } return 0; /* No s/w counters enabled */ } static void mali_counter_initialize(void) { /* If a Mali driver is present and exporting the appropriate symbol * then we can request the HW counters (of which there are only 2) * be configured to count the desired events */ mali_profiling_set_event_type *mali_set_hw_event; mali_osk_fb_control_set_type *mali_set_fb_event; mali_profiling_control_type *mali_control; mali_set_hw_event = symbol_get(_mali_profiling_set_event); if (mali_set_hw_event) { int i; pr_debug("gator: mali online _mali_profiling_set_event symbol @ %p\n", mali_set_hw_event); for (i = FIRST_HW_COUNTER; i <= LAST_HW_COUNTER; i++) { if (counter_enabled[i]) { mali_set_hw_event(i, counter_event[i]); } else { mali_set_hw_event(i, 0xFFFFFFFF); } } symbol_put(_mali_profiling_set_event); } else { printk("gator: mali online _mali_profiling_set_event symbol not found\n"); } mali_set_fb_event = symbol_get(_mali_osk_fb_control_set); if (mali_set_fb_event) { pr_debug("gator: mali online _mali_osk_fb_control_set symbol @ %p\n", mali_set_fb_event); mali_set_fb_event(0, (counter_enabled[COUNTER_FILMSTRIP] ? 1 : 0)); symbol_put(_mali_osk_fb_control_set); } else { printk("gator: mali online _mali_osk_fb_control_set symbol not found\n"); } /* Generic control interface for Mali DDK. */ mali_control = symbol_get(_mali_profiling_control); if (mali_control) { /* The event attribute in the XML file keeps the actual frame rate. */ unsigned int rate = counter_event[COUNTER_FILMSTRIP] & 0xff; unsigned int resize_factor = (counter_event[COUNTER_FILMSTRIP] >> 8) & 0xff; pr_debug("gator: mali online _mali_profiling_control symbol @ %p\n", mali_control); mali_control(SW_EVENTS_ENABLE, (is_any_sw_counter_enabled() ? 1 : 0)); mali_control(FBDUMP_CONTROL_ENABLE, (counter_enabled[COUNTER_FILMSTRIP] ? 1 : 0)); mali_control(FBDUMP_CONTROL_RATE, rate); mali_control(FBDUMP_CONTROL_RESIZE_FACTOR, resize_factor); pr_debug("gator: sent mali_control enabled=%d, rate=%d\n", (counter_enabled[COUNTER_FILMSTRIP] ? 1 : 0), rate); symbol_put(_mali_profiling_control); } else { printk("gator: mali online _mali_profiling_control symbol not found\n"); } mali_get_counters = symbol_get(_mali_profiling_get_counters); if (mali_get_counters) { pr_debug("gator: mali online _mali_profiling_get_counters symbol @ %p\n", mali_get_counters); counter_prev[COUNTER_L2_C0] = 0; counter_prev[COUNTER_L2_C1] = 0; } else { pr_debug("gator WARNING: mali _mali_profiling_get_counters symbol not defined"); } } static void mali_counter_deinitialize(void) { mali_profiling_set_event_type *mali_set_hw_event; mali_osk_fb_control_set_type *mali_set_fb_event; mali_profiling_control_type *mali_control; mali_set_hw_event = symbol_get(_mali_profiling_set_event); if (mali_set_hw_event) { int i; pr_debug("gator: mali offline _mali_profiling_set_event symbol @ %p\n", mali_set_hw_event); for (i = FIRST_HW_COUNTER; i <= LAST_HW_COUNTER; i++) { mali_set_hw_event(i, 0xFFFFFFFF); } symbol_put(_mali_profiling_set_event); } else { printk("gator: mali offline _mali_profiling_set_event symbol not found\n"); } mali_set_fb_event = symbol_get(_mali_osk_fb_control_set); if (mali_set_fb_event) { pr_debug("gator: mali offline _mali_osk_fb_control_set symbol @ %p\n", mali_set_fb_event); mali_set_fb_event(0, 0); symbol_put(_mali_osk_fb_control_set); } else { printk("gator: mali offline _mali_osk_fb_control_set symbol not found\n"); } /* Generic control interface for Mali DDK. */ mali_control = symbol_get(_mali_profiling_control); if (mali_control) { pr_debug("gator: mali offline _mali_profiling_control symbol @ %p\n", mali_set_fb_event); /* Reset the DDK state - disable counter collection */ mali_control(SW_EVENTS_ENABLE, 0); mali_control(FBDUMP_CONTROL_ENABLE, 0); symbol_put(_mali_profiling_control); } else { printk("gator: mali offline _mali_profiling_control symbol not found\n"); } if (mali_get_counters) { symbol_put(_mali_profiling_get_counters); } } static int start(void) { // register tracepoints if (GATOR_REGISTER_TRACE(mali_hw_counter)) { printk("gator: mali_hw_counter tracepoint failed to activate\n"); return -1; } #if GATOR_MALI_INTERFACE_STYLE == 1 /* None. */ #elif GATOR_MALI_INTERFACE_STYLE == 2 /* For patched Mali driver. */ if (GATOR_REGISTER_TRACE(mali_sw_counter)) { printk("gator: mali_sw_counter tracepoint failed to activate\n"); return -1; } #elif GATOR_MALI_INTERFACE_STYLE == 3 /* For Mali drivers with built-in support. */ if (GATOR_REGISTER_TRACE(mali_sw_counters)) { printk("gator: mali_sw_counters tracepoint failed to activate\n"); return -1; } #else #error Unknown GATOR_MALI_INTERFACE_STYLE option. #endif trace_registered = 1; mali_counter_initialize(); return 0; } static void stop(void) { unsigned int cnt; pr_debug("gator: mali stop\n"); if (trace_registered) { GATOR_UNREGISTER_TRACE(mali_hw_counter); #if GATOR_MALI_INTERFACE_STYLE == 1 /* None. */ #elif GATOR_MALI_INTERFACE_STYLE == 2 /* For patched Mali driver. */ GATOR_UNREGISTER_TRACE(mali_sw_counter); #elif GATOR_MALI_INTERFACE_STYLE == 3 /* For Mali drivers with built-in support. */ GATOR_UNREGISTER_TRACE(mali_sw_counters); #else #error Unknown GATOR_MALI_INTERFACE_STYLE option. #endif pr_debug("gator: mali timeline tracepoint deactivated\n"); trace_registered = 0; } for (cnt = FIRST_ACTIVITY_EVENT; cnt < NUMBER_OF_EVENTS; cnt++) { counter_enabled[cnt] = 0; counter_event[cnt] = 0; counter_address[cnt] = NULL; } mali_counter_deinitialize(); } static int read(int **buffer) { int cnt, len = 0; if (!on_primary_core()) return 0; // Read the L2 C0 and C1 here. if (counter_enabled[COUNTER_L2_C0] || counter_enabled[COUNTER_L2_C1]) { u32 src0 = 0; u32 val0 = 0; u32 src1 = 0; u32 val1 = 0; // Poke the driver to get the counter values if (mali_get_counters) { mali_get_counters(&src0, &val0, &src1, &val1); } if (counter_enabled[COUNTER_L2_C0]) { // Calculate and save src0's counter val0 counter_dump[len++] = counter_key[COUNTER_L2_C0]; counter_dump[len++] = get_difference(val0, counter_prev[COUNTER_L2_C0]); } if (counter_enabled[COUNTER_L2_C1]) { // Calculate and save src1's counter val1 counter_dump[len++] = counter_key[COUNTER_L2_C1]; counter_dump[len++] = get_difference(val1, counter_prev[COUNTER_L2_C1]); } // Save the previous values for the counters. counter_prev[COUNTER_L2_C0] = val0; counter_prev[COUNTER_L2_C1] = val1; } // Process other (non-timeline) counters. for (cnt = COUNTER_VP_C0; cnt <= LAST_SW_COUNTER; cnt++) { if (counter_enabled[cnt]) { counter_dump[len++] = counter_key[cnt]; counter_dump[len++] = counter_data[cnt]; counter_data[cnt] = 0; } } /* * Add in the voltage and frequency counters if enabled. Note that, since these are * actually passed as events, the counter value should not be cleared. */ cnt = COUNTER_FREQUENCY; if (counter_enabled[cnt]) { counter_dump[len++] = counter_key[cnt]; counter_dump[len++] = counter_data[cnt]; } cnt = COUNTER_VOLTAGE; if (counter_enabled[cnt]) { counter_dump[len++] = counter_key[cnt]; counter_dump[len++] = counter_data[cnt]; } if (buffer) { *buffer = (int *)counter_dump; } return len; } static struct gator_interface gator_events_mali_interface = { .create_files = create_files, .start = start, .stop = stop, .read = read, }; extern void gator_events_mali_log_dvfs_event(unsigned int frequency_mhz, unsigned int voltage_mv) { counter_data[COUNTER_FREQUENCY] = frequency_mhz; counter_data[COUNTER_VOLTAGE] = voltage_mv; } int gator_events_mali_init(void) { unsigned int cnt; pr_debug("gator: mali init\n"); for (cnt = FIRST_ACTIVITY_EVENT; cnt < NUMBER_OF_EVENTS; cnt++) { counter_enabled[cnt] = 0; counter_event[cnt] = 0; counter_key[cnt] = gator_events_get_key(); counter_address[cnt] = NULL; counter_data[cnt] = 0; } trace_registered = 0; return gator_events_install(&gator_events_mali_interface); } gator_events_init(gator_events_mali_init);