/** * Copyright (C) ARM Limited 2012-2013. All rights reserved. * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. * */ #include "gator.h" #include #include #include #include #include /* Mali T6xx DDK includes */ #include "linux/mali_linux_trace.h" #include "kbase/src/common/mali_kbase.h" #include "kbase/src/linux/mali_kbase_mem_linux.h" #include "gator_events_mali_common.h" /* * Mali-T6xx */ typedef struct kbase_device *kbase_find_device_type(int); typedef kbase_context *kbase_create_context_type(kbase_device *); typedef void kbase_destroy_context_type(kbase_context *); typedef void *kbase_va_alloc_type(kbase_context *, u32); typedef void kbase_va_free_type(kbase_context *, void *); typedef mali_error kbase_instr_hwcnt_enable_type(kbase_context *, kbase_uk_hwcnt_setup *); typedef mali_error kbase_instr_hwcnt_disable_type(kbase_context *); typedef mali_error kbase_instr_hwcnt_clear_type(kbase_context *); typedef mali_error kbase_instr_hwcnt_dump_irq_type(kbase_context *); typedef mali_bool kbase_instr_hwcnt_dump_complete_type(kbase_context *, mali_bool *); static kbase_find_device_type *kbase_find_device_symbol; static kbase_create_context_type *kbase_create_context_symbol; static kbase_va_alloc_type *kbase_va_alloc_symbol; static kbase_instr_hwcnt_enable_type *kbase_instr_hwcnt_enable_symbol; static kbase_instr_hwcnt_clear_type *kbase_instr_hwcnt_clear_symbol; static kbase_instr_hwcnt_dump_irq_type *kbase_instr_hwcnt_dump_irq_symbol; static kbase_instr_hwcnt_dump_complete_type *kbase_instr_hwcnt_dump_complete_symbol; static kbase_instr_hwcnt_disable_type *kbase_instr_hwcnt_disable_symbol; static kbase_va_free_type *kbase_va_free_symbol; static kbase_destroy_context_type *kbase_destroy_context_symbol; /** The interval between reads, in ns. * * Earlier we introduced * a 'hold off for 1ms after last read' to resolve MIDBASE-2178 and MALINE-724. * However, the 1ms hold off is too long if no context switches occur as there is a race * between this value and the tick of the read clock in gator which is also 1ms. If we 'miss' the * current read, the counter values are effectively 'spread' over 2ms and the values seen are half * what they should be (since Streamline averages over sample time). In the presence of context switches * this spread can vary and markedly affect the counters. Currently there is no 'proper' solution to * this, but empirically we have found that reducing the minimum read interval to 950us causes the * counts to be much more stable. */ static const int READ_INTERVAL_NSEC = 950000; #if GATOR_TEST #include "gator_events_mali_t6xx_hw_test.c" #endif /* Blocks for HW counters */ enum { JM_BLOCK = 0, TILER_BLOCK, SHADER_BLOCK, MMU_BLOCK }; /* Counters for Mali-T6xx: * * - HW counters, 4 blocks * For HW counters we need strings to create /dev/gator/events files. * Enums are not needed because the position of the HW name in the array is the same * of the corresponding value in the received block of memory. * HW counters are requested by calculating a bitmask, passed then to the driver. * Every millisecond a HW counters dump is requested, and if the previous has been completed they are read. */ /* Hardware Counters */ static const char *const hardware_counter_names[] = { /* Job Manager */ "", "", "", "", "MESSAGES_SENT", "MESSAGES_RECEIVED", "GPU_ACTIVE", /* 6 */ "IRQ_ACTIVE", "JS0_JOBS", "JS0_TASKS", "JS0_ACTIVE", "", "JS0_WAIT_READ", "JS0_WAIT_ISSUE", "JS0_WAIT_DEPEND", "JS0_WAIT_FINISH", "JS1_JOBS", "JS1_TASKS", "JS1_ACTIVE", "", "JS1_WAIT_READ", "JS1_WAIT_ISSUE", "JS1_WAIT_DEPEND", "JS1_WAIT_FINISH", "JS2_JOBS", "JS2_TASKS", "JS2_ACTIVE", "", "JS2_WAIT_READ", "JS2_WAIT_ISSUE", "JS2_WAIT_DEPEND", "JS2_WAIT_FINISH", "JS3_JOBS", "JS3_TASKS", "JS3_ACTIVE", "", "JS3_WAIT_READ", "JS3_WAIT_ISSUE", "JS3_WAIT_DEPEND", "JS3_WAIT_FINISH", "JS4_JOBS", "JS4_TASKS", "JS4_ACTIVE", "", "JS4_WAIT_READ", "JS4_WAIT_ISSUE", "JS4_WAIT_DEPEND", "JS4_WAIT_FINISH", "JS5_JOBS", "JS5_TASKS", "JS5_ACTIVE", "", "JS5_WAIT_READ", "JS5_WAIT_ISSUE", "JS5_WAIT_DEPEND", "JS5_WAIT_FINISH", "JS6_JOBS", "JS6_TASKS", "JS6_ACTIVE", "", "JS6_WAIT_READ", "JS6_WAIT_ISSUE", "JS6_WAIT_DEPEND", "JS6_WAIT_FINISH", /*Tiler */ "", "", "", "JOBS_PROCESSED", "TRIANGLES", "QUADS", "POLYGONS", "POINTS", "LINES", "VCACHE_HIT", "VCACHE_MISS", "FRONT_FACING", "BACK_FACING", "PRIM_VISIBLE", "PRIM_CULLED", "PRIM_CLIPPED", "LEVEL0", "LEVEL1", "LEVEL2", "LEVEL3", "LEVEL4", "LEVEL5", "LEVEL6", "LEVEL7", "COMMAND_1", "COMMAND_2", "COMMAND_3", "COMMAND_4", "COMMAND_4_7", "COMMAND_8_15", "COMMAND_16_63", "COMMAND_64", "COMPRESS_IN", "COMPRESS_OUT", "COMPRESS_FLUSH", "TIMESTAMPS", "PCACHE_HIT", "PCACHE_MISS", "PCACHE_LINE", "PCACHE_STALL", "WRBUF_HIT", "WRBUF_MISS", "WRBUF_LINE", "WRBUF_PARTIAL", "WRBUF_STALL", "ACTIVE", "LOADING_DESC", "INDEX_WAIT", "INDEX_RANGE_WAIT", "VERTEX_WAIT", "PCACHE_WAIT", "WRBUF_WAIT", "BUS_READ", "BUS_WRITE", "", "", "", "", "", "UTLB_STALL", "UTLB_REPLAY_MISS", "UTLB_REPLAY_FULL", "UTLB_NEW_MISS", "UTLB_HIT", /* Shader Core */ "", "", "", "SHADER_CORE_ACTIVE", "FRAG_ACTIVE", "FRAG_PRIMATIVES", "FRAG_PRIMATIVES_DROPPED", "FRAG_CYCLE_DESC", "FRAG_CYCLES_PLR", "FRAG_CYCLES_VERT", "FRAG_CYCLES_TRISETUP", "FRAG_CYCLES_RAST", "FRAG_THREADS", "FRAG_DUMMY_THREADS", "FRAG_QUADS_RAST", "FRAG_QUADS_EZS_TEST", "FRAG_QUADS_EZS_KILLED", "FRAG_QUADS_LZS_TEST", "FRAG_QUADS_LZS_KILLED", "FRAG_CYCLE_NO_TILE", "FRAG_NUM_TILES", "FRAG_TRANS_ELIM", "COMPUTE_ACTIVE", "COMPUTE_TASKS", "COMPUTE_THREADS", "COMPUTE_CYCLES_DESC", "TRIPIPE_ACTIVE", "ARITH_WORDS", "ARITH_CYCLES_REG", "ARITH_CYCLES_L0", "ARITH_FRAG_DEPEND", "LS_WORDS", "LS_ISSUES", "LS_RESTARTS", "LS_REISSUES_MISS", "LS_REISSUES_VD", "LS_REISSUE_ATTRIB_MISS", "LS_NO_WB", "TEX_WORDS", "TEX_BUBBLES", "TEX_WORDS_L0", "TEX_WORDS_DESC", "TEX_THREADS", "TEX_RECIRC_FMISS", "TEX_RECIRC_DESC", "TEX_RECIRC_MULTI", "TEX_RECIRC_PMISS", "TEX_RECIRC_CONF", "LSC_READ_HITS", "LSC_READ_MISSES", "LSC_WRITE_HITS", "LSC_WRITE_MISSES", "LSC_ATOMIC_HITS", "LSC_ATOMIC_MISSES", "LSC_LINE_FETCHES", "LSC_DIRTY_LINE", "LSC_SNOOPS", "AXI_TLB_STALL", "AXI_TLB_MIESS", "AXI_TLB_TRANSACTION", "LS_TLB_MISS", "LS_TLB_HIT", "AXI_BEATS_READ", "AXI_BEATS_WRITTEN", /*L2 and MMU */ "", "", "", "", "MMU_TABLE_WALK", "MMU_REPLAY_MISS", "MMU_REPLAY_FULL", "MMU_NEW_MISS", "MMU_HIT", "", "", "", "", "", "", "", "UTLB_STALL", "UTLB_REPLAY_MISS", "UTLB_REPLAY_FULL", "UTLB_NEW_MISS", "UTLB_HIT", "", "", "", "", "", "", "", "", "", "L2_WRITE_BEATS", "L2_READ_BEATS", "L2_ANY_LOOKUP", "L2_READ_LOOKUP", "L2_SREAD_LOOKUP", "L2_READ_REPLAY", "L2_READ_SNOOP", "L2_READ_HIT", "L2_CLEAN_MISS", "L2_WRITE_LOOKUP", "L2_SWRITE_LOOKUP", "L2_WRITE_REPLAY", "L2_WRITE_SNOOP", "L2_WRITE_HIT", "L2_EXT_READ_FULL", "L2_EXT_READ_HALF", "L2_EXT_WRITE_FULL", "L2_EXT_WRITE_HALF", "L2_EXT_READ", "L2_EXT_READ_LINE", "L2_EXT_WRITE", "L2_EXT_WRITE_LINE", "L2_EXT_WRITE_SMALL", "L2_EXT_BARRIER", "L2_EXT_AR_STALL", "L2_EXT_R_BUF_FULL", "L2_EXT_RD_BUF_FULL", "L2_EXT_R_RAW", "L2_EXT_W_STALL", "L2_EXT_W_BUF_FULL", "L2_EXT_R_W_HAZARD", "L2_TAG_HAZARD", "L2_SNOOP_FULL", "L2_REPLAY_FULL" }; #define NUMBER_OF_HARDWARE_COUNTERS (sizeof(hardware_counter_names) / sizeof(hardware_counter_names[0])) #define GET_HW_BLOCK(c) (((c) >> 6) & 0x3) #define GET_COUNTER_OFFSET(c) ((c) & 0x3f) /* Memory to dump hardware counters into */ static void *kernel_dump_buffer; /* kbase context and device */ static kbase_context *kbcontext = NULL; static struct kbase_device *kbdevice = NULL; /* * The following function has no external prototype in older DDK revisions. When the DDK * is updated then this should be removed. */ struct kbase_device *kbase_find_device(int minor); static volatile bool kbase_device_busy = false; static unsigned int num_hardware_counters_enabled; /* * gatorfs variables for counter enable state */ static mali_counter counters[NUMBER_OF_HARDWARE_COUNTERS]; /* An array used to return the data we recorded * as key,value pairs hence the *2 */ static unsigned long counter_dump[NUMBER_OF_HARDWARE_COUNTERS * 2]; #define SYMBOL_GET(FUNCTION, ERROR_COUNT) \ if(FUNCTION ## _symbol) \ { \ printk("gator: mali " #FUNCTION " symbol was already registered\n"); \ (ERROR_COUNT)++; \ } \ else \ { \ FUNCTION ## _symbol = symbol_get(FUNCTION); \ if(! FUNCTION ## _symbol) \ { \ printk("gator: mali online " #FUNCTION " symbol not found\n"); \ (ERROR_COUNT)++; \ } \ } #define SYMBOL_CLEANUP(FUNCTION) \ if(FUNCTION ## _symbol) \ { \ symbol_put(FUNCTION); \ FUNCTION ## _symbol = NULL; \ } /** * Execute symbol_get for all the Mali symbols and check for success. * @return the number of symbols not loaded. */ static int init_symbols(void) { int error_count = 0; SYMBOL_GET(kbase_find_device, error_count); SYMBOL_GET(kbase_create_context, error_count); SYMBOL_GET(kbase_va_alloc, error_count); SYMBOL_GET(kbase_instr_hwcnt_enable, error_count); SYMBOL_GET(kbase_instr_hwcnt_clear, error_count); SYMBOL_GET(kbase_instr_hwcnt_dump_irq, error_count); SYMBOL_GET(kbase_instr_hwcnt_dump_complete, error_count); SYMBOL_GET(kbase_instr_hwcnt_disable, error_count); SYMBOL_GET(kbase_va_free, error_count); SYMBOL_GET(kbase_destroy_context, error_count); return error_count; } /** * Execute symbol_put for all the registered Mali symbols. */ static void clean_symbols(void) { SYMBOL_CLEANUP(kbase_find_device); SYMBOL_CLEANUP(kbase_create_context); SYMBOL_CLEANUP(kbase_va_alloc); SYMBOL_CLEANUP(kbase_instr_hwcnt_enable); SYMBOL_CLEANUP(kbase_instr_hwcnt_clear); SYMBOL_CLEANUP(kbase_instr_hwcnt_dump_irq); SYMBOL_CLEANUP(kbase_instr_hwcnt_dump_complete); SYMBOL_CLEANUP(kbase_instr_hwcnt_disable); SYMBOL_CLEANUP(kbase_va_free); SYMBOL_CLEANUP(kbase_destroy_context); } /** * Determines whether a read should take place * @param current_time The current time, obtained from getnstimeofday() * @param prev_time_s The number of seconds at the previous read attempt. * @param next_read_time_ns The time (in ns) when the next read should be allowed. * * Note that this function has been separated out here to allow it to be tested. */ static int is_read_scheduled(const struct timespec *current_time, u32 *prev_time_s, s32 *next_read_time_ns) { /* If the current ns count rolls over a second, roll the next read time too. */ if (current_time->tv_sec != *prev_time_s) { *next_read_time_ns = *next_read_time_ns - NSEC_PER_SEC; } /* Abort the read if the next read time has not arrived. */ if (current_time->tv_nsec < *next_read_time_ns) { return 0; } /* Set the next read some fixed time after this one, and update the read timestamp. */ *next_read_time_ns = current_time->tv_nsec + READ_INTERVAL_NSEC; *prev_time_s = current_time->tv_sec; return 1; } static int start(void) { kbase_uk_hwcnt_setup setup; mali_error err; int cnt; u16 bitmask[] = { 0, 0, 0, 0 }; /* Setup HW counters */ num_hardware_counters_enabled = 0; if (NUMBER_OF_HARDWARE_COUNTERS != 256) { pr_debug("Unexpected number of hardware counters defined: expecting 256, got %d\n", NUMBER_OF_HARDWARE_COUNTERS); } /* Calculate enable bitmasks based on counters_enabled array */ for (cnt = 0; cnt < NUMBER_OF_HARDWARE_COUNTERS; cnt++) { const mali_counter *counter = &counters[cnt]; if (counter->enabled) { int block = GET_HW_BLOCK(cnt); int enable_bit = GET_COUNTER_OFFSET(cnt) / 4; bitmask[block] |= (1 << enable_bit); pr_debug("gator: Mali-T6xx: hardware counter %s selected [%d]\n", hardware_counter_names[cnt], cnt); num_hardware_counters_enabled++; } } /* Create a kbase context for HW counters */ if (num_hardware_counters_enabled > 0) { if (init_symbols() > 0) { clean_symbols(); /* No Mali driver code entrypoints found - not a fault. */ return 0; } kbdevice = kbase_find_device_symbol(-1); /* If we already got a context, fail */ if (kbcontext) { pr_debug("gator: Mali-T6xx: error context already present\n"); goto out; } /* kbcontext will only be valid after all the Mali symbols are loaded successfully */ kbcontext = kbase_create_context_symbol(kbdevice); if (!kbcontext) { pr_debug("gator: Mali-T6xx: error creating kbase context\n"); goto out; } /* * The amount of memory needed to store the dump (bytes) * DUMP_SIZE = number of core groups * * number of blocks (always 8 for midgard) * * number of counters per block (always 64 for midgard) * * number of bytes per counter (always 4 in midgard) * For a Mali-T6xx with a single core group = 1 * 8 * 64 * 4 */ kernel_dump_buffer = kbase_va_alloc_symbol(kbcontext, 2048); if (!kernel_dump_buffer) { pr_debug("gator: Mali-T6xx: error trying to allocate va\n"); goto destroy_context; } setup.dump_buffer = (uintptr_t)kernel_dump_buffer; setup.jm_bm = bitmask[JM_BLOCK]; setup.tiler_bm = bitmask[TILER_BLOCK]; setup.shader_bm = bitmask[SHADER_BLOCK]; setup.mmu_l2_bm = bitmask[MMU_BLOCK]; /* These counters do not exist on Mali-T60x */ setup.l3_cache_bm = 0; /* Use kbase API to enable hardware counters and provide dump buffer */ err = kbase_instr_hwcnt_enable_symbol(kbcontext, &setup); if (err != MALI_ERROR_NONE) { pr_debug("gator: Mali-T6xx: can't setup hardware counters\n"); goto free_buffer; } pr_debug("gator: Mali-T6xx: hardware counters enabled\n"); kbase_instr_hwcnt_clear_symbol(kbcontext); pr_debug("gator: Mali-T6xx: hardware counters cleared \n"); kbase_device_busy = false; } return 0; free_buffer: kbase_va_free_symbol(kbcontext, kernel_dump_buffer); destroy_context: kbase_destroy_context_symbol(kbcontext); out: clean_symbols(); return -1; } static void stop(void) { unsigned int cnt; kbase_context *temp_kbcontext; pr_debug("gator: Mali-T6xx: stop\n"); /* Set all counters as disabled */ for (cnt = 0; cnt < NUMBER_OF_HARDWARE_COUNTERS; cnt++) { counters[cnt].enabled = 0; } /* Destroy the context for HW counters */ if (num_hardware_counters_enabled > 0 && kbcontext != NULL) { /* * Set the global variable to NULL before destroying it, because * other function will check this before using it. */ temp_kbcontext = kbcontext; kbcontext = NULL; kbase_instr_hwcnt_disable_symbol(temp_kbcontext); kbase_va_free_symbol(temp_kbcontext, kernel_dump_buffer); kbase_destroy_context_symbol(temp_kbcontext); pr_debug("gator: Mali-T6xx: hardware counters stopped\n"); clean_symbols(); } } static int read(int **buffer) { int cnt; int len = 0; u32 value = 0; mali_bool success; struct timespec current_time; static u32 prev_time_s = 0; static s32 next_read_time_ns = 0; if (!on_primary_core()) { return 0; } getnstimeofday(¤t_time); /* * Discard reads unless a respectable time has passed. This reduces the load on the GPU without sacrificing * accuracy on the Streamline display. */ if (!is_read_scheduled(¤t_time, &prev_time_s, &next_read_time_ns)) { return 0; } /* * Report the HW counters * Only process hardware counters if at least one of the hardware counters is enabled. */ if (num_hardware_counters_enabled > 0) { const unsigned int vithar_blocks[] = { 0x700, /* VITHAR_JOB_MANAGER, Block 0 */ 0x400, /* VITHAR_TILER, Block 1 */ 0x000, /* VITHAR_SHADER_CORE, Block 2 */ 0x500 /* VITHAR_MEMORY_SYSTEM, Block 3 */ }; if (!kbcontext) { return -1; } /* Mali symbols can be called safely since a kbcontext is valid */ if (kbase_instr_hwcnt_dump_complete_symbol(kbcontext, &success) == MALI_TRUE) { kbase_device_busy = false; if (success == MALI_TRUE) { for (cnt = 0; cnt < NUMBER_OF_HARDWARE_COUNTERS; cnt++) { const mali_counter *counter = &counters[cnt]; if (counter->enabled) { const int block = GET_HW_BLOCK(cnt); const int counter_offset = GET_COUNTER_OFFSET(cnt); const u32 *counter_block = (u32 *) ((uintptr_t)kernel_dump_buffer + vithar_blocks[block]); const u32 *counter_address = counter_block + counter_offset; value = *counter_address; if (block == SHADER_BLOCK) { /* (counter_address + 0x000) has already been accounted-for above. */ value += *(counter_address + 0x100); value += *(counter_address + 0x200); value += *(counter_address + 0x300); } counter_dump[len++] = counter->key; counter_dump[len++] = value; } } } } if (!kbase_device_busy) { kbase_device_busy = true; kbase_instr_hwcnt_dump_irq_symbol(kbcontext); } } /* Update the buffer */ if (buffer) { *buffer = (int *)counter_dump; } return len; } static int create_files(struct super_block *sb, struct dentry *root) { unsigned int event; /* * Create the filesystem for all events */ int counter_index = 0; const char *mali_name = gator_mali_get_mali_name(); for (event = 0; event < NUMBER_OF_HARDWARE_COUNTERS; event++) { if (gator_mali_create_file_system(mali_name, hardware_counter_names[counter_index], sb, root, &counters[event]) != 0) return -1; counter_index++; } return 0; } static struct gator_interface gator_events_mali_t6xx_interface = { .create_files = create_files, .start = start, .stop = stop, .read = read }; int gator_events_mali_t6xx_hw_init(void) { pr_debug("gator: Mali-T6xx: sw_counters init\n"); #if GATOR_TEST test_all_is_read_scheduled(); #endif gator_mali_initialise_counters(counters, NUMBER_OF_HARDWARE_COUNTERS); return gator_events_install(&gator_events_mali_t6xx_interface); } gator_events_init(gator_events_mali_t6xx_hw_init);