1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
|
/**
* Copyright (C) ARM Limited 2010-2014. All rights reserved.
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*/
#include "Child.h"
#include <stdlib.h>
#include <string.h>
#include <signal.h>
#include <unistd.h>
#include <sys/prctl.h>
#include "Logging.h"
#include "CapturedXML.h"
#include "SessionData.h"
#include "LocalCapture.h"
#include "Sender.h"
#include "OlyUtility.h"
#include "OlySocket.h"
#include "StreamlineSetup.h"
#include "ConfigurationXML.h"
#include "Driver.h"
#include "PerfSource.h"
#include "DriverSource.h"
#include "UserSpaceSource.h"
#include "ExternalSource.h"
static sem_t haltPipeline, senderThreadStarted, startProfile, senderSem; // Shared by Child and spawned threads
static Source *primarySource = NULL;
static Source *userSpaceSource = NULL;
static Source *externalSource = NULL;
static Sender* sender = NULL; // Shared by Child.cpp and spawned threads
Child* child = NULL; // shared by Child.cpp and main.cpp
extern void cleanUp();
void handleException() {
if (child && child->numExceptions++ > 0) {
// it is possible one of the below functions itself can cause an exception, thus allow only one exception
logg->logMessage("Received multiple exceptions, terminating the child");
exit(1);
}
fprintf(stderr, "%s", logg->getLastError());
if (child && child->socket) {
if (sender) {
// send the error, regardless of the command sent by Streamline
sender->writeData(logg->getLastError(), strlen(logg->getLastError()), RESPONSE_ERROR);
// cannot close the socket before Streamline issues the command, so wait for the command before exiting
if (gSessionData->mWaitingOnCommand) {
char discard;
child->socket->receiveNBytes(&discard, 1);
}
// Ensure all data is flushed
child->socket->shutdownConnection();
// this indirectly calls close socket which will ensure the data has been sent
delete sender;
}
}
if (gSessionData->mLocalCapture)
cleanUp();
exit(1);
}
// CTRL C Signal Handler for child process
static void child_handler(int signum) {
static bool beenHere = false;
if (beenHere == true) {
logg->logMessage("Gator is being forced to shut down.");
exit(1);
}
beenHere = true;
logg->logMessage("Gator is shutting down.");
if (signum == SIGALRM || !primarySource) {
exit(1);
} else {
child->endSession();
alarm(5); // Safety net in case endSession does not complete within 5 seconds
}
}
static void *durationThread(void *) {
prctl(PR_SET_NAME, (unsigned long)&"gatord-duration", 0, 0, 0);
sem_wait(&startProfile);
if (gSessionData->mSessionIsActive) {
// Time out after duration seconds
// Add a second for host-side filtering
sleep(gSessionData->mDuration + 1);
if (gSessionData->mSessionIsActive) {
logg->logMessage("Duration expired.");
child->endSession();
}
}
logg->logMessage("Exit duration thread");
return 0;
}
static void *stopThread(void *) {
OlySocket* socket = child->socket;
prctl(PR_SET_NAME, (unsigned long)&"gatord-stopper", 0, 0, 0);
while (gSessionData->mSessionIsActive) {
// This thread will stall until the APC_STOP or PING command is received over the socket or the socket is disconnected
unsigned char header[5];
const int result = socket->receiveNBytes((char*)&header, sizeof(header));
const char type = header[0];
const int length = (header[1] << 0) | (header[2] << 8) | (header[3] << 16) | (header[4] << 24);
if (result == -1) {
child->endSession();
} else if (result > 0) {
if ((type != COMMAND_APC_STOP) && (type != COMMAND_PING)) {
logg->logMessage("INVESTIGATE: Received unknown command type %d", type);
} else {
// verify a length of zero
if (length == 0) {
if (type == COMMAND_APC_STOP) {
logg->logMessage("Stop command received.");
child->endSession();
} else {
// Ping is used to make sure gator is alive and requires an ACK as the response
logg->logMessage("Ping command received.");
sender->writeData(NULL, 0, RESPONSE_ACK);
}
} else {
logg->logMessage("INVESTIGATE: Received stop command but with length = %d", length);
}
}
}
}
logg->logMessage("Exit stop thread");
return 0;
}
static void *senderThread(void *) {
char end_sequence[] = {RESPONSE_APC_DATA, 0, 0, 0, 0};
sem_post(&senderThreadStarted);
prctl(PR_SET_NAME, (unsigned long)&"gatord-sender", 0, 0, 0);
sem_wait(&haltPipeline);
while (!primarySource->isDone() || (userSpaceSource != NULL && !userSpaceSource->isDone()) || (externalSource != NULL && !externalSource->isDone())) {
sem_wait(&senderSem);
primarySource->write(sender);
if (userSpaceSource != NULL) {
userSpaceSource->write(sender);
}
if (externalSource != NULL) {
externalSource->write(sender);
}
}
// write end-of-capture sequence
if (!gSessionData->mLocalCapture) {
sender->writeData(end_sequence, sizeof(end_sequence), RESPONSE_APC_DATA);
}
logg->logMessage("Exit sender thread");
return 0;
}
Child::Child() {
initialization();
gSessionData->mLocalCapture = true;
}
Child::Child(OlySocket* sock, int conn) {
initialization();
socket = sock;
mNumConnections = conn;
}
Child::~Child() {
}
void Child::initialization() {
// Set up different handlers for signals
gSessionData->mSessionIsActive = true;
signal(SIGINT, child_handler);
signal(SIGTERM, child_handler);
signal(SIGABRT, child_handler);
signal(SIGALRM, child_handler);
socket = NULL;
numExceptions = 0;
mNumConnections = 0;
// Initialize semaphores
sem_init(&senderThreadStarted, 0, 0);
sem_init(&startProfile, 0, 0);
sem_init(&senderSem, 0, 0);
}
void Child::endSession() {
gSessionData->mSessionIsActive = false;
primarySource->interrupt();
sem_post(&haltPipeline);
}
void Child::run() {
LocalCapture* localCapture = NULL;
pthread_t durationThreadID, stopThreadID, senderThreadID;
prctl(PR_SET_NAME, (unsigned long)&"gatord-child", 0, 0, 0);
// Disable line wrapping when generating xml files; carriage returns and indentation to be added manually
mxmlSetWrapMargin(0);
// Instantiate the Sender - must be done first, after which error messages can be sent
sender = new Sender(socket);
if (mNumConnections > 1) {
logg->logError(__FILE__, __LINE__, "Session already in progress");
handleException();
}
// Populate gSessionData with the configuration
{ ConfigurationXML configuration; }
// Set up the driver; must be done after gSessionData->mPerfCounterType[] is populated
if (!gSessionData->perf.isSetup()) {
primarySource = new DriverSource(&senderSem, &startProfile);
} else {
primarySource = new PerfSource(&senderSem, &startProfile);
}
// Initialize all drivers
for (Driver *driver = Driver::getHead(); driver != NULL; driver = driver->getNext()) {
driver->resetCounters();
}
// Set up counters using the associated driver's setup function
for (int i = 0; i < MAX_PERFORMANCE_COUNTERS; i++) {
Counter & counter = gSessionData->mCounters[i];
if (counter.isEnabled()) {
counter.getDriver()->setupCounter(counter);
}
}
// Start up and parse session xml
if (socket) {
// Respond to Streamline requests
StreamlineSetup ss(socket);
} else {
char* xmlString;
xmlString = util->readFromDisk(gSessionData->mSessionXMLPath);
if (xmlString == 0) {
logg->logError(__FILE__, __LINE__, "Unable to read session xml file: %s", gSessionData->mSessionXMLPath);
handleException();
}
gSessionData->parseSessionXML(xmlString);
localCapture = new LocalCapture();
localCapture->createAPCDirectory(gSessionData->mTargetPath);
localCapture->copyImages(gSessionData->mImages);
localCapture->write(xmlString);
sender->createDataFile(gSessionData->mAPCDir);
free(xmlString);
}
// Must be after session XML is parsed
if (!primarySource->prepare()) {
logg->logError(__FILE__, __LINE__, "Unable to prepare for capture");
handleException();
}
// Sender thread shall be halted until it is signaled for one shot mode
sem_init(&haltPipeline, 0, gSessionData->mOneShot ? 0 : 2);
// Create the duration, stop, and sender threads
bool thread_creation_success = true;
if (gSessionData->mDuration > 0 && pthread_create(&durationThreadID, NULL, durationThread, NULL)) {
thread_creation_success = false;
} else if (socket && pthread_create(&stopThreadID, NULL, stopThread, NULL)) {
thread_creation_success = false;
} else if (pthread_create(&senderThreadID, NULL, senderThread, NULL)){
thread_creation_success = false;
}
if (gSessionData->hwmon.countersEnabled()) {
userSpaceSource = new UserSpaceSource(&senderSem);
if (!userSpaceSource->prepare()) {
logg->logError(__FILE__, __LINE__, "Unable to prepare for capture");
handleException();
}
userSpaceSource->start();
}
if (access("/tmp/gator", F_OK) == 0) {
externalSource = new ExternalSource(&senderSem);
if (!externalSource->prepare()) {
logg->logError(__FILE__, __LINE__, "Unable to prepare for capture");
handleException();
}
externalSource->start();
}
if (!thread_creation_success) {
logg->logError(__FILE__, __LINE__, "Failed to create gator threads");
handleException();
}
// Wait until thread has started
sem_wait(&senderThreadStarted);
// Start profiling
primarySource->run();
if (externalSource != NULL) {
externalSource->join();
}
if (userSpaceSource != NULL) {
userSpaceSource->join();
}
// Wait for the other threads to exit
pthread_join(senderThreadID, NULL);
// Shutting down the connection should break the stop thread which is stalling on the socket recv() function
if (socket) {
logg->logMessage("Waiting on stop thread");
socket->shutdownConnection();
pthread_join(stopThreadID, NULL);
}
// Write the captured xml file
if (gSessionData->mLocalCapture) {
CapturedXML capturedXML;
capturedXML.write(gSessionData->mAPCDir);
}
logg->logMessage("Profiling ended.");
delete externalSource;
delete userSpaceSource;
delete primarySource;
delete sender;
delete localCapture;
}
|