1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
|
/**
* Copyright (C) ARM Limited 2010-2012. All rights reserved.
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*/
#include <stdint.h>
#include <stdlib.h>
#include <signal.h>
#include <ctype.h>
#include <sys/wait.h>
#include <unistd.h>
#include <sys/syscall.h>
#include <sys/prctl.h>
#include <sys/types.h>
#include <sys/stat.h>
#include <sys/mount.h>
#include <fcntl.h>
#include <sys/mman.h>
#include "Child.h"
#include "SessionData.h"
#include "OlySocket.h"
#include "Logging.h"
#include "OlyUtility.h"
#define DEBUG false
extern Child* child;
extern void handleException();
int shutdownFilesystem();
static pthread_mutex_t numSessions_mutex;
static int numSessions = 0;
static OlySocket* socket = NULL;
static bool driverRunningAtStart = false;
static bool driverMountedAtStart = false;
struct cmdline_t {
int port;
char* module;
};
void cleanUp() {
if (shutdownFilesystem() == -1) {
logg->logMessage("Error shutting down gator filesystem");
}
delete socket;
delete util;
delete logg;
}
// CTRL C Signal Handler
void handler(int signum) {
logg->logMessage("Received signal %d, gator daemon exiting", signum);
// Case 1: both child and parent receive the signal
if (numSessions > 0) {
// Arbitrary sleep of 1 second to give time for the child to exit;
// if something bad happens, continue the shutdown process regardless
sleep(1);
}
// Case 2: only the parent received the signal
if (numSessions > 0) {
// Kill child threads - the first signal exits gracefully
logg->logMessage("Killing process group as %d child was running when signal was received", numSessions);
kill(0, SIGINT);
// Give time for the child to exit
sleep(1);
if (numSessions > 0) {
// The second signal force kills the child
logg->logMessage("Force kill the child");
kill(0, SIGINT);
// Again, sleep for 1 second
sleep(1);
if (numSessions > 0) {
// Something bad has really happened; the child is not exiting and therefore may hold the /dev/gator resource open
printf("Unable to kill the gatord child process, thus gator.ko may still be loaded.\n");
}
}
}
cleanUp();
exit(0);
}
// Child exit Signal Handler
void child_exit(int signum) {
int status;
int pid = wait(&status);
if (pid != -1) {
pthread_mutex_lock(&numSessions_mutex);
numSessions--;
pthread_mutex_unlock(&numSessions_mutex);
logg->logMessage("Child process %d exited with status %d", pid, status);
}
}
// retval: -1 = failure; 0 = was already mounted; 1 = successfully mounted
int mountGatorFS() {
// If already mounted,
if (access("/dev/gator/buffer", F_OK) == 0) {
return 0;
}
// else, mount the filesystem
mkdir("/dev/gator", S_IRWXU | S_IRWXG | S_IROTH | S_IXOTH);
if (mount("nodev", "/dev/gator", "gatorfs", 0, NULL) != 0) {
return -1;
} else {
return 1;
}
}
bool init_module (const char * const location) {
bool ret(false);
const int fd = open(location, O_RDONLY);
if (fd >= 0) {
struct stat st;
if (fstat(fd, &st) == 0) {
void * const p = mmap(NULL, st.st_size, PROT_READ, MAP_PRIVATE, fd, 0);
if (p != MAP_FAILED) {
if (syscall(__NR_init_module, p, st.st_size, "") == 0) {
ret = true;
}
munmap(p, st.st_size);
}
}
close(fd);
}
return ret;
}
int setupFilesystem(char* module) {
int retval;
// Verify root permissions
uid_t euid = geteuid();
if (euid) {
logg->logError(__FILE__, __LINE__, "gatord must be launched with root privileges");
handleException();
}
if (module) {
// unmount and rmmod if the module was specified on the commandline, i.e. ensure that the specified module is indeed running
shutdownFilesystem();
// if still mounted
if (access("/dev/gator/buffer", F_OK) == 0) {
logg->logError(__FILE__, __LINE__, "Unable to remove the running gator.ko. Manually remove the module or use the running module by not specifying one on the commandline");
handleException();
}
}
retval = mountGatorFS();
if (retval == 1) {
logg->logMessage("Driver already running at startup");
driverRunningAtStart = true;
} else if (retval == 0) {
logg->logMessage("Driver already mounted at startup");
driverRunningAtStart = driverMountedAtStart = true;
} else {
char command[256]; // arbitrarily large amount
char location[256]; // arbitrarily large amount
if (module) {
strncpy(location, module, sizeof(location));
} else {
// Is the driver co-located in the same directory?
if (util->getApplicationFullPath(location, sizeof(location)) != 0) { // allow some buffer space
logg->logMessage("Unable to determine the full path of gatord, the cwd will be used");
}
strncat(location, "gator.ko", sizeof(location) - strlen(location) - 1);
}
if (access(location, F_OK) == -1) {
logg->logError(__FILE__, __LINE__, "Unable to locate gator.ko driver:\n >>> gator.ko should be co-located with gatord in the same directory\n >>> OR insmod gator.ko prior to launching gatord\n >>> OR specify the location of gator.ko on the command line");
handleException();
}
// Load driver
bool success = init_module(location);
if (!success) {
logg->logMessage("init_module failed, trying insmod");
snprintf(command, sizeof(command), "insmod %s >/dev/null 2>&1", location);
if (system(command) != 0) {
logg->logMessage("Unable to load gator.ko driver with command: %s", command);
logg->logError(__FILE__, __LINE__, "Unable to load (insmod) gator.ko driver:\n >>> gator.ko must be built against the current kernel version & configuration\n >>> See dmesg for more details");
handleException();
}
}
if (mountGatorFS() == -1) {
logg->logError(__FILE__, __LINE__, "Unable to mount the gator filesystem needed for profiling.");
handleException();
}
}
return 0;
}
int shutdownFilesystem() {
if (driverMountedAtStart == false) {
umount("/dev/gator");
}
if (driverRunningAtStart == false) {
if (syscall(__NR_delete_module, "gator", O_NONBLOCK) != 0) {
logg->logMessage("delete_module failed, trying rmmod");
if (system("rmmod gator >/dev/null 2>&1") != 0) {
return -1;
}
}
}
return 0; // success
}
struct cmdline_t parseCommandLine(int argc, char** argv) {
struct cmdline_t cmdline;
cmdline.port = 8080;
cmdline.module = NULL;
char version_string[256]; // arbitrary length to hold the version information
int c;
// build the version string
if (PROTOCOL_VERSION < PROTOCOL_DEV) {
snprintf(version_string, sizeof(version_string), "Streamline gatord version %d (DS-5 v5.%d)", PROTOCOL_VERSION, PROTOCOL_VERSION + 1);
} else {
snprintf(version_string, sizeof(version_string), "Streamline gatord development version %d", PROTOCOL_VERSION);
}
while ((c = getopt(argc, argv, "hvp:s:c:e:m:o:")) != -1) {
switch(c) {
case 'c':
gSessionData->mConfigurationXMLPath = optarg;
break;
case 'e':
gSessionData->mEventsXMLPath = optarg;
break;
case 'm':
cmdline.module = optarg;
break;
case 'p':
cmdline.port = strtol(optarg, NULL, 10);
break;
case 's':
gSessionData->mSessionXMLPath = optarg;
break;
case 'o':
gSessionData->mTargetPath = optarg;
break;
case 'h':
case '?':
logg->logError(__FILE__, __LINE__,
"%s. All parameters are optional:\n"
"-c config_xml path and filename of the configuration.xml to use\n"
"-e events_xml path and filename of the events.xml to use\n"
"-h this help page\n"
"-m module path and filename of gator.ko\n"
"-p port_number port upon which the server listens; default is 8080\n"
"-s session_xml path and filename of a session xml used for local capture\n"
"-o apc_dir path and name of the output for a local capture\n"
"-v version information\n"
, version_string);
handleException();
break;
case 'v':
logg->logError(__FILE__, __LINE__, version_string);
handleException();
break;
}
}
// Error checking
if (cmdline.port != 8080 && gSessionData->mSessionXMLPath != NULL) {
logg->logError(__FILE__, __LINE__, "Only a port or a session xml can be specified, not both");
handleException();
}
if (gSessionData->mTargetPath != NULL && gSessionData->mSessionXMLPath == NULL) {
logg->logError(__FILE__, __LINE__, "Missing -s command line option required for a local capture.");
handleException();
}
if (optind < argc) {
logg->logError(__FILE__, __LINE__, "Unknown argument: %s. Use '-h' for help.", argv[optind]);
handleException();
}
return cmdline;
}
// Gator data flow: collector -> collector fifo -> sender
int main(int argc, char** argv, char* envp[]) {
setsid();
gSessionData = new SessionData(); // Global data class
logg = new Logging(DEBUG); // Set up global thread-safe logging
util = new OlyUtility(); // Set up global utility class
prctl(PR_SET_NAME, (unsigned long)&"gatord-main", 0, 0, 0);
pthread_mutex_init(&numSessions_mutex, NULL);
signal(SIGINT, handler);
signal(SIGTERM, handler);
signal(SIGABRT, handler);
// Set to high priority
if (setpriority(PRIO_PROCESS, syscall(__NR_gettid), -19) == -1) {
logg->logMessage("setpriority() failed");
}
// Initialize session data
gSessionData->initialize();
// Parse the command line parameters
struct cmdline_t cmdline = parseCommandLine(argc, argv);
// Call before setting up the SIGCHLD handler, as system() spawns child processes
setupFilesystem(cmdline.module);
// Handle child exit codes
signal(SIGCHLD, child_exit);
// Ignore the SIGPIPE signal so that any send to a broken socket will return an error code instead of asserting a signal
// Handling the error at the send function call is much easier than trying to do anything intelligent in the sig handler
signal(SIGPIPE, SIG_IGN);
// If the command line argument is a session xml file, no need to open a socket
if (gSessionData->mSessionXMLPath) {
child = new Child();
child->run();
delete child;
} else {
socket = new OlySocket(cmdline.port, true);
// Forever loop, can be exited via a signal or exception
while (1) {
logg->logMessage("Waiting on connection...");
socket->acceptConnection();
int pid = fork();
if (pid < 0) {
// Error
logg->logError(__FILE__, __LINE__, "Fork process failed. Please power cycle the target device if this error persists.");
} else if (pid == 0) {
// Child
socket->closeServerSocket();
child = new Child(socket, numSessions + 1);
child->run();
delete child;
exit(0);
} else {
// Parent
socket->closeSocket();
pthread_mutex_lock(&numSessions_mutex);
numSessions++;
pthread_mutex_unlock(&numSessions_mutex);
// Maximum number of connections is 2
int wait = 0;
while (numSessions > 1) {
// Throttle until one of the children exits before continuing to accept another socket connection
logg->logMessage("%d sessions active!", numSessions);
if (wait++ >= 10) { // Wait no more than 10 seconds
// Kill last created child
kill(pid, SIGALRM);
break;
}
sleep(1);
}
}
}
}
cleanUp();
return 0;
}
|