summaryrefslogtreecommitdiffstats
blob: 1275aef1cb7938ffe804f7168095c7cd47b6e187 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
/**
 * Copyright (C) ARM Limited 2010-2014. All rights reserved.
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License version 2 as
 * published by the Free Software Foundation.
 */

#include <arpa/inet.h>
#include <fcntl.h>
#include <pthread.h>
#include <sys/mman.h>
#include <sys/mount.h>
#include <sys/prctl.h>
#include <sys/resource.h>
#include <sys/socket.h>
#include <sys/stat.h>
#include <sys/syscall.h>
#include <sys/wait.h>
#include <unistd.h>

#include "Child.h"
#include "KMod.h"
#include "Logging.h"
#include "OlySocket.h"
#include "OlyUtility.h"
#include "SessionData.h"

#define DEBUG false

extern Child* child;
static int shutdownFilesystem();
static pthread_mutex_t numSessions_mutex;
static int numSessions = 0;
static OlyServerSocket* sock = NULL;
static bool driverRunningAtStart = false;
static bool driverMountedAtStart = false;

struct cmdline_t {
	int port;
	char* module;
};

#define DEFAULT_PORT 8080

void cleanUp() {
	if (shutdownFilesystem() == -1) {
		logg->logMessage("Error shutting down gator filesystem");
	}
	delete sock;
	delete util;
	delete logg;
}

// CTRL C Signal Handler
static void handler(int signum) {
	logg->logMessage("Received signal %d, gator daemon exiting", signum);

	// Case 1: both child and parent receive the signal
	if (numSessions > 0) {
		// Arbitrary sleep of 1 second to give time for the child to exit;
		// if something bad happens, continue the shutdown process regardless
		sleep(1);
	}

	// Case 2: only the parent received the signal
	if (numSessions > 0) {
		// Kill child threads - the first signal exits gracefully
		logg->logMessage("Killing process group as %d child was running when signal was received", numSessions);
		kill(0, SIGINT);

		// Give time for the child to exit
		sleep(1);

		if (numSessions > 0) {
			// The second signal force kills the child
			logg->logMessage("Force kill the child");
			kill(0, SIGINT);
			// Again, sleep for 1 second
			sleep(1);

			if (numSessions > 0) {
				// Something bad has really happened; the child is not exiting and therefore may hold the /dev/gator resource open
				printf("Unable to kill the gatord child process, thus gator.ko may still be loaded.\n");
			}
		}
	}

	cleanUp();
	exit(0);
}

// Child exit Signal Handler
static void child_exit(int) {
	int status;
	int pid = wait(&status);
	if (pid != -1) {
		pthread_mutex_lock(&numSessions_mutex);
		numSessions--;
		pthread_mutex_unlock(&numSessions_mutex);
		logg->logMessage("Child process %d exited with status %d", pid, status);
	}
}

static int udpPort(int port) {
	int s;
	struct sockaddr_in6 sockaddr;
	int on;
	int family = AF_INET6;

	s = socket(AF_INET6, SOCK_DGRAM, IPPROTO_UDP);
	if (s == -1) {
		family = AF_INET;
		s = socket(AF_INET, SOCK_DGRAM, IPPROTO_UDP);
		if (s == -1) {
			logg->logError(__FILE__, __LINE__, "socket failed");
			handleException();
		}
	}

	on = 1;
	if (setsockopt(s, SOL_SOCKET, SO_REUSEADDR, (const char*)&on, sizeof(on)) != 0) {
		logg->logError(__FILE__, __LINE__, "setsockopt failed");
		handleException();
	}

	memset((void*)&sockaddr, 0, sizeof(sockaddr));
	sockaddr.sin6_family = family;
	sockaddr.sin6_port = htons(port);
	sockaddr.sin6_addr = in6addr_any;
	if (bind(s, (struct sockaddr *)&sockaddr, sizeof(sockaddr)) < 0) {
		logg->logError(__FILE__, __LINE__, "socket failed");
		handleException();
	}

	return s;
}

#define UDP_ANS_PORT 30000
#define UDP_REQ_PORT 30001

typedef struct {
	char rviHeader[8];
	uint32_t messageID;
	uint8_t ethernetAddress[8];
	uint32_t ethernetType;
	uint32_t dhcp;
	char dhcpName[40];
	uint32_t ipAddress;
	uint32_t defaultGateway;
	uint32_t subnetMask;
	uint32_t activeConnections; 
} RVIConfigureInfo;

static const char DST_REQ[] = { 'D', 'S', 'T', '_', 'R', 'E', 'Q', ' ', 0, 0, 0, 0x64 };

static void* answerThread(void* pVoid) {
	prctl(PR_SET_NAME, (unsigned long)&"gatord-discover", 0, 0, 0);
	const struct cmdline_t * const cmdline = (struct cmdline_t *)pVoid;
	RVIConfigureInfo dstAns;
	int req = udpPort(UDP_REQ_PORT);
	int ans = udpPort(UDP_ANS_PORT);

	// Format the answer buffer
	memset(&dstAns, 0, sizeof(dstAns));
	memcpy(dstAns.rviHeader, "STR_ANS ", sizeof(dstAns.rviHeader));
	if (gethostname(dstAns.dhcpName, sizeof(dstAns.dhcpName) - 1) != 0) {
		logg->logError(__FILE__, __LINE__, "gethostname failed");
		handleException();
	}
	// Subvert the defaultGateway field for the port number
	if (cmdline->port != DEFAULT_PORT) {
		dstAns.defaultGateway = cmdline->port;
	}
	// Subvert the subnetMask field for the protocol version
	dstAns.subnetMask = PROTOCOL_VERSION;

	for (;;) {
		char buf[128];
		struct sockaddr_in6 sockaddr;
		socklen_t addrlen;
		int read;
		addrlen = sizeof(sockaddr);
		read = recvfrom(req, &buf, sizeof(buf), 0, (struct sockaddr *)&sockaddr, &addrlen);
		if (read < 0) {
			logg->logError(__FILE__, __LINE__, "recvfrom failed");
			handleException();
		} else if ((read == 12) && (memcmp(buf, DST_REQ, sizeof(DST_REQ)) == 0)) {
			if (sendto(ans, &dstAns, sizeof(dstAns), 0, (struct sockaddr *)&sockaddr, addrlen) != sizeof(dstAns)) {
				logg->logError(__FILE__, __LINE__, "sendto failed");
				handleException();
			}
		}
	}
}

// retval: -1 = failure; 0 = was already mounted; 1 = successfully mounted
static int mountGatorFS() {
	// If already mounted,
	if (access("/dev/gator/buffer", F_OK) == 0) {
		return 0;
	}

	// else, mount the filesystem
	mkdir("/dev/gator", S_IRWXU | S_IRWXG | S_IROTH | S_IXOTH);
	if (mount("nodev", "/dev/gator", "gatorfs", 0, NULL) != 0) {
		return -1;
	} else {
		return 1;
	}
}

static bool init_module (const char * const location) {
	bool ret(false);
	const int fd = open(location, O_RDONLY);
	if (fd >= 0) {
		struct stat st;
		if (fstat(fd, &st) == 0) {
			void * const p = mmap(NULL, st.st_size, PROT_READ, MAP_PRIVATE, fd, 0);
			if (p != MAP_FAILED) {
				if (syscall(__NR_init_module, p, st.st_size, "") == 0) {
					ret = true;
				}
				munmap(p, st.st_size);
			}
		}
		close(fd);
	}

	return ret;
}

static bool setupFilesystem(char* module) {
	if (module) {
		// unmount and rmmod if the module was specified on the commandline, i.e. ensure that the specified module is indeed running
		shutdownFilesystem();

		// if still mounted
		if (access("/dev/gator/buffer", F_OK) == 0) {
			logg->logError(__FILE__, __LINE__, "Unable to remove the running gator.ko. Manually remove the module or use the running module by not specifying one on the commandline");
			handleException();
		}
	}

	const int retval = mountGatorFS();
	if (retval == 1) {
		logg->logMessage("Driver already running at startup");
		driverRunningAtStart = true;
	} else if (retval == 0) {
		logg->logMessage("Driver already mounted at startup");
		driverRunningAtStart = driverMountedAtStart = true;
	} else {
		char command[256]; // arbitrarily large amount
		char location[256]; // arbitrarily large amount

		if (module) {
			strncpy(location, module, sizeof(location));
		} else {
			// Is the driver co-located in the same directory?
			if (util->getApplicationFullPath(location, sizeof(location)) != 0) { // allow some buffer space
				logg->logMessage("Unable to determine the full path of gatord, the cwd will be used");
			}
			strncat(location, "gator.ko", sizeof(location) - strlen(location) - 1);
		}

		if (access(location, F_OK) == -1) {
			// The gator kernel is not already loaded and unable to locate gator.ko
			return false;
		}

		// Load driver
		bool success = init_module(location);
		if (!success) {
			logg->logMessage("init_module failed, trying insmod");
			snprintf(command, sizeof(command), "insmod %s >/dev/null 2>&1", location);
			if (system(command) != 0) {
				logg->logMessage("Unable to load gator.ko driver with command: %s", command);
				logg->logError(__FILE__, __LINE__, "Unable to load (insmod) gator.ko driver:\n  >>> gator.ko must be built against the current kernel version & configuration\n  >>> See dmesg for more details");
				handleException();
			}
		}

		if (mountGatorFS() == -1) {
			logg->logError(__FILE__, __LINE__, "Unable to mount the gator filesystem needed for profiling.");
			handleException();
		}
	}

	return true;
}

static int shutdownFilesystem() {
	if (driverMountedAtStart == false) {
		umount("/dev/gator");
	}
	if (driverRunningAtStart == false) {
		if (syscall(__NR_delete_module, "gator", O_NONBLOCK) != 0) {
			logg->logMessage("delete_module failed, trying rmmod");
			if (system("rmmod gator >/dev/null 2>&1") != 0) {
				return -1;
			}
		}
	}

	return 0; // success
}

static struct cmdline_t parseCommandLine(int argc, char** argv) {
	struct cmdline_t cmdline;
	cmdline.port = DEFAULT_PORT;
	cmdline.module = NULL;
	char version_string[256]; // arbitrary length to hold the version information
	int c;

	// build the version string
	if (PROTOCOL_VERSION < PROTOCOL_DEV) {
		snprintf(version_string, sizeof(version_string), "Streamline gatord version %d (DS-5 v5.%d)", PROTOCOL_VERSION, PROTOCOL_VERSION);
	} else {
		snprintf(version_string, sizeof(version_string), "Streamline gatord development version %d", PROTOCOL_VERSION);
	}

	while ((c = getopt(argc, argv, "hvp:s:c:e:m:o:")) != -1) {
		switch(c) {
			case 'c':
				gSessionData->mConfigurationXMLPath = optarg;
				break;
			case 'e':
				gSessionData->mEventsXMLPath = optarg;
				break;
			case 'm':
				cmdline.module = optarg;
				break;
			case 'p':
				cmdline.port = strtol(optarg, NULL, 10);
				break;
			case 's':
				gSessionData->mSessionXMLPath = optarg;
				break;
			case 'o':
				gSessionData->mTargetPath = optarg;
				break;
			case 'h':
			case '?':
				logg->logError(__FILE__, __LINE__,
					"%s. All parameters are optional:\n"
					"-c config_xml   path and filename of the configuration.xml to use\n"
					"-e events_xml   path and filename of the events.xml to use\n"
					"-h              this help page\n"
					"-m module       path and filename of gator.ko\n"
					"-p port_number  port upon which the server listens; default is 8080\n"
					"-s session_xml  path and filename of a session xml used for local capture\n"
					"-o apc_dir      path and name of the output for a local capture\n"
					"-v              version information\n"
					, version_string);
				handleException();
				break;
			case 'v':
				logg->logError(__FILE__, __LINE__, version_string);
				handleException();
				break;
		}
	}

	// Error checking
	if (cmdline.port != DEFAULT_PORT && gSessionData->mSessionXMLPath != NULL) {
		logg->logError(__FILE__, __LINE__, "Only a port or a session xml can be specified, not both");
		handleException();
	}

	if (gSessionData->mTargetPath != NULL && gSessionData->mSessionXMLPath == NULL) {
		logg->logError(__FILE__, __LINE__, "Missing -s command line option required for a local capture.");
		handleException();
	}

	if (optind < argc) {
		logg->logError(__FILE__, __LINE__, "Unknown argument: %s. Use '-h' for help.", argv[optind]);
		handleException();
	}

	return cmdline;
}

// Gator data flow: collector -> collector fifo -> sender
int main(int argc, char** argv) {
	// Ensure proper signal handling by making gatord the process group leader
	//   e.g. it may not be the group leader when launched as 'sudo gatord'
	setsid();

	logg = new Logging(DEBUG);  // Set up global thread-safe logging
	gSessionData = new SessionData(); // Global data class
	util = new OlyUtility();	// Set up global utility class

	// Initialize drivers
	new KMod();

	prctl(PR_SET_NAME, (unsigned long)&"gatord-main", 0, 0, 0);
	pthread_mutex_init(&numSessions_mutex, NULL);

	signal(SIGINT, handler);
	signal(SIGTERM, handler);
	signal(SIGABRT, handler);

	// Set to high priority
	if (setpriority(PRIO_PROCESS, syscall(__NR_gettid), -19) == -1) {
		logg->logMessage("setpriority() failed");
	}

	// Parse the command line parameters
	struct cmdline_t cmdline = parseCommandLine(argc, argv);

	// Verify root permissions
	uid_t euid = geteuid();
	if (euid) {
		logg->logError(__FILE__, __LINE__, "gatord must be launched with root privileges");
		handleException();
	}

	// Call before setting up the SIGCHLD handler, as system() spawns child processes
	if (!setupFilesystem(cmdline.module)) {
		logg->logMessage("Unable to setup gatorfs, trying perf");
		if (!gSessionData->perf.setup()) {
			logg->logError(__FILE__, __LINE__,
										 "Unable to locate gator.ko driver:\n"
										 "  >>> gator.ko should be co-located with gatord in the same directory\n"
										 "  >>> OR insmod gator.ko prior to launching gatord\n"
										 "  >>> OR specify the location of gator.ko on the command line\n"
										 "  >>> OR run Linux 3.12 or later with perf support to collect data via userspace only");
			handleException();
		}
	}

	gSessionData->hwmon.setup();

	// Handle child exit codes
	signal(SIGCHLD, child_exit);

	// Ignore the SIGPIPE signal so that any send to a broken socket will return an error code instead of asserting a signal
	// Handling the error at the send function call is much easier than trying to do anything intelligent in the sig handler
	signal(SIGPIPE, SIG_IGN);

	// If the command line argument is a session xml file, no need to open a socket
	if (gSessionData->mSessionXMLPath) {
		child = new Child();
		child->run();
		delete child;
	} else {
		pthread_t answerThreadID;
		if (pthread_create(&answerThreadID, NULL, answerThread, &cmdline)) {
			logg->logError(__FILE__, __LINE__, "Failed to create answer thread");
			handleException();
		}
		sock = new OlyServerSocket(cmdline.port);
		// Forever loop, can be exited via a signal or exception
		while (1) {
			logg->logMessage("Waiting on connection...");
			OlySocket client(sock->acceptConnection());

			int pid = fork();
			if (pid < 0) {
				// Error
				logg->logError(__FILE__, __LINE__, "Fork process failed. Please power cycle the target device if this error persists.");
			} else if (pid == 0) {
				// Child
				sock->closeServerSocket();
				child = new Child(&client, numSessions + 1);
				child->run();
				delete child;
				exit(0);
			} else {
				// Parent
				client.closeSocket();

				pthread_mutex_lock(&numSessions_mutex);
				numSessions++;
				pthread_mutex_unlock(&numSessions_mutex);

				// Maximum number of connections is 2
				int wait = 0;
				while (numSessions > 1) {
					// Throttle until one of the children exits before continuing to accept another socket connection
					logg->logMessage("%d sessions active!", numSessions);
					if (wait++ >= 10) { // Wait no more than 10 seconds
						// Kill last created child
						kill(pid, SIGALRM);
						break;
					}
					sleep(1);
				}
			}
		}
	}

	cleanUp();
	return 0;
}