summaryrefslogtreecommitdiffstats
blob: ffacb490194cb60a7161bea3b2f7886f1b732891 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
/**
 * Copyright (C) ARM Limited 2010-2013. All rights reserved.
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License version 2 as
 * published by the Free Software Foundation.
 *
 */

/*
 * EABI backtrace stores {fp,lr} on the stack.
 */
struct stack_frame_eabi {
	union {
		struct {
			unsigned long fp;
			// May be the fp in the case of a leaf function or clang
			unsigned long lr;
			// If lr is really the fp, lr2 is the corresponding lr
			unsigned long lr2;
		};
		// Used to read 32 bit fp/lr from a 64 bit kernel
		struct {
			u32 fp_32;
			// same as lr above
			u32 lr_32;
			// same as lr2 above
			u32 lr2_32;
		};
	};
};

static void arm_backtrace_eabi(int cpu, struct pt_regs *const regs, unsigned int depth)
{
#if defined(__arm__) || defined(__aarch64__)
	struct stack_frame_eabi *curr;
	struct stack_frame_eabi bufcurr;
#if defined(__arm__)
	const bool is_compat = false;
	unsigned long fp = regs->ARM_fp;
	unsigned long sp = regs->ARM_sp;
	unsigned long lr = regs->ARM_lr;
	const int gcc_frame_offset = sizeof(unsigned long);
#else
	// Is userspace aarch32 (32 bit)
	const bool is_compat = compat_user_mode(regs);
	unsigned long fp = (is_compat ? regs->regs[11] : regs->regs[29]);
	unsigned long sp = (is_compat ? regs->compat_sp : regs->sp);
	unsigned long lr = (is_compat ? regs->compat_lr : regs->regs[30]);
	const int gcc_frame_offset = (is_compat ? sizeof(u32) : 0);
#endif
	// clang frame offset is always zero
	int is_user_mode = user_mode(regs);

	// pc (current function) has already been added

	if (!is_user_mode) {
		return;
	}

	// Add the lr (parent function)
	// entry preamble may not have executed
	gator_add_trace(cpu, lr);

	// check fp is valid
	if (fp == 0 || fp < sp) {
		return;
	}

	// Get the current stack frame
	curr = (struct stack_frame_eabi *)(fp - gcc_frame_offset);
	if ((unsigned long)curr & 3) {
		return;
	}

	while (depth-- && curr) {
		if (!access_ok(VERIFY_READ, curr, sizeof(struct stack_frame_eabi)) ||
				__copy_from_user_inatomic(&bufcurr, curr, sizeof(struct stack_frame_eabi))) {
			return;
		}

		fp = (is_compat ? bufcurr.fp_32 : bufcurr.fp);
		lr = (is_compat ? bufcurr.lr_32 : bufcurr.lr);

#define calc_next(reg) ((reg) - gcc_frame_offset)
		// Returns true if reg is a valid fp
#define validate_next(reg, curr) \
		((reg) != 0 && (calc_next(reg) & 3) == 0 && (unsigned long)(curr) < calc_next(reg))

		// Try lr from the stack as the fp because gcc leaf functions do not push lr
		// If gcc_frame_offset is non-zero, the lr will also be the clang fp
		// This assumes code is at a lower address than the stack
		if (validate_next(lr, curr)) {
			fp = lr;
			lr = (is_compat ? bufcurr.lr2_32 : bufcurr.lr2);
		}

		gator_add_trace(cpu, lr);

		if (!validate_next(fp, curr)) {
			return;
		}

		// Move to the next stack frame
		curr = (struct stack_frame_eabi *)calc_next(fp);
	}
#endif
}

#if defined(__arm__) || defined(__aarch64__)
static int report_trace(struct stackframe *frame, void *d)
{
	unsigned int *depth = d, cookie = NO_COOKIE;
	unsigned long addr = frame->pc;

	if (*depth) {
#if defined(MODULE)
		unsigned int cpu = get_physical_cpu();
		struct module *mod = __module_address(addr);
		if (mod) {
			cookie = get_cookie(cpu, current, mod->name, false);
			addr = addr - (unsigned long)mod->module_core;
		}
#endif
		marshal_backtrace(addr & ~1, cookie);
		(*depth)--;
	}

	return *depth == 0;
}
#endif

// Uncomment the following line to enable kernel stack unwinding within gator, note it can also be defined from the Makefile
// #define GATOR_KERNEL_STACK_UNWINDING

#if (defined(__arm__) || defined(__aarch64__)) && !defined(GATOR_KERNEL_STACK_UNWINDING)
// Disabled by default
MODULE_PARM_DESC(kernel_stack_unwinding, "Allow kernel stack unwinding.");
bool kernel_stack_unwinding = 0;
module_param(kernel_stack_unwinding, bool, 0644);
#endif

static void kernel_backtrace(int cpu, struct pt_regs *const regs)
{
#if defined(__arm__) || defined(__aarch64__)
#ifdef GATOR_KERNEL_STACK_UNWINDING
	int depth = gator_backtrace_depth;
#else
	int depth = (kernel_stack_unwinding ? gator_backtrace_depth : 1);
#endif
	struct stackframe frame;
	if (depth == 0)
		depth = 1;
#if defined(__arm__)
	frame.fp = regs->ARM_fp;
	frame.sp = regs->ARM_sp;
	frame.lr = regs->ARM_lr;
	frame.pc = regs->ARM_pc;
#else
	frame.fp = regs->regs[29];
	frame.sp = regs->sp;
	frame.pc = regs->pc;
#endif
	walk_stackframe(&frame, report_trace, &depth);
#else
	marshal_backtrace(PC_REG & ~1, NO_COOKIE);
#endif
}