1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
|
/*
* Example events provider
*
* Copyright (C) ARM Limited 2010-2013. All rights reserved.
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*
* Similar entries to those below must be present in the events.xml file.
* To add them to the events.xml, create an events-mmap.xml with the
* following contents and rebuild gatord:
*
* <counter_set name="mmapped_cnt" count="3"/>
* <category name="mmapped" counter_set="mmapped_cnt" per_cpu="no">
* <event event="0x0" title="Simulated1" name="Sine" display="maximum" average_selection="yes" description="Sort-of-sine"/>
* <event event="0x1" title="Simulated2" name="Triangle" display="maximum" average_selection="yes" description="Triangular wave"/>
* <event event="0x2" title="Simulated3" name="PWM" display="maximum" average_selection="yes" description="PWM Signal"/>
* </category>
*
* When adding custom events, be sure do the following
* - add any needed .c files to the gator driver Makefile
* - call gator_events_install in the events init function
* - add the init function to GATOR_EVENTS_LIST in gator_main.c
* - add a new events-*.xml file to the gator daemon and rebuild
*/
#include <linux/init.h>
#include <linux/io.h>
#include <linux/ratelimit.h>
#include "gator.h"
#define MMAPPED_COUNTERS_NUM 3
static int mmapped_global_enabled;
static struct {
unsigned long enabled;
unsigned long event;
unsigned long key;
} mmapped_counters[MMAPPED_COUNTERS_NUM];
static int mmapped_buffer[MMAPPED_COUNTERS_NUM * 2];
static s64 prev_time;
/* Adds mmapped_cntX directories and enabled, event, and key files to /dev/gator/events */
static int gator_events_mmapped_create_files(struct super_block *sb,
struct dentry *root)
{
int i;
for (i = 0; i < MMAPPED_COUNTERS_NUM; i++) {
char buf[16];
struct dentry *dir;
snprintf(buf, sizeof(buf), "mmapped_cnt%d", i);
dir = gatorfs_mkdir(sb, root, buf);
if (WARN_ON(!dir))
return -1;
gatorfs_create_ulong(sb, dir, "enabled",
&mmapped_counters[i].enabled);
gatorfs_create_ulong(sb, dir, "event",
&mmapped_counters[i].event);
gatorfs_create_ro_ulong(sb, dir, "key",
&mmapped_counters[i].key);
}
return 0;
}
static int gator_events_mmapped_start(void)
{
int i;
struct timespec ts;
getnstimeofday(&ts);
prev_time = timespec_to_ns(&ts);
mmapped_global_enabled = 0;
for (i = 0; i < MMAPPED_COUNTERS_NUM; i++) {
if (mmapped_counters[i].enabled) {
mmapped_global_enabled = 1;
break;
}
}
return 0;
}
static void gator_events_mmapped_stop(void)
{
}
/* This function "simulates" counters, generating values of fancy
* functions like sine or triangle... */
static int mmapped_simulate(int counter, int delta_in_us)
{
int result = 0;
switch (counter) {
case 0: /* sort-of-sine */
{
static int t = 0;
int x;
t += delta_in_us;
if (t > 2048000)
t = 0;
if (t % 1024000 < 512000)
x = 512000 - (t % 512000);
else
x = t % 512000;
result = 32 * x / 512000;
result = result * result;
if (t < 1024000)
result = 1922 - result;
}
break;
case 1: /* triangle */
{
static int v, d = 1;
v = v + d * delta_in_us;
if (v < 0) {
v = 0;
d = 1;
} else if (v > 1000000) {
v = 1000000;
d = -1;
}
result = v;
}
break;
case 2: /* PWM signal */
{
static int dc, x, t = 0;
t += delta_in_us;
if (t > 1000000)
t = 0;
if (x / 1000000 != (x + delta_in_us) / 1000000)
dc = (dc + 100000) % 1000000;
x += delta_in_us;
result = t < dc ? 0 : 10;
}
break;
}
return result;
}
static int gator_events_mmapped_read(int **buffer)
{
int i;
int len = 0;
int delta_in_us;
struct timespec ts;
s64 time;
/* System wide counters - read from one core only */
if (!on_primary_core() || !mmapped_global_enabled)
return 0;
getnstimeofday(&ts);
time = timespec_to_ns(&ts);
delta_in_us = (int)(time - prev_time) / 1000;
prev_time = time;
for (i = 0; i < MMAPPED_COUNTERS_NUM; i++) {
if (mmapped_counters[i].enabled) {
mmapped_buffer[len++] = mmapped_counters[i].key;
mmapped_buffer[len++] =
mmapped_simulate(mmapped_counters[i].event,
delta_in_us);
}
}
if (buffer)
*buffer = mmapped_buffer;
return len;
}
static struct gator_interface gator_events_mmapped_interface = {
.create_files = gator_events_mmapped_create_files,
.start = gator_events_mmapped_start,
.stop = gator_events_mmapped_stop,
.read = gator_events_mmapped_read,
};
/* Must not be static! */
int __init gator_events_mmapped_init(void)
{
int i;
for (i = 0; i < MMAPPED_COUNTERS_NUM; i++) {
mmapped_counters[i].enabled = 0;
mmapped_counters[i].key = gator_events_get_key();
}
return gator_events_install(&gator_events_mmapped_interface);
}
|