summaryrefslogtreecommitdiffstats
blob: 332b3f6ba965d99f6ab2dfc18255821028532ff2 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
/**
 * Copyright (C) ARM Limited 2010-2013. All rights reserved.
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License version 2 as
 * published by the Free Software Foundation.
 *
 */

#include <trace/events/sched.h>
#include "gator.h"

#define TASK_MAP_ENTRIES		1024	/* must be power of 2 */
#define TASK_MAX_COLLISIONS		2

enum {
	STATE_WAIT_ON_OTHER = 0,
	STATE_CONTENTION,
	STATE_WAIT_ON_IO,
	CPU_WAIT_TOTAL
};

static DEFINE_PER_CPU(uint64_t *, taskname_keys);
static DEFINE_PER_CPU(int, collecting);
static DEFINE_PER_CPU(bool, in_scheduler_context);

// this array is never read as the cpu wait charts are derived counters
// the files are needed, nonetheless, to show that these counters are available
static ulong cpu_wait_enabled[CPU_WAIT_TOTAL];
static ulong sched_cpu_key[CPU_WAIT_TOTAL];

static int sched_trace_create_files(struct super_block *sb, struct dentry *root)
{
	struct dentry *dir;

	// CPU Wait - Contention
	dir = gatorfs_mkdir(sb, root, "Linux_cpu_wait_contention");
	if (!dir) {
		return -1;
	}
	gatorfs_create_ulong(sb, dir, "enabled", &cpu_wait_enabled[STATE_CONTENTION]);
	gatorfs_create_ro_ulong(sb, dir, "key", &sched_cpu_key[STATE_CONTENTION]);

	// CPU Wait - I/O
	dir = gatorfs_mkdir(sb, root, "Linux_cpu_wait_io");
	if (!dir) {
		return -1;
	}
	gatorfs_create_ulong(sb, dir, "enabled", &cpu_wait_enabled[STATE_WAIT_ON_IO]);
	gatorfs_create_ro_ulong(sb, dir, "key", &sched_cpu_key[STATE_WAIT_ON_IO]);

	return 0;
}

void emit_pid_name(struct task_struct *task)
{
	bool found = false;
	char taskcomm[TASK_COMM_LEN + 3];
	unsigned long x, cpu = get_physical_cpu();
	uint64_t *keys = &(per_cpu(taskname_keys, cpu)[(task->pid & 0xFF) * TASK_MAX_COLLISIONS]);
	uint64_t value;

	value = gator_chksum_crc32(task->comm);
	value = (value << 32) | (uint32_t)task->pid;

	// determine if the thread name was emitted already
	for (x = 0; x < TASK_MAX_COLLISIONS; x++) {
		if (keys[x] == value) {
			found = true;
			break;
		}
	}

	if (!found) {
		// shift values, new value always in front
		uint64_t oldv, newv = value;
		for (x = 0; x < TASK_MAX_COLLISIONS; x++) {
			oldv = keys[x];
			keys[x] = newv;
			newv = oldv;
		}

		// emit pid names, cannot use get_task_comm, as it's not exported on all kernel versions
		if (strlcpy(taskcomm, task->comm, TASK_COMM_LEN) == TASK_COMM_LEN - 1) {
			// append ellipses if task->comm has length of TASK_COMM_LEN - 1
			strcat(taskcomm, "...");
		}

		marshal_thread_name(task->pid, taskcomm);
	}
}

static void collect_counters(u64 time, struct task_struct *task)
{
	int *buffer, len, cpu = get_physical_cpu();
	long long *buffer64;
	struct gator_interface *gi;

	if (marshal_event_header(time)) {
		list_for_each_entry(gi, &gator_events, list) {
			if (gi->read) {
				len = gi->read(&buffer);
				marshal_event(len, buffer);
			} else if (gi->read64) {
				len = gi->read64(&buffer64);
				marshal_event64(len, buffer64);
			}
			if (gi->read_proc && task != NULL) {
				len = gi->read_proc(&buffer64, task);
				marshal_event64(len, buffer64);
			}
		}
		// Only check after writing all counters so that time and corresponding counters appear in the same frame
		buffer_check(cpu, BLOCK_COUNTER_BUF, time);

		// Commit buffers on timeout
		if (gator_live_rate > 0 && time >= per_cpu(gator_buffer_commit_time, cpu)) {
			static const int buftypes[] = { NAME_BUF, COUNTER_BUF, BLOCK_COUNTER_BUF, SCHED_TRACE_BUF };
			unsigned long flags;
			int i;

			local_irq_save(flags);
			for (i = 0; i < ARRAY_SIZE(buftypes); ++i) {
				gator_commit_buffer(cpu, buftypes[i], time);
			}
			local_irq_restore(flags);

			// Try to preemptively flush the annotate buffer to reduce the chance of the buffer being full
			if (on_primary_core() && spin_trylock(&annotate_lock)) {
				gator_commit_buffer(0, ANNOTATE_BUF, time);
				spin_unlock(&annotate_lock);
			}
		}
	}
}

// special case used during a suspend of the system
static void trace_sched_insert_idle(void)
{
	marshal_sched_trace_switch(0, 0, 0, 0);
}

GATOR_DEFINE_PROBE(sched_process_fork, TP_PROTO(struct task_struct *parent, struct task_struct *child))
{
	int cookie;
	int cpu = get_physical_cpu();

	cookie = get_exec_cookie(cpu, child);
	emit_pid_name(child);

	marshal_sched_trace_start(child->tgid, child->pid, cookie);
}

#if LINUX_VERSION_CODE < KERNEL_VERSION(2, 6, 35)
GATOR_DEFINE_PROBE(sched_switch, TP_PROTO(struct rq *rq, struct task_struct *prev, struct task_struct *next))
#else
GATOR_DEFINE_PROBE(sched_switch, TP_PROTO(struct task_struct *prev, struct task_struct *next))
#endif
{
	int cookie;
	int state;
	int cpu = get_physical_cpu();

	per_cpu(in_scheduler_context, cpu) = true;

	// do as much work as possible before disabling interrupts
	cookie = get_exec_cookie(cpu, next);
	emit_pid_name(next);
	if (prev->state == TASK_RUNNING) {
		state = STATE_CONTENTION;
	} else if (prev->in_iowait) {
		state = STATE_WAIT_ON_IO;
	} else {
		state = STATE_WAIT_ON_OTHER;
	}

	per_cpu(collecting, cpu) = 1;
	collect_counters(gator_get_time(), prev);
	per_cpu(collecting, cpu) = 0;

	marshal_sched_trace_switch(next->tgid, next->pid, cookie, state);

	per_cpu(in_scheduler_context, cpu) = false;
}

GATOR_DEFINE_PROBE(sched_process_free, TP_PROTO(struct task_struct *p))
{
	marshal_sched_trace_exit(p->tgid, p->pid);
}

static void do_nothing(void *info)
{
	// Intentionally do nothing
	(void)info;
}

static int register_scheduler_tracepoints(void)
{
	// register tracepoints
	if (GATOR_REGISTER_TRACE(sched_process_fork))
		goto fail_sched_process_fork;
	if (GATOR_REGISTER_TRACE(sched_switch))
		goto fail_sched_switch;
	if (GATOR_REGISTER_TRACE(sched_process_free))
		goto fail_sched_process_free;
	pr_debug("gator: registered tracepoints\n");

	// Now that the scheduler tracepoint is registered, force a context switch
	// on all cpus to capture what is currently running.
	on_each_cpu(do_nothing, NULL, 0);

	return 0;

	// unregister tracepoints on error
fail_sched_process_free:
	GATOR_UNREGISTER_TRACE(sched_switch);
fail_sched_switch:
	GATOR_UNREGISTER_TRACE(sched_process_fork);
fail_sched_process_fork:
	pr_err("gator: tracepoints failed to activate, please verify that tracepoints are enabled in the linux kernel\n");

	return -1;
}

int gator_trace_sched_start(void)
{
	int cpu, size;

	for_each_present_cpu(cpu) {
		size = TASK_MAP_ENTRIES * TASK_MAX_COLLISIONS * sizeof(uint64_t);
		per_cpu(taskname_keys, cpu) = (uint64_t *)kmalloc(size, GFP_KERNEL);
		if (!per_cpu(taskname_keys, cpu))
			return -1;
		memset(per_cpu(taskname_keys, cpu), 0, size);
	}

	return register_scheduler_tracepoints();
}

void gator_trace_sched_offline(void)
{
	trace_sched_insert_idle();
}

static void unregister_scheduler_tracepoints(void)
{
	GATOR_UNREGISTER_TRACE(sched_process_fork);
	GATOR_UNREGISTER_TRACE(sched_switch);
	GATOR_UNREGISTER_TRACE(sched_process_free);
	pr_debug("gator: unregistered tracepoints\n");
}

void gator_trace_sched_stop(void)
{
	int cpu;
	unregister_scheduler_tracepoints();

	for_each_present_cpu(cpu) {
		kfree(per_cpu(taskname_keys, cpu));
	}
}

void gator_trace_sched_init(void)
{
	int i;
	for (i = 0; i < CPU_WAIT_TOTAL; i++) {
		cpu_wait_enabled[i] = 0;
		sched_cpu_key[i] = gator_events_get_key();
	}
}