1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
|
/**
* Copyright (C) ARM Limited 2010-2012. All rights reserved.
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*
*/
#include <trace/events/sched.h>
#include "gator.h"
#define SCHED_SWITCH 1
#define SCHED_PROCESS_EXIT 2
#define TASK_MAP_ENTRIES 1024 /* must be power of 2 */
#define TASK_MAX_COLLISIONS 2
static DEFINE_PER_CPU(uint64_t *, taskname_keys);
static DEFINE_PER_CPU(int, collecting);
enum {
STATE_WAIT_ON_OTHER = 0,
STATE_CONTENTION,
STATE_WAIT_ON_IO,
STATE_WAIT_ON_MUTEX,
};
void emit_pid_name(struct task_struct *task)
{
bool found = false;
char taskcomm[TASK_COMM_LEN + 3];
unsigned long x, cpu = smp_processor_id();
uint64_t *keys = &(per_cpu(taskname_keys, cpu)[(task->pid & 0xFF) * TASK_MAX_COLLISIONS]);
uint64_t value;
value = gator_chksum_crc32(task->comm);
value = (value << 32) | (uint32_t)task->pid;
// determine if the thread name was emitted already
for (x = 0; x < TASK_MAX_COLLISIONS; x++) {
if (keys[x] == value) {
found = true;
break;
}
}
if (!found) {
// shift values, new value always in front
uint64_t oldv, newv = value;
for (x = 0; x < TASK_MAX_COLLISIONS; x++) {
oldv = keys[x];
keys[x] = newv;
newv = oldv;
}
// emit pid names, cannot use get_task_comm, as it's not exported on all kernel versions
if (strlcpy(taskcomm, task->comm, TASK_COMM_LEN) == TASK_COMM_LEN - 1) {
// append ellipses if task->comm has length of TASK_COMM_LEN - 1
strcat(taskcomm, "...");
}
marshal_thread_name(task->pid, taskcomm);
}
}
static void collect_counters(void)
{
int *buffer, len;
long long *buffer64;
struct gator_interface *gi;
if (marshal_event_header()) {
list_for_each_entry(gi, &gator_events, list) {
if (gi->read) {
len = gi->read(&buffer);
marshal_event(len, buffer);
} else if (gi->read64) {
len = gi->read64(&buffer64);
marshal_event64(len, buffer64);
}
}
}
}
static void probe_sched_write(int type, struct task_struct *task, struct task_struct *old_task)
{
int cookie = 0, state = 0;
int cpu = smp_processor_id();
int tgid = task->tgid;
int pid = task->pid;
if (type == SCHED_SWITCH) {
// do as much work as possible before disabling interrupts
cookie = get_exec_cookie(cpu, task);
emit_pid_name(task);
if (old_task->state == TASK_RUNNING) {
state = STATE_CONTENTION;
} else if (old_task->in_iowait) {
state = STATE_WAIT_ON_IO;
#ifdef CONFIG_DEBUG_MUTEXES
} else if (old_task->blocked_on) {
state = STATE_WAIT_ON_MUTEX;
#endif
} else {
state = STATE_WAIT_ON_OTHER;
}
per_cpu(collecting, cpu) = 1;
collect_counters();
per_cpu(collecting, cpu) = 0;
}
// marshal_sched_trace() disables interrupts as the free may trigger while switch is writing to the buffer; disabling preemption is not sufficient
// is disable interrupts necessary now that exit is used instead of free?
if (type == SCHED_SWITCH) {
marshal_sched_trace_switch(tgid, pid, cookie, state);
} else {
marshal_sched_trace_exit(tgid, pid);
}
}
// special case used during a suspend of the system
static void trace_sched_insert_idle(void)
{
marshal_sched_trace_switch(0, 0, 0, 0);
}
#if LINUX_VERSION_CODE < KERNEL_VERSION(2, 6, 35)
GATOR_DEFINE_PROBE(sched_switch, TP_PROTO(struct rq *rq, struct task_struct *prev, struct task_struct *next))
#else
GATOR_DEFINE_PROBE(sched_switch, TP_PROTO(struct task_struct *prev, struct task_struct *next))
#endif
{
probe_sched_write(SCHED_SWITCH, next, prev);
}
GATOR_DEFINE_PROBE(sched_process_exit, TP_PROTO(struct task_struct *p))
{
probe_sched_write(SCHED_PROCESS_EXIT, p, 0);
}
static void do_nothing(void *info)
{
// Intentionally do nothing
(void)info;
}
static int register_scheduler_tracepoints(void)
{
// register tracepoints
if (GATOR_REGISTER_TRACE(sched_switch))
goto fail_sched_switch;
if (GATOR_REGISTER_TRACE(sched_process_exit))
goto fail_sched_process_exit;
pr_debug("gator: registered tracepoints\n");
// Now that the scheduler tracepoint is registered, force a context switch
// on all cpus to capture what is currently running.
on_each_cpu(do_nothing, NULL, 0);
return 0;
// unregister tracepoints on error
fail_sched_process_exit:
GATOR_UNREGISTER_TRACE(sched_switch);
fail_sched_switch:
pr_err("gator: tracepoints failed to activate, please verify that tracepoints are enabled in the linux kernel\n");
return -1;
}
int gator_trace_sched_start(void)
{
int cpu, size;
for_each_present_cpu(cpu) {
size = TASK_MAP_ENTRIES * TASK_MAX_COLLISIONS * sizeof(uint64_t);
per_cpu(taskname_keys, cpu) = (uint64_t *)kmalloc(size, GFP_KERNEL);
if (!per_cpu(taskname_keys, cpu))
return -1;
memset(per_cpu(taskname_keys, cpu), 0, size);
}
return register_scheduler_tracepoints();
}
void gator_trace_sched_offline(void)
{
trace_sched_insert_idle();
}
static void unregister_scheduler_tracepoints(void)
{
GATOR_UNREGISTER_TRACE(sched_switch);
GATOR_UNREGISTER_TRACE(sched_process_exit);
pr_debug("gator: unregistered tracepoints\n");
}
void gator_trace_sched_stop(void)
{
int cpu;
unregister_scheduler_tracepoints();
for_each_present_cpu(cpu) {
kfree(per_cpu(taskname_keys, cpu));
}
}
|