diff options
author | Misael Lopez Cruz | 2013-11-05 20:32:55 -0600 |
---|---|---|
committer | Misael Lopez Cruz | 2013-11-11 13:01:16 -0600 |
commit | 50db622848f29e112a98ef910dbaa3e82fe3be28 (patch) | |
tree | 25b78d565c92c4321d0c13b532e71ba2a741e5cb | |
parent | 3dadd189dc6a30f7eb1e07f2afaac04207c3b21e (diff) | |
download | device-ti-common-open-50db622848f29e112a98ef910dbaa3e82fe3be28.tar.gz device-ti-common-open-50db622848f29e112a98ef910dbaa3e82fe3be28.tar.xz device-ti-common-open-50db622848f29e112a98ef910dbaa3e82fe3be28.zip |
audio: utils: Add null pcm ports
Null PCM playback and capture ports are dummy ports that produce
and consume audio buffers at the same rate that an actual hardware
port would. They can be used to provide valid sources or sinks to
PCM readers/writers when actual hardware ports are not available.
Change-Id: Ibe54104b8542534fe0414bdc6ad0beedaba303d7
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
-rw-r--r-- | audio/utils/Android.mk | 1 | ||||
-rw-r--r-- | audio/utils/include/tiaudioutils/NullPcm.h | 230 | ||||
-rw-r--r-- | audio/utils/src/NullPcm.cpp | 96 |
3 files changed, 327 insertions, 0 deletions
diff --git a/audio/utils/Android.mk b/audio/utils/Android.mk index c038c56..13983ca 100644 --- a/audio/utils/Android.mk +++ b/audio/utils/Android.mk | |||
@@ -21,6 +21,7 @@ LOCAL_MODULE := libtiaudioutils | |||
21 | LOCAL_SRC_FILES := \ | 21 | LOCAL_SRC_FILES := \ |
22 | src/Base.cpp \ | 22 | src/Base.cpp \ |
23 | src/Pcm.cpp \ | 23 | src/Pcm.cpp \ |
24 | src/NullPcm.cpp \ | ||
24 | src/ALSAPcm.cpp \ | 25 | src/ALSAPcm.cpp \ |
25 | src/ALSAMixer.cpp \ | 26 | src/ALSAMixer.cpp \ |
26 | src/SimpleStream.cpp \ | 27 | src/SimpleStream.cpp \ |
diff --git a/audio/utils/include/tiaudioutils/NullPcm.h b/audio/utils/include/tiaudioutils/NullPcm.h new file mode 100644 index 0000000..8995759 --- /dev/null +++ b/audio/utils/include/tiaudioutils/NullPcm.h | |||
@@ -0,0 +1,230 @@ | |||
1 | /* | ||
2 | * Copyright (C) 2013 Texas Instruments | ||
3 | * | ||
4 | * Licensed under the Apache License, Version 2.0 (the "License"); | ||
5 | * you may not use this file except in compliance with the License. | ||
6 | * You may obtain a copy of the License at | ||
7 | * | ||
8 | * http://www.apache.org/licenses/LICENSE-2.0 | ||
9 | * | ||
10 | * Unless required by applicable law or agreed to in writing, software | ||
11 | * distributed under the License is distributed on an "AS IS" BASIS, | ||
12 | * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. | ||
13 | * See the License for the specific language governing permissions and | ||
14 | * limitations under the License. | ||
15 | */ | ||
16 | |||
17 | /** | ||
18 | * \file NullPcm.h | ||
19 | * \brief Classes for accessing the PCM interface of a null card | ||
20 | * | ||
21 | * Contains classes required to play and capture data from a null sound card. | ||
22 | */ | ||
23 | |||
24 | #ifndef _TIAUDIOUTILS_NULLPCM_H_ | ||
25 | #define _TIAUDIOUTILS_NULLPCM_H_ | ||
26 | |||
27 | #include <limits.h> | ||
28 | |||
29 | #include <tiaudioutils/Base.h> | ||
30 | #include <tiaudioutils/Pcm.h> | ||
31 | |||
32 | namespace tiaudioutils { | ||
33 | |||
34 | /** | ||
35 | * \class NullInPort | ||
36 | * \brief Null capture port | ||
37 | * | ||
38 | * The null PCM port used for capture. Buffers are filled with silence by the | ||
39 | * null port at the same rate that an actual hardware port would. | ||
40 | */ | ||
41 | class NullInPort : public PcmInPort { | ||
42 | public: | ||
43 | /** | ||
44 | * \brief Null input port constructor | ||
45 | * | ||
46 | * Constructs a null input/capture port. | ||
47 | */ | ||
48 | NullInPort(); | ||
49 | |||
50 | /** | ||
51 | * \brief Null input port destructor | ||
52 | * | ||
53 | * Destroys a null input/capture port object. | ||
54 | */ | ||
55 | virtual ~NullInPort() {} | ||
56 | |||
57 | /** | ||
58 | * \brief Get the id of the sound card | ||
59 | * | ||
60 | * Gets the id of the sound card that this port belongs to. Neither the | ||
61 | * null port or the card actually exist in the system (as opposite to | ||
62 | * the ALSA dummy/null card), so the returned id is chosen not to | ||
63 | * conflict with any valid card that may be registered in the system. | ||
64 | * | ||
65 | * \return The sound card id | ||
66 | */ | ||
67 | uint32_t getCardId() const { return UINT_MAX; } | ||
68 | |||
69 | /** | ||
70 | * \brief Get the port id | ||
71 | * | ||
72 | * Gets the null input/capture port id. The id itself is valid but | ||
73 | * meaningless since there is no sound card in the system for the null PCM. | ||
74 | * | ||
75 | * \return The PCM port id | ||
76 | */ | ||
77 | uint32_t getPortId() const { return 0; } | ||
78 | |||
79 | /** | ||
80 | * \brief Open the null port for capture | ||
81 | * | ||
82 | * Opens the null PCM port for capture with the given parameters. There is | ||
83 | * no hardware port actually opened by this method. The PCM parameters | ||
84 | * used to open the port are used to calculate the buffer time in read(). | ||
85 | * | ||
86 | * \param params PcmParams used to open the port | ||
87 | * \return 0 on success, otherwise negative error code | ||
88 | */ | ||
89 | int open(const PcmParams ¶ms); | ||
90 | |||
91 | /** | ||
92 | * \brief Close the null PCM port | ||
93 | * | ||
94 | * Closes the null PCM port opened by calling open(). There is no hardware | ||
95 | * port actually closed by this method. | ||
96 | */ | ||
97 | void close(); | ||
98 | |||
99 | /** | ||
100 | * \brief Test if the PCM port is open and ready | ||
101 | * | ||
102 | * Tests if the PCM port is open and ready for capture. | ||
103 | * | ||
104 | * \return true if the port is open, false otherwise | ||
105 | */ | ||
106 | bool isOpen() const { return mOpen; } | ||
107 | |||
108 | /** | ||
109 | * \brief Read audio data from the null PCM input port | ||
110 | * | ||
111 | * Reads data from the null port which produces a buffer filled with silence. | ||
112 | * No actual data is read from hardware, but the call blocks for the time | ||
113 | * equivalent to the requested frames. | ||
114 | * | ||
115 | * \param buffer Pointer to the destination buffer | ||
116 | * \param frames Number of frames to be read | ||
117 | * \return 0 on success, otherwise negative error code | ||
118 | */ | ||
119 | int read(void *buffer, size_t frames); | ||
120 | |||
121 | private: | ||
122 | NullInPort(const NullInPort &port); | ||
123 | NullInPort& operator=(const NullInPort &port); | ||
124 | |||
125 | protected: | ||
126 | bool mOpen; /**< State of the port: open or closed */ | ||
127 | PcmParams mParams; /**< PCM params of the port */ | ||
128 | Mutex mLock; /**< Synchronize PCM port use */ | ||
129 | }; | ||
130 | |||
131 | /** | ||
132 | * \class NullOutPort | ||
133 | * \brief Null playback port | ||
134 | * | ||
135 | * The null PCM port used for playback. Buffers are consumed by the null port | ||
136 | * at the same rate that an actual hardware port would. | ||
137 | */ | ||
138 | class NullOutPort : public PcmOutPort { | ||
139 | public: | ||
140 | /** | ||
141 | * \brief Null output port constructor | ||
142 | * | ||
143 | * Constructs a null output/playback port. | ||
144 | */ | ||
145 | NullOutPort(); | ||
146 | |||
147 | /** | ||
148 | * \brief Null output port destructor | ||
149 | * | ||
150 | * Destroys a null output/playback port object. | ||
151 | */ | ||
152 | virtual ~NullOutPort() {} | ||
153 | |||
154 | /** | ||
155 | * \brief Get the id of the sound card | ||
156 | * | ||
157 | * | ||
158 | * Gets the id of the sound card that this port belongs to. Neither the | ||
159 | * null port or the card actually exist in the system (as opposite to | ||
160 | * the ALSA dummy/null card), so the returned id is chosen not to | ||
161 | * conflict with any valid card that may be registered in the system. | ||
162 | * | ||
163 | * \return The sound card id | ||
164 | */ | ||
165 | uint32_t getCardId() const { return UINT_MAX; } | ||
166 | |||
167 | /** | ||
168 | * \brief Get the port id | ||
169 | * | ||
170 | * Gets the null output/playback port id. The id itself is valid but | ||
171 | * meaningless since there is no sound card in the system for the null PCM. | ||
172 | * | ||
173 | * \return The PCM port id | ||
174 | */ | ||
175 | uint32_t getPortId() const { return 0; } | ||
176 | |||
177 | /** | ||
178 | * \brief Open the null port for playback | ||
179 | * | ||
180 | * Opens the null PCM port for playback with the given parameters. There is | ||
181 | * no hardware port actually opened by this method. The PCM parameters | ||
182 | * used to open the port are used to calculate the buffer time in write(). | ||
183 | * | ||
184 | * \param params PcmParams used to open the port | ||
185 | * \return 0 on success, otherwise negative error code | ||
186 | */ | ||
187 | int open(const PcmParams ¶ms); | ||
188 | |||
189 | /** | ||
190 | * \brief Close the null PCM port | ||
191 | * | ||
192 | * Closes the null PCM port opened by calling open(). There is no hardware | ||
193 | * port actually closed by this method. | ||
194 | */ | ||
195 | void close(); | ||
196 | |||
197 | /** | ||
198 | * \brief Test if the PCM port is open and ready | ||
199 | * | ||
200 | * Tests if the PCM port is open and ready for playback. | ||
201 | * | ||
202 | * \return true if the port is open, false otherwise | ||
203 | */ | ||
204 | bool isOpen() const { return mOpen; } | ||
205 | |||
206 | /** | ||
207 | * \brief Write audio data to the null PCM output port | ||
208 | * | ||
209 | * Writes data to the null output port. No data write actually occurs | ||
210 | * but the call blocks for the time equivalent to the requested frames. | ||
211 | * | ||
212 | * \param buffer Pointer to the source buffer | ||
213 | * \param frames Number of frames to be written | ||
214 | * \return Number of frames written, otherwise negative error code | ||
215 | */ | ||
216 | int write(const void *buffer, size_t frames); | ||
217 | |||
218 | private: | ||
219 | NullOutPort(const NullOutPort &port); | ||
220 | NullOutPort& operator=(const NullOutPort &port); | ||
221 | |||
222 | protected: | ||
223 | bool mOpen; /**< State of the port: open or closed */ | ||
224 | PcmParams mParams; /**< PCM params of the port */ | ||
225 | Mutex mLock; /**< Synchronize PCM port use */ | ||
226 | }; | ||
227 | |||
228 | } /* namespace tiaudioutils */ | ||
229 | |||
230 | #endif /* _TIAUDIOUTILS_NULLPCM_H_ */ | ||
diff --git a/audio/utils/src/NullPcm.cpp b/audio/utils/src/NullPcm.cpp new file mode 100644 index 0000000..3e0a0b0 --- /dev/null +++ b/audio/utils/src/NullPcm.cpp | |||
@@ -0,0 +1,96 @@ | |||
1 | /* | ||
2 | * Copyright (C) 2013 Texas Instruments | ||
3 | * | ||
4 | * Licensed under the Apache License, Version 2.0 (the "License"); | ||
5 | * you may not use this file except in compliance with the License. | ||
6 | * You may obtain a copy of the License at | ||
7 | * | ||
8 | * http://www.apache.org/licenses/LICENSE-2.0 | ||
9 | * | ||
10 | * Unless required by applicable law or agreed to in writing, software | ||
11 | * distributed under the License is distributed on an "AS IS" BASIS, | ||
12 | * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. | ||
13 | * See the License for the specific language governing permissions and | ||
14 | * limitations under the License. | ||
15 | */ | ||
16 | |||
17 | // #define LOG_NDEBUG 0 | ||
18 | // #define VERY_VERBOSE_LOGGING | ||
19 | |||
20 | #include <errno.h> | ||
21 | |||
22 | #include <tiaudioutils/Log.h> | ||
23 | #include <tiaudioutils/NullPcm.h> | ||
24 | |||
25 | namespace tiaudioutils { | ||
26 | |||
27 | NullInPort::NullInPort() | ||
28 | : mOpen(false) | ||
29 | { | ||
30 | } | ||
31 | |||
32 | int NullInPort::open(const PcmParams ¶ms) | ||
33 | { | ||
34 | AutoMutex lock(mLock); | ||
35 | mParams = params; | ||
36 | mOpen = true; | ||
37 | |||
38 | return 0; | ||
39 | } | ||
40 | |||
41 | void NullInPort::close() | ||
42 | { | ||
43 | AutoMutex lock(mLock); | ||
44 | mOpen = false; | ||
45 | } | ||
46 | |||
47 | int NullInPort::read(void *buffer, size_t frames) | ||
48 | { | ||
49 | AutoMutex lock(mLock); | ||
50 | if (!mOpen) { | ||
51 | ALOGE("NullInPort: port is closed, cannot read"); | ||
52 | return -EAGAIN; | ||
53 | } | ||
54 | |||
55 | memset(buffer, 0, mParams.framesToBytes(frames)); | ||
56 | usleep((frames * 1000000) / mParams.sampleRate); | ||
57 | |||
58 | return frames; | ||
59 | } | ||
60 | |||
61 | /* ---------------------------------------------------------------------------------------- */ | ||
62 | |||
63 | NullOutPort::NullOutPort() | ||
64 | : mOpen(false) | ||
65 | { | ||
66 | } | ||
67 | |||
68 | int NullOutPort::open(const PcmParams ¶ms) | ||
69 | { | ||
70 | AutoMutex lock(mLock); | ||
71 | mParams = params; | ||
72 | mOpen = true; | ||
73 | |||
74 | return 0; | ||
75 | } | ||
76 | |||
77 | void NullOutPort::close() | ||
78 | { | ||
79 | AutoMutex lock(mLock); | ||
80 | mOpen = false; | ||
81 | } | ||
82 | |||
83 | int NullOutPort::write(const void *buffer, size_t frames) | ||
84 | { | ||
85 | AutoMutex lock(mLock); | ||
86 | if (!mOpen) { | ||
87 | ALOGE("NullOutPort: port is closed, cannot write"); | ||
88 | return -EAGAIN; | ||
89 | } | ||
90 | |||
91 | usleep((frames * 1000000) / mParams.sampleRate); | ||
92 | |||
93 | return frames; | ||
94 | } | ||
95 | |||
96 | } /* namespace tiaudioutils */ | ||