diff options
author | Misael Lopez Cruz | 2014-01-28 14:06:45 -0600 |
---|---|---|
committer | Misael Lopez Cruz | 2014-01-30 17:05:44 -0600 |
commit | 7c835cd660854083860e2ee8793ab6b5dff84c21 (patch) | |
tree | 0387420e7e4dcf1677091e6779b2b7e97dd0daad | |
parent | 46be7175bc6fdbbfad4cb143a69f7417b7066c55 (diff) | |
download | device-ti-common-open-7c835cd660854083860e2ee8793ab6b5dff84c21.tar.gz device-ti-common-open-7c835cd660854083860e2ee8793ab6b5dff84c21.tar.xz device-ti-common-open-7c835cd660854083860e2ee8793ab6b5dff84c21.zip |
audio: utils: Add flush() and size() methods to MonoPipe
Add two new methods to the MonoPipe class:
- flush(): Flushes the audio frames available in the pipe.
It should be called when te pipe is already in shutdown
state to ensure that no more new data is pushed.
- size(): Queries the pipe size.
Change-Id: Ia8c2ac287a475bd3e72f48368d297fc544b19eed
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
-rw-r--r-- | audio/utils/include/tiaudioutils/MonoPipe.h | 21 | ||||
-rw-r--r-- | audio/utils/src/MonoPipe.cpp | 28 |
2 files changed, 49 insertions, 0 deletions
diff --git a/audio/utils/include/tiaudioutils/MonoPipe.h b/audio/utils/include/tiaudioutils/MonoPipe.h index 7fcef8c..8445ddc 100644 --- a/audio/utils/include/tiaudioutils/MonoPipe.h +++ b/audio/utils/include/tiaudioutils/MonoPipe.h | |||
@@ -139,6 +139,27 @@ class MonoPipe { | |||
139 | virtual int availableToWrite() const; | 139 | virtual int availableToWrite() const; |
140 | 140 | ||
141 | /** | 141 | /** |
142 | * \brief Query the size of the pipe | ||
143 | * | ||
144 | * Queries the size of the pipe. It might be different to the requested | ||
145 | * number of frames if the pipe implementation relies does size rounding. | ||
146 | * | ||
147 | * \return Size of the pipe (in frames) | ||
148 | */ | ||
149 | virtual size_t size() const; | ||
150 | |||
151 | /** | ||
152 | * \brief Flush the pipe | ||
153 | * | ||
154 | * Flushes all frames present in the pipe. It should be called when the | ||
155 | * pipe is in shutdown state to ensure no new data is written to the | ||
156 | * pipe. | ||
157 | * | ||
158 | * \return 0 on success, otherwise negative error code | ||
159 | */ | ||
160 | virtual int flush(); | ||
161 | |||
162 | /** | ||
142 | * \brief Shut down the pipe | 163 | * \brief Shut down the pipe |
143 | * | 164 | * |
144 | * Shuts down the pipe, causing any blocking write() calls to unblock | 165 | * Shuts down the pipe, causing any blocking write() calls to unblock |
diff --git a/audio/utils/src/MonoPipe.cpp b/audio/utils/src/MonoPipe.cpp index e463f79..be021f1 100644 --- a/audio/utils/src/MonoPipe.cpp +++ b/audio/utils/src/MonoPipe.cpp | |||
@@ -110,6 +110,34 @@ int MonoPipe::availableToWrite() const | |||
110 | return mSink->availableToWrite(); | 110 | return mSink->availableToWrite(); |
111 | } | 111 | } |
112 | 112 | ||
113 | size_t MonoPipe::size() const | ||
114 | { | ||
115 | return mSink->maxFrames(); | ||
116 | } | ||
117 | |||
118 | int MonoPipe::flush() | ||
119 | { | ||
120 | ALOGW_IF(!isShutdown(), "MonoPipe: flushing while not in shutdown state"); | ||
121 | |||
122 | int avail = availableToRead(); | ||
123 | int16_t buffer[mParams.channels * avail]; | ||
124 | |||
125 | /* Read all frames still present in the pipe */ | ||
126 | while (avail > 0) { | ||
127 | int ret = read(buffer, avail); | ||
128 | if (ret < 0) { | ||
129 | ALOGE("MonoPipe: failed to flush the pipe %d", ret); | ||
130 | return ret; | ||
131 | } | ||
132 | avail -= ret; | ||
133 | } | ||
134 | |||
135 | avail = availableToRead(); | ||
136 | ALOGW_IF(avail, "MonoPipe: %d frames were not flushed", avail); | ||
137 | |||
138 | return 0; | ||
139 | } | ||
140 | |||
113 | void MonoPipe::shutdown(bool state) | 141 | void MonoPipe::shutdown(bool state) |
114 | { | 142 | { |
115 | mSink->shutdown(state); | 143 | mSink->shutdown(state); |