/*
* Copyright (C) 2013 Texas Instruments
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#ifndef _AUDIO_HW_H_
#define _AUDIO_HW_H_
#include <vector>
#include <system/audio.h>
#include <hardware/audio_effect.h>
#include <tiaudioutils/Pcm.h>
#include <tiaudioutils/ALSAPcm.h>
#include <tiaudioutils/ALSAMixer.h>
#include <tiaudioutils/MumStream.h>
#include <tiaudioutils/Stream.h>
#include <tiaudioutils/Base.h>
namespace android {
using namespace tiaudioutils;
using std::vector;
class AudioHwDevice;
class AudioStream {
public:
virtual ~AudioStream() {}
virtual uint32_t getSampleRate() const = 0;
virtual int setSampleRate(uint32_t rate) = 0;
virtual size_t getBufferSize() const = 0;
virtual audio_channel_mask_t getChannels() const = 0;
virtual audio_format_t getFormat() const = 0;
virtual int setFormat(audio_format_t format) = 0;
virtual int standby() = 0;
virtual int dump(int fd) const = 0;
virtual audio_devices_t getDevice() const = 0;
virtual int setDevice(audio_devices_t device) { return 0; } /* unused */
virtual int setParameters(const char *kv_pairs) = 0;
virtual char *getParameters(const char *keys) const = 0;
virtual int addAudioEffect(effect_handle_t effect) const = 0;
virtual int removeAudioEffect(effect_handle_t effect) const = 0;
};
class AudioStreamOut : public RefBase, public AudioStream {
public:
AudioStreamOut(AudioHwDevice *hwDev,
PcmWriter *writer,
const PcmParams ¶ms,
const SlotMap &map,
audio_devices_t devices);
virtual ~AudioStreamOut() {};
int initCheck() const;
/* From AudioStream */
virtual uint32_t getSampleRate() const;
virtual int setSampleRate(uint32_t rate);
virtual size_t getBufferSize() const;
virtual audio_channel_mask_t getChannels() const;
virtual audio_format_t getFormat() const;
virtual int setFormat(audio_format_t format);
virtual int standby();
virtual int dump(int fd) const;
virtual audio_devices_t getDevice() const;
virtual int setParameters(const char *kv_pairs);
virtual char *getParameters(const char *keys) const;
virtual int addAudioEffect(effect_handle_t effect) const;
virtual int removeAudioEffect(effect_handle_t effect) const;
/* AudioStreamOut specific */
uint32_t getLatency() const;
int setVolume(float left, float right);
ssize_t write(const void* buffer, size_t bytes);
int getRenderPosition(uint32_t *dsp_frames) const;
int getNextWriteTimestamp(int64_t *timestamp) const;
protected:
int resume();
void idle();
AudioHwDevice *mHwDev;
PcmWriter *mWriter;
PcmParams mParams;
audio_devices_t mDevices;
sp<OutStream> mStream;
bool mStandby;
Mutex mLock;
};
class AudioStreamIn : public RefBase, public AudioStream {
public:
AudioStreamIn(AudioHwDevice *hwDev,
PcmReader *reader,
const PcmParams ¶ms,
const SlotMap &map,
audio_devices_t devices);
virtual ~AudioStreamIn() {};
int initCheck() const;
/* From AudioStream */
virtual uint32_t getSampleRate() const;
virtual int setSampleRate(uint32_t rate);
virtual size_t getBufferSize() const;
virtual audio_channel_mask_t getChannels() const;
virtual audio_format_t getFormat() const;
virtual int setFormat(audio_format_t format);
virtual int standby();
virtual int dump(int fd) const;
virtual audio_devices_t getDevice() const;
virtual int setParameters(const char *kv_pairs);
virtual char *getParameters(const char *keys) const;
virtual int addAudioEffect(effect_handle_t effect) const;
virtual int removeAudioEffect(effect_handle_t effect) const;
/* AudioStreamIn specific */
int setGain(float gain);
ssize_t read(void* buffer, size_t bytes);
uint32_t getInputFramesLost();
protected:
int resume();
void idle();
AudioHwDevice *mHwDev;
PcmReader *mReader;
PcmParams mParams;
audio_devices_t mDevices;
audio_source_t mSource;
sp<InStream> mStream;
bool mStandby;
Mutex mLock;
};
class AudioHwDevice {
public:
AudioHwDevice(uint32_t card);
virtual ~AudioHwDevice();
uint32_t getSupportedDevices() const;
int initCheck() const;
int setVoiceVolume(float volume);
int setMasterVolume(float volume);
int setMode(audio_mode_t mode);
int setMicMute(bool state);
int getMicMute(bool *state) const;
int setParameters(const char *kv_pairs);
char *getParameters(const char *keys) const;
size_t getInputBufferSize(const struct audio_config *config) const;
int dump(int fd) const;
int setMasterMute(bool mute);
AudioStreamIn* openInputStream(audio_io_handle_t handle,
audio_devices_t devices,
struct audio_config *config);
void closeInputStream(AudioStreamIn *in);
AudioStreamOut* openOutputStream(audio_io_handle_t handle,
audio_devices_t devices,
audio_output_flags_t flags,
struct audio_config *config);
void closeOutputStream(AudioStreamOut *out);
friend class AudioStreamIn;
friend class AudioStreamOut;
static const uint32_t kNumPorts = 2;
static const uint32_t kCPUPortId = 0;
static const uint32_t kJAMR3PortId = 1;
static const uint32_t kCPUNumChannels = 2;
static const uint32_t kJAMR3NumChannels = 8;
static const uint32_t kSampleRate = 44100;
static const uint32_t kSampleSize = 16;
static const uint32_t kCaptureFrameCount = 882;
static const uint32_t kPlaybackFrameCount = 1024;
protected:
typedef set< sp<AudioStreamIn> > StreamInSet;
typedef set< sp<AudioStreamOut> > StreamOutSet;
typedef vector<ALSAInPort*> InPortVect;
typedef vector<ALSAOutPort*> OutPortVect;
typedef vector<PcmReader*> ReaderVect;
typedef vector<PcmWriter*> WriterVect;
const char *getModeName(audio_mode_t mode) const;
uint32_t mCardId;
ALSAMixer mMixer;
InPortVect mInPorts;
OutPortVect mOutPorts;
ReaderVect mReaders;
WriterVect mWriters;
StreamInSet mInStreams;
StreamOutSet mOutStreams;
bool mMicMute;
};
}; // namespace android
#endif /* _AUDIO_HW_H_ */